This operation temporarily disables access to chip's resources. Use the

Erase

button to clear chip protection and move the target to the open state.

  1. Connect the device to the host computer and select it in the

    Programmer

    ,

    Board

    , and

    Device

    drop-downs.

  2. Select the

    Chip Protection

    pull-down and select

    Protected

    mode.

    A warning message asking for confirmation is displays.



  3. Click

    Yes

    to apply

    Protected

    mode for your PSOC™ 4, PMG1, PAG2S and CCGx.

When the operation completes, the log is appended with a message, and the device is disconnected from the programmer automatically.