About this document​

Scope and purpose​

This application note introduces the

PSOC™ Edge

MCU, which is a dual-CPU programmable system-on-chip with Arm® Cortex® -M33 as the system processor, enabling low-power application and Arm® Cortex® -M55 as a primary application processor coupled with Arm® Ethos-U55 as a neural net co-processor.

This application note provides information on the

PSOC™ Edge

MCU architecture and development tools and shows how to create a first application using the ModusToolbox™ software. This application note also guides you to additional resources available online to accelerate the learning about

PSOC™ Edge

MCU.

Intended audience​

This document is intended for the users who are new to

PSOC™ Edge

MCU and ModusToolbox™ software.

Software version​

ModusToolbox™ Software

3.6 or above

Introduction​

Note:

The initial sections 1 to 3 introduce the

PSOC™ Edge

MCU and its features including an introduction to software tools and resources. To quickly get started by creating a sample application, please consider going directly to section 4

First

PSOC™ Edge

MCU design using Eclipse IDE for ModusToolbox™ software

.


The

PSOC™ Edge

MCU is a programmable embedded system-on-chip having dual-CPUs. It integrates Arm® Cortex®-M33 up to 200 MHz and Arm® Cortex®-M55 up to 400 MHz coupled with an Arm® Ethos-U55 neural network coprocessor, graphics, audio block, and DSP capability. It also includes Secure Enclave having crypto accelerators and protection units. This MCU has high-performance memory expansion capability (QSPI), low-power analog subsystem with high-performance analog-to-digital conversion, low-power comparators, on-board IoT connectivity module (on SOM), communication channels, programmable analog and digital blocks allowing higher flexibility, in-field tuning of the design with faster time-to-market.

The

PSOC™ Edge

MCU is suitable for power sensitive applications including:

  • Smart thermostat

  • Smart lock

  • Smart home appliance

  • Industrial HMI

  • Smart Wearable

The ModusToolbox™ software environment supports the

PSOC™ Edge

MCU application development with a set of tools for configuring the device, setting up peripherals, and complementing projects with world-class middleware. See the Infineon GitHub repositories for board support packages (BSPs) for all kits and libraries along with a comprehensive array of example applications to get you started.

This application note introduces you to the capabilities of the

PSOC™ Edge

MCU, which provides an overview of the development ecosystem, and gets you started with a simple 'Hello World' application wherein you learn to use the

PSOC™ Edge

MCU. You can learn how to create the application from an empty starter application, but the completed design is available as a code example for ModusToolbox™.

Development ecosystem​

PSOC™ resources​

A wealth of data available here that helps you to select the right

PSOC™

MCU and quickly and effectively integrate it into your design. For more

PSOC™ Edge

MCU related documents, see the PSOC™ Edge MCU webpage .

Firmware/application development​

ModusToolbox™ software

The ModusToolbox™ software is a modern, extensible development environment supporting a wide range of Infineon microcontroller devices. It provides a flexible set of tools and a diverse, high-quality collection of application-focused software. These include configuration tools, low-level drivers, libraries, and operating system support, most of which are compatible with Linux-, macOS-, and Windows-hosted environments.

Software resources available at GitHub support one or more of the target ecosystems:

  • MCU and Bluetooth® SoC ecosystem: A full-featured platform for PSOC™ MCU, Bluetooth®, and Bluetooth® low-energy application development

  • Connectivity ecosystem: A set of libraries providing core functionality of Wi-Fi, including connectivity, security, firmware upgrade support, and application layer protocols for applications

  • Amazon FreeRTOS ecosystem: Extends the FreeRTOS kernel with software libraries that make it easy to securely connect small, low-power Infineon devices to most cloud services

ModusToolbox™ tools and resources can also be used on the command line. For more details, see the build system chapter in the

ModusToolbox™ tools package user guide

.

Installing ModusToolbox™ tools package

The ModusToolbox™ tools package can be installed using any of the below methods:

  1. ModusToolbox™ Setup program

    : It is highly recommended to use the ModusToolbox™ Setup program for a simplified installation experience. You can download and use the ModusToolbox™ Setup program from

    Infineon Development Center

    to install the tools package, as well as many other packages such as early access packs, Programming tools, etc. Refer to the

    Setup program user guide

    for more details

  2. Standalone installation

    : The user may also download just the ModusToolbox™ tools package from the

    Infineon Development Center

    for offline installation. For more details, see the

    ModusToolbox™ tools package installation guide

After installing the software, see the

ModusToolbox™ tools package user guide

to get an overview of the software.

Choosing an IDE

The ModusToolbox™ software is supported across Windows, Linux, and macOS platforms. The ModusToolbox™ software supports third-party IDEs, including the Eclipse IDE, Visual Studio Code, Arm® MDK (μVision), and IAR Embedded Workbench. The tools package includes an implementation for the Eclipse IDE for convenience. The associated BSP and library configurators also work on all three host operating systems.

Beginning with the ModusToolbox™ tools package version 3.4.0, the Eclipse IDE for ModusToolbox™ is no longer included by default. Instead, it is a separate package that you can install via the ModusToolbox™ Setup program.

You can develop firmware for the

PSOC™

Edge MCU using any one of the following IDEs: Eclipse, IAR Embedded Workbench, Keil μVision 5, or Visual Studio Code. This application note uses Eclipse IDE for demonstration purpose.

See the following documents to learn how to use ModusToolbox™ with the different IDEs:

Software features

The ModusToolbox™ tools package installer includes the design configurators and tools and the build system infrastructure.

The build system infrastructure includes the new project creation wizard that can execute independent of the Eclipse IDE, the make infrastructure, and other tools. This means you can choose your compiler, IDE, RTOS, and ecosystem without compromising usability or access to our wide portfolio of middleware assets, which include HMI, machine learning, Wi-Fi, Bluetooth®, security, and various other features.

Design configurators are the tools that help you create the configurable code for required BSP or middleware. For more details, see the

Configurators

section.

Figure 1.

ModusToolbox™ software stack


Figure 1

shows a high-level view of the application capabilities of Infineon devices using the ModusToolbox™ software. For more details on the overview of the ModusToolbox™ software, see the

ModusToolbox™ tools package user guide

.

All the application-level development flows depend on the low-level resources provided. These include the following:

  • Libraries/middleware (MW): Extensive middleware libraries that provide specific capabilities to an application. The available middleware spans across connectivity (OTA, Bluetooth®, AWS IoT, Bluetooth® LE, Secure Sockets to

    PSOC™

    MCU-specific functionality (USB, device firmware upgrade (DFU), and emWin). All the middleware is delivered as libraries via GitHub repositories

  • Board Support Packages (BSP): A BSP is the layer of firmware containing board-specific drivers and other functions. The BSP is a set of libraries that provide APIs to initialize the board and provide access to board-level peripherals. It includes low-level resources such as the Peripheral Driver Library (PDL) for the

    PSOC™

    MCU and macros for board peripherals. Custom BSPs can be created to enable support for end-application boards. See BSP Assistant to create your BSP

  • Device Support Library (DSL): A device support library combines content from several distinct software packages into a single package which includes the following major assets:

    • PSOC™

      MCU Peripheral Driver Library (PDL): The PDL integrates device header files, start-up code, and peripheral drivers into a single package. The PDL supports the

      PSOC™

      MCU family. The drivers abstract the hardware functions into a set of easy-to-use APIs. These are fully documented in the PDL API Reference.

      The PDL reduces the need to understand register usage and bit structures, therefore easing software development for the extensive set of peripherals in the

      PSOC™

      MCU series. Configure the driver for the application and then call APIs to initialize and use the peripheral

    • Hardware Abstraction Layer (HAL): The HAL provides a high-level interface to configure and use hardware blocks on MCUs. It is a generic interface that can be used across multiple product families. The focus on ease-of-use and portability means the HAL does not expose all the low-level peripheral functionality. The HAL wraps the lower-level drivers (such as

      PSOC™

      MCU PDL) and middlewares to provides a high-level interface to the MCU. The interface is abstracted to work on any MCU. This helps you write the application firmware independent of the target MCU

    • Device Utilities (device-utils): This asset handles the pre-defined System Power Management (SysPm) callback implementations for peripherals which require special handling when the MCU enters or exits DeepSleep

  • Configurators:ModusToolbox™ Configurators are stand-alone tools that can be used to set up and configure

    PSOC™

    Edge MCU resources and other middleware components without using the Eclipse IDE. The Device configurators and middleware configurators use the

    design.x

    files within the application workspace. You can then point to the generated source code and continue developing firmware in your IDE.

    If there is a change in the device configuration, edit the

    design.x

    files using the configurators and regenerate the code. It is recommended that you generate resource configurations using the configuration tool provided with ModusToolbox™ software.

    For more details on configurators, see the

    Configurators

    section

Application structure

The ModusToolbox™ v3.x release supports multi-core functionality. All applications for the

PSOC™ Edge

MCU will have a dual-core three project structure. The applications have app-owned BSPs, meaning the BSP will be common to all projects inside a multi-core application.

The folder structure of a typical code example application is illustrated below.


├───mtb-example-app
│ │ common.mk
│ │ common_app.mk
│ │ Makefile (MTB_TYPE = APPLICATION)
│ │
│ ├───bsps
│ │ └───TARGET_BSP1 (app-owned BSP)
│ │
│ ├───images
│ │
│ ├───proj_cm33_s (First Project)
│ │ │ main.c
│ │ │ Makefile (MTB_TYPE = PROJECT)
│ │ │ project1_helper.c
│ │ │ project1_helper.h
│ │ │
│ │ ├───deps
│ │ │ lib1.mtb (Local)
│ │ │ lib2.mtb (Shared)
│ │ │
│ │ └───libs
│ │ lib1 (Infineon Git repo)
│ │
│ ├───proj_cm33_ns (Second Project)
│ │
│ ├───proj_cm55 (Third Project)
│ │
│ └───templates
│ └───TARGET_BSP1
│ └───config
│ design.modus
│
└───mtb-shared
└───lib2 (Infineon Git repo)

PSOC™ Edge software resources

The software for the

PSOC™ Edge

MCU includes configurators, drivers, libraries, and middleware, as well as various utilities, makefiles, and scripts. It also includes relevant drivers, middleware, examples for use with IoT devices, and connectivity solutions. You may use any or all tools in any environment that you prefer. The following sections provide detailed information about these software resources.

Configurators

The ModusToolbox™ software provides graphical applications called configurators that make it easier to configure a hardware block. For example, instead of having to search through all the documentation to configure a serial communication block as a UART with a desired configuration, open the device configurator and set the baud rate, parity, and stop bits. Upon saving the hardware configuration, the tool generates the "C" code to initialize the hardware with the desired configuration.

Two types of configurators are:

  • BSP configurators that configure items that are specific to the MCU hardware

  • Library configurators that configure options for middleware libraries

Configurators are independent of each other, but they can be used together to provide flexible configuration options. They can be used stand-alone, in conjunction with other tools, or within a complete IDE. Configurators are used for:

  • Setting options and generating code to configure drivers

  • Setting up connections such as pins and clocks for a peripheral

  • Setting options and generating code to configure middleware

For the

PSOC™ Edge

MCU applications, the available configurators include the following:

  • Device Configurator: Set up the system (platform) functions, pins, and the basic peripherals (e.g., UART, Timer, and PWM)

  • ML Configurator: To fit the pre-trained model of choice to the target device with a set of optimization parameters (only available as a part of a separate pack)

  • QSPI Configurator: Configure an external memory and generate the required code

  • Smart I/O Configurator: Configure smart I/O pins

  • Bluetooth® Configurator: Configure the Bluetooth® settings

Each of the above configurators creates their own design files. BSP configurator file (e.g.,

design.modus

) are provided as part of the BSP with default configurations, while library configurators (e.g.,

design.cybt

) are provided by the application. When an application is created based on Infineon BSP, the application makes use of BSP configurator files from the Infineon BSP repository. You can customize or create all the configurator files as per the application requirements using the ModusToolbox™ software. To create a custom BSP, see

BSP Assistant

. For more details, see the

ModusToolbox™ help

section.

Library management for PSOC™ Edge MCU

The application can have shared or local libraries for the projects. If needed, different projects can use different versions of the same library. The shared libraries are downloaded in the mtb_shared directory. The application should use the

deps

folder to add library dependencies. The

deps

folder contains files with the

.mtb

file extension, which is used by ModusToolbox™ to download its git repository. These libraries are direct dependencies of the ModusToolbox™ project.

The Library Manager helps to add, remove, or update the libraries of your projects. It also identifies whether the particular library has a direct dependency on any other library using the manifest repository available on GitHub and fetches all the dependencies of that particular library. These dependency libraries are indirect dependencies of the ModusToolbox™ project. These dependencies can be seen in the

libs

folder. For more information, see the

Library Manager user guide

located at

<install_dir>/ModusToolbox/tools_<version>/library-manager/docs/library-manager.pdf

.

Software development for PSOC™ Edge MCU

The ModusToolbox™ ecosystem provides significant source code and tools to enable software development for PSOC™ Edge MCUs. You can use tools to:

  • Specify how you want to configure the hardware

  • Generate code that you can use in the firmware

  • Include various middleware libraries for additional functionality, such as emUSB or FreeRTOS

This source code makes it easier to develop the firmware for supported devices. It helps you quickly customize and build firmware without needing to understand the register set.

In the ModusToolbox™ environment, you can use configurators to configure either the device or a middleware library, such as the Bluetooth® LE stack. The BSP configurator files are used to configure device peripherals, pins, and memory using peripheral driver library code. The middleware is delivered as separate libraries for each feature or function so that it can be used across multiple platforms. For example, abstraction-rtos, lwIP, USB, and so on.

Firmware developers who wish to work at the register level should refer to the driver source code from the PDL. The PDL includes all the device-specific header files and startup code you need for the project. It also serves as a reference for each driver. Because the PDL is provided as source code, you can see how it accesses the hardware at the register level.

Some devices do not support particular peripherals. The PDL is a superset of all the drivers for any supported device. This superset design means:

  • All API elements needed to initialize, configure, and use a peripheral are available

  • The PDL is useful across various PSOC™ Edge MCUs, regardless of available peripherals

  • The PDL includes error checking to ensure that the targeted peripheral is present on the selected device

This enables the code to maintain compatibility across members of the

PSOC™ Edge

MCU family, as long as the peripherals are available. A device header file specifies the peripherals that are available for a device. If you write code that attempts to use an unsupported peripheral, you will get an error at compile time. Before writing code to use a peripheral, consult the datasheet for the particular device to confirm support for that peripheral.

As

Figure 2

shows, with the ModusToolbox™ software, you can do the following:

  1. Choose a BSP (Project Creator)

  2. Create a new application based on a list of starter applications, filtered by the BSPs that each application supports (Project Creator)

  3. Add BSP or middleware libraries (Library Manager)

  4. Develop the application firmware for the

    PSOC™ Edge

    MCU (IDE of choice or command line)

Figure 2.

ModusToolbox™ resources and middleware


ModusToolbox™ help

The ModusToolbox™ ecosystem provides documentation and training. One way to access it is launching the Eclipse IDE for ModusToolbox™ software and navigating to the following

Help

menu items:

Choose

Help

>

ModusToolbox™ General Documentation

:

  • ModusToolbox™ Documentation Index:

    Provides brief descriptions and links to various types of documentation included as part the ModusToolbox™ software

  • ModusToolbox™ Installation Guide:

    Provides instructions for installing the ModusToolbox™ software

  • ModusToolbox™ User Guide:

    This guide primarily covers the ModusToolbox™ aspects of building, programming and debugging applications. It also covers various aspects of the tools installed along with the IDE

  • ModusToolbox™ Training Class Material:

    For the training material, see the ModusToolbox™ Software Training webpage.

  • Release Notes

For documentation on Eclipse IDE for ModusToolbox™, choose

Help

>

Eclipse IDE for ModusToolbox™ General Documentation

:

  • Quick Start Guide:

    Provides you the basics for using Eclipse IDE for ModusToolbox™

  • User Guide:

    Provides descriptions about creating applications as well as building, programming, and debugging them using Eclipse IDE

  • Eclipse IDE for ModusToolbox™ Help:

    Provides description on how to create new applications, update application code, change middleware settings, and program/debug applications

  • Eclipse IDE Survival Guide

FreeRTOS support with ModusToolbox™​

Adding native FreeRTOS support to a ModusToolbox™ application project is like adding any middleware library. You can include the FreeRTOS middleware in your application by using the Library Manager.

If using the Eclipse IDE, do the following as marked in

Figure 3

:

  1. Open

    Library Manager

    from the Quick Panel.

  2. Select

    "Add Library"

    in the Library manager.

  3. Select the project

    to add the FreeRTOS middleware.

  4. Select

    FreeRTOS library

    that is present in the "core" tab. Click

    OK

    to close the "Add Library" dialog.

  5. Click

    "Update"

    in Library Manager to fetch the FreeRTOS library.

  6. The

    freertos.mtb

    file pointing to the FreeRTOS middleware is added to the application project's deps directory. The middleware content is also downloaded and placed inside the corresponding

    freertos

    folder. The default location is in the shared asset

    mtb_shared

    repository.

Figure 3.

Import FreeRTOS middleware in ModusToolbox™ application


To continue working with FreeRTOS, follow the steps mentioned in the Quick Start section of

FreeRTOS documentation

.

Programming and Debugging​

The ModusToolbox™ software supports the

Open On-Chip Debugger

(OpenOCD) using a GDB server and supports the J-Link debug probe.

You can use various IDEs to program devices and establish a debug session (see

Choosing an IDE

). For programming, the

PSOC™ Programmer

is available separately. It is a cross-platform application for programming Infineon microcontroller devices. It can program, erase, verify, and read the flash of the target device.

The

PSOC™ Edge

MCU has a KitProg3 onboard programmer and debugger. It supports the Cortex® microcontroller Software Interface Standard - Debug Access Port (CMSIS-DAP). For more details, see the

KitProg3 user guide

.

ModusToolbox™ requires KitProg3 or an external programmer which then uses the OpenOCD protocol for debugging the

PSOC™ Edge

MCU applications. It also supports GDB debugging using industry-standard probes such as the Segger J-Link.

For more information on debugging firmware on the

PSOC™ Edge

MCU with ModusToolbox™, see the Program and Debug section in the

Eclipse IDE for ModusToolbox™ user guide

.

PSOC™ Edge MCU development kit​

This application note uses the

PSOC™

Edge E84 Evaluation Kit for developing and programming the application on the MCU. There are two categories of parts in this family, the Edge Protect Category 2 (EPC 2) and the Edge Protect Category 4 (EPC 4) parts. These parts are compliant to the Edge Protect categories 2 and 4 as described

here

. Each part is supported by its dedicated Board Support Package (BSP). For further details on the distinction and comparison between the two Edge Protect Categories, refer to

AN237849 - Getting Started with the

PSOC™

Edge Security

document.

For the purposes of this document, we will use the Board Support Package (BSP) with the EPC 2 part (KIT_PSE84_EVAL_EPC2).

The evaluation kit carries a

PSOC™

Edge E84 MCU on a SODIMM-based detachable SOM board connected to the baseboard. The MCU SOM also has 128 Mb of QSPI flash, 1Gb of Octal flash, 128 Mb of Octal RAM,

PSOC™

4000T as the CAPSENSE™ co-processor, and an on-board AIROC™ Wi-Fi & Bluetooth ®combo.

The baseboard has the following:

  • M.2 interface connectors for interfacing external radio modules based on AIROC™ Wi-Fi & Bluetooth ® combos and external memory interfaces

  • An on-board programmer and debugger (KitProg3)

  • ETM/JTAG/SWD debug headers

  • Custom display capacitive touch panel connector

  • R-Pi-compatible MIPI-DSI and MIPI-DSI custom display

  • Analog and PDM microphones

  • Headphone connector and a speaker

  • USB host type-A and USB device type-C connectors

  • RJ45 Ethernet connector

  • M.2 (B-key) memory interface and M.2 (E-key) radio interface

  • Infineon’s Shield2Go interface and Mikroelektronika's mikroBUS compatible headers

  • 6-Axis IMU sensor and 3-axis magnetometer

  • microSD cardholder

  • CAPSENSE™ buttons and slider

  • User LEDs and buttons

For more details, see the

PSOC™

Edge E84 Evaluation Kit user guide.

Device features​

The

PSOC™

Edge product line has extensive features as shown in

Figure 4

. For more information, see the device datasheet, the reference manual, and the

References

section. The following are the major features:

  • Always-on domain

    • Acoustic activity detection

    • ADC, operational amplifiers, comparator, and DACs

  • Autonomous Analog

    • 2x Continuous-Time Blocks (CTB) offering Analog Front-End (AFE) functions such as:

      • Programmable Gain Amplifier (PGA)

      • Transimpedance Amplifier (TIA)

      • Pseudo-Differential Amplifier

      • Comparator

    • SAR ADC with

      • 5 Msps sample rate at 12 bits or 250 ksps at 16 bits in System High Performance mode

      • 200 ksps sample rate at 12 bits or 12.5 ksps at 16 bits in System Deep-Sleep mode

      • Accumulation and averaging – 2x, 4x, 8x … 256x

      • Limit detection, Offset and gain calibration

    • 2x 12-bit DAC with 1 μS refresh time, automatic waveform generation

    • 2x Programmable Threshold Comparators (PTComp) with post-processing supporting Audio Activity Detection (AAD) and Motor Control

    • Autonomous Controller capable of performing following functions in Device DeepSleep Mode

      • Power cycling of individual blocks

      • Send triggers and/or interrupts to the CPU

      • Digital output to as many as four GPIOs

  • Security features

    • Lockstep secure enclave in low‑power always‑on domain

      • Secure Infineon RoT key storage; secure boot

      • Tamper detection, side channel attack (SCA) mitigation, and protection against fault injection attacks

      • Secure enclave runtime services for Arm® Platform Security Architecture (PSA) compliant cryptography, key management, secure storage and attestation services; available on EPC 4 part numbers only. (See device datasheet)

    • Up to Infineon Edge Protect Category 4 (EPC 4), depending on part number. (See device datasheet)

    • Off‑the‑shelf Trusted Firmware‑M enablement and Mbed‑TLS for crypto operations

    • Secure isolation of processing environments via Arm® TrustZone with root-of-trust established at boot by Cortex®‑M33 CPU

    • Factory-provisioned device unique keypair (DICE_DeviceID), Hardware Unique Key (HUK), Unique DeviceSecret (UDS) and Infineon device certificates

    • Infineon proprietary protection units for memory and peripherals

    • Secure firmware update; secure debug, secure RMA mode for field failure analysis

  • Low‑power security, control, and communication CPU

    • Cortex®‑M33 with FPU, DSP, and MPU up to 200 MHz in System High Performance (HP) power mode. (See device datasheet for power modes)

    • 16 KB I‑cache

    • RRAM module for NVM

    • DMA

    • Hardware crypto accelerator with comprehensive support of cryptographic algorithms

  • High-performance compute, DSP, and machine learning (ML) blocks

    • Cortex®‑M55 CPU with DSP extension at 400 MHz in System High Performance (HP) power mode

    • FPU, MVE extension with vectored fixed and floating point

    • 32‑KB I‑cache and 32‑KB D‑cache

    • 256‑KB I- and 256‑KB D‑TCMs

    • Ethos‑U55 NN coprocessor with 128 multiply-accumulate operations (MACs) per cycle; 51.2 billion operations per second

    • HPDMA

    • Multi‑AXI high‑bandwidth interconnect

  • Communications and connectivity

    • HS USB host/device, 480 Mbps

    • SD host controllers with eMMC mode

    • Serial memory interfaces (SMIF) with octal DDR

    • Ethernet 10/100 media access control (MAC)

    • CAN FD

    • I3C bus for 2‑wire sensor hubs

    • I2C, SPI, and UART via serial communication blocks (SCB)

  • HMI functional blocks

    • 2.5D graphics processor for rendering images and text

    • Display controller with MIPI DSI

    • Audio multi‑microphone interface for far-field applications

  • Optimizable power

    • Independent voltage domains allowing selectable domain power for low-power or high-performance (See device datasheet)

    • Active, sleep, deep sleep, and hibernate modes

    • On‑chip DC‑DC buck converter

    • Dynamic voltage and frequency scaling, for real‑time power optimization

    • Granular SRAM blocks for selectable SRAM retention

  • Programmable GPIO pins

    • Programmable drive modes, strengths, and slew rates

    • Overvoltage tolerant (OVT) pins for I2C compliance

  • ModusToolbox™ design environment

    • Code development and debugging in a cross-OS (Windows, Linux, Mac OS) IDE-neutral environment supporting Visual Studio Code, IAR, Keil and Eclipse IDEs

    • Installable software development kits (SDK) for peripheral initialization, clock and pin configuration, and middleware selection

    • Peripheral driver library (PDL) for peripheral APIs, including SD host controller for connection to IoT devices; and ML library

    • Industry-standard CMSIS pack support

    • RTOS support, including FreeRTOS

  • DEEPCRAFT™ Studio enabling the full journey from ML model development to embedded software

Figure 4.

PSOC™ Edge

MCU block diagram


First PSOC™ Edge MCU design using Eclipse IDE for ModusToolbox™ software​

This section describes the following:

  • How to build a simple PSOC™ Edge MCU-based design and program it onto the development kit

  • Makes it easy to learn PSOC™ Edge MCU design techniques and how to use the ModusToolbox™ software and Eclipse IDE

Prerequisites​

Before you get started, make sure that you have the appropriate development kit for the

PSOC™ Edge

MCU product line, and have installed the required software. You also need internet access to the GitHub repositories during project creation.

Hardware prerequisites

The following design example is developed for the

PSOC™

Edge E84 Evaluation kit with the Edge Protect Category 2 (EPC 2) part (KIT_PSE84_EVAL_EPC2). However, you can build the application for other development kits including the Edge Protect Category 4 (EPC 4) part (KIT_PSE84_EVAL_EPC4). For more details, see the

Application development instructions

section.

For the design example shown in this application note, the minimum required revision for the

PSOC™

Edge E84 Evaluation kit is Rev *G.

For the provisioning flow, the minimum version of KitProg3 firmware required on

PSOC™

Edge E84 Evaluation kit is

2.60.1412

. Please see

Program the device

section for steps to upgrade the KitProg3 firmware.

On the

PSOC™

Edge E84 Evaluation kit please ensure below jumper and pin configuration are correctly placed on board.

  • Ensure

    Boot SW

    should be in 'High'/ON position

  • Ensure

    J20

    and

    J21

    should be in Tristate/Not-Connected(NC) position

Software prerequisites

Following are the software prerequisites

Note:

If you install the ModusToolbox™ tools package using the ModusToolbox™ Setup program, the Edge Protect Security Suite, Programming Tools and GCC Toolchain are installed automatically as required dependencies. If you instead get the tools package from the Infineon Developer Center, you must download and install these dependencies manually.


About the design​

This design uses the Arm® Cortex® M33 core of the

PSOC™ Edge

MCU to execute the following two tasks: UART communication and LED control.

At device reset, the secure boot process starts from the ROM boot with the secure enclave (SE) as the root of trust (RoT). It passes through a series of immutable boot codes and starts the CM33 secure application. This application needs to be in MCUboot format. The ModusToolbox™ build process supports the converting of the user image into MCUboot format using the combiner-signer feature of EdgeProtectTools.

The CM33 secure application performs the TrustZone configurations and launches the non secure application running on the same CM33 core.

The non-secure CM33 application is started and then proceeds to initialize the board peripherals and other resources. It enables the CM55 core and the project for CM55 core puts it to deepsleep. The CM33 non-secure application uses the UART to print a “Hello World” message to the serial port stream, and starts blinking the user LED on the kit.

Create a new application​

This section provides a step-by-step guideline for creating a new application. It uses the

Empty App

starter application and manually adds the functionality from the

Hello World

starter application. The Eclipse IDE for ModusToolbox™ is used in the instructions, but you can use any IDE or the command line if you prefer.

If you are familiar with developing projects with ModusToolbox™ software, you can use the

Hello World

starter application directly. It is a complete design, with all the firmware written for the supported kits. You can walk through the instructions and observe how the steps are implemented in the code example.

If you start from scratch and follow all the instructions in this application note, you can use the

Hello World

code example as a reference while following the instructions.

Launch the

Dashboard

application to get started. Note that the

Dashboard

application needs access to the internet to successfully clone the starter application onto your machine.

The

Dashboard

application helps you get started using the various tools with easy access to documentation and training material, a simple path for creating applications, and creating and editing BSPs.

Do the following to create a new application:

  1. Open the Dashboard application by clicking on

    [ModusToolbox installation path]/tools_X.X/dashboard/dashboard.exe

  2. In the right pane of the

    Dashboard

    window, select

    Eclipse IDE for ModusToolbox™

    in the

    Target IDE

    drop-down list and click

    Launch Eclipse IDE for ModusToolbox™

    Figure 5.

    Dashboard application


  3. Select a new workspace

    At launch, Eclipse IDE for ModusToolbox™ presents a dialog to choose a directory to use as the workspace directory. The workspace directory is used to store workspace preferences and development artifacts. You can choose an existing empty directory by clicking the Browse button, as shown in the following

    Figure 6

    . Alternatively, you can type in a directory name to be used as the workspace directory along with the complete path, and the Eclipse IDE will create the directory for you.

    Figure 6.

    Select a directory as the workspace


  4. Create a new ModusToolbox™ application

    1. From the Quick Panel, Click on

      Start

      , and then click

      New Application

    2. Alternatively, you can choose

      File > New > ModusToolbox™ Application

      , as shown in

      Figure 7

    The Project Creator opens.

    Figure 7.

    Create a new ModusToolbox™ application


  5. Select a target

    PSOC™

    development kit.

    ModusToolbox™ speeds up the development process by providing BSPs that set various workspace project options for the specified development kit in the new application dialog

    1. In the

      Choose Board Support Package (BSP)

      dialog, choose the

      Kit Name

      . For example, choose

      KIT_PSE84_EVAL_EPC2

      , as shown in

      Figure 8

    2. Click

      Next

      .

      Figure 8.

      Choose target hardware


    3. In the

      Select Application

      dialog, select

      Empty App

      starter application, as shown in

      Figure 9

    4. In the name field, type a name for the application, such as

      Hello_World

      . You can choose to leave the default name if you prefer

    5. Click on

      Create

      and wait for the Project Creator to automatically close once the project is successfully created.

      Figure 9.

      Choose starter application


A new ModusToolbox™ application is created successfully.

View and modify the design​

Figure 10

shows the Eclipse IDE Project interface, displaying the structure of the application project.

All

PSOC™ Edge

MCU applications have a dual-CPU three-project structure to develop code for the CM33 and CM55 cores. The CM33 core has two separate projects for the Secure Processing Environment (SPE) and Non-Secure Processing Environment (NSPE). A project folder consists of various subfolders, each denoting a specific aspect of the project.

Figure 10.

Project

PSOC™ Edge

view


The following is the folder structure for one of the projects (proj_cm33_ns), as shown in

Figure 10

. A similar folder structure is present for the other two projects (proj_cm33_s) and (proj_cm55).

  1. bsps folder

    The bsps folder is common to all projects in a multi-core application. The files provided by the BSP are present here and are listed under the

    TARGET_<bsp name>

    sub-folders. All the input files for the device and peripheral configurators are in the

    config

    folder inside the BSP. The

    Generated Source

    folder in the BSP contains the files that are generated by the configurators and are prefixed with

    cycfg_

    . These files contain the design configuration as defined by the BSP. From ModusToolbox™ 3.x or later, you can directly customize BSP configurator files for the application rather than overriding the default design configurator files with custom design configurator files since BSPs are completely owned by the application.

    The BSP folder also contains the linker scripts and the start-up code for the

    PSOC™ Edge

    MCU used on the board.

  2. build folder

    The build folder contains all the artifacts resulting from a build of the project. The output files are organized by target BSPs.

  3. deps folder

    The deps folder contains

    .mtb

    files, which provide the locations from which ModusToolbox™ pulls the libraries that are directly referenced by the application. For assets present in the manifest files, we use

    mtb://

    to fetch them into the project. For assets not present in the manifest, we use the GitHub location of that asset library in the

    .mtb

    file. The

    .mtb

    files also contain a git Commit Hash or Tag that tells which version of the library is to be fetched and a path as to where the library should be stored locally.

    For example, if retarget-io is needed (as will be added later in this application note), then

    retarget-io.mtb

    points to

    mtb://retarget-io#release-v2.0.200#$$ASSET_REPO$$/retarget-io/release-v2.0.200

    . The variable

    $$ASSET_REPO$$

    points to the root of the shared location, which defaults to mtb_shared. If the library must be local to the application instead of shared, you may change to 'Local' in Library Manager.

    This sub-directory also contains the

    locking_commit.log

    file, which keeps track of the version for each dependent library.

  4. libs folder

    The libs folder also contains

    .mtb

    files. In this case, they point to libraries that are included indirectly as a dependency of a BSP or another library. For each indirect dependency, the Library Manager places an .mtb file in this folder. These files have been populated based on the targets available in deps folder.

    The libs folder contains the file

    mtb.mk

    , which stores the relative paths of the all the libraries required by the application. The build system uses this file to find all the libraries required by the application.

    Everything in the libs folder is generated by the Library Manager; therefore, user is not expected to manually edit anything in that folder.

  5. main.c

    file

    This is the file containing the source code of the project. Each project has its own source code file. If a project has multiple source code files, they can be grouped under a "source" folder.

  6. Project-level Makefile

    This is the project's Makefile. It includes numerous variables used for the projects, such as

    COMPONENTS

    ,

    CORE

    ,

    CORE_NAME

    , and other variables used to specify flags and pre-build and post build commands. This file also includes path information for source code discovery, shared repo location, and path to the compiler. Plus, it includes the

    common.mk

    file from the application and the path information to the start.mk file in the installation tools directory.

  7. common_app.mk

    file

    This makefile is shared across the entire application and all its projects. It contains path information to indicate the location of the installation

    tools_<version>

    directory.

  8. common.mk

    file

    This Makefile is shared across all projects. It contains variables including: MTB_TYPE, TARGET, TOOLCHAIN, and CONFIG. This file includes a reference to the

    common_app.mk

    file.

  9. Application-level Makefile

    An application contains a Makefile which is at the application's root folder. This file contains the set of directives that the make tool uses to compile and link the application project. This Makefile contains the

    MTB_TYPE

    variable set to

    APPLICATION

    , plus the

    MTB_PROJECTS

    variable to specify the included projects. This file also includes the

    common_app.mk

    file and the path information to the

    application.mk

    file in the installation

    tools_<version>

    directory. This is responsible for forwarding build related requests to the individual core projects and dealing with post-build activities (for example, generating single monolithic HEX files that can be used to program all projects simultaneously) when they are complete.

  10. mtb_shared folder

    By default, when creating a new application or adding a library to an existing application and specifying it as shared, all libraries are placed in an

    mtb_shared

    directory adjacent to the application directories.

    The

    mtb_shared

    folder is shared between different applications within a workspace. Different applications may use different versions of shared libraries if necessary.

    Each workspace you create with one or more applications will include a

    mtb_shared

    directory adjacent to the application directories, and this is where the shared libraries are cloned by default. To modify this location, specify the

    CY_GETLIBS_PATH

    variable. Duplicate libraries are checked to see if they point to the same commit, and if so, only one copy is kept in the

    mtb_shared

    directory. You can regenerate these files using the Library Manager as and when needed.

Opening the Device Configurator

BSP configurator files are in the

bsps/TARGET_<BSP-name>/config

folder. For example, click

<Application-name>

from

Project Explorer

then click

Device Configurator

link in the

Quick Panel

to open the file design.modus in the

Device Configurator

as shown in

Figure 12

. You can also open other configuration files in their respective configurators or click the corresponding links in the

Quick Panel

.

Note that this section is for information only and aims to get the user familiarized with the device configurator tool. All configurations needed for the Hello World demo is already present in the default design file. The user is not expected to do any device configuration changes for this demo.

Figure 11.

Select device configurator from quick panel


Figure 12.

Device Configurator



Figure 12

shows the following various panes in the device configurator GUI tool:

  1. Resources and Categories pane

  2. List of Resources

  3. Parameters pane

  4. Code Review pane

  5. Notices pane

The

Device Configurator

provides a set of

Resources Categories

tabs. Here, you can choose between different resources available in the device such as peripherals, pins, and clocks from the

List of Resources

.

You can choose how a resource behaves by choosing a

Personality

for the resource. For example, a

Serial Communication Block (SCB)

resource can have

EZI2C

,

I2C

,

SPI

, or

UART

personalities. The

Alias

is the resource name, which is used in the firmware development. One or more aliases can be specified by using a comma or spaces to separate them.

The

Parameters

pane is where you enter the configuration parameters for each enabled resource and the selected personality. The

Code Preview

pane shows the configuration code generated per the configuration parameters selected. This code is populated in the

cycfg_

files in the

Generated Source

folder. The Parameters pane and Code Preview pane may be displayed as tabs instead of separate windows but the contents will be the same. Any errors, warnings, and information messages arising out of the configuration are displayed in the

Notices

pane. For more details, see the

Device Configurator userguide

.

The default BSP comes with a few peripherals pre-configured. You may change these configurations and settings or add your own as per requirement of your application. These configurations can be directly utilized by the application code to implement the functionality of configured resources. For more details, see

Write firmware

.

Add retarget-io middleware

In this step, add the

retarget-io

middleware to redirect standard input and output streams to the UART configured by the BSP. The middleware initialization is done in the

main.c

file. Do the following to add this middleware, as shown in

Figure 13

:

  1. First select the application in the project explorer and then In the

    Quick Panel

    , click

    Library Manager

  2. In the subsequent dialog, click

    Add Libraries

  3. Select the

    Target Project

    as

    proj_cm33_ns

    because this is the project in which we will be writing our application code

  4. Under

    Peripherals

    , select and enable

    retarget-io

    and click

    OK

  5. Click

    Update

    to add the library to that project

  6. The

    retarget-io.mtb

    file pointing to the Retarget-IO middleware is added to the application project's deps directory. The middleware content is also downloaded and placed inside the corresponding folder called retarget-io. The default location is in the shared asset repo that is mtb_shared

Figure 13.

Add the retarget-io middleware



Remove FreeRTOS library

The FreeRTOS library comes with the Empty Application code example. If you are using the Empty Application to create an application which does not use FreeRTOS, you will need to remove the library.

In this example, Empty Application is being modified into a Hello World application which does not require any RTOS for its functionality; thus, FreeRTOS should be removed from the library manager. You should also remove the RTOS related contents of the

"COMPONENTS"

variable in the project-level Makefiles.

Follow the next steps to remove the middleware, as shown in

Figure 14

:

  1. Open

    Library Manager

    from the Quick Panel

  2. Select

    FreeRTOS

    in the proj_cm33_ns libraries list and click on the "cross" button next to the library

  3. Click

    Update

    to remove FreeRTOS from the project. Similarly, the library can be removed from other project (proj_cm55) as well

  4. In each of the project-level

    Makefiles

    , delete the "

    FREERTOS

    and

    RTOS_AWARE

    " from the

    COMPONENTS

    variable

    COMPONENTS+=

    FREERTOS RTOS_AWARE

  5. Delete the

    FreeRTOSConfig.h

    file present in each project

Figure 14.

Remove FreeRTOS from the project



Write firmware​

At this stage in the development process, an application was created with the assistance of an application template and modified it to add the

retarget-io

middleware and remove freeRTOS middleware. In this section, the firmware implementing the design functionality will be written.

If you are working from scratch using the

PSOC™

Edge

Empty Application

, copy the respective source code to the

main.c

of the application project from the code snippet provided in this section. If you are using the

Hello World

code example, all the required files are already in the application.

Firmware flow

Examine the code in the

main.c

files of the non-secure CM33 project and the CM55 project. A basic secure CM33 project is also provided with applications for necessary security initializations and configurations. In this example, we use the default secure CM33 project; however, this can be modified to suit the use-case.

Figure 15

shows the firmware flowchart.

At device reset, the secure boot process starts from the ROM boot with the secure enclave (SE) as the root of trust (RoT). From the secure enclave, the boot flow is passed on to the system CPU subsystem where the secure CM33 application starts. After all necessary secure configurations, the flow is passed on to the non-secure CM33 application. Resource initialization for this example is performed by this CM33 non-secure project. It configures the system clocks, pins, clock to peripheral connections, and other platform resources. It then enables the CM55 core using the

Cy_SysEnableCM55()

function and the CM55 core is subsequently put to DeepSleep mode.

In the CM33 non-secure application, the BSP initialization function initializes the clocks and system resources. The

retarget-io

middleware is configured to use the debug UART. The debug UART prints a “Hello World!” message on the terminal emulator using the on-board KitProg3 acting as a USB-UART bridge to create a virtual COM port. The user LED's output logic state is continuously toggled with a delay of 1000 milliseconds.

Note that the application code uses BSP, PDL, and middleware functions to execute the intended functionality. You can open the Device Configurator to view the aliases that are setup in the BSP.

  • cybsp_init(): Sets up the BSP and initializes all the system resources of the device including system clocks and power regulators. It also performs device and memory security configurations when called from the Secure Processing Environment (SPE)
  • init_retarget_io() : This is a user defined function to initialize the debug UART. It uses the aliases set up in the BSP for the debug UART pins to configure the debug UART using the Retarget IO middleware with a standard baud rate of 115200 and redirects the input/output stream to the debug UART
  • Cy_SysEnableCM55()

    : This API is used to enable the CM55 core

  • Cy_GPIO_Inv()

    : The user LED is already configured in the BSP. This API is used to toggle the pin's output logic state

Figure 15.

Firmware flowchart


Code Listing 1

:

main.c

file from the non-secure CM33 project

proj_cm33_ns


/*******************************************************************************
* File Name : main.c
*
* Description : This source file contains the main routine for non-secure
* application in the CM33 CPU
*
* Related Document : See README.md
*
********************************************************************************
* $ Copyright 2023-YEAR Cypress Semiconductor $
*******************************************************************************/

/*******************************************************************************
* Header Files
*******************************************************************************/

#include "cybsp.h"
#include "retarget_io_init.h"

/*******************************************************************************
* Macros
*******************************************************************************/
#define BLINKY_LED_DELAY_MSEC (1000U)

/* The timeout value in microseconds used to wait for CM55 core to be booted */
#define CM55_BOOT_WAIT_TIME_USEC (10U)

/* App boot address for CM55 project */
#define CM55_APP_BOOT_ADDR (CYMEM_CM33_0_m55_nvm_START + \
CYBSP_MCUBOOT_HEADER_SIZE)

/*******************************************************************************
* Function Name: main
********************************************************************************
* Summary:
* This is the main function of the CM33 non-secure application.
*
* It initializes the device and board peripherals. It also initializes the
* retarget-io middleware to be used with the debug UART port using which
* "Hello World!" is printed on the debug UART. The LED pin is initialized with
* default configurations. The CM55 core is enabled and then the programs enters
* an infinite while loop which toggles the LED1 with a frequency of 1 Hz.
*
* Parameters:
* none
*
* Return:
* int
*
*******************************************************************************/
int main(void)
{
cy_rslt_t result = CY_RSLT_SUCCESS;

/* Initialize the device and board peripherals. */
result = cybsp_init();

/* Board initialization failed. Stop program execution. */
if (CY_RSLT_SUCCESS != result)
{
handle_app_error();
}

/* Enable global interrupts */
__enable_irq();

/* Initialize retarget-io middleware */
init_retarget_io();

/* \x1b[2J\x1b[;H - ANSI ESC sequence for clear screen. */
printf("\x1b[2J\x1b[;H");

printf("****************** "
"PSOC Edge MCU: Hello world "
"****************** \r\n\n");

printf("Hello World!\r\n\n");
printf("For more projects, "
"visit our code examples repositories:\r\n\n");

printf("https://github.com/Infineon/"
"Code-Examples-for-ModusToolbox-Software\r\n\n");

/* Enable CM55. */
/* CM55_APP_BOOT_ADDR must be updated if CM55 memory layout is changed.*/
Cy_SysEnableCM55(MXCM55, CM55_APP_BOOT_ADDR, CM55_BOOT_WAIT_TIME_USEC);

for(;;)
{
Cy_GPIO_Inv(CYBSP_USER_LED1_PORT, CYBSP_USER_LED1_PIN);
Cy_SysLib_Delay(BLINKY_LED_DELAY_MSEC);
}
}

/* [] END OF FILE */

Code Listing 3

:

retarget_io_init.h

file from the CM33 project

proj_cm33_ns

project

/*******************************************************************************
* File Name: retarget_io_init.h
*
* Description: This file is the public interface of retarget_io_init.c and
* contains the necessary UART configuration parameters.
*
* Related Document: See README.md
*
*******************************************************************************
* $ Copyright 2023-YEAR Cypress Semiconductor $
*******************************************************************************/

#ifndef _RETARGET_IO_INIT_H_
#define _RETARGET_IO_INIT_H_

/*******************************************************************************
* Header Files
*******************************************************************************/
#include "cybsp.h"
#include "mtb_hal.h"
#include "cy_retarget_io.h"
#include "mtb_syspm_callbacks.h"

/*******************************************************************************
* Macros
*******************************************************************************/

/* retarget-io deepsleep callback macros */
#define DEBUG_UART_RTS_PORT (NULL)
#define DEBUG_UART_RTS_PIN (0U)

/* Default syspm callback configuration elements */
#define SYSPM_SKIP_MODE (0U)
#define SYSPM_CALLBACK_ORDER (1U)


/*******************************************************************************
* Function prototypes
*******************************************************************************/
void init_retarget_io(void);

/*******************************************************************************
* Function Name: handle_app_error
********************************************************************************
* Summary:
* User defined error handling function
*
* Parameters:
* void
*
* Return:
* void
*
*******************************************************************************/
__STATIC_INLINE void handle_app_error(void)
{
/* Disable all interrupts. */
__disable_irq();

CY_ASSERT(0);

/* Infinite loop */
while(true);
}

#endif /* _RETARGET_IO_INIT_H_ */

/* [] END OF FILE */

Code Listing 4

:

main.c

file from the CM55 project

proj_cm55

/*******************************************************************************
* File Name : main.c
*
* Description : This source file contains the main routine for CM55 CPU
*
* Related Document : See README.md
*
********************************************************************************
* $ Copyright 2023-YEAR Cypress Semiconductor $
*******************************************************************************/

/*******************************************************************************
* Header File
*******************************************************************************/

#include "cybsp.h"

/*******************************************************************************
* Function Name: main
********************************************************************************
* Summary:
* This is the main function for CM55 application.
*
* CM33 application enables the CM55 CPU and then the CM55 CPU enters
* deep sleep.
*
* Parameters:
* void
*
* Return:
* int
*
*******************************************************************************/
int main(void)
{
cy_rslt_t result;

/* Initialize the device and board peripherals */
result = cybsp_init();

/* Board init failed. Stop program execution */
if (CY_RSLT_SUCCESS != result)
{
/* Disable all interrupts. */
__disable_irq();

CY_ASSERT(0);

/* Infinite loop */
while(true);
}

/* Enable global interrupts */
__enable_irq();

/* Put the CPU to Deep Sleep */
for (;;)
{
Cy_SysPm_CpuEnterDeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT);
}
}

/* [] END OF FILE */

This completes the summary of how the firmware works in the code example. For more detailed information, see the source files.

Build the application​

This section explains how to build the application. Follow these steps, as shown in

Figure 16

:

  1. Select the application project in the

    Project Explorer

    view

  2. Click

    Build Application

    shortcut under the

    Hello_World (APP_KIT_PSE84_EVAL_EPC2)

    group in the

    Quick Panel

  3. It selects the build configuration from Makefiles and compiles or links all projects that constitute the application. By default, debug configurations are selected. The

    Console view

    lists the results of the build operation, as shown in

    Figure 16

Figure 16.

Build the Application


Note:

You can also use the command-line interface (CLI) to build the application. See the

Build system chapter

in the

ModusToolbox™ tools package user guide

. This document is located in the

/ docs_<version>/

folder in the ModusToolbox™ installation directory.


Program the device​

This section explains how to program the

PSOC™ Edge

MCU.

The ModusToolbox™ software uses the

Open On-Chip Debugger (OpenOCD)

to program and debug applications on

PSOC™ Edge

MCUs. For ModusToolbox™ software to identify the device on the kit, the kit must be running KitProg3. For more details, see

Programming and Debugging

.

If you are using a development kit with a built-in programmer, connect the board to the computer using the USB cable. You may also need to update KitProg firmware using the fw-loader tool. The tool and instructions are available in the

Firmware Loader

GitHub repository. If you do not upgrade, you will see an error, such as "unable to find CMSIS-DAP device" or "KitProg firmware is out of date". For more information, please refer to

Firmware Loader user guide

.

Note that for the provisioning flow, the minimum required version of KitProg3 firmware is 2.60.1412. To update the KitProg3 firmware on

PSOC™

Edge E84 Evaluation kit (KIT_PSE84_EVAL_EPC2), do the following:

  1. Open modus-shell present at location

    <install-location>/ModusToolbox/tools_x.x/modus-shell

    in the ModusToolbox™ installation directory

  2. Paste and run the following command

    fw-loader --update-kp3

If you are developing on your own hardware, you may need a hardware programmer and debugger; for example, a

JLink

or

ULinkpro

.

To program the application, do the following, as shown in

Figure 17

:

  1. Select the project

    Hello_World

  2. Select the application project and click the

    Hello_World Program Application (KitProg3_MiniProg4)

    shortcut under the

    Launches

    group in the

    Quick Panel

    , as

    Figure 17

    shows. The IDE selects and runs the appropriate run configuration

  3. The

    Console

    lists the results of the programming operation

Figure 17.

Programming an application to a device


Note:

This step also performs a build if any files have been modified since the last build.

Test your design​

This section describes how to test the design.

Do the following steps to observe the output of the design. This application note uses TeraTerm as the UART terminal emulator to view the results. You can use any serial terminal to view the output.

  1. Select the serial port

    Launch

    Tera Term

    and select the USB-UART COM port as

    Figure 18

    shows. Note that COM port number may be different.

    Figure 18.

    Selecting the KitProg3 COM port in Tera Term


  2. Set the baud rate

    Set the baud rate to 115200 under Setup > Serial port, as shown in

    Figure 19

    .

    Figure 19.

    Configuring the baud rate in Tera Term


  3. Reset the device

    Press the reset switch (SW1) on the kit. A message appears on the terminal, as shown in

    Figure 20

    . The user LED on the kit starts blinking.

    Figure 20.

    Printed UART message


Booting from external OSPI flash​

The

PSOC™

Edge Evaluation Kit (EVK) supports booting from the following two external memories:

  • Quad Serial Peripheral Interface (QSPI) flash

  • Octal Serial Peripheral Interface (OSPI) flash

They are connected to the same serial memory interface (SMIF) through two different slave select lines. All code examples including the Hello World application, are configured to boot from the external QSPI flash.

Note:

This section is entirely optional and serves as a guide for users who wish to switch from the external Quad SPI flash memory to the external Octal SPI flash memory.

Note:

To check the version of Extended Boot, open modus-shell and execute one of the following command depending on the device. This command expects edgeprotecttools bin directory in the path environment variable.

edgeprotecttools -t pse8xs2 device-info or edgeprotecttools -t pse8xs4 device-info

To update/replace the Extended Boot present in the

PSOC™

Edge​ device, see section ​

Replacing the Extended Boot​

in the

AN237849 - Getting Started with ​

PSOC™

Edge ​Security

document.

  1. Provision the

    PSOC™

    Edge EVK with the correct set of configurations required for switching the boot flow to Octal SPI. For details about provisioning and policy configurations, see section

    Switching between Octal and Quad SPI external flash memory

    in the

    AN237849 - Getting Started with the

    PSOC™

    Edge Security

    document

  2. Open Device Configurator. In the' Memory Tab', delete all configured memory regions under Serial Memory Interface (SMIF) Block 0, Memory 1. For details on editing memory regions, refer the section 'Memory tab' of the

    Infineon Device Configurator User Guide

  3. Use the ModusToolbox™ QSPI configurator to update configuration files, configure memory slots, and generate code for your application to allow it to program into the external Octal SPI flash, see

    Figure 21

    .

    1. You can launch the QSPI configurator GUI using either of the below methods:

      1. On the Eclipse IDE, click on the

        QSPI configurator

        under BSP configurators (APP_KIT_PSE84_EVAL_EPC2)

      2. On the command-line, open modus-shell, navigate to the

        <application-directory>

        of the code example, and run the following 'make' command:

        make qspi-configurator

    2. It can be observed that the current configuration supports the external Quad SPI flash. In the first row, with

      QSPI Instance 0

      and

      Slave Slot 0

      , click on the drop-down menu for the column

      Memory Part Number

      and select

      Auto Detect SFDP

      . For the second row with

      QSPI Instance 0

      and

      Slave Slot 1

      , set the

      Memory Part Number

      and select

      Not Used

    3. Set the memory start address for the Octal SPI flash to

      0x60000000

      , the same as configured for the Quad SPI flash. The memory size can be left as the default

      0x20000000

      as the SMIF0 (XIP_Port0) region has a maximum size of 64 MB

    4. Save the QSPI configuration file

    Figure 21.

    Launching the QSPI configurator and configuring the booting from OSPI flash



  4. In the Device Configurator, open the Memory tab. Under Serial Memory Interface (SMIF) Block 0, Memory 0, add the memory regions to match the layout shown in

    Figure 22

    . Adjust each region’s size as needed for your application.

    Figure 22.

    Memory regions for OSPI flash



  5. We can now program the application into the external Octal SPI flash. Build the code example and program it onto the

    PSOC™

    Edge EVK. The

    PSOC™

    Edge EVK is now provisioned with configurations to enable boot from external OSPI flash (SMIF0)

Note:

The EVK can either boot from the internal RRAM memory or from the external OSPI flash, depending on the BOOT SW switch configuration. The EVK will not work with the other code examples that are configured to run from Quad SPI flash out of the box. To move back to Quad SPI flash, revert the SMIF policy configurations and provision the

PSOC™

Edge EVK again with the updated policy. Refer to the

AN237849 - Getting Started with

PSOC™

Edge Security document

for more detail.

Summary​

This application note demonstrated the

PSOC™ Edge

MCU device architecture and the associated development tools required for creating and modifying an application to utilize the varied functionality of this MCU.

The

PSOC™ Edge

MCU is a truly programmable embedded system-on-chip with configurable analog and digital peripheral functions and memory. It is highly versatile dual-CPU microcontroller with a neural net companion processor on a single chip. The integrated features and low-power modes make

PSOC™ Edge

MCU an ideal choice for smart home, IoT gateways, and other related applications.

Glossary​

This section lists the most commonly used terms that you might encounter while working with

PSOC™

family of devices.

  • Board support package (BSP) : A BSP is the layer of firmware containing board-specific drivers and other functions. The board support package is a set of libraries that provide firmware APIs to initialize the board and provide access to board level peripherals

  • PSOC™ Programmer : Cypress Programmer is a flexible, cross-platform application for programming Cypress devices. It can Program, Erase, Verify, and Read the flash of the target device

  • KitProg: The KitProg is an onboard programmer/debugger with USB-I2C and USB-UART bridge functionality. The KitProg is integrated onto most PSOC™ development kits

  • MiniProg3 / MiniProg4 : Programming hardware for development that is used to program PSOC™ devices on your custom board or PSOC™ development kits that do not support a built-in programmer

  • Personality: A personality expresses the configurability of a resource for a functionality. For example, the SCB resource can be configured to be an UART, SPI or I2C personalities

  • PSOC™ : A programmable, embedded design platform that includes a CPU, such as the 32-bit Arm® Cortex®-M0, with both analog and digital programmable blocks. It accelerates embedded system design with reliable, easy-to-use solutions, such as touch sensing, and enables low-power designs

  • Middleware : Middleware is a set of firmware modules that provide specific capabilities to an application. Some middleware may provide network protocols (e.g. MQTT), and some may provide high level software interfaces to device features (e.g. USB, audio)

  • Peripheral driver library (PDL): The peripheral driver library (PDL) simplifies software development for the PSOC™ MCU family. PDL contains a set of low-level APIs to control hardware peripherals such as UART and SPI. The interfaces are usually specific to a particular micro-controller or micro-controller family. Since the PDL interacts with the hardware at a lower level it is less portable between devices, especially those with different architectures. The PDL reduces the need to understand register usage and bit structures, therefore easing software development for the extensive set of peripherals available

  • Hardware abstraction layer (HAL): HAL provides a generic, device agnostic interface that can be used across multiple product families. The HAL is designed for portability, not as a general-purpose user library. HAL drivers are thin wrappers around lower-level device specific (e.g.: PDL) APIs and are focused on the runtime behavior of the hardware, not initialization. The HAL is designed to be compatible with a wide range of devices including low memory, multi-core, connectivity and secure devices

  • ModusToolbox™ : An Eclipse based embedded design platform for IoT designers that provides a single, coherent, and familiar design experience combining the industry's most deployed Wi-Fi and Bluetooth® technologies, and the lowest power, most flexible MCUs with best-in-class sensing

Revision history​

Document revision

Date

Description of changes

*I

2025-09-15

Release to web

Trademarks​

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc., and any use of such marks by Infineon is under license.

PSOC™, formerly known as PSoC™, is a trademark of Infineon Technologies. Any references to PSoC™ in this document or others shall be deemed to refer to PSOC™.