LBIST (Logic Built-In Self Test) is an on-chip hardware mechanism that can be used to detect latent faults in the microcontroller. The LBIST implementation in the platform allows the execution of periodic self-tests of the microcontroller logic. It is accessed through registers in the test register interface (TRI) unit.