Inter-Integrated Circuit (I2C)
The I2C module is a functional block that offers communication functionality according to the I2C-bus specification version 2.1. I2C is either connected to the SPB bus or the COMPB bus with a slave interface including a set of special function registers (SFRs). The bus interface used by the I2C module is defined in the device specific chapter.