The PSI5-S module performs communication according to the PSI5 specification. It communicates with the external world using one ASC interface for all channels. This ASC interface is built into the PSI5-S module. If the optional bidirectional mode is used, the commands to the external Physical Layer Interface (PHY) are transmitted through this interface.