The clock system is built up as a chain composed from different building blocks which allow different function parts for the complete chain.

The building blocks as shown in the following figure are:

  • Basic clock generation with internal and external oscillators (Clock Source)

  • Clock speed up-scaling with phase locked loops (

    PLL

    )

  • Clock distribution with clock control units (

    CCU

    )

  • Individual clock configuration within other functional blocks

Figure 1. Clock tree

A device specific overview can be found in the device specific section.