Feature list
A dedicated WDT for each implemented CPU, a dedicated WDT for cyber-security CPU (CPUcs) and a system WDT that can be freely used by the application
Programmable 16-bit timer
Programmable password protection with configurable automatic password sequencing
Programmable timestamp checking with programmable window
Alarm is triggered if the WDT is not serviced before timer overflows
Alarm is triggered if wrong password is provided during unlock or check access
Configurable unlock-restriction if the respective SMU state-machine is not in RUN state
Wake-up signal to respective CPU on timer-value transition from
7FFF
to
8000
WDT functions can be suspended during test and debug