The

Solutions

tab displays for supported devices that provide configurations for a multi-resource solution. This tab provides configurable elements that generally consist of multiple hardware blocks. These elements pre-configure many of the low-level details and just present a higher-level interface to configure the solution-level element itself. All hardware that makes up the solution is configured in one

Parameters

pane, instead of having individual blocks on different panes. This tab allows you to enter one or more

Name(s)

for the resource. It also shows the selected

Personality

where applicable.