About this document​

Scope and purpose​

This application note describes the features of low-power modes in the PSOC™ Control C3 MCU family and explains how to enter low-power modes and return to Active mode.

Intended audience​

This application note is intended for users who are new to the PSOC™ Control C3 MCU to enable them to use the MCU efficiently to implement solutions using the low-power modes of the microcontroller. In addition to that, this application note briefly explains the different low-power modes available in the MCU.

This application note assumes that you are familiar with PSOC™ Control C3 and the ModusToolbox™ development environment. If you are new to PSOC™ Control C3, see AN238329 - Getting started with PSOC™ Control C3 MCU on ModusToolbox™. If you are new to ModusToolbox™, see the

ModusToolbox™ home page

.

Associated part​

family

All PSOC™ Control C3 devices.

Introduction​

This application note describes low-power modes in Infineon’s PSOC™ Control C3 family MCUs. This MCU family includes Arm® Cortex® CPU, CAN FD, memory, and analog and digital peripheral functions in a single chip. The PSOC™ Control C3 MCU has several different power modes. These modes are intended to minimize the average power consumption in an application.

This application note explains the features of the power modes and how to set up the power mode transition. To understand the described functionality and terminology used in this application note, see the “Device power modes” chapter of the architecture reference manual for more details.

This application note also introduces system power management library of the

peripheral driver library

(PDL). The PDL is a complete software tool that includes APIs for configuring peripherals and system registers to implement the desired functionality. PDL provides direct access to almost all hardware resources of the target device. It reduces the need to understand and directly access registers and bit structures. PDL is downloaded from GitHub while creating an application in ModusToolbox™ using the Project Creator tool and is not installed along with the ModusToolbox™ IDE.

Power modes of PSOC™ Control C3 MCU​

PSOC™ Control C3 MCU has the following power modes:

  • Active mode

    1

    : All peripherals and CPU are available. In Active mode, the core voltage can be set to any of the four values. This impacts both power consumption and maximum clock frequency for CPU and peripherals. The following active modes are supported:

    • Ultra low power (ULP): 0.9 V core voltage with 50 MHz CPU frequency

    • Medium frequency (MF): 1.0 V core voltage with 70 MHz CPU frequency

    • Low power (LP): 1.1 V core voltage with 150 MHz CPU frequency

    • Overdrive (OD): 1.2 V core voltage with 180 MHz CPU frequency

  • Sleep mode

    : All peripherals except the CPU are available

  • Deep Sleep mode

    : Low speed functions are available. The CPU is in retention mode. RAM content is also retained. Only Deep Sleep capable peripherals can wake up the system

  • Deep Sleep-RAM mode

    : The CPU is turned off. Full RAM is retained for a warm boot after wakeup. Only Deep Sleep-capable peripherals are operational if enabled and can wake up the system

  • Deep Sleep-OFF mode

    : Same as Deep Sleep-RAM mode except RAM is also turned off

  • Hibernate mode

    : Device and I/O states are frozen. All peripherals except low-power comparator (LPCOMP) and backup domain peripherals are turned off. All clocks except the backup domain clock and all internal regulators are turned off

Figure 1

shows the relationship between power modes and the power supply current.

Figure 1.

Power modes and power supply current



Note:

Figure 1is only an indication of the power supply currents for each mode. Actual current values depend on the clock configuration and peripheral setting in each mode. For more details on power supply current characteristics, see the datasheet.


Power modes​

Table 1

summarizes the states of each power mode and the entry and wakeup conditions. For more details on power modes, see the architecture reference manual.

Table 1. PSOC™ Control C3 MCU power modes

Power mode

Description

Entry condition

Wakeup source

Wakeup action

Active

Primary mode of operation; all peripherals and CPU are available. Current consumption as low as 7 mA (Typ.)

Wake up from sleep, all deep sleep modes, hibernate reset, or any other reset

Not applicable

Not applicable

Sleep

CPU is in Sleep mode; all other peripherals are available. Current consumption as low as 4 mA (Typ.)

Register write from Active mode or wake up from Deep Sleep through debugger

Any interrupt to CPU

Interrupt

Deep Sleep

All high-frequency clocks and peripherals are turned off. Low-frequency clock and low-power analog and digital peripherals are available for operation and as wakeup sources. Current consumption as low as 7 μA (Typ.)

Register write from active

GPIO interrupt, low-power comparator (LPCOMP), Deep Sleep serial communication block (SCB), watchdog timer (WDT), real time clock (RTC) alarms, and debugger

Interrupt or debug

Deep Sleep-RAM

A low-power mode, like Deep Sleep, except most configuration states are not retained. Wake up causes the processors to reboot. The software can use the retained SRAM contents (programmable) to more quickly recover the application state, that is perform a “warm” reboot

Register write from active

GPIO interrupt, Deep Sleep SCB, WDT, RTC alarms

Warm boot

Deep Sleep-OFF

A low-power mode, like Deep Sleep, except most configuration states and memories are not retained. Wakeup causes the processors to "cold" reboot

Register write from active

GPIO interrupt, Deep Sleep SCB, WDT, RTC alarms

Cold boot (Reset)

Hibernate

GPIO states are frozen; all high frequency clocks and peripherals are switched off. Low-frequency clocks, and WCO can function. Device resets on wake up event. Current consumption as low as 300 nA (Typ.)

Register write from active

Hibernate WAKEUP pins, LPCOMP, RTC alarm, and WDT

Cold boot (Reset)

Note:

Before entering Deep Sleep, Deep Sleep-RAM, or Deep Sleep-OFF mode, configures all Power Policy Units (PPUs) to correct states for the difference Deep Sleep mode. See the Power control architecture for the details of PPU.



CPU sleep and wakeup instructions​

Arm® Cortex® CPU transitions between sleep and wakeup independently. Wait-for-Interrupt (__WFI) is the core sleep instruction. After a CPU executes __WFI, the CPU goes to sleep and stays in sleep until any interrupt is asserted. Wait-for-Event (__WFE) is similar to __WFI, but it wakes up when the wakeup event is received instead of an interrupt. Set Event (__SEV) is used for waking up other CPUs in sleep mode because of a __WFE. CPU Deep Sleep uses the same instructions for sleep and wakeup, but the SLEEPDEEP bit[2] of the Arm® System Control Register (SCR) is set before a sleep instruction. For more information on SCR, see

Arm® system control register user guide

. This process is implemented in SysPm PDL library, see

System power management (SysPm) library

.

Boot​

The boot procedure involves the initialization of various blocks of the PSOC™ Control C3 MCU to get into basic operational mode before entering the application main() function. The boot procedure is invoked on POR, software reset, Deep Sleep-RAM wakeup, Deep Sleep-OFF wakeup, and Hibernate wakeup.

PSOC™ Control C3 MCU supports two types of boot procedures depending on the power mode:

  • Cold boot: POR, software reset, Deep Sleep-OFF wakeup, and Hibernate wakeup will go through the cold boot procedure

  • Warm boot: Deep Sleep-RAM wakeup will go through the warm boot procedure

Note:

The boot procedure is not involved when waking up from CPU Sleep and Deep Sleep power modes. The type of boot procedure can be determined using theCy_SysPm_GetBootMode()function of PDL that can be called in the beginning of the main() function so that appropriate action can be taken in the application according to the type of boot executed.


Cold boot​

In this boot mode, the system clocks and related clock paths are initialized and then the C runtime environment is set up before entering the main () function. For Deep Sleep-OFF and Hibernate wakeup, the device resets everything except the backup power domain resources. There is a small difference for initial power ON where even the backup power domain is reset.

Warm boot​

Waking up from Deep Sleep-RAM mode results in a warm boot procedure. Warm boot is a shortened version of the complete boot process. The application can specify an entry point for warm boot, which is the starting point of execution for the CPU upon waking up from Deep Sleep-RAM. This results in shortened boot procedure execution time.

This is done using the

Cy_Syslib_SetWarmBootEntryPoint()

function of PDL. Using this function, an entry point such as a function address can be specified along with the stack pointer value that needs to be restored. See

Implementing low-power mode transitions

section. This feature enables you to implement a variety of use cases such as the device can enter the Deep Sleep-RAM state after setting an RTC alarm interrupt, GPIO or WDT interrupt. When the interrupt is triggered, the device wakes up from Deep Sleep-RAM, the CPU executes the warm boot procedure, and the control is transferred to the entry point function.

Power control architecture​

PSOC™ Control C3 MCU uses the Arm® power control architecture. The components used to control a single power domain are shown in following figure. For more information, see

Arm® power control architecture

.

Figure 2.

Power gating in power control architecture



  • Power Policy Unit (PPU)

    : Usually controls the power domain, but it can also be used to implement separate reset domains within a single power domain. The "SW IF" is the software interface from the system controller (for example, M33 processor). It is an Advanced Peripheral Bus (APB) interface at the PPU, and it is mapped to the Advanced High-performance Bus (AHB) memory-mapped I/O (MMIO) through an asynchronous bus bridge. The device interface labeled “LPI” stands for Low Power Interface, which is usually implemented as a Q- or P-channel

  • Power Control State Machine (PCSM)

    : A custom hardware module that controls the power switches. System Controller refers to an MCU (for example, M33). For the specific use case where the main active PPU that controls VCCACT_PD, the system controller is inside the power-gated domain. For this, the software interface (SW IF) and interrupt signals are isolated as required

Additionally, there is a custom component called Power Dependency Control Matrix (PDCM) that is present in Arm® reference design. All PPUs interface with the PDCM, which handles dependency relationships between power domains.

Power states supported by each PPU​

PSOC™ Control C3 MCU has three PPUs. See

Table 2

and

Table 3

for more information.

Table 2. Power modes supported by each PPU

PPU

PPU state

PPU_MAIN

ON

FULL_RETENTION

MEMORY_RETENTION

OFF

PPU_CPUSS

ON

FULL_RETENTION

OFF

PPU_SRAM

ON

MEMORY_RETENTION

OFF

Table 3. PPU configuration towards Deep Sleep state

Deep Sleep state

PPU power modes

Deep Sleep

PPU_MAIN: FULL_RETENTION

PPU_CPUSS: FULL_RETENTION

PPU_SRAM: MEMORY_RETENTION

Deep Sleep-RAM

PPU_MAIN: MEMORY_RETENTION

PPU_CPUSS: OFF

PPU_SRAM: MEMORY_RETENTION

Deep Sleep-OFF

PPU_MAIN: OFF

PPU_CPUSS: OFF

PPU_SRAM: OFF

The PDL implements the

Cy_SysPm_SetDeepSleepMode()

function to set the different Deep Sleep mode by configuring three PPUs. See the

Implementing low-power mode transitions

section.

Power modes transition​

Figure 3

shows the different states that the device can be in along with the possible power mode transition paths. The transitions are described in detail in subsequent sections of this document.

Figure 3.

Power mode transitions



RESET/OFF state

  • OFF state

    • Represents the state with no power applied

    • Go to RESET, when powered up above power-on reset level (POR event)

  • RESET state

    • Detected reset event: POR, External Reset (XRES), or Internal Reset

    • Go to Active mode after reset sequence completion

    • Device will enter RESET state upon assertion of XRES in any of the power modes

Entering low power mode​

Table 4

shows how to enter low-power mode and the actions in low power modes.

Table 4. Low power mode transitions

Initial mode

Final mode

Trigger

Hardware actions

Active

Sleep

Firmware action

  1. Clear the SLEEPDEEP bit [2] of the SCR register for CPU

  2. Optionally, set the SLEEPONEXIT bit [1] of the SCR register, if the CPU runs only on interrupts. When this bit is set, the CPU will not return to application code after the WFI/WFE instruction is executed. The CPU will wake up on any enabled interrupt or event and will enter Sleep/Deep Sleep mode as soon as it exits the interrupt or services the event

  3. Optionally, set the SEVONPEND bit [4] of the SCR register if the application needs to wake up the CPU from any pending interrupt. If this bit is set, any interrupt that enters a pending state will wake up the CPU

  4. Execute WFI/WFE instruction on the CPU

Tip:

PDL provides

Cy_SysPm_CpuEnterSleep()

API to implement the above steps, see

System power management (SysPm) library

chapter for more details.

  1. CPU clocks are gated OFF

  2. CPU waits for an interrupt or event to wake up

Active

Deep Sleep

Firmware action

Perform these steps to enter Deep Sleep mode (LPM_READY bit [5] of the PWR_CTL register should read ‘1’ before performing these steps):

  1. Set the power mode policy of PPU_MAIN, PPU_CPUSS and PPU_SRAM to Deep Sleep state based on

    Table 3

  2. Set the SLEEPDEEP bit [2] of the SCR register for CPU

  3. Optionally, set the SLEEPONEXIT bit [1] of the SCR register, if the CPU runs only on interrupts. When this bit is set, the CPU will not return to application code after the WFI/WFE instruction is executed. The CPU will wake up on any enabled interrupt or event and will enter Sleep/Deep Sleep mode as soon as it exits the interrupt or services the event

  4. Optionally, set the SEVONPEND bit [4] of the SCR register if the application needs to wake up the CPU from any pending interrupt. If this bit is set, any interrupt that enters a pending state will wake up the CPU

  5. Execute WFI/WFE instruction on the CPU

Tip:

PDL provides

Cy_SysPm_SetDeepSleepMode()

and

Cy_SysPm_CpuEnterDeepSleep()

APIs to configure PPUs and enter into Deep Sleep mode, see

System power management (SysPm) library

section for more details.

  1. CPU enters low-power mode

  2. High-frequency clocks are shut down

  3. I/O cells will be frozen automatically

  4. Retention is enabled and non-retention logic is reset

  5. Active regulator is disabled and Deep Sleep regulator takes over

Active

Deep Sleep-RAM

Firmware action

Perform these steps to enter Deep Sleep mode (LPM_READY bit [5] of the PWR_CTL register should read ‘1’ before performing these steps):

  1. Set the entry point of SRSS BOOT_ENTRY register for warm boot, which is the starting point of execution for the CPU upon waking up

  2. Set the power mode policy of PPU_MAIN, PPU_CPUSS and PPU_SRAM to Deep Sleep-RAM state based on

    Table 3

  3. Set the SLEEPDEEP bit [2] of the SCR register for CPU

  4. Optionally, set the SLEEPONEXIT bit [1] of the SCR register, if the CPU runs only on interrupts. When this bit is set, the CPU will not return to application code after the WFI/WFE instruction is executed. The CPU will wake up on any enabled interrupt or event and will enter Sleep/Deep Sleep mode as soon as it exits the interrupt or services the event

  5. Optionally, set the SEVONPEND bit [4] of the SCR register if the application needs to wake up the CPU from any pending interrupt. If this bit is set, any interrupt that enters a pending state will wake up the CPU

  6. Execute WFI/WFE instruction on the CPU

Tip:

PDL provides

Cy_SysPm_SetDeepSleepMode()

and

Cy_SysPm_CpuEnterDeepSleep()

APIs to configure PPUs and enter into Deep Sleep-RAM mode, see

System power management (SysPm) library

section for more details.

  1. CPU is turned off

  2. High-frequency clocks are shut down

  3. I/O cells will be frozen automatically

  4. Active mode logic is not retained, the SRAM can be retained

  5. Active regulator is disabled and Deep Sleep regulator takes over

Active

Deep Sleep-OFF

Firmware action

Perform these steps to enter Deep Sleep mode (LPM_READY bit [5] of the PWR_CTL register should read ‘1’ before performing these steps):

  1. Set the entry point of SRSS BOOT_ENTRY register for cold boot

  2. Set the power mode policy of PPU_MAIN, PPU_CPUSS and PPU_SRAM to Deep Sleep-OFF state based on

    Table 3

  3. Set the SLEEPDEEP bit [2] of the SCR register for CPU

  4. Optionally, set the SLEEPONEXIT bit [1] of the SCR register, if the CPU runs only on interrupts. When this bit is set, the CPU will not return to application code after the WFI/WFE instruction is executed. The CPU will wake up on any enabled interrupt or event and will enter Sleep/Deep Sleep mode as soon as it exits the interrupt or services the event

  5. Optionally, set the SEVONPEND bit [4] of the SCR register if the application needs to wake up the CPU from any pending interrupt. If this bit is set, any interrupt that enters a pending state will wake up the CPU

  6. Execute WFI/WFE instruction on the CPU

Tip:

PDL provides

Cy_SysPm_SetDeepSleepMode()

and

Cy_SysPm_CpuEnterDeepSleep()

APIs to configure PPUs and enter into Deep Sleep-OFF mode, see

System power management (SysPm) library

section for more details.

  1. CPU is turned off

  2. High-frequency clocks are shut down

  3. I/O cells will be frozen automatically

  4. Active mode logic and SARM are not retained at all

  5. Active regulator is disabled and Deep Sleep regulator takes over

Active

Hibernate

Firmware action

  1. Configure wakeup sources (Hibernate wakeup pins P2.0/P9.0, LPCOMP0/LPCOMP1) HIB_WAKE_SRC bits [3:0], wakeup RTC alarm mask HIB_WAKE_RTC bit [30], and wakeup WDT mask HIB_WAKE_WDT bit [31] of the PWR_HIB_WAKE_CTL register, and configure the polarity for wakeup sources HIB_WAKE_SRC bits [3:0] of the PWR_HIB_WAKE_CTL2 register based on the application requirement

  2. Set TOKEN bits [7:0] of the PWR_HIBERNATE register to specific branching data that can be used on a wakeup event from Hibernate mode

  3. Set UNLOCK bits [8:15] of the PWR_HIBERNATE register to 0x3A for FREEZE and HIBERNATE bits of the PWR_HIBERNATE register to operate

  4. Set FREEZE bit [17] of the PWR_HIBERNATE register to freeze the I/O pins

  5. Set HIBERNATE bit [31] of the PWR_HIBERNATE register to enter Hibernate mode

  6. Read the PWR_HIBERNATE register to make sure that the write has taken effect

  7. Execute WFI instruction on the CPU

Tip:

PDL provides

Cy_SysPm_SetHibernateWakeupSource()

and

Cy_SysPm_SystemEnterHibernate()

APIs to set wakeup source and implement the above steps to enter Hibernate mode, see

System power management (SysPm) library

section for more details.

Note:

It is recommended to trigger Hibernate mode automatically. Therefore, when entering Hibernate mode, disable all the interrupts and do a write operation on the PWR_Hibernate register.

  1. CPU is turned off

  2. Both high-frequency and low-frequency clocks are shut down

  3. Retention is enabled and non-retention logic is reset

  4. Both Active and Deep Sleep regulators are powered down. The peripherals that are active in the hibernate domain operate directly out of VDDD

  5. I/O cells are frozen

Sleep

Deep Sleep

When the debugger is not connected and Deep Sleep mode is triggered, but LPM_READY==0, the device internally enters Sleep mode. The device will automatically transit to Deep Sleep when LPM_READY == 1.

If the debugger is connected and Deep Sleep mode is triggered by the firmware, the device will enter Deep Sleep only when the following conditions are met:

  1. LPM_READY == 1

  2. Debugger is disconnected

  1. High-frequency clocks are shut down

  2. I/O cells will be frozen automatically

  3. Retention is enabled and non-retention logic is reset

  4. Active regulator is disabled and Deep Sleep regulator takes over

Figure 4

shows the software and hardware operation for the transition from Active mode to Deep Sleep mode.

Figure 4.

Active mode to Deep Sleep mode transition



Note:

InFigure 4andFigure 5, the gray boxes indicate hardware operation. Therefore, processing with software is not required.

Figure 5

shows the software and hardware operation for the transition from Active mode to Hibernate mode.

Figure 5.

Active mode to Hibernate mode transition



Waking up from low power modes​

Table 5

shows the hardware triggers for wakeup and the actions after wakeup.

Table 5. Wakeup actions

Initial mode

Final mode

Trigger source

Hardware action

Sleep

Active

Any enabled interrupt in Sleep mode

CPU exits Sleep mode and executes the interrupt

Deep Sleep

Active

Any enabled interrupt in Deep Sleep mode

The device returns to the configuration it had while entering Deep Sleep mode. (Active reference and core regulator turn on; IMO/clocks enabled, retention disabled, non-retained resets, freeze release; CPU exits low-power mode and takes interrupt)

Deep Sleep

Sleep

Debug wakeup

  • Retention disabled and non-retained reset

  • Freeze release

  • HF and LF are ON

  • CPU remains in a Sleep state

Deep Sleep-RAM

Active

Any enabled interrupt in Deep Sleep mode

The device executes warm boot. (Active reference and core regulator turn on; IMO/clocks enabled, retention and non-retained resets, freeze release; high frequency clocks turn on, FLL/PLL enable)

Deep Sleep-OFF

Active

Any enabled interrupt in Deep Sleep mode

The device resets (cold boot). (Active reference and core regulator turn on; IMO/clocks enabled, retention and non-retained resets, freeze release; high frequency clocks turn on, FLL/PLL enable)

Hibernate

Active

Hibernate wakeup pins, RTC alarms, LPCOMP, WDT

Hibernate wakeup is implemented as a transition to Active mode through reset:

  1. Low-voltage (internal Active and Deep Sleep mode) regulators and references are ramped up

  2. All low-voltage logic (operating from internal regulators) is reset

  3. IMO clock is started

  4. Core starts execution

Figure 6

shows the software and hardware operation for the transition from Deep Sleep mode to Active mode.

Figure 6.

Deep Sleep mode to Active mode transition



Note:

The gray boxes indicate hardware operation inFigure 6. Therefore, processing with software is not required.


System power management (SysPm) library​

Within the PDL, the system power management (SysPm) API provides functions to change power modes as shown in

Figure 3

. The API can also register callback functions to execute a peripheral function before or after power mode transitions. For more information, see

SysPM documentation

of the PDL.

Mode transition functions​

The system can enter the Sleep, Deep Sleep, Deep Sleep-RAM, Deep Sleep-OFF, and Hibernate modes using the PDL APIs.

Table 6

lists some PDL APIs to configure the different power modes.

Table 6. Power mode configuration APIs

API

Description

Cy_SysPm_CpuEnterSleep

Sets executing CPU to Sleep mode

Cy_SysPm_SetDeepSleepMode

Sets the Deep Sleep mode: Deep Sleep or Deep Sleep-RAM or Deep Sleep-OFF

Cy_SysPm_CpuEnterDeepSleep

Sets executing CPU to the Deep Sleep mode

Cy_SysPm_SetHibernateWakeupSource

Configures sources to wake up the device from the system Hibernate power mode

Cy_SysPm_SystemEnterHibernate

Sets the device into system Hibernate mode

The SysPm PDL driver manages low-power callbacks registered by the application. When a power mode transition is about to occur, the driver calls the registered callbacks to allow the application to prepare for the transition. This may involve disabling peripherals or ensuring that no data is being transmitted or received.

To enable this, the SysPm driver implements a callback mechanism. When a lower power mode transition is about to take place (either entering or exiting low-power modes), the registered callbacks for that transition are called. Every callback function should handle the five possible steps shown in

Table 7

.

Table 7. Transition function options

Callback function option

Description

CY_SYSPM_CHECK_READY

Checks the ready state to transition to other mode. Exits without transition if it returns

CY_SYSPM_FAIL

CY_SYSPM_BEFORE_TRANSITION

Callbacks execute and configure required actions before mode transition

CY_SYSPM_AFTER_TRANSITION

Callbacks execute after mode transition or configuration

CY_SYSPM_CHECK_FAIL

Callbacks execute only when CY_SYSPM_CHECK_READY fails. It executes the rollback action

CY_SYSPM_AFTER_DS_WFI_TRANSITION

Performs the actions to be done after exiting Deep Sleep if entered and before interrupts are enabled

A callback function can skip some steps.

Table 8

outlines the available skip options.

Table 8. Transition function skip options

Callback function skip option

Description

CY_SYSPM_SKIP_CHECK_READY

Define to skip check ready mode in the SysPm callback

CY_SYSPM_SKIP_CHECK_FAIL

Define to skip check fail mode in the SysPm callback

CY_SYSPM_SKIP_BEFORE_TRANSITION

Define to skip before transition mode in the SysPm callback

CY_SYSPM_SKIP_AFTER_TRANSITION

Define to skip after transition mode in the SysPm callback

The SysPm driver organizes all the callbacks into a linked list. While entering a low-power mode, SysPm goes through that linked list from first to last, executing the callbacks one after another. While exiting low-power mode, SysPm goes through that linked list again, but in the opposite direction from last to first. This ordering supports prioritization of callbacks relative to the transition event.

By calling the mode transition function, the device starts to transition with five callback operations. The CPU Sleep and CPU Deep Sleep modes use Arm® sleep instructions __WFI() or __WFE(). Code execution stops and waits for an interrupt during the CPU Sleep mode. After waking up from Sleep mode, the device automatically transitions to CPU Active.

Figure 7.

Sleep/Deep Sleep/Hibernate mode transition



Implementing low-power mode transitions​

Use the System Power Management (SysPm) driver to change power modes and reduce system power consumption in power sensitive designs. The functions and other declarations used in this driver are in

cy_syspm.h

. You can include

cy_pdl.h

to get access to all functions and declarations in the PDL.

Switching the CPU into Sleep mode​

The

Cy_SysPm_CpuEnterSleep()

function switches the calling CPU into the CPU Sleep power mode. You must clear all pending interrupts before putting the CPU into Sleep mode, even if they are masked.

/* Prepare the system for CPU Sleep mode here.
* This may include clearing pending interrupts,
* disabling peripherals, and saving necessary states.
*/

if (CY_SYSPM_SUCCESS != Cy_SysPm_CpuEnterSleep(CY_SYSPM_WAIT_FOR_INTERRUPT))
{
/* Error: System failed to enter CPU Sleep mode.
A registered CPU Sleep "check ready" callback returned an error status.*/
}
else
{
/* System successfully exited CPU Sleep mode.
The program has resumed execution after waking up from CPU Sleep.*/
}
Switching the MCU into Deep Sleep mode​

The

Cy_SysPm_CpuEnterDeepSleep()

function switches the CPU into Deep Sleep power mode. The following code snippet demonstrates how to configure the system to enter Deep Sleep mode, showcasing the necessary steps to achieve System Deep Sleep state.

int main(void) 
{
...

/* Deep Sleep mode configuration */
Cy_SysPm_SetDeepSleepMode(CY_SYSPM_MODE_DEEPSLEEP);

for (;;)
{
/* Wait for UART traffic to stop */
while (cy_retarget_io_is_tx_active()) {};

if (CY_SYSPM_SUCCESS != Cy_SysPm_CpuEnterDeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT))
{
/* Error: System failed to enter CPU Deep Sleep mode.
A registered CPU Deep Sleep "check ready" callback returned an error status.*/
}
else
{
/* System successfully exited CPU Deep Sleep mode.
The program has resumed execution after waking up from CPU Sleep.*/
}
}
}
Switching the MCU into Deep Sleep-RAM mode​

Before the

Cy_SysPm_CpuEnterDeepSleep()

function switches the CPU into Deep Sleep-RAM power mode, the following steps need to performed:

  • The warm boot entry point is set by using the

    Cy_Syslib_SetWarmBootEntryPoint()

    function. This is automatically taken care as part of auto-generated code inside the

    cybsp_init()

    . To know more about warm boot entry, see

    Warm boot

  • Register the Deep Sleep-RAM callback to store NVIC registers to the RAM by using the

    System_Store_NVIC_Reg()

    function to ensure that the NVIC register data is persistent after the device wakes up from Deep Sleep-RAM

  • Set Deep Sleep mode to Deep Sleep-RAM power mode by calling the

    Cy_SysPm_SetDeepSleepMode()

    function

After wake up from Deep Sleep-RAM mode, the warm boot entry point handler

cybsp_warmboot_handler()

is performed. In the

cybsp_warmboot_handler()

function, the

SystemInit_Warmboot_CAT1B_CM33()

function is called to enable all peripheral blocks through the peripheral control registers and unfreeze all the I/Os, initialize the device and board peripherals, and execute the after-transition callback to restore the NVIC data from the RAM by using the

System_Restore_NVIC_Reg()

function, then jump to

main()

.

The following code snippet demonstrates how to configure the system to enter Deep Sleep-RAM mode and wake up from this mode, showcasing the necessary steps to achieve Deep Sleep-RAM state and wakeup.

/* Function prototypes */
cy_en_syspm_status_t deepsleep_ram_callback_func(cy_stc_syspm_callback_params_t*callbackParams, cy_en_syspm_callback_mode_t mode);
int main(void);

/* Callback declaration for Deep Sleep-RAM */
cy_stc_syspm_callback_params_t deepsleep_ram_callback_param = {NULL, NULL};
cy_stc_syspm_callback_t deepsleep_ram_callback =
{
.callback = &deepsleep_ram_callback_func,
.type = CY_SYSPM_DEEPSLEEP_RAM,
.callbackParams = &deepsleep_ram_callback_param,
.order = 0u
};

/* The variable of boot mode */
CY_NOINIT cy_en_syspm_boot_mode_t boot_mode;

/* This function is called before entering main() */
void Cy_SystemInit(void)
{
/* Gets from which Deep Sleep mode the device has woke up */
boot_mode = Cy_SysPm_GetBootMode();
}

/* This function is called in cybsp_warmboot_handler(), and jump to main() */
void cybsp_syspm_do_warmboot(void)
{
/* Execute DeepSleep-RAM callback function after the device has woke up */
(void)Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP_RAM, CY_SYSPM_AFTER_TRANSITION);

/* Desired resume point of the application */
(void)main();
}

/* GPIO interrupt handler */
void user_button_intr_handler(void)
{
Cy_GPIO_ClearInterrupt(CYBSP_USER_BTN_PORT, CYBSP_USER_BTN_PIN);
}

int main(void)
{
cy_rslt_t result;

/* Checks if system woke up(From DeepSleep-RAM) through warm boot */
if(Cy_SysLib_IsDSRAMWarmBootEntry())
{
/* Free the required peripherals after waking-up from DS-RAM */
cy_retarget_io_deinit();
}
else
{
/* Initialize the device and board peripherals */
result = cybsp_init();
/* Board init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(0);
}
}

/* Initialize UART and retarget-io to use the debug UART port */
...

/*Enable wake up interrupt, for example: initialize GPIO interrupt and enable IRQ */
cy_stc_sysint_t user_button_intr_config =
{
.intrSrc = CYBSP_USER_BTN_IRQ,
.intrPriority = 0U,
};
Cy_SysInt_Init(&user_button_intr_config, user_button_intr_handler);
NVIC_EnableIRQ(user_button_intr_config.intrSrc);

if(CY_SYSPM_WARM_BOOT_MODE == boot_mode)
{
/* Warm boot (wake up form Deep Sleep-RAM mode */
}
else if(CY_SYSPM_POR_BOOT_MODE == boot_mode)
{
/* POR boot */
}

/* Check the Warm Boot entry Status flag */
if(!Cy_SysLib_IsDSRAMWarmBootEntry())
{
/* When POR, register the Deep Sleep-RAM callback function */
if (!Cy_SysPm_RegisterCallback(&deepsleep_ram_callback))
{
CY_ASSERT(0);
}
}
else /* The device woke up(From Deep Sleep-RAM) through warm boot */
{
/* Clears the Warm Boot entry Status flag */
Cy_SysLib_ClearDSRAMWarmBootEntryStatus();
}

/* Set Deep Sleep mode to Deep Sleep-RAM */
Cy_SysPm_SetDeepSleepMode(CY_SYSPM_MODE_DEEPSLEEP_RAM);

/* Enable global interrupts */
__enable_irq();

for (;;)
{
/* Wait for UART traffic to stop */
while (cy_retarget_io_is_tx_active()) {};

if(CY_SYSPM_SUCCESS != Cy_SysPm_CpuEnterDeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT))
{
/* Error: System failed to enter CPU Deep Sleep-RAM mode.
A registered Deep Sleep-RAM "check ready" callback returned an error status.*/
}
else
{
/* CY_SYSPM_SUCCESS is never seen here as successfully entering
* Deep Sleep-RAM mode. This is because a wake up from
* Deep Sleep-RAM mode goes through the warm boot. */
}
}
}

cy_en_syspm_status_t deepsleep_ram_callback_func(cy_stc_syspm_callback_params_t*callbackParams, cy_en_syspm_callback_mode_t mode)
{
cy_en_syspm_status_t retVal = CY_SYSPM_FAIL;
CY_UNUSED_PARAMETER(callbackParams);

switch (mode)
{
case CY_SYSPM_CHECK_READY:
retVal = CY_SYSPM_SUCCESS;
break;

case CY_SYSPM_CHECK_FAIL:
retVal = CY_SYSPM_SUCCESS;
break;

case CY_SYSPM_BEFORE_TRANSITION:
/* Store NVIC registers to the RAM */
System_Store_NVIC_Reg();
retVal = CY_SYSPM_SUCCESS;
break;

case CY_SYSPM_AFTER_DS_WFI_TRANSITION:
/* Restore the NVIC data from the RAM */
System_Restore_NVIC_Reg();
retVal = CY_SYSPM_SUCCESS;
break;

case CY_SYSPM_AFTER_TRANSITION:
retVal = CY_SYSPM_SUCCESS;
break;

default:
break;
}
return retVal;
}
Switching the MCU into Deep Sleep-OFF mode​

Before the

Cy_SysPm_CpuEnterDeepSleep()

function switches the CPU into Deep Sleep-OFF power mode, set Deep Sleep mode to Deep Sleep-OFF power mode by calling the

Cy_SysPm_SetDeepSleepMode()

function. The following code snippet demonstrates how to configure the system to enter Deep Sleep-OFF mode, showcasing the steps necessary to achieve Deep Sleep-OFF state.

/* The variable of boot mode */
CY_NOINIT cy_en_syspm_boot_mode_t boot_mode;

/* This function is called before entering main */
void Cy_SystemInit(void)
{
/* Checks from which Deep Sleep mode the system has woke up */
boot_mode = Cy_SysPm_GetBootMode();

/* Checks whether IOs are frozen during DEEPSLEEP-RAM/OFF */
if (Cy_SysPm_DeepSleepIoIsFrozen())
{
Cy_SysPm_DeepSleepIoUnfreeze();
}
}

/* GPIO interrupt handler */
void user_button_intr_handler(void)
{
Cy_GPIO_ClearInterrupt(CYBSP_USER_BTN_PORT, CYBSP_USER_BTN_PIN);
}

int main(void)
{
...
/*Enable wake up interrupt, for example: initialize GPIO interrupt and enable IRQ */
cy_stc_sysint_t user_button_intr_config =
{
.intrSrc = CYBSP_USER_BTN_IRQ,
.intrPriority = 0U,
};
Cy_SysInt_Init(&user_button_intr_config, user_button_intr_handler);
NVIC_EnableIRQ(user_button_intr_config.intrSrc);

if(CY_SYSPM_COLD_BOOT_MODE == boot_mode)
{
/* Cold boot (wake up form Deep Sleep-OFF mode */
}
else if(CY_SYSPM_POR_BOOT_MODE == boot_mode)
{
/* POR boot */
}

/* Update boot entry point before entering Deep Sleep-OFF mode */
SRSS_BOOT_ENTRY = CY_FLASH_S_CBUS_BASE;

/* Set Deep Sleep mode to Deep Sleep-OFF */
Cy_SysPm_SetDeepSleepMode(CY_SYSPM_MODE_DEEPSLEEP_OFF);

/* Enable global interrupts */
__enable_irq();

for (;;)
{
/* Wait for UART traffic to stop */
while (cy_retarget_io_is_tx_active()) {};

if (CY_SYSPM_SUCCESS != Cy_SysPm_CpuEnterDeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT))
{
/* Error: System failed to enter CPU Deep Sleep-OFF mode.
A registered Deep Sleep-OFF "check ready" callback returned an error status.*/
}
else
{
/* CY_SYSPM_SUCCESS is never seen here as successfully
* entering Deep Sleep-OFF mode. This is because a wake up
* from Deep Sleep-OFF mode goes through the cold boot. */
}
}
}
Switching the MCU to Hibernate mode​

If you call the

Cy_SysPm_SystemEnterHibernate

function, the system will be switched into the Hibernate power mode directly.

int main(void) 
{
...

uint32_t reset_reason;

/* Check the IO status. If current status is frozen, unfreeze the system. */
if (Cy_SysPm_GetIoFreezeStatus())
{
/* Unfreeze the system */
Cy_SysPm_IoUnfreeze();
}

/* Get the reset cause */
reset_reason = Cy_SysLib_GetResetReason();

if ((reset_reason & CY_SYSLIB_RESET_HIB_WAKEUP))
{
/* The reset has occurred on a wakeup from Hibernate power mode */
}

/* Enable global interrupts */
__enable_irq();

for (;;)
{
Cy_SysPm_ClearHibernateWakeupSource(CY_SYSPM_HIBERNATE_PIN0_LOW);

/* There is a need to put the device into the system Hibernate modeSetup the
* Hibernate wakeup source.*/
Cy_SysPm_SetHibernateWakeupSource(CY_SYSPM_HIBERNATE_PIN0_LOW);

/* Prepare the device for system Hibernate mode here */
if (CY_SYSPM_SUCCESS != Cy_SysPm_SystemEnterHibernate())
{
/* System did not enter Hibernate mode because a registered
* Hibernate "check ready" callback returned a "not success" status */
}
else
{
/* CY_SYSPM_SUCCESS is never seen here as successfully entering
* system Hibernate mode. This is because a wake up from
* system Hibernate mode goes through the system reset. */
}
}
}

The system can wake up from Hibernate mode by configuring the following wakeup sources: GPIO Wakeup pin, LPCOMP, RTC alarm, WDT.

A device-specific pin or pins with programmable polarity can wake up the system. Additionally, certain unregulated peripherals can trigger wakeup under specific conditions. For instance, a low-power comparator can wake the system by comparing two external voltages or compare an external voltage to an internally generated voltage. The Watchdog Timer (WDT) can also be configured to wake up the system by generating a WDT interrupt.

Note:

When booting from Hibernate mode, call theCy_SysPm_IoUnfreeze()function to unfreeze the GPIOs, which are frozen when the device enters System Hibernate mode.


Register callback functions using PDL​

The following code snippet showcases how to register the SysPm callbacks.

/******************************************************************************
* Callback prototypes
******************************************************************************/
cy_en_syspm_status_t DeepSleepCallback(cy_stc_syspm_callback_params_t *callbackParams, cy_en_syspm_callback_mode_t mode);

/******************************************************************************
* Parameter structures for callback functions
******************************************************************************/
cy_stc_syspm_callback_params_t DeepSleepCallbackParams =
{
&HW1_address,
&context
};

/******************************************************************************
* Callback structure
******************************************************************************/
cy_stc_syspm_callback_t myDeepSleep =
{
&DeepSleepCallback,
CY_SYSPM_DEEPSLEEP,
CY_SYSPM_SKIP_BEFORE_TRANSITION,
&DeepSleepCallbackParams,
NULL,
NULL,
0
};

/******************************************************************************
* Register DeepSleepCallback
******************************************************************************/
if (true != Cy_SysPm_RegisterCallback( &myDeepSleep)
{
/* Insert error handling */
}

Implementing custom callback functions using PDL​

In the SysPm callback, you can define the actions to be performed before and after the power mode transition.

/******************************************************************************
* * DeepSleepCallback implementation
* ******************************************************************************/
cy_en_syspm_status_t DeepSleepCallback(cy_stc_syspm_callback_params_t *callbackParams, cy_en_syspm_callback_mode_t mode)
{
cy_en_syspm_status_t retVal = CY_SYSPM_FAIL;
if (NULL != callbackParams)
{
CySCB_Type *hwBase = (CySCB_Type *)callbackParams->base;
cy_stc_scb_spi_context_t *context = (cy_stc_scb_spi_context_t *)callbackParams->context;
}
switch (mode)
{
/* In this case ensure that firmware/hardware is ready for CPU Deep Sleep mode */
case CY_SYSPM_CHECK_READY:
{ /* Process the "check ready" condition */
retVal = CY_SYSPM_SUCCESS;
}
break;

/* One of the registered callback returned CY_SYSPM_FAIL, need to
revert changes (if any) performed in the CY_SYSPM_CHECK_READY case. */
case CY_SYSPM_CHECK_FAIL:
{ /* Revert changes done in the CY_SYSPM_CHECK_READY case */
retVal = CY_SYSPM_SUCCESS;
}
break;

/* This case will be skipped during callbacks execution */
case CY_SYSPM_BEFORE_TRANSITION:
break;

/* This case is executed after wakeup from system Deep Sleep */
case CY_SYSPM_AFTER_TRANSITION:
{ /* Perform actions, if required, after wakeup from the system Deep Sleep
mode */
retVal = CY_SYSPM_SUCCESS;
}
break;

default:
break;
}
return(retVal);
}

Low power code examples​

This chapter lists the code examples that describe how to use the low power procedure using the

Peripheral Driver Library

(PDL).

CE239867 – Hibernate GPIO wakeup​

This code example demonstrates the use of Hibernate mode and wakeup from GPIO (Hibernate wakeup pin) using the PDL functions.

The example sets pin P2.0 to low level to wake up the MCU before the MCU enters the Hibernate mode. When P2.0 is low level, wake up MCU from Hibernate mode, then the reset reason message is sent on the UART terminal. For more information of the code example, see

CE239867 – Hibernate GPIO wake up

.

CE240527 – RTC alarm periodic wakeup​

This code example demonstrates how to enter Deep Sleep and Hibernate modes, and use RTC to generate an RTC alarm to wake up the MCU from these modes.

The MCU enters either Deep Sleep or Hibernate mode based on the duration that the user button is pressed. The RTC alarm wakes up the system and prints the wakeup information to the UART terminal. The following figure shows the state machine implemented in the firmware to execute the transitions. For more information, see

CE240527 – PDL RTC alarm periodic wake up

.

Figure 8.

RTC periodic wakeup timer using alarm interrupt



CE240257 – Wake up from Deep Sleep/Hibernate mode using a low-power comparator​

This code example demonstrates the functionality of wake up from Deep Sleep or Hibernate mode using the low-power comparator (LPCOMP). It uses a dedicated GPIO input to compare the input voltage to an internal reference voltage to wake the PSOC™ Control C3 MCU from Deep Sleep or Hibernate mode. A user LED indicates the current power mode.

The following figure shows the firmware flow. The main loop checks the output of LPCOMP and toggles the LED when the output is high. Otherwise, the system goes into the Deep Sleep or Hibernate mode after turning the LED ON for two seconds. The system will wake up immediately if the LPCOMP output goes high during Deep Sleep or Hibernate mode. For more information of code example, see

CE240257 - Wakeup from DeepSleep/Hibernate mode using a low-power comparator

.

Figure 9.

Wake up from Deep Sleep/Hibernate mode using a low-power comparator



CE240361 – I2C slave Deep Sleep wakeup​

This code example demonstrates the operation of the I2C resource in Deep Sleep mode. After programming, the application starts automatically. The UART terminal displays the slave initialization and the MCU entering Deep Sleep mode. Using the Bridge Control Panel (BCP) software to transmit and receive the data over I2C, BCP is installed automatically as part of the

PSOC™ Programmer

installation. Send the command to wake the device up from Deep Sleep and display a wake up message on the terminal.

The I2C driver provides callback function

Cy_SCB_I2C_DeepSleepCallback()

to handle power mode transition. It calls the

Cy_SysPm_RegisterCallback()

function to register I2C Deep Sleep callback in initialization of main. For more information of the code example, see

CE240361 – I2C slave Deep Sleep wake up

.

Summary​

Table 9

shows available resources which are active in certain power modes and its wakeup parameters.

Table 9. Power modes and wakeup parameters

Active/Sleep

Deep Sleep

Deep Sleep-RAM

Deep Sleep-OFF

Hibernate

Off

Parameters

Wake source

2

Any interrupt

Deep Sleep peripherals

Deep Sleep peripherals

Deep Sleep peripherals

RTC/Hibernate peripherals

Power on

Wake action

Resume

Resume

Warm boot

Reset/cold boot

Reset

Reset

Wake time

One CPU cycle

< 20 µs

Deep Sleep + warm boot

Deep Sleep + cold boot

POR + cold boot < 1 ms

Resources

ECO

On/Off

Off

Off

Off

Off

Off

IHO

On

Off

Off

Off

Off

Off

IMO

On

On/Off

Off

Off

Off

Off

ILO

On/Off

On/Off

On/Off

On/Off

On/Off

Off

WCO

On/Off

On/Off

On/Off

On/Off

On/Off

Off

CPU

On/Sleep

Retention

Off

Off

Off

Off

SRAM

On

On

On/Off

Off

Off

Off

The operational states possible in low-power modes are generally limited in functionality and parametric performance as compared to their capabilities in the Active modes. Also, blocks that do not support low-power modes, such as Deep Sleep and Hibernate, cannot wake up the CPU from these modes.

Table 10

captures various device components and their availability during the device power modes/states.

Table 10. Block power modes

Block

Power mode

Active

Sleep

Deep Sleep

Hibernate

Backup

CPUSS

CPU

Y

N

N

N

N

NVIC

Y

Y

N

N

N

WIC

Y

Y

Y

Y

N

FLASH

Y

Y

N

N

N

SRAM

Y

Y

Y

N

N

DMA

Y

Y

N

N

N

Programmable digital

SMART I/O

Y

Y

Y

N

N

Fixed function digital

TCPWM

Y

Y

N

N

N

SCB

Y

Y

Y

3

N

N

CAN FD™

Y

Y

N

N

N

Special function

CORDIC

Y

N

N

N

N

Analog

HPPASS (SAR, CSG)

Y

Y

N

N

N

LPCOMP

Y

Y

Y

4

Y

N

I/O

GPIO

Y

Y

Y

Y

5

N

Backup

RTC

Y

Y

Y

Y

Y

Registers

Y

Y

Y

Y

Y

References​

The datasheets and references manuals of

family are listed here.

Contact

Technical Support

to obtain these documents.

  1. Datasheets

    • PSOC™ Control C3 - PSC3P5xD, PSC3M5xD datasheet

    • PSOC™ Control C3 - PSC3P2xD, PSC3M3xD datasheet

  2. Reference manuals

    • PSOC™ Control C3 MCU architecture reference manual

    • PSOC™ Control C3 MCU registers reference manual

  3. Application notes and user guides

    • AN238329 - Getting started with PSOC™ Control C3 MCU on ModusToolbox™ software

    • PSOC™ Control C3 MCU hardware design guide

    • KIT_PSC3M5_EVK PSOC™ Control C3 Evaluation Kit guide

Revision history​

Document revision

Date

Description of changes

**

2024-11-29

Initial release

1

The core voltage can be configured in Device Configurator of ModusToolbox™. It will be automatically configured in the auto-generated code inside the

cybsp_init()

.

2

See

Table 10

for the list of peripherals available in Deep Sleep and Hibernate power modes.

3

Only SCB 0 (I2C, SPI)

4

Cannot wake up from Deep Sleep-RAM and Deep Sleep-OFF mode using LPCOMP.

5

Only hibernate_wakeup pins (P2.0 and P9.0) are operational and capable of waking up the device from Hibernate mode. For more information, see the datasheet.