About this document​

Scope and purpose

This application note is to introduce the

PSOC™⁠ Control C3

MCU, which is a single-core, high-performance, low-power, and secure MCU designed for real-time control, enhanced sensing, and secure and low-power applications. This application note helps you to explore the

PSOC™⁠ Control C3

MCU architecture and development tools and shows you how to create your first project using the Eclipse IDE for ModusToolbox™ software. This application note also guides you to more resources available online to accelerate your learning about the

PSOC™⁠ Control C3

MCU.

Intended audience

This document is intended for the users who are new to

PSOC™ Control C3

and ModusToolbox™ software.

Associated part family

All

PSOC™⁠ Control C3

devices.

Software version

ModusToolbox™ software

3.3 or above.

More code examples? We heard you.

To access an ever-growing list of

PSOC™⁠ Control C3

code examples using ModusToolbox™, please visit the

GitHub

site

.

Introduction​

The

PSOC™⁠ Control C3

device is a microcontroller targeted at industrial applications. The

PSOC™⁠ Control C3

integrates the following features on a single chip:

  • Single core 180 MHz 32-bit Arm® Cortex®-M33 CPU with

    • Floating-point unit (FPU)

    • DSP

    • Memory protection unit (MPU)

    • TrustZone framework support

    • 16 KB I-cache

  • Up to 256 KB Read-While-Write Flash with ECC support

  • 64 KB ROM for boot code

  • 64 KB SRAM with ECC support

  • Industrial control peripherals: Coordinate rotation digital computer (CORDIC) and timer/counter pulse-width modulator (TCPWM) supporting high-resolution pulse-width modulator (HRPWM)

  • High-performance programmable analog subsystem (HPPASS): 12-bit, up to 12-Msps SAR ADC with parallel idle sampling of up to 16 analog channels and five comparators with <10 ns, built-in 10-bit DAC, and slope generator

  • ModusToolbox™ development environment with installable SDKs and libraries, industry standard Arm® tools, and RTOS support

This application note introduces you to the capabilities of the

PSOC™ Control C3

, gives an overview of the development ecosystem, and gets you started with a simple 'Hello World' application wherein you learn to use the

PSOC™ Control C3

. Additionally, it shows you how to create an application from an empty starter application. The completed design of this application is available as a

code example for ModusToolbox™ on GitHub

.

For hardware design considerations, see the Hardware design guide for the

PSOC™ Control C3

family.

Architecture and product lines

Figure 1

shows a detailed block diagram of the MCU.

Figure 1.

Functional block diagram



There are four variants in the

PSOC™ Control C3

.

Table 1

provides an overview of different product lines.

Table 1.

PSOC™ Control C3

product lines

Product line

Device series

Details

Entry line

PSC3P2x

Single-core 100 MHz Arm® Cortex®-M33, up to 256 KB flash and 64 KB RAM, 12-channel 6 Msps ADC

PSC3M3x

Single-core 100 MHz Arm® Cortex®-M33, up to 256 KB flash and 64 KB RAM, 12-channel 6 Msps ADC, CORDIC, MOTIF

Main line

PSC3P5x

Single-core 180 MHz Arm® Cortex®-M33, up to 256 KB flash and 64 KB RAM, 12-channel 12 Msps ADC

PSC3M5x

Single-core 180 MHz Arm® Cortex®-M33, up to 256 KB flash and 64 KB RAM, 12-channel 12 Msps ADC, CORDIC, MOTIF

PSOC™ Control C3 features

PSOC™⁠ Control C3

MCUs have extensive features as shown in

Figure 1

. The following is a list of major features. For more information, see the device datasheet, reference manuals, and

References

section.

  • CPU subsystem

    • Arm® Cortex®-M33 running up to

      100 MHz

    • Digital signal processor (DSP), floating-point unit (FPU), memory protection unit (MPU), 16 KB I-cache

    • Two direct memory access (DMA) controllers with 16 channels each

    • Security

      • Platform security architecture level 2 (PSA L2) certified

      • Step-wise authentication of execution images until the control is handed over to the user code

      • Secure execution of code in the execute-only mode for protected routines

      • Image authentication and integrity check

      • TrustZone framework that establishes an isolated device root of trust (RoT) for trust attestation and software management

  • Memory

    • On-chip flash with ECC support

      • Up to 256-KB flash with read while write (RWW) capability, 64 KB ROM for boot code, and bootloader functions

      • Built-in device firmware upgrade (DFU) support in boot ROM via serial interface (UART/I2C/SPI)

    • SRAM with ECC support

      • 64 KB

        full SRAM available in Deep Sleep

        • SRAM data path is protected with a hardware mechanism (ECC) for soft error detection and correction

  • Clocking subsystem

    • 8 MHz IMO with Deep Sleep operation offering ±2% accuracy

    • 48 MHz internal high-frequency oscillator (IHO) offering ±1% accuracy

    • 32 kHz internal low frequency oscillator (ILO) offering ±10% accuracy

    • 4 to 35 MHz external crystal oscillator (ECO) support

    • 32.768 kHz external watch crystal oscillator (WCO) usable for real-time clock (RTC)

    • External clock (EXTCLK): Maximum frequency 80 MHz

    • One frequency lock loop (FLL) with 24-100 MHz output range

    • Two digital phase-locked loops, DPLL#0 and DPLL#1, with 25-250 MHz output range

  • Low power (1.71 V to 3.6 V) operation

    • Six power modes (Active, Sleep, Deep Sleep, Deep Sleep-RAM, Deep Sleep-OFF, and Hibernate) for fine-grained power management

    • Deep Sleep mode current of 11 µA at 3.3-V external supply using an internal voltage regulator with 64-KB SRAM retention, LPComp, and Deep Sleep SCB

    • Hibernate mode current with RTC and LPComp of up to 1000 nA

  • Communication peripherals

    • Serial communication blocks (SCBs)

      • Up to six independent run-time-reconfigurable SCBs; each is software-configurable as I2C, SPI, or UART in master or slave mode

      • One SCB also supports Deep Sleep operation and wake-up from Deep Sleep in I2C slave and SPI slave modes

      • SCB supports single-wire half-duplex mode for UART

    • CAN FD

      • Up to two CAN FD channels with a single instance with operation of up to 8 Mbps

  • High-performance, programmable analog subsystem (HPPASS)

    • Analog-to-digital converter (ADC)

      • One 12-bit,

        6-Msps

        SAR ADC

      • Up to 16 dedicated analog pads, connected to up to 16 parallel sample stages

      • Two additional GPIOs can be used as analog inputs

      • Up to 16 sample/hold (S/H) circuits in SAR ADC connected to pins directly or through AMUX

      • One S/H circuit in SAR ADC is internally connected to analog references and a temperature sensor

      • Configurable input gain of 1, 3, 6, and 12 on all 16 S/H circuits

      • Digital comparator at the output to compare the ADC result against programmed boundary values

      • Digital comparator outputs can be connected to timer/counter pulse-width modulator (TCPWM) (low latency between the modules)

    • Analog comparators

      • Five Active comparators without Deep Sleep functionality, each with a 10-bit DAC to generate the comparator reference

      • Each comparator supports an external reference/threshold through pins

      • Active comparator can be used with the built-in DAC in Hysteresis mode

      • Two additional comparators in LPComp are available in Active/Deep Sleep/Hibernate modes

      • Comparator outputs can be brought to pins for control loop applications

      • Comparator outputs can be connected to TCPWM (low latency between the modules)

      • Logical OR of multiple comparator trigger outputs connected as an input trigger to TCPWM via trigger MUX

  • Real-time control peripherals

    • Coordinate rotation digital computer (CORDIC)

      • Supports all CORDIC operating modes for solving circular (trigonometric), hyperbolic functions, and integrated independent lookup tables to accelerate calculation

    • Timer/counter pulse-width modulator (TCPWM)

      • Sixteen 16-bit TCPWM channels

      • Four 32-bit TCPWM channels

      • Center-aligned, edge, and pseudorandom modes

      • Comparator-based triggering of kill signals

      • Shadow update of duty, period, dead-time, output signal polarity, and dithering (pseudorandom mode)

      • Multichannel control: In a group of eight TCPWM channels, one channel within a group can trigger another channel

      • Ability to logically combine the outputs of multiple channels through Smart I/O

      • Dedicated output triggers mux in a group to allow flexibility to the PWM channel as a trigger and/or gate signals to the HPPASS

      • Hall sensor interface with autonomous BLDC block commutation support

      • Quadrature encoder interface to decode motor speed and rotor position

  • I/O subsystem

    • Programmable GPIO pins

      • Up to

        55

        functional pins (

        39

        digital GPIOs; 2 out of

        39

        GPIOs can be used for analog inputs + 16 dedicated analog-only inputs)

      • Programmable drive modes, strengths, and slew rates

    • Programmable digital

      • Up to

        six

        Smart I/O capable ports (

        22

        I/Os, 56 LUTs) enable Boolean operations on I/O signals

  • Cryptography

    • Cryptography accelerator

      • Hardware acceleration for symmetric (AES-128) and asymmetric cryptographic algorithms (RSA and elliptic curve cryptography (ECC)) supported by vector unit (VU) and hash functions (SHA-256)

      • True random number generator (TRNG) function

Target applications

The versatile, secured, low-power, feature-rich offerings in the

PSOC™ Control C3

make it an ideal choice for a wide variety of end applications. Some of these applications are listed below.

The

ModusToolbox™ software

environment supports

PSOC™ Control C3

application development with a set of tools for configuring the device, setting up peripherals, and complementing your projects with world-class middleware. See the Infineon GitHub repos for board support packages (BSPs) for all kits, libraries for popular functionality like motor control and power stage converter, and a comprehensive array of example applications to get you started.

Figure 2

shows an application-level block diagram for a real-world use case using

PSOC™ Control C3

.

Figure 2.

Application-level block diagram using

PSOC™ Control C3



PSOC™ Control C3

is a highly capable and flexible solution for industrial applications. For example, the real-world use case in the

Figure 2

takes advantage of the following features:

  • TCPWM to drive the gates in the motor inverter and the power factor correction (PFC) circuit

  • ADC in the HPPASS for reading data from analog sensors

  • ADC in the HPPASS for reading the analog feedback, such as voltage and currents from the motor inverter and PFC circuit

  • CORDIC peripheral to do the mathematical operations used in motor control application

  • LPCOMP to compare the analog signals for protection

  • Inbuilt security features for firmware protection

  • Serial communication blocks (SCBs) to interface with external devices like motion sensors

  • Programmable Smart I/O to implement CPU independent simple logical operations on internal/external inputs

  • CAN FD channels to communicate with CAN FD capable peripherals

PSOC™ Control C3 resources​

A wealth of technical resources is available to develop applications with the

PSOC™ Control C3

. These resources are listed below.

  • Overview

    :

    PSOC™ Control C3

    webpage

  • Product selectors

    :

    PSOC™ Control C3

  • Entry line datasheet

    and

    main line datasheet

    describes each device family and provides electrical specifications

  • Application notes

    and

    code examples

    cover a broad range of topics, from basic to advanced level. You can also browse our collection of code examples

  • Reference manuals

    (architecture and register) provide detailed descriptions of the architecture and registers in each device family

  • Development tools

    : Many low-cost kits are available for evaluation, design, and development of different applications using

    PSOC™ Control C3

    s

  • Training videos

    : Video training on our products and tools, including

    PSOC™ Control C3

  • Technical support

    :

    PSOC™ Control C3

    community forum

PSOC™ Control C3 development kits​

Infineon provides a wide variety of hardware development kits in various form factors and features to enable easy and rapid evaluation and prototyping of

PSOC™⁠ Control C3

based applications.

The following table lists the

PSOC™⁠ Control C3

kits with various features.

ModusToolbox™ software is the software development platform for creating embedded applications using the development kits.

Table 2.

Development kits

Kit MPN

Product

Kit name

BSP GitHub repo

KIT_PSC3M5_EVK

PSC3M5xD

PSOC™⁠ Control C3M5

Evaluation Kit

BSP

KIT_PSC3M5_MC1

PSC3M5xD

PSOC™⁠ Control C3M5

Complete System Motor Control Kit

BSP

KIT_PSC3M5_CC2

PSC3M5xD

PSOC™⁠ Control C3M5

Motor Drive Control Card

BSP

KIT_PSC3M5_DP1

PSC3M5xD

PSOC™⁠ Control C3M5

Complete System Dual Buck Evaluation Kit

BSP

KIT_PSC3M5_CC1

PSC3M5xD

PSOC™⁠ Control C3M5

Digital Power Control Card

BSP

For the complete list of kits for the

PSOC™ Control C3

along with the shield modules, see the

PSOC™ Control C3

webpage.

PSOC™ Control C3 ecosystem for firmware/application development​

Infineon provides the ModusToolbox™ software for firmware/application development on

PSOC™⁠ Control C3

MCUs. ModusToolbox™ Software is a modern, extensible development ecosystem supporting a wide range of Infineon microcontroller devices, including PSOC™ Arm® Cortex® Microcontrollers, TRAVEO™ T2G Arm® Cortex® Microcontroller, XMC™ Industrial Microcontrollers, AIROC™ Wi-Fi devices, AIROC™ Bluetooth® devices, and USB-C Power Delivery Microcontrollers. This software includes configuration tools, low-level drivers, middleware libraries, and other packages that enable you to create MCU and wireless applications. All tools run on Windows, macOS, and Linux. ModusToolbox™ includes an Eclipse IDE, which provides an integrated flow with all the ModusToolbox™ tools. Other IDEs such as Visual Studio Code, IAR Embedded Workbench and Arm® MDK (μVision) are also supported.

ModusToolbox™ software supports stand-alone device and middleware configurators. Use the configurators to set the configuration of different blocks in the device and generate code that can be used in firmware development.

Libraries and enablement software are available at the

GitHub

site.

ModusToolbox™ tools and resources can also be used on the command line. See the build system chapter in the

ModusToolbox™ tools package user guide

for detailed documentation.

Choosing an IDE

ModusToolbox™ software, the latest-generation toolset, is supported across Windows, Linux, and macOS platforms. ModusToolbox™ software supports 3rd-party IDEs, including the Eclipse IDE, Visual Studio Code, Arm® MDK (μVision), and IAR Embedded Workbench. The tools package includes an implementation for all the supported IDEs. The tools support all

PSOC™ Control C3

s. The associated BSP and library configurators also work on all three host operating systems.

Figure 3.

ModusToolbox™ environment



ModusToolbox help

The ModusToolbox™ ecosystem provides documentation and training. Launch the Eclipse IDE for ModusToolbox™ software and navigate to the following Help menu items:

Choose

Help > ModusToolbox™ General Documentation

:

  • ModusToolbox™ Documentation Index

    : Provides brief descriptions and links to various types of documentation included as part of the ModusToolbox™ software

  • ModusToolbox™ Installation Guide

    : Provides instructions for installing the ModusToolbox™ software

  • ModusToolbox™ User Guide

    : This guide primarily covers the ModusToolbox™ aspects of building, programming, and debugging applications. Additionally, it covers various aspects of the tools installed along with the IDE

  • ModusToolbox™ Training Material

    : Links to the training material available at

    https://github.com/Infineon/training-modustoolbox

  • Release Notes:

    Describes the features and known limitations for the ModusToolbox™ software, provided as part of the ModusToolbox™ tools package included with the installer

For documentation on Eclipse IDE for ModusToolbox™, choose

Help > Eclipse IDE for ModusToolbox™ documentation

.

  • User Guide

    : Provides descriptions about creating applications as well as building, programming, and debugging them using Eclipse IDE

  • Eclipse IDE Survival Guide:

    This is a link to a forum with answers for questions about how to get common tasks done

Getting started with PSOC™ Control C3 design​

This section

does

the following:

  • Demonstrate how to build a simple

    PSOC™ Control C3

    -based design and program

    into

    the development kit

  • Makes it easy to learn

    PSOC™ Control C3

    design techniques and how to use the ModusToolbox™ software with different IDEs.

Prerequisites

Before you get started

with the application development instructions

, make sure that you have the appropriate development kit for your

PSOC™ Control C3

product line and have installed the required software. You also need internet to access the GitHub repositories during project creation.

About the design

This design uses the

PSOC™ Control C3

to execute two tasks: UART communication and LED control.

After device reset, the CPU uses the UART to print a "Hello World" message to the serial port stream and starts blinking the user LED on the kit. When you press the 'Enter' key on the serial console, the blinking of the LED is paused or resumed.

Create a new application

This section takes you on a step-by-step guided tour of the new application creation process. It uses the

Empty App

starter application and manually adds the functionality from the

Hello World

starter application.

As mentioned in section

Choosing an IDE

, ModusToolbox™ software supports the following third-party IDEs:

  1. Eclipse IDE

  2. Visual Studio Code (VS Code)

  3. IAR Embedded Workbench

  4. Keil µvision

The following sections provide details on how to create a new application on different IDEs.

Eclipse IDE for ModusToolbox

If you are familiar with developing projects with ModusToolbox™ software, you can use the

Hello World

starter application directly. It is a complete design, with all the firmware written for the supported kits. You can walk through the instructions and observe how the steps are implemented in the code example.

If you start from scratch and follow all the instructions in this application note, you can use the

Hello World

code example as a reference while following the instructions.

Launch the

Dashboard 3.3

application to get started.

Note:

Dashboard 3.3

application needs access to the internet to successfully clone the starter application onto your machine.

The

Dashboard 3.3

application helps you get started using the various tools with easy access to documentation and training material, a simple path for creating applications and creating and editing BSPs.

  1. Open the Dashboard 3.3 application.

    To open the

    Dashboard 3.3

    application, do one of these:

    • Windows:

      Navigate to

      [ModusToolbox installation path]/tools_3.2/dashboard/dashboard.exe

      [ModusToolbox installation path]/tools_3.3/dashboard/dashboard.exe

      or you can also select the "

      dashboard

      ModusToolbox™ Dashboard 3.3

      " item from the Windows Start menu.

    • Linux:

      [ModusToolbox installation path]/tools_3.2/dashboard and run the executable

      [ModusToolbox installation path]/tools_3.3/dashboard and run the executable

    • macOS:

      Run the "dashboard" app

  2. On the Dashboard 3.3 window, in the right pane, in the Target IDE drop-down list, select Eclipse IDE for ModusToolbox™, and click Launch Eclipse IDE for ModusToolbox™.

    Figure 4.

    Dashboard 3.3

    application





  3. Select a new workspace.

    At launch, Eclipse IDE for ModusToolbox™ displays a dialog to choose a directory for use as the workspace directory. The workspace directory is used to store workspace preferences and development artifacts. You can choose an existing empty directory by clicking the

    Browse

    button, as shown in the following figure. Alternatively, you can type in a directory name to be used as the workspace directory along with the complete path, and the IDE will create the directory for you.

    Figure 5.

    Select a directory as the workspace





  4. Create a new ModusToolbox™ application.
    1. Click New Application in the Start group of the Quick Panel.

    2. Alternatively, you can choose File>New>ModusToolbox™ Application, as Figure 6 shows. Displays the Eclipse IDE for ModusToolbox™ Application window.

    Figure 6.

    Create a New ModusToolbox™ Application



  5. Select a target PSOC™⁠ Control C3M5Evaluation Kit.

    ModusToolbox™ speeds up the development process by providing BSPs that set various workspace/project options for the specified development kit in the new application dialog.

    1. In the Choose Board Support Package (BSP)dialog, choose the Kit Name that you have. The steps that are followed use KIT_PSC3M5_EVK, as shown in Figure 7.

    2. Click Next.

      Figure 7.

      Choose target hardware



    3. In the Select Application dialog, select Empty App starter application, as shown in the following figure.

    4. In the Name field, type in a name for the application, such as Hello_World. You can choose to leave the default name if you prefer.

      Note:

      Try to use a short name without spaces in between.

    5. Click Create to create the application, as shown in the following figure, wait for the Project Creator to automatically close once the project is successfully created.

    Figure 8.

    Choose starter application



You have successfully created a new ModusToolbox™ application for a

PSOC™ Control C3

.

The BSP uses

PSC3M5FDS2AFQ1

as the default device that is mounted on the

PSOC™⁠ Control C3M5

Evaluation Kit.

If you are using custom hardware based on the

PSOC™ Control C3

or a different

PSOC™ Control C3

part number, see the "Creating your Own BSP" section in the

ModusToolbox™ user guide

.

View and modify the design

Figure 9

shows the ModusToolbox™ project explorer interface displaying the structure of the application project.

PSOC™ Control C3

has one CM33 core. This application note shows the firmware development using the CM33 core with ModusToolbox™.

Figure 9.

Project Explorer view



A project folder consists of various subfolders – each denoting a specific aspect of the project.

  1. The files provided by the BSP are in the bsps folder and are listed under TARGET_<bsp name> subfolders. All the input files for the device and peripheral configurators are in the config folder inside the BSP. The GeneratedSource folder in the BSP contains the files that are generated by the configurators and are prefixed with cycfg_. These files contain the design configuration as defined by the BSP. From ModusToolbox™ 3.x or later, you can directly customize configurator files of BSP for your application rather than overriding the default design configurator files with custom design configurator files since BSPs are completely owned by the application.

    The BSP folder also contains the linker scripts and the start-up code for the

    PSOC™ Control C3

    used on the board.

  2. The build folder contains all the artifacts resulting from a build of the project. The output files are organized by target BSPs.

  3. The

    deps

    folder contains

    .mtb

    files, which provide the locations from which ModusToolbox™ pulls the libraries that are directly referenced by the application. These files typically each contain the GitHub location of a library. The

    .mtb

    files also contain a git Commit Hash or Tag that tells which version of the library is to be fetched and a path as to where the library should be stored locally.

    For example, here, retarget-io.mtb points to

    mtb://retarget-io#latest-v1.X#$$ASSET_REPO$$/retarget-io/latest-v1.X

    . The variable $$ASSET_REPO$$ points to the root of the shared location which defaults to

    mtb_shared

    . If the library must be local to the application instead of shared, use $$LOCAL$$ instead of $$ASSET_REPO$$.

  4. The libs folder also contains .mtb files. In this case, they point to libraries that are included indirectly as a dependency of a BSP or another library. For each indirect dependency, the Library Manager places a .mtb file in this folder. These files have been populated based on the targets available in deps folder.

    For example, using BSP

    KIT_XMC72_EVK

    populates

    libs

    folder with the following

    .mtb

    files:

    cmsis.mtb

    ,

    core-lib.mtb

    ,

    core-make.mtb

    ,

    mtb-hal-cat1.mtb

    ,

    mtb-pdl-cat1.mtb

    ,

    cat1cm0p.mtb

    ,

    recipe-make-cat1a.mtb

    .

    For example, using BSP KIT_PSC3M5_EVK populates the libs folder with the following

    .mtb

    files:

    cmsis.mtb

    ,

    core-lib.mtb

    ,

    core-make.mtb

    ,

    deivce-db.mtb

    ,

    mtb-hal-psc3.mtb

    ,

    mtb-pdl-cat1.mtb

    ,

    receipe-make-cat1b

    .

    The

    libs

    folder contains the file mtb.mk, which stores the relative paths of all the libraries required by the application. The build system uses this file to find all the libraries required by the application.

    Everything in the libs folder is generated by the Library Manager so you should not manually edit anything in that folder.

  5. An application contains a Makefile which is at the application's root folder. This file contains the set of directives that the make tool uses to compile and link the application project. There can be more than one project in an application. In that case there is a Makefile at the application level and one inside each project.

  6. By default, when creating a new application or adding a library to an existing application and specifying it as shared, all libraries are placed in an mtb_shared directory adjacent to the application directories.

    The

    mtb_shared

    folder is shared between different applications within a workspace. Different applications may use different versions of shared libraries if necessary.

Open the Device Configurator

BSP configurator files are in the

bsps/TARGET_<BSP-name>/config

folder.

For example, click

Click

<Application-name>

from

Project Explorer

then click

Device Configurator

link in the

Quick Panel

to open the file

design.modus

in the

Device Configurator

as shown in the following figure. You can also open other configuration files in their respective configurators or click the corresponding links in the

Quick Panel

.

Figure 10.

Device Configurator

-UART configuration



The

Device Configurator

provides a set of

Resources Categories

tabs. Here you can choose between different resources available in the device such as peripherals, pins, and clocks from the

List of Resources

.

You can choose how a resource behaves by choosing a

Personality

for the resource. For example, a

serial communication block (SCB)

resource can have

EZI2C

,

I2C

,

SPI

, or

UART

personalities. The

Alias

Name(s)

is your name for the resource, which is used in firmware development. One or more aliases can be specified by using a comma to separate them (with no spaces).

The

Parameters

pane is where you enter the configuration parameters for each enabled resource and the selected personality. The

Code Preview

pane shows the configuration code generated per the configuration parameters selected. This code is populated in the

cycfg_

files in the

GeneratedSource

folder. The Parameters pane and Code Preview pane may be displayed as tabs instead of separate windows but the contents will be the same.

Any errors, warnings, and information messages arising out of the configuration are displayed in the

Notices

pane.

Configuring the peripheral is required for both PDL and HAL based implementations to work.

Figure 10

also shows that the SCB 3 is enabled and configured. As the SCB 3 is used for communicating with the user through the debug UART terminal, replicate the same configuration in your setup for the Hello World application.

Figure 11.

Device Configurator - Timer configuration



Figure 11

shows that the timer

TCPWM[0] Group[0] 16 bit Counter 0

is configured in

Timer - Counter

mode. This configuration is used in the code to generate interrupts for LED toggling. Make the same configuration in your setup. To make the LED toggle every second, the input clock frequency is set to 1 MHz. Ensure that this configuration is also made in your setup.

In the Hello World application, you are using a GPIO connected to the LED on the EVK. To use the GPIO, enable the pin P8.5 in the

Pins

tab in the resource categories pane. Also, make sure that the

Drive Mode

is set to

‘Strong Drive. Input buffer off’

.

As the Hello World application that you are now developing, is going to be a secure application, ensure that the

‘Secure attribute’

of all pins selected is set as

‘Secure access(0)’

.

The application project contains source files that help you create an application for the

CM33

core (for example,

main.c

). This

C

file is compiled and linked with the

CM33

image as part of the normal build process.

At this point in the development process, the required middleware is ready to be added to the design. The only middleware required for the Hello World application is the

retarget-io

library.

Add retarget-io middleware

In this section, you will add the

retarget-io

middleware to redirect standard input and output streams to the UART configured by the BSP. The initialization of the middleware will be done in

main.c

file.

  1. In the

    Quick Panel

    , click the

    Library Manager

    link.

  2. In the subsequent dialog, click

    Add Libraries

    .

  3. Under

    Peripherals

    , select and enable

    retarget-io

    .

  4. Click

    OK

    and then

    Update

    .

The files necessary to use the

retarget-io

middleware are added in the

mtb_shared > retarget_io

folder, and the

.mtb

file is added to the

deps

folder, as shown in the following figure.

Figure 12.

Add the retarget-io middleware



Write firmware

At this point in the development process, you have created an application with the assistance of an application template

, configured the peripherals using the device configurator,

and modified it to add the

retarget-io

middleware. In this section, you will write the firmware that implements the design functionality.

If you are working from scratch using the

Empty

PSOC™⁠ Control C3

starter application,

you can copy the code snippet provided in this section to the

main.c

file of the application project.

If you are using the

Hello World

code example, all the required files are already in the application.

Firmware flow

Examine the code in the

main.c

file of the application.

Figure 13

shows the firmware flowchart.

After reset, resource initialization for this example is performed by the

CM33

CPU. It configures the system clocks, pins, clock to peripheral connections, and other platform resources.

Then

the clocks and system resources are initialized by the BSP initialization function. The retarget-io middleware is configured to use the debug UART, and the user LED is initialized. The debug UART prints a “Hello World!” message on the terminal emulator – the onboard KitProg3 acts as the USB-to-UART bridge to create the virtual COM port. A timer object is configured to generate an interrupt every 1000 milliseconds. At each timer interrupt, the

CM33

CPU toggles the LED state on the kit.

The firmware is designed to accept the 'Enter' key as an input, and on every press of the 'Enter' key, the firmware starts or stops the blinking of the LED.

Note that this application code uses BSP/HAL/middleware functions to execute the intended functionality.

cybsp_init()

– This BSP function initializes all the system resources of the device, including but not limited to the system clocks and power regulators.

Cy_SCB_UART_Init()

– This function initializes the debug UART.

mtb_hal_uart_setup()

and

cy_retarget_io_init()

– These functions set up the HAL UART and redirect the input/output stream to the debug UART.

mtb_hal_uart_get()

– The while loop calls this function to detect the pressing of the 'Enter Key', which start or stop the LED toggling.

timer_init()

– This function wraps a set of timer function calls to instantiate and configure a hardware timer. It also sets up a callback for the timer interrupt.

isr_timer()

– This is the timer ISR getting executed in every 1000 milliseconds. This function sets a flag for toggling the LED.

The flag set by the timer ISR is checked in the main loop, and the LED is toggled based on it.

Copy the following code snippet to the

main.c

file of your application project.

Code listing 1:

main.c

file

/*******************************************************************************
* Header Files
*******************************************************************************/
#include "cy_pdl.h"
#include "cybsp.h"
#include "cy_retarget_io.h"
#include "mtb_hal.h"

/*******************************************************************************
* Macros
*******************************************************************************/

/*******************************************************************************
* Global Variables
*******************************************************************************/
const cy_stc_sysint_t intrCfg1 =
{
.intrSrc = TCPWM_COUNTER_IRQ,
.intrPriority = 7u
};

volatile bool timer_interrupt_flag = false;
bool led_blink_active_flag = true;

/* Variable for storing character read from terminal */
uint8_t uart_read_value;

/* For the Retarget -IO (Debug UART) usage */
static cy_stc_scb_uart_context_t DEBUG_UART_context;
static mtb_hal_uart_t DEBUG_UART_hal_obj;

/*******************************************************************************
* Function Prototypes
*******************************************************************************/
void timer_init(void);
void isr_timer(void);

/*******************************************************************************
* Function Definitions
*******************************************************************************/

/*******************************************************************************
* Function Name: main
********************************************************************************
* Summary:
* This is the main function. It sets up a timer to trigger a periodic interrupt.
* The main while loop checks for the status of a flag set by the interrupt and
* toggles an LED at 1Hz to create an LED blinky. Will be achieving the 1Hz Blink
* rate. The while loop also checks whether the 'Enter' key was pressed and
* stops/restarts LED blinking.
*
* Parameters:
* void
*
* Return:
* int
*
*******************************************************************************/
int main(void)
{
cy_rslt_t result;

/* Initialize the device and board peripherals */
result = cybsp_init();

/* Board init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(0);
}

/* Enable global interrupts */
__enable_irq();

/* Debug UART init */
result = (cy_rslt_t)Cy_SCB_UART_Init(DEBUG_UART_HW, &DEBUG_UART_config, &DEBUG_UART_context);

/* UART init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(0);
}

Cy_SCB_UART_Enable(DEBUG_UART_HW);

/* Setup the HAL UART */
result = mtb_hal_uart_setup(&DEBUG_UART_hal_obj, &DEBUG_UART_hal_config, &DEBUG_UART_context, NULL);

/* HAL UART init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(0);
}

result = cy_retarget_io_init(&DEBUG_UART_hal_obj);

/* HAL retarget_io init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(0);
}

/* \x1b[2J\x1b[;H - ANSI ESC sequence for clear screen */
printf("\x1b[2J\x1b[;H");

printf("****************** "
"PDL: Hello World! Example "
"****************** \r\n\n");

printf("Hello World!!!\r\n\n");
printf("For more projects, "
"visit our code examples repositories:\r\n\n");

printf("https://github.com/Infineon/"
"Code-Examples-for-ModusToolbox-Software\r\n\n");

/* Initialize timer to toggle the LED */
timer_init();

printf("Press 'Enter' key to pause or "
"resume blinking the user LED \r\n\r\n");

for (;;)
{
/* Check if 'Enter' key was pressed */
if (mtb_hal_uart_get(&DEBUG_UART_hal_obj, &uart_read_value, 1) == CY_RSLT_SUCCESS)
{

if (uart_read_value == '\r')
{
/* Pause LED blinking by stopping the timer */
if (led_blink_active_flag)
{
Cy_TCPWM_TriggerStopOrKill_Single(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM);

printf("LED blinking paused \r\n");
}
else /* Resume LED blinking by starting the timer */
{
Cy_TCPWM_TriggerStart_Single(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM);

printf("LED blinking resumed\r\n");
}

/* Move cursor to previous line */
printf("\x1b[1F");

led_blink_active_flag ^= 1;
}
}

/* Check if timer elapsed (interrupt fired) and toggle the LED */
if (timer_interrupt_flag)
{
/* Clear the flag */
timer_interrupt_flag = false;

/* Invert the USER LED state */
Cy_GPIO_Inv(CYBSP_USER_LED_PORT, CYBSP_USER_LED_PIN);
}
}
}

/*******************************************************************************
* Function Name: timer_init
********************************************************************************
* Summary:
* This function creates and configures a Timer object. The timer ticks
* continuously and produces a periodic interrupt on every terminal count
* event. The period is defined by the 'period' and 'compare_value' of the
* timer configuration structure 'led_blink_timer_cfg'. Without any changes,
* this application is designed to produce an interrupt every 1 second.
*
* Parameters:
* none
*
*******************************************************************************/
void timer_init(void)
{
/* Enable interrupts */
__enable_irq();

/*TCPWM Counter Mode initial*/
if (CY_TCPWM_SUCCESS != Cy_TCPWM_Counter_Init(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM, &TCPWM_COUNTER_config))
{
CY_ASSERT(0);
}

/* Enable the initialized counter */
Cy_TCPWM_Counter_Enable(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM);

/* Configure GPIO interrupt */
Cy_TCPWM_SetInterruptMask(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM, CY_GPIO_INTR_EN_MASK);

/* Configure CM4+ CPU GPIO interrupt vector for Port 0 */
Cy_SysInt_Init(&intrCfg1, isr_timer);
NVIC_EnableIRQ(TCPWM_COUNTER_IRQ);

/* Start the counter */
Cy_TCPWM_TriggerStart_Single(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM);
}

/*******************************************************************************
* Function Name: isr_timer
********************************************************************************
* Summary:
* This is the interrupt handler function for the timer interrupt.
*
* Parameters:
* none
*
*******************************************************************************/
void isr_timer(void)
{

uint32_t interrupts = Cy_TCPWM_GetInterruptStatusMasked(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM);

/* Clear the interrupt */
Cy_TCPWM_ClearInterrupt(TCPWM_COUNTER_HW, TCPWM_COUNTER_NUM, interrupts);

if (0UL != (CY_TCPWM_INT_ON_TC & interrupts))
{
/* Set the interrupt flag and process it from the main while(1) loop */
timer_interrupt_flag = true;
}
}
/* [] END OF FILE */

Figure 13.

Firmware flowchart



This completes the summary of how the firmware works in the code example. Feel free to explore the source files for a deeper understanding.

Build the application

This section shows how to build the application.

  1. Select the application project in the Project Explorer view.

  2. Click Build Project shortcut under the Hello_World group in the Quick Panel.

    It selects the build configuration from the Makefile and compiles/links all projects that constitute the application. By default, Debug configurations are selected.

  3. The Console view lists the results of the build operation, as Figure 14shows.

Figure 14.

Build the application



If you encounter errors, revisit earlier steps to ensure that you completed all the required tasks.

Note:

You can also use the command-line interface (CLI) to build the application. See the

Build system

section in the

ModusToolbox™ tools package user guide

. This document is located in the

/docs_<version>/

folder in the ModusToolbox™ installation.

Program the device

This section shows how to program the

PSOC™ Control C3

.

ModusToolbox™ software uses the

OpenOCD

protocol to program and debug applications on

PSOC™ Control C3

s

on the evaluation kit

.

As the evaluation kit is

with a built-in programmer, connect the board to your computer using the

provided

USB cable.

If you are developing on your own hardware, you may need a hardware programmer/debugger, for example, a

J-Link,

or

ULinkpro

, or

MiniProg

.

  1. Program the application.

    1. Connect to the board and perform the following.

    2. Select the application project and click on the Hello_World Program (KitProg3_MiniProg4) shortcut under the Launches group in the Quick Panel, as Figure 15 shows. The IDE will select and run the appropriate run configuration. Note that this step will also perform a build if any files have been modified since the last build.

      Figure 15.

      Programming an application to a device



The

Console

view lists the results of the programming operation, as

Figure 16

shows.

Figure 16.

Console – programming results



Test your design

This section describes how to test your design.

Follow these steps to observe the output of your design. This note uses Tera Term as the UART terminal emulator to view the results, but you can use any terminal of your choice to view the output.

  1. Select the serial port

    Launch Tera Term and select the USB-UART COM port as

    Figure 17

    shows. Note that your COM port number may be different.

    Figure 17.

    Selecting the KitProg3 COM port in Tera Term



  2. Set the baud rate

    Set the baud rate to 115200 under

    Setup > Serial port

    as

    Figure 18

    shows.

    Figure 18.

    Configuring the baud rate in Tera Term



  3. Reset the device

    Press the reset switch (

    SW1

    ) on the kit.

    The message shown in

    Figure 19

    appears on the terminal

    . The user LED on the kit will start blinking.

    Figure 19.

    Printed UART message



  4. Pause/resume LED blinking functionality

    Press the

    Enter

    key to pause/resume blinking the LED. When the LED blinking is paused, a corresponding message will be displayed on the terminal as shown in

    Figure 20

    .

    Figure 20.

    Printed UART message



Debugging the application using KitProg3/MiniProg4

PSOC™ Control C3 kits come with either the KitProg3 or J-Link onboard programmer/debugger. See the

KitProg3 user guide

for details of KitProg3 or see the

J-Link

user guide for the details of J-Link.

The Eclipse IDE contains several launch configurations that control various settings for programming the devices and launching the debugger. Depending on the kit and the type of applications you are using, there are various launch configurations available. One such configuration is the KitProg3/MiniProg4 launch configuration. Refer to the "PSOC™ MCU programming/debugging" section in the

Eclipse IDE for ModusToolbox™ user guide

for more details on the launch configurations.

When an application is created, the tool generates the launch configurations for KitProg3_MiniProg4

or J-link

under

Launches

in the

Quick Panel

. For the PSOC™ Control C3 Evaluation Kit, it will generate launch configurations for KitProg3

, as shown in the following figure.

Figure 21.

KitProg3/MiniProg4 launch configuration



Connect the device to the host machine and click on the

Hello_World Debug (KitProg3_MiniProg4)

launch to start debugging, as shown in

Figure 21

. Once the debugging starts, the execution halts at the main() function, and the user can start debugging from the start of main(), as shown in the following figure.

Figure 22.

Debug main()



Summary​

This application note explored the

PSOC™ Control C3

device architecture and the associated development tools.

PSOC™ Control C3

is a truly programmable embedded system-on-chip with configurable analog and digital peripheral functions, memory, and a powerful processor on a chip. The integrated features and low-power modes make

PSOC™ Control C3

an ideal choice for industrial drives, smart appliances, power stage converters, and other related applications.

References​

For a complete and up-to-date list of

PSOC™ Control C3

code examples, visit

Infineon GitHub page

. For additional

PSOC™ Control C3

-related documents, visit

PSOC™ Control C3

product webpage.

Table 3.

General and system-level application notes

Document

Document name

AN239527

PSOC™ Control C3

hardware design guide

Table 4.Other documents related to PSOC™ Control C3

Document

Document name

Motor control and power conversion

AN239646

PMSM FOC using

PSOC™ Control C3

AN239961

Synchronous buck converter with

PSOC™ Control C3

Kit user guides

002-39385

KIT_PSC3M5_EVK

PSOC™⁠ Control C3M5

Evaluation Kit guide

002-39715

KIT_PSC3M5_CC1

PSOC™⁠ Control C3M5

Digital Power Control Card user guide

002-39714

KIT_PSC3M5_DP1

PSOC™⁠ Control C3M5

Complete System Dual Buck Evaluation Kit user guide

002-39971

KIT_PSC3M5_CC2 PSOC™ Control C3 Motor Control Evaluation Kit guide

002-40071

KIT_PSC3M5_MC1 PSOC™ Control C3 Motor Control Evaluation Kit guide

Security

AN240106

Getting started with PSOC™ Control C3 security

Table 5.

ModusToolbox™

ModusToolbox™ tools package installation guide

ModusToolbox™ tools package release notes

ModusToolbox™ tools package quick start guide

ModusToolbox™ tools package user guide

Eclipse IDE for ModusToolbox™ user guide

Visual Studio Code for ModusToolbox™ user guide

Keil µVision for ModusToolbox™ user guide

IAR Embedded Workbench for ModusToolbox™ user guide

Glossary​

This section lists the most commonly used terms that you might encounter while working with

PSOC™

family of devices.

  • Board support package (BSP)

    : A BSP is the layer of firmware containing board-specific drivers and other functions. The board support package is a set of libraries that provide firmware APIs to initialize the board and provide access to board level peripherals.

  • KitProg

    : The KitProg is an onboard programmer/debugger with USB-I2C and USB-to-UART bridge functionality. The KitProg is integrated onto most PSOC™ development kits.

  • MiniProg3

    /

    MiniProg4

    : Programming hardware for development that is used to program

    PSOC™

    devices on your custom board or

    PSOC™

    development kits that do not support a built-in programmer.

  • Personality

    : A personality expresses the configurability of a resource for a functionality. For example, the SCB resource can be configured to be an UART, SPI, or I2C personalities.

  • Middleware

    : Middleware is a set of firmware modules that provide specific capabilities to an application. Some middleware may provide network protocols (e.g., CAN FD), and some may provide high-level software interfaces to device features (e.g., TCPWM, HPPASS).

  • ModusToolbox™

    : An Eclipse-based embedded design platform for embedded systems designers that provides a single, coherent, and familiar design experience, combining the industry’s most deployed Wi-Fi and Bluetooth® technologies, and the lowest power, most flexible MCUs with best-in-class sensing.

  • Peripheral driver library (PDL)

    : The PDL simplifies software development for the

    PSOC™ Control C3

    architecture. The PDL reduces the need to understand register usage and bit structures, so easing software development for the extensive set of peripherals available.

Revision history​

Document revision

Date

Description of changes

**

2024-05-22

Initial release

*A

2024-12-03

Updated the content structure

Updated figures and sections

Added new sections

Trademarks​

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc., and any use of such marks by Infineon is under license.