Skip to main content

AN220222 Low-power mode procedure in TRAVEO™ T2G family

PDF File

About this document​

Scope and purpose​

This application note describes the features of low-power modes in TRAVEO™ T2G family MCUs and explains how to enter low-power modes and return to active mode.

Associated part family​

TRAVEO™ T2G family CYT2/CYT3/CYT4 series

Introduction​

This application note describes low-power modes in TRAVEO™ T2G family MCU. The series includes Arm® Cortex® CPUs, CAN FD, memory, and analog and digital peripheral functions in a single chip.

The CYT2 series has one Arm® Cortex®-M4F-based CPU (CM4) and Cortex®-M0+-based CPU (CM0+). The CYT4 series has two Arm® Cortex®-M7-based CPUs (CM7) and CM0+, and the CYT3 series has one CM7 and CM0+.

TRAVEO™ T2G family MCUs have several different power modes. These modes are intended to minimize the average power consumption in an application.

This application note explains the features of power modes and how to set up the power mode transition.

To understand the described functionality and terminology used in this application note, see the “Device power modes” chapter of the architecture technical reference manual (TRM).

Power modes of TRAVEO™ T2G family​

TRAVEO™ T2G family MCUs have the following power modes:

  • Active mode: All peripherals are available.
  • Sleep mode: All peripherals except the CPU are available.
  • DeepSleep mode: Only low-frequency peripherals are available.
  • Hibernate mode: Device and I/O states are frozen.

Figure 1 shows the relationship between power modes and the power supply current.

Figure 1. Power modes and power supply current​

Figure 1

Note: Figure 1 is only an indication of the degree of power supply currents for each mode. Actual current values depend on the clock configuration and peripheral setting in each mode. For more details on power supply current characteristics, see the datasheet.

Power consumption is reduced in the order of Active, Sleep, DeepSleep, and Hibernate. Each power mode optimizes power consumption for user applications.

Table 1 summarizes the states of each power mode and the entry and wakeup conditions. For more details on power modes, see the architecture TRM.

Table 1. TRAVEO™ T2G power modes​

Power mode

Description

Entry condition

Wakeup source

Wakeup action

Active

Primary mode of operation; all peripherals are available (programmable).

Wake up from Sleep/DeepSleep modes, Hibernate reset, or any other reset.

Not applicable

Not applicable

Sleep

CPU is in Sleep mode; all other peripherals are available.

Interrupt

DeepSleep

All high-frequency clocks and peripherals are turned off. Low-frequency clock (32 kHz) and low-power analog and digital peripherals are available for operation and as wakeup sources. SRAM can be retained (configurable).

Register write from Active modes or debugger session ends.

GPIO interrupt, event generators, SCB, watchdog timer, and RTC alarms1 and debugger

Interrupt or debug

Hibernate

GPIO states are frozen. Almost all peripherals and clocks in the device are turned off. Device resets on wakeup.

Register write from Active mode.

WAKEUP pin and RTC alarms

Hibernate reset

TRAVEO™ T2G family MCUs have the following features:

  • Software can use power modes to optimize power consumption in an application
  • Low-power DeepSleep mode with support for multiple wakeup sources and configurable amount of SRAM retention
  • Ultra-low-power Hibernate mode with wakeup from I/O and RTC alarms

The power consumption in different power modes is controlled by using the following methods:

  • Enabling and disabling clocks to peripherals
  • Powering ON/OFF clock sources
  • Powering ON/OFF peripherals and parts inside the MCUs

1 RTC (along with WCO) is supplied with VDDD and is available irrespective of the device power mode. RTC alarms can wake up the device from any power mode.

Power modes transition​

This section describes how to use low-power mode procedure using the sample driver library (SDL). The code snippets in this application note are part of SDL. See Other references for the SDL.

SDL has a configuration part and a driver part. The configuration part mainly configures the parameter values for the desired operation. The driver part configures each register based on the parameter values in the configuration part. You can configure the configuration part according to your system.

In this example, CYT2B7 series is used.

Entering power modes​

Figure 2 shows various states the device can be in along with possible power mode transition paths. The transitions are described in detail later in this application note.

Figure 2. Power mode transitions​

Figure 2

RESET/OFF state​

  • OFF state:
    • Represents the state with no power applied
    • Go to RESET, when powered up above Power-On reset level (POR event)
  • RESET state:
    • Detected reset event: POR, External reset (XRES), or Internal reset
    • Go to Active mode after reset sequence completion
    • IMO is started
    • Device will enter RESET state upon assertion of XRES in any of the power modes

Entering low-power mode​

Table 2 shows how to enter low-power mode, and the actions in low-power modes.

Table 2. Low-power mode transitions​

Initial state

Final state

Trigger

Hardware actions

Active

Sleep

Firmware action

  1. Clear the SLEEPDEEP bit [2] of the SCR register for all CPUs (For CYT2, CPUs are CM4 and CM0+. For CYT3/CYT4, CPUs are CM7 and CM0+).
  2. Optionally, set the SLEEPONEXIT bit [1] of the SCR register, if the CPU runs only on interrupts. When this bit is set, the CPU will not return to application code after the WFI/WFE instruction is executed. The CPU will wake up on any enabled interrupt or event and will enter Sleep/DeepSleep mode as soon as it exits the interrupt or services the event.
  3. Optionally, set the SEVONPEND bit [4] of the SCR register if the application needs to wake up the CPU from any pending interrupt. If this bit is set, any interrupt that enters a pending state will wake up the CPU.
  4. Execute WFI/WFE instruction on all of CPUs. (For CYT2, CPUs are CM4 and CM0+. For CYT3/CYT4, CPUs are CM7 and CM0+).
  1. CPU clocks are gated OFF.
  2. CPU waits for an interrupt or event to wake it up.

Active

DeepSleep

Firmware action

Perform these steps to enter DeepSleep mode (LPM_READY bit [5] of the PWR_CTL register should read ‘1’ before performing these steps):

  1. Set the SLEEPDEEP bit [2] of the SCR register for all CPUs (For CYT2, CPUs are CM4 and CM0+. For CYT3/CYT4, CPUs are CM7 and CM0+).
  2. Optionally, set the SLEEPONEXIT bit [1] of the SCR register, if the CPU runs only on interrupts. When this bit is set, the CPU will not return to application code after the WFI/WFE instruction is executed. The CPU will wake up on any enabled interrupt or event and will enter Sleep/DeepSleep mode as soon as it exits the interrupt or services the event.
  3. Optionally, set the SEVONPEND bit [4] of the SCR register if the application needs to wake up the CPU from any pending interrupt. If this bit is set, any interrupt that enters a pending state will wake up the CPU.
  4. Execute WFI/WFE instruction on all of CPUs (For CYT2, CPUs are CM4 and CM0+. For CYT3/CYT4, CPUs are CM7 and CM0+).

Note: Executing the above sequence before the low-power mode is ready (LPM_READY==1) will transition first to Sleep mode. The device state will automatically move to DeepSleep state once LPM_READY bit is set.

Note: Make sure that any write transfer made before executing the WFI instruction is followed by the read access to the same memory location. This ensures that the write operation is successful.

  1. CPU enters low-power mode.
  2. High-frequency clocks are shut down.
  3. I/O cells will be frozen automatically.
  4. Retention is enabled and non-retention logic is reset.
  5. Active regulator is disabled and DeepSleep regulator takes over.

Active

Hibernate

Firmware action

  1. Set TOKEN bits [7:0] of the PWR_HIBERNATE register (optional) and PWR_HIB_DATA register to some application-specific branching data that can be used on a wakeup event from Hibernate mode.
  2. Set UNLOCK bits [8:15] of the PWR_HIBERNATE register to 0x3A for FREEZE and HIBERNATE bits of the PWR_HIBERNATE register to operate.
  3. Configure wakeup pins polarity (POLARITY_HIBPIN bits [23:20]), wakeup pins mask (MASK_HIBPIN bits [27:24]) and wakeup alarm mask (MASK_HIBALARM bit [18]) in the PWR_HIBERNATE register based on the application requirement.
  4. Set FREEZE bit [17] of the PWR_HIBERNATE register to freeze the I/O pins.
  5. Set HIBERNATE bit [31] of the PWR_HIBERNATE register to enter Hibernate mode.
  6. Read the PWR_HIBERNATE register to make sure that the write has taken effect.
  7. Execute WFI instruction on all of CPUs.

Note: It is recommended to trigger Hibernate mode atomically. That means, when entering Hibernate mode, disable all the interrupts and do a write operation on the PWR_Hibernate register.

Note: Make sure that any write transfer made before executing the WFI instruction is followed by the read access to the same memory location. This ensures that the write operation is successful.

  1. CPU enters low-power mode.
  2. Both high-frequency and low-frequency clocks are shut down.
  3. Retention is enabled and non-retention logic is reset.
  4. Both Active and DeepSleep regulators are powered down. The peripherals that are active in the Hibernate domain operate directly out of VDDD.
  5. I/O cells are frozen.

Sleep

DeepSleep

When the debugger is not connected and DeepSleep mode is triggered, but LPM_READY==0, the device internally enters Sleep mode. The device will automatically transit to DeepSleep when LPM_READY==1.

If the debugger is connected and DeepSleep mode is triggered by the firmware, the device will enter DeepSleep only when the following conditions are met:

  1. LPM_READY==1
  2. Debugger is disconnected
  1. High-frequency clocks are shut down.
  2. I/O cells will be frozen automatically.
  3. Retention is enabled and non-retention logic is reset.
  4. Active regulator is disabled and DeepSleep regulator takes over.

Figure 3 shows the software and hardware operation for the transition from Active mode to DeepSleep mode.

Figure 3. Active mode to DeepSleep mode transition​

Figure 3

Note: In Figure 3, the gray boxes indicate hardware operation. Therefore, processing with software is not required.

Figure 4 shows the software and hardware operation for the transition from Active mode to Hibernate mode.

Figure 4. Active mode to Hibernate mode transition​

Figure 4

Note: The gray boxes indicate hardware operation in Figure 4. Therefore, processing with software is not required.

Wakeup from low-power modes​

Table 3 shows the hardware triggers for wakeup and the actions after wakeup.

Table 3. Wakeup action​

Initial state

Final state

Trigger source

Hardware action

Sleep

Active

Any enabled interrupt in Sleep mode

CPU exits Sleep mode and executes the interrupt

DeepSleep

Active

Any enabled interrupt in DeepSleep mode

Device returns to the configuration it had while entering DeepSleep mode.

(IMO/clocks enabled, retention disabled, non-retained resets, freeze release; CPU exits low-power mode and takes interrupt)

DeepSleep

Sleep

Debug wakeup

Retention disabled and non-retained reset

Freeze release

HF and LF are on

CPU remains in Sleep state

Hibernate

Active

Wakeup pins, RTC alarms

Hibernate wakeup is implemented as a transition to Active mode through reset:

  1. Low-voltage (internal Active and DeepSleep mode) regulators and references are ramped up
  2. All low-voltage logic (operating from internal regulators) is reset
  3. IMO clock is started
  4. Core starts execution

Figure 5 shows the software and hardware operation for the transition from DeepSleep mode to Active mode.

Figure 5. DeepSleep mode to Active mode transition​

Figure 5

Note: The gray boxes indicate hardware operation in Figure 5. Therefore, processing with software is not required.

WDT setting during low-power modes​

The watchdog timer (WDT) in TRAVEO™ T2G automatically resets the device in the event of an unexpected software execution path. In addition, the WDT can be used as an interrupt source or a wakeup source in low-power modes. Software can select the resets or interrupts.

This section describes WDT setting and operation in low-power modes. For more details on the WDT, see the architecture TRM.

Features​

TRAVEO™ T2G supports two types of WDT: Basic WDT and multi-counter WDT (MCWDT). Table 4 shows the supported WDT settings during low-power modes.

Table 4. List of PCLK (example of the TCPWM timer) settings parameters​

Power mode

Basic WDT

MCWDT

Remarks

Subcounter0

Subcounter1

Subcounter2

Active

Reset2 and interrupt

Reset3, interrupt, and FAULT4

Interrupt

In Active mode, the WDT can send the interrupt to the CPU.

Sleep

Reset3 and interrupt4

Reset3, interrupt4, and FAULT5

Interrupt

In Sleep mode, the CPU subsystem is powered down. Therefore, the interrupt request from the WDT is directly sent to the wakeup interrupt controller (WIC), which will then wake up the CPU.

DeepSleep

Reset3 and interrupt4

Reset3, interrupt4, and FAULT5

Interrupt6

In DeepSleep mode, the CPU subsystem is powered down. Therefore, the interrupt request from the WDT is directly sent to the WIC, which will then wake up the CPU.

Pauses/runs the counter is selectable during DeepSleep mode.

Hibernate

Reset3 and interrupt4

Not supported

  • Can pause or run the counter; this option is selectable during Hibernate mode.
  • In Hibernate mode, any interrupt to wake up the device results in reset.

2 Reset occurs when the counter value reaches UPPER_LIMIT or when the counter is cleared before LOWER_LIMIT.

3 Interrupt occurs when the counter value reaches WARN_LIMIT.

4 The fault manager converts this to a high-priority interrupt (such as non- mskable interrupt, NMI) that gives the processor an opportunity to return to a safe state, such as halting memory writes and releasing peripherals.

5 Interrupt occurs when the BIT specified by MCWDT2_CTR2_CONFIG [20:16] toggles.

Example of WDT wakeup operation​

Figure 6 shows an example of the operation with Subcounter0/1 of MCWDT. In this example, Subcounter0 of MCWDT is used as a supervisor of an unexpected software execution path, and Subcounter1 of MCWDT is used as a periodic wakeup interrupt generator during low-power mode. For more details on the WDT, see the architecture TRM.

Figure 6. Example of WDT operation (wakeup cause is interrupt of WARN_LIMIT of Subcounter1)​

Subcounter0 is paused during low-power mode. If MCU wakes up from low-power mode, Subcounter0 resumes counting upwards.

Subcounter1 continues counting upwards during low-power mode. If counter value reaches the setting value of “WARN_LIMIT”, MCU wakes up from low-power mode. If AUTO_SERVICE setting is used, hardware resets the counter value.

Configuration and example code​

Table 5 lists the parameters and Table 6 lists the functions of the configuration part in SDL for WDT settings during low-power modes.

Table 5. List of WDT settings during low-power modes configuration parameters​

Parameters

Description

Value

.coreSelect

Select the CPU to be used for SleepDeepPause

CY_MCWDT_PAUSED_BY_NO_CORE

.c0LowerLimit

Select the CPU to be used for SleepDeepPause

0ul

.c0UpperLimit

Select the CPU to be used for SleepDeepPause

0xFFFFul

.c0WarnLimit

Set the Subcounter0 warn limit (unsigned integer 32-bit)

MCWDT_TICKS_PER_SECOND

.c0LowerAction

Set Subcounter0 lower action to “no action”, “fault”, or “fault then reset”

CY_MCWDT_ACTION_FAULT_THEN_RESET

.c0UpperAction

Set Subcounter0 upper action to “no action”, “fault”, or “fault then reset”

CY_MCWDT_ACTION_FAULT_THEN_RESET

.c0WarnAction

Set Subcounter0 warn action to “no action”, or “interrupt”

CY_MCWDT_WARN_ACTION_NONE

.c0AutoService

Configure to automatically clear MCWDT when Subcounter0 value reaches WARN_LIMIT

CY_MCWDT_DISABLE

.c0SleepDeepPause

Enable to pause Subcounter0 when the corresponding CPU is in DeepSleep

CY_MCWDT_ENABLE

.c0DebugRun

Set the debugger configuration. It needs when using debugger

CY_MCWDT_ENABLE

.c1LowerLimit

Set Subcounter1 lower limit (unsigned integer 32-bit)

0ul

.c1UpperLimit

Set Subcounter1 upper limit (unsigned integer 32-bit)

0xFFFFul

.c1WarnLimit

Set Subcounter1 warn limit (unsigned integer 32-bit)

MCWDT_TICKS_PER_SECOND

.c1LowerAction

Set Subcounter1 lower action to “no action”, “fault”, or “fault then reset”

CY_MCWDT_ACTION_NONE

.c1UpperAction

Set Subcounter1 upper action to “no action”, “fault”, or “fault then reset”

CY_MCWDT_ACTION_NONE

.c1WarnAction

Set Subcounter1 warn action to “no action”, or “interrupt”

CY_MCWDT_WARN_ACTION_INT

.c1AutoService

Configure to automatically clear MCWDT when Subcounter1 value reaches WARN_LIMIT

CY_MCWDT_ENABLE

.c1SleepDeepPause

Enable to pause Subcounter1 when the corresponding CPU is in DeepSleep

CY_MCWDT_DISABLE

.c1DebugRun

Set the debugger configuration (required when using debugger)

CY_MCWDT_ENABLE

.c2ToggleBit

Select the bit to observe for a toggle

CY_MCWDT_CNT2_MONITORED_BIT15

.c2Action

Set Subcounter2 action to “no action” or “interrupt”

CY_MCWDT_CNT2_ACTION_NONE

.c2SleepDeepPause

Enable to pause Subcounter2 when the corresponding CPU is in DeepSleep

CY_MCWDT_ENABLE

.c2DebugRun

Set the debugger configuration (required when using debugger)

CY_MCWDT_ENABLE

Table 6. List of WDT settings during low-power modes configuration functions​

Functions

Description

Remarks

Cy_MCWDT_DeInit()

De-initializes the MCWDT block, returns register values to their default state.

See Code Listing 3

Cy_MCWDT_Init()

Initializes the MCWDT block.

See Code Listing 4

Cy_MCWDT_Unlock()

Unlocks the MCWDT configuration registers.

See Code Listing 5

Cy_MCWDT_SetInterruptMask()

Writes MCWDT interrupt mask register.

See Code Listing 6

Cy_MCWDT_Enable()

Enables all specified counters.

See Code Listing 7

Cy_MCWDT_Lock()

Locks out configuration changes to all MCWDT registers.

See Code Listing 8

Cy_MCWDT_ClearWatchdog()

Clears the MC watchdog counter, to prevent a XRES device reset or fault.

See Code Listing 9

Cy_SysPm_DeepSleep()

Sets a CPU core to the DeepSleep mode

See Code Listing 10

Code Listing 1 demonstrates an example program to WDT wakeup operation in power mode transition. See the architecture TRM and application note for GPIO and WDT.

The following description will help you understand the register notation of the driver part of SDL:

  • Base signifies the pointer to the MCWDT register base address. Counters specify the Subcounter within the MCWDT.

  • To improve the register setting performance, the SDL writes a complete 32-bit data to the register. Each bit field is generated and written to the register as the final 32-bit data.

    tempCNT2ConfigParams.stcField.u5BITS = config->c2ToggleBit; tempCNT2ConfigParams.stcField.u1ACTION = config->c2Action; tempCNT2ConfigParams.stcField.u1SLEEPDEEP_PAUSE = config->c2SleepDeepPause; tempCNT2ConfigParams.stcField.u1DEBUG_RUN = config->c2DebugRun; base->unCTR2_CONFIG.u32Register = tempCNT2ConfigParams.u32Register;

See cyip_srss_v2.h under hdr/rev_x/ip for more information on the union and structure representation of registers.

Code Listing 1 Example to WDT wakeup operation in power mode transition​
    int main(void)
{
Cy_SysInt_SetSystemIrqVector(srss_interrupt_mcwdt_1_IRQn, irqMCWDT1Handler); /*Assign MCWDT interrupt*/
:
/*MCWDT configuration See (a) of Figure 6.
See Code Listing 3, Code Listing 4, Code Listing 5, Code Listing 6, Code Listing 7, Code Listing 8
*/
Cy_MCWDT_DeInit(MCWDT1);
Cy_MCWDT_Init(MCWDT1, &mcwdtConfig);

Cy_MCWDT_Unlock(MCWDT1);
Cy_MCWDT_SetInterruptMask
(MCWDT1, CY_MCWDT_CTR_Msk);
Cy_MCWDT_Enable(MCWDT1,
CY_MCWDT_CTR_Msk,
0ul);
Cy_MCWDT_Lock(MCWDT1);

/* Put the system to DeeSleep */
/*See (b) of Figure 6. Set to the DeepSleep mode. See Code Listing 10*/
Cy_SysPm_DeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT);

for(;;)
{
/* Clear Watchdog counter 0 */
/*Clears the MCWD counter See (d) of Figure 6. See Code Listing 9*/
Cy_MCWDT_ClearWatchdog(MCWDT1, CY_MCWDT_COUNTER0);

while( tFlag == 0ul );
tFlag = 0ul;
/*See (b) of Figure 6. See Code Listing 10*/
Cy_SysPm_DeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT);
}
}
Code Listing 2 MCWDT configuration​
    /**
* \var cy_stc_mcwdt_config_t mcwdtConfig
* \brief MCWDT configuration
*/
cy_stc_mcwdt_config_t mcwdtConfig = /*Configure MCWDT parameter*/
{
.coreSelect = CY_MCWDT_PAUSED_BY_NO_CORE,
.c0LowerLimit = 0ul,
.c0UpperLimit = 0xFFFFul,
.c0WarnLimit = MCWDT_TICKS_PER_SECOND, /* 1 sec, ignored */
.c0LowerAction = CY_MCWDT_ACTION_FAULT_THEN_RESET,
.c0UpperAction = CY_MCWDT_ACTION_FAULT_THEN_RESET,
.c0WarnAction = CY_MCWDT_WARN_ACTION_NONE,
.c0AutoService = CY_MCWDT_DISABLE,
.c0SleepDeepPause = CY_MCWDT_ENABLE,
.c0DebugRun = CY_MCWDT_ENABLE,
.c1LowerLimit = 0ul,
.c1UpperLimit = 0xFFFFul,
.c1WarnLimit = MCWDT_TICKS_PER_SECOND, /* 1 sec */
.c1LowerAction = CY_MCWDT_ACTION_NONE,
.c1UpperAction = CY_MCWDT_ACTION_NONE,
.c1WarnAction = CY_MCWDT_WARN_ACTION_INT,
.c1AutoService = CY_MCWDT_ENABLE,
.c1SleepDeepPause = CY_MCWDT_DISABLE,
.c1DebugRun = CY_MCWDT_ENABLE,
.c2ToggleBit = CY_MCWDT_CNT2_MONITORED_BIT15,
.c2Action = CY_MCWDT_CNT2_ACTION_NONE,
.c2SleepDeepPause = CY_MCWDT_ENABLE,
.c2DebugRun = CY_MCWDT_ENABLE,
};
Code Listing 3 Cy_MCWDT_DeInit() function​
    /* De-initializes the MCWDT block, returns register values to their default state.*/

void Cy_MCWDT_DeInit(volatile stc_MCWDT_t *base)
{
Cy_MCWDT_Unlock(base);

// disable all counter
for(uint32_t loop = 0ul; loop < CY_MCWDT_NUM_OF_SUBCOUNTER; loop++)
{
base->CTR[loop].unCTL.u32Register = 0ul;
}
base->unCTR2_CTL.u32Register = 0ul;

for(uint32_t loop = 0ul; loop < CY_MCWDT_NUM_OF_SUBCOUNTER; loop++)
{
while(base->CTR[loop].unCTL.u32Register != 0x0ul); // wait until enabled bit become 1
base->CTR[loop].unLOWER_LIMIT.u32Register = 0x0ul;
base->CTR[loop].unUPPER_LIMIT.u32Register = 0x0ul;
base->CTR[loop].unWARN_LIMIT.u32Register = 0x0ul;
base->CTR[loop].unCONFIG.u32Register = 0x0ul;
base->CTR[loop].unCNT.u32Register = 0x0ul;
}

while(base->unCTR2_CNT.u32Register != 0ul); // wait until enabled bit become 1
base->unCPU_SELECT.u32Register = 0ul;
base->unCTR2_CONFIG.u32Register = 0ul;
base->unSERVICE.u32Register = 0x00000003ul;
base->unINTR.u32Register = 0xFFFFFFFFul;
base->unINTR_MASK.u32Register = 0ul;

Cy_MCWDT_Lock(base);
}
Code Listing 4 Cy_MCWDT_Init() function​
    /* Initializes the MCWDT block.*/

cy_en_mcwdt_status_t Cy_MCWDT_Init(volatile stc_MCWDT_t *base, cy_stc_mcwdt_config_t const *config)
{
cy_en_mcwdt_status_t ret = CY_MCWDT_BAD_PARAM;
if ((base != NULL) && (config != NULL))
{
Cy_MCWDT_Unlock(base);
un_MCWDT_CTR_CONFIG_t tempConfigParams = { 0ul };
un_MCWDT_CTR2_CONFIG_t tempCNT2ConfigParams = { 0ul };

base->unCPU_SELECT.u32Register = config->coreSelect;
base->CTR[0].unLOWER_LIMIT.stcField.u16LOWER_LIMIT = config->c0LowerLimit;
base->CTR[0].unUPPER_LIMIT.stcField.u16UPPER_LIMIT = config->c0UpperLimit;
base->CTR[0].unWARN_LIMIT.stcField.u16WARN_LIMIT = config->c0WarnLimit;
tempConfigParams.stcField.u2LOWER_ACTION = config->c0LowerAction;
tempConfigParams.stcField.u2UPPER_ACTION = config->c0UpperAction;
tempConfigParams.stcField.u1WARN_ACTION = config->c0WarnAction;
tempConfigParams.stcField.u1AUTO_SERVICE = config->c0AutoService;
tempConfigParams.stcField.u1SLEEPDEEP_PAUSE = config->c0SleepDeepPause;
tempConfigParams.stcField.u1DEBUG_RUN = config->c0DebugRun;
base->CTR[0].unCONFIG.u32Register = tempConfigParams.u32Register;

base->CTR[1].unLOWER_LIMIT.stcField.u16LOWER_LIMIT = config->c1LowerLimit;
base->CTR[1].unUPPER_LIMIT.stcField.u16UPPER_LIMIT = config->c1UpperLimit;
base->CTR[1].unWARN_LIMIT.stcField.u16WARN_LIMIT = config->c1WarnLimit;
tempConfigParams.stcField.u2LOWER_ACTION = config->c1LowerAction;
tempConfigParams.stcField.u2UPPER_ACTION = config->c1UpperAction;
tempConfigParams.stcField.u1WARN_ACTION = config->c1WarnAction;
tempConfigParams.stcField.u1AUTO_SERVICE = config->c1AutoService;
tempConfigParams.stcField.u1SLEEPDEEP_PAUSE = config->c1SleepDeepPause;
tempConfigParams.stcField.u1DEBUG_RUN = config->c1DebugRun;
base->CTR[1].unCONFIG.u32Register = tempConfigParams.u32Register;

tempCNT2ConfigParams.stcField.u5BITS = config->c2ToggleBit;
tempCNT2ConfigParams.stcField.u1ACTION = config->c2Action;
tempCNT2ConfigParams.stcField.u1SLEEPDEEP_PAUSE = config->c2SleepDeepPause;
tempCNT2ConfigParams.stcField.u1DEBUG_RUN = config->c2DebugRun;
base->unCTR2_CONFIG.u32Register = tempCNT2ConfigParams.u32Register;

Cy_MCWDT_Lock(base);

ret = CY_MCWDT_SUCCESS;
}

return (ret);
}
Code Listing 5 Cy_MCWDT_Unlock() function​
    /* Unlocks the MCWDT configuration registers.*/

STATIC_INLINE void Cy_MCWDT_Unlock(volatile stc_MCWDT_t *base)
{
uint32_t interruptState;

interruptState = Cy_SysLib_EnterCriticalSection();

base->unLOCK.stcField.u2MCWDT_LOCK = CY_MCWDT_LOCK_CLR0;
base->unLOCK.stcField.u2MCWDT_LOCK = CY_MCWDT_LOCK_CLR1;

Cy_SysLib_ExitCriticalSection(interruptState);
}
Code Listing 6 Cy_MCWDT_SetInterruptMask() function​
    /* Writes MCWDT interrupt mask register.*/

__STATIC_INLINE void Cy_MCWDT_SetInterruptMask(volatile stc_MCWDT_t *base, uint32_t counters)
{
if (counters & CY_MCWDT_CTR0)
{
base->unINTR_MASK.stcField.u1CTR0_INT = 1ul;
}
if (counters & CY_MCWDT_CTR1)
{
base->unINTR_MASK.stcField.u1CTR1_INT = 1ul;
}
if (counters & CY_MCWDT_CTR2)
{
base->unINTR_MASK.stcField.u1CTR2_INT = 1ul;
}
}
Code Listing 7 Cy_MCWDT_Enable() function​
    /* Enables all specified counters. */

__STATIC_INLINE void Cy_MCWDT_Enable(volatile stc_MCWDT_t *base, uint32_t counters, uint16_t waitUs)
{
if (counters & CY_MCWDT_CTR0)
{
base->CTR[0].unCTL.stcField.u1ENABLE = 1ul;
}
if (counters & CY_MCWDT_CTR1)
{
base->CTR[1].unCTL.stcField.u1ENABLE = 1ul;
}
if (counters & CY_MCWDT_CTR2)
{
base->unCTR2_CTL.stcField.u1ENABLE = 1ul;
}
Cy_SysLib_DelayUs(waitUs);
}
Code Listing 8 Cy_MCWDT_Lock() function​
    /* Locks out configuration changes to all MCWDT registers. */
__STATIC_INLINE void Cy_MCWDT_Lock(volatile stc_MCWDT_t *base)
{
uint32_t interruptState;

interruptState = Cy_SysLib_EnterCriticalSection();

base->unLOCK.stcField.u2MCWDT_LOCK = CY_MCWDT_LOCK_SET01;

Cy_SysLib_ExitCriticalSection(interruptState);
}
Code Listing 9 Cy_MCWDT_ClearWatchdog() function​
    /* Clears the MC watchdog counter, to prevent a XRES device reset or fault. */
void Cy_MCWDT_ClearWatchdog(volatile stc_MCWDT_t *base, cy_en_mcwdtctr_t counter)
{
Cy_MCWDT_Unlock(base);
Cy_MCWDT_ResetCounters(base, (1u << (uint8_t)counter), 0u);
Cy_MCWDT_Lock(base);
}
Code Listing 10 Cy_SysPm_DeepSleep() function​
    /* Sets a CPU core to the DeepSleep mode */
cy_en_syspm_status_t Cy_SysPm_DeepSleep(cy_en_syspm_waitfor_t waitFor)
{
uint32_t interruptState;
cy_en_syspm_status_t retVal = CY_SYSPM_SUCCESS;

/* Call the registered callback functions with
* the CY_SYSPM_CHECK_READY parameter.
*/
if(0u != currentRegisteredCallbacksNumber)
{
retVal = Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_CHECK_READY);
}

/* The device (core) can switch into the deep sleep power mode only when
* all executed registered callback functions with the CY_SYSPM_CHECK_READY
* parameter returned CY_SYSPM_SUCCESS.
*/
if(retVal == CY_SYSPM_SUCCESS)
{
/* Call the registered callback functions with the CY_SYSPM_BEFORE_TRANSITION
* parameter. The return value is ignored.
*/
interruptState = Cy_SysLib_EnterCriticalSection();
if(0u != currentRegisteredCallbacksNumber)
{
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_BEFORE_ENTER);
}

#if(0u != CY_CPU_CORTEX_M0P)

/* The CPU enters the deep sleep mode upon execution of WFI/WFE */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

if(waitFor != CY_SYSPM_WAIT_FOR_EVENT)
{
__WFI();
}
else
{
__WFE();
}
#else

/* Repeat WFI/WFE instructions if wake up was not intended.
* Cypress Ticket #272909
*/
do
{
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

if(waitFor != CY_SYSPM_WAIT_FOR_EVENT)
{
__WFI();
}
else
{
__WFE();
}
} while (0); //rmkn _FLD2VAL(CPUSS_CM4_PWR_CTL_PWR_MODE, CPUSS->unCM4_PWR_CTL.u32Register) == CY_SYSPM_CM4_PWR_CTL_PWR_MODE_RETAINED);

#endif /* (0u != CY_CPU_CORTEX_M0P) */

Cy_SysLib_ExitCriticalSection(interruptState);

/* Call the registered callback functions with the CY_SYSPM_AFTER_TRANSITION
* parameter. The return value is ignored.
*/
if(0u != currentRegisteredCallbacksNumber)
{
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_AFTER_EXIT);
}
}
else
{
/* Execute callback functions with the CY_SYSPM_CHECK_FAIL parameter to
* undo everything done in the callback with the CY_SYSPM_CHECK_READY
* parameter. The return value is ignored.
*/
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_CHECK_FAIL);
retVal = CY_SYSPM_FAIL;
}
return retVal;
}

2 Reset occurs when the counter value reaches UPPER_LIMIT or when the counter is cleared before LOWER_LIMIT.

3 Interrupt occurs when the counter value reaches WARN_LIMIT.

4 The fault manager converts this to a high-priority interrupt (such as non- mskable interrupt, NMI) that gives the processor an opportunity to return to a safe state, such as halting memory writes and releasing peripherals.

5 Interrupt occurs when the BIT specified by MCWDT2_CTR2_CONFIG [20:16] toggles.

Cyclic wakeup operation​

Cyclic wakeup operation is an intermittent MCU operation. For example, when the electronic control unit (ECU) is in Sleep mode, MCU cyclically enters DeepSleep mode and wakes up. This operation is intended to minimize the average power consumption in an application. This section describes an implementation example of cyclic wakeup operation by using TRAVEO™ T2G family MCUs.

Usage example of cyclic wakeup​

Figure 7 shows an example of a user system. MCU controls the GPIO and ADC for monitoring external devices, sensors, and so on.

Figure 7. Block diagram of an example user system​

Figure 7

The external device is connected to MCU via GPIO. The external device wakes up the sensor by the control signal from the MCU. The sensor outputs are connected to the ADC of the MCU.

However, the sensor generally requires a stabilization wait time to correctly output after wakeup.

Therefore, the MCU outputs the sensor wakeup signal to the external device, and activates ADC after a certain time to convert the sensor signal. For generating these two different timings, two timer interrupts (Comp 0 and Comp1) of the event generator are used. In this case, Comp0 is used as a trigger for ADC activation, and Comp1 is used for CPU wakeup.

Cyclic wakeup operation​

Figure 8 shows the concept of the cyclic wakeup operation. TRAVEO™ T2G device cyclically wakes up to check the external sensor information when the ECU enters Sleep mode.

Figure 8. Cyclic wakeup operation​

Figure 8

(0) After a reset, TRAVEO™ T2G enters Active mode and operates the user software.

(1) The CPU core configures and runs the event generator with the 32.768 kHz low-frequency oscillator.

(The source clock of the event generator can be selected from ILO0, ILO1, and WCO.)

(2) TRAVEO™ T2G enters DeepSleep mode; the CPU core goes to DeepSleep state.

(3) If the counter value of the event generator matches Comp1, the Comp1 trigger wakes up the CPU core.

(4) The CPU (software) controls the GPIO to output a wakeup trigger activation for external devices.

(5) Comp0 trigger starts an ADC range comparison.

(6) The CPU (software) observes ADC results.

(7) The CPU (software) controls the GPIO.

[If ADC results of range detection are in range, ECU continues to run cyclic wakeup operation.]

(8) The CPU (software) restarts the event generator. The CPU goes back to DeepSleep mode. [Go to (2)]

[If ADC results of range detection are out of range, ECU exits from cyclic wakeup operation.]

(9) CPU (software) restarts the operation of the ECU system.

For more details on event generator, ADC, GPIO, and clock, see the architecture TRM.

Flowchart of cyclic wakeup operation​

Figure 9. Flowchart of cyclic wakeup operation​

Figure 9

Note: The gray boxes indicate hardware operation in Figure 9. Therefore, processing with software is not required.

  1. Initial setting for using resources

    • Initialized ADC, event generator, GPIO, and wakeup interrupt configuration
  2. Event generator start

    • Comp0 for ADC activation and Comp1 for CPU wakeup start to count.
    • Comp1 is determined by the period time for cyclic wakeup.
  3. Enter DeepSleep mode

  4. Cyclic wakeup

    • When a wakeup trigger occurs, CPU will check whether interrupt is cyclic wakeup.
    • If it is not cyclic wakeup, CPU returns to Active mode as the abnormal interrupt occurrence.
  5. Checking the sensor outputs

    • CPU outputs control signal to external device to deactivate sensor after ADC conversion completion.
    • CPU checks the flags of all conversion channels.
    • If flags are set, CPU transfers to ACTIVE mode.
    • If flags are not set, CPU transfers to DeepSleep mode again after restarting timers of Comp0 and Comp1.
Configuration and example code​

Table 7 lists the parameters and Table 8 lists the functions of the configuration part in SDL for cyclic wakeup operation.

Table 7. List of cyclic wakeup operation configuration parameters​

Parameters

Description

Value

.frequencyRef

clk_ref

8000000

.frequencyLf

clk_lf

32000

.frequencyTick

Event generator clock (clk_ref_div)

1000000 (Setting 1,000,000 Hz)

.ratioControlMode

Event generator ratio control mode

CY_EVTGEN_RATIO_CONTROL_HW

.ratioValueDynamicMode

Event generator dynamic mode

CY_EVTGEN_RATIO_DYNAMIC_MODE0

.functionalitySelection

Event generator select functionality

CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY

.triggerOutEdge

Event generator trigger

CY_EVTGEN_EDGE_SENSITIVE

.valueDeepSleepComparator

Wakes up the CPU after time

1000000 (1 sec)

.valueActiveComparator

Triggers ADC after time

1500000 (1.5 sec)

.userIsr

Event generator struct handler

NULL

Table 8. List of cyclic wakeup operation configuration functions​

Functions

Description

Remarks

AdcIntHandler()

Interrupt handler for ADC

See Code Listing 11

irqEVTGEN_sleep()

Interrupt setting for event generator

See Code Listing 11

Cy_Evtgen_ClearStructInterruptDeepSleep()

Clears the DeepSleep interrupt factor of the corresponding structure

See Code Listing 12

Cy_Evtgen_DeinitializeCompStruct()

Deinitializes the event generator structure

See Code Listing 13

Cy_Evtgen_Deinitialize()

Deinitializes the event generator

See Code Listing 14

Cy_Evtgen_Initialize()

Initializes the event generator

See Code Listing 15

Cy_Evtgen_InitializeCompStruct()

Initializes the comparator structure

See Code Listing 16

Cy_SysInt_SetSystemIrqVector()

Changes the user ISR vector for the system interrupt

See Code Listing 18

Cy_SysPm_DeepSleep()

Sets a CPU core to the DeepSleep mode

See Code Listing 17

Code Listing 11 demonstrates an example program to cyclic wakeup operation. See the architecture TRM and application note for GPIO and ADC.

Code Listing 11 Example of cyclic wakeup operation​
    /* Eventgenerator Configration */

const cy_stc_evtgen_config_t evtgenTestConfig =
{
#else
.frequencyRef = 8000000, // clk_ref = clk_hf1
.frequencyLf = 32000, // clk_lf = 32,000 for silicon
#endif
.frequencyTick = 1000000, // Setting 1,000,000 Hz for event generator clock
.ratioControlMode = CY_EVTGEN_RATIO_CONTROL_HW,
.ratioValueDynamicMode = CY_EVTGEN_RATIO_DYNAMIC_MODE0,
};


const cy_stc_evtgen_struct_config_t evtgenTestStructureConfig =
{
.functionalitySelection = CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY,
.triggerOutEdge = CY_EVTGEN_EDGE_SENSITIVE,
.valueDeepSleepComparator = 1000000, // It wake CPU up after 1s.
.valueActiveComparator = 1500000, // It triggers ADC after 1.5s.
.userIsr = NULL,
};

/* See (d) of Figure 9. Interrupt handler for ADC */
void AdcIntHandler(void)
{
cy_stc_adc_interrupt_source_t intrSource = { false };
/* Get the result(s) */
Cy_Adc_Channel_GetResult(&BB_POTI_ANALOG_MACRO->CH[ADC_LOGICAL_CHANNEL], &resultBuff[resultIdx], &statusBuff[resultIdx]);
resultIdx = (resultIdx + 1) % (sizeof(resultBuff) / sizeof(resultBuff[0]));
/* Clear inerrupt source */
Cy_Adc_Channel_GetInterruptMaskedStatus(&BB_POTI_ANALOG_MACRO->CH[ADC_LOGICAL_CHANNEL], &intrSource);
Cy_Adc_Channel_ClearInterruptStatus(&BB_POTI_ANALOG_MACRO->CH[ADC_LOGICAL_CHANNEL], &intrSource);

adcCompletedFlag = 1;
}

void irqEVTGEN_sleep(void)
{
/* See (c) of Figure 9. See Code Listing 12 */
Cy_Evtgen_ClearStructInterruptDeepSleep(EVTGEN0,0);
}

int main(void)
{
:
/* Event generator configuration.See (a) of Figure 9. */
/*******************************************/
/* Deinitialize peripherals */
/*******************************************/
Cy_Evtgen_DeinitializeCompStruct(EVTGEN0, 0); /* See Code Listing 13 */
Cy_Evtgen_Deinitialize(EVTGEN0); /* See Code Listing 14 */

/*******************************************/
/* Initialize and start Event generator */
/*******************************************/
Cy_Evtgen_Initialize(EVTGEN0,&evtgenTestConfig); /* See Code Listing 15 */

/*******************************************/
/* Initialize comparator structure 0 */
/*******************************************/
Cy_Evtgen_InitializeCompStruct(EVTGEN0, 0, /* See Code Listing 16 */
&evtgenTestStructureConfig, &evtgenStruct0Context);

/* Register ADC interrupt handler and enable interrupt */
Cy_SysInt_SetSystemIrqVector(irq_cfg_adc.sysIntSrc, AdcIntHandler);

/* Put the system to DeeSleep */
Cy_SysPm_DeepSleep((cy_en_syspm_waitfor_t)CY_SYSPM_WAIT_FOR_INTERRUPT);

/* See (b) of Figure 9. Set to the DeepSleep mode. See Code Listing 17 */
for(;;)
{
while(adcCompletedFlag == 0);
adcCompletedFlag = 0;

Cy_Evtgen_DeinitializeCompStruct(EVTGEN0, 0);
Cy_Evtgen_InitializeCompStruct(EVTGEN0, 0, &evtgenTestStructureConfig, &evtgenStruct0Context);
/* Put the system to DeeSleep */
Cy_SysPm_DeepSleep((cy_en_syspm_waitfor_t)CY_SYSPM_WAIT_FOR_INTERRUPT);
}

}
Code Listing 12 Cy_Evtgen_ClearStructInterruptDeepSleep() function​
    /* Clear DeepSleep interrupt factor of corresponding structure */
__STATIC_INLINE void Cy_Evtgen_ClearStructInterruptDeepSleep(volatile stc_EVTGEN_t *base, uint8_t structNumber)
{
base->unINTR_DPSLP.u32Register = ((uint32_t)1 << structNumber);

// Dummy read. This is to wait for reflection above write operation.
base->unINTR_DPSLP;
}
Code Listing 13 Cy_Evtgen_DeinitializeCompStruct() function​
    void Cy_Evtgen_DeinitializeCompStruct(volatile stc_EVTGEN_t *base, uint8_t structNum)
{
/* Deinitialize event generator structure */
base->COMP_STRUCT[structNum].unCOMP_CTL.u32Register = 0;
base->COMP_STRUCT[structNum].unCOMP0.stcField.u32INT32 = 0;
base->COMP_STRUCT[structNum].unCOMP1.stcField.u32INT32 = 0;
evtgenContext[structNum] = NULL;
}
Code Listing 14 Cy_Evtgen_Deinitialize() function​
    void Cy_Evtgen_Deinitialize(volatile stc_EVTGEN_t *base)
{
/* Deinitialize event generator */
base->unCTL.u32Register = 0;
base->unREF_CLOCK_CTL.u32Register = 0;
base->unRATIO.u32Register = 0;
base->unRATIO_CTL.u32Register = 0;
base->unINTR_MASK.u32Register = 0;
base->unINTR_DPSLP_MASK.u32Register = 0;
}
Code Listing 15 Cy_Evtgen_Initialize() function​
    cy_en_evtgendrv_status_t Cy_Evtgen_Initialize(volatile stc_EVTGEN_t *base, const cy_stc_evtgen_config_t* config)
{

/* Initialize the event generator */
uint16_t refDiv;

un_EVTGEN_RATIO_CTL_t ratioCtl;

/* 1. Checking input parameter valid */
if(config == NULL)
{
return CY_EVTGEN_ERR;
}

/* 2. Initialize internal variable */
for(uint32_t i = 0; i < EVTGEN_COMP_STRUCT_NR; i++)
{
evtgenContext[i] = NULL;
}
mapUsed = 0;

Cy_Evtgen_Enable(base);

/* 2. Setting divider value of clk_ref */
refDiv = config->frequencyRef / config->frequencyTick;
if(config->frequencyRef % config->frequencyTick != 0)
{
return CY_EVTGEN_ERR;
}
else if(refDiv > 256 || refDiv < 1)
{
return CY_EVTGEN_ERR;
}
else
{
base->unREF_CLOCK_CTL.stcField.u8INT_DIV = refDiv - 1u;
}

/* 3. Setting ratio operation */
if(config->ratioControlMode == CY_EVTGEN_RATIO_CONTROL_SW)
{
/* SW controll: setting value for ratio value should be ratio between tick_ref_div and clk_lf. */
uint64_t temp = (uint64_t)(config->frequencyRef / refDiv) << EVTGEN_RATIO_INT16_Pos;
temp = temp / (uint64_t)(config->frequencyLf);
base->unRATIO.u32Register = ((uint32_t)temp) & (EVTGEN_RATIO_INT16_Msk | EVTGEN_RATIO_FRAC8_Msk);

base->unRATIO_CTL.stcField.u1DYNAMIC = 0u;

/* SW controll: valid bit should be set manually. */
base->unRATIO_CTL.stcField.u1VALID = 1u; /* Set VALID bit */
}
else
{
/* HW controll: */
ratioCtl.u32Register = base->unRATIO_CTL.u32Register;
ratioCtl.stcField.u1DYNAMIC = 1u; /* Set Dynamic bit */
ratioCtl.stcField.u3DYNAMIC_MODE = config->ratioValueDynamicMode; /* Set Dynamic bit */
base->unRATIO_CTL.u32Register = ratioCtl.u32Register;

/* Waiting until valid bit is set. */
while(base->unRATIO_CTL.stcField.u1VALID == 0u);
}

/* Waiting until counter become ready. */
while(base->unCOUNTER_STATUS.stcField.u1VALID == 0u);

return CY_EVTGEN_OK;
}
Code Listing 16 Cy_Evtgen_InitializeCompStruct() function​
    cy_en_evtgendrv_status_t Cy_Evtgen_InitializeCompStruct(volatile stc_EVTGEN_t *base,
uint8_t structNum,
const cy_stc_evtgen_struct_config_t* configStruct,
cy_stc_evtgen_struct_context_t* context)
{

/* Initialize a comparator structure */

un_EVTGEN_COMP_STRUCT_COMP_CTL_t compCtr;
uint64_t tempCounterValue;
uint32_t savedIntrStatus;

/* Checking input parameter valid */
if(configStruct == NULL)
{
return CY_EVTGEN_ERR;
}

if(structNum >= EVTGEN_COMP_STRUCT_NR)
{
return CY_EVTGEN_ERR;
}

if(configStruct->functionalitySelection != CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY)
{
if(context == NULL)
{
return CY_EVTGEN_ERR;
}
evtgenContext[structNum] = context;
evtgenContext[structNum]->addValueForCOMP0 = configStruct->valueActiveComparator;
evtgenContext[structNum]->userIsr = configStruct->userIsr;
mapUsed |= 1 << structNum;
}

compCtr.u32Register = base->COMP_STRUCT[structNum].unCOMP_CTL.u32Register;

if(configStruct->functionalitySelection == CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY)
{
compCtr.stcField.u1COMP1_EN = 1u;
}

compCtr.stcField.u1COMP0_EN = 1u;

compCtr.stcField.u1TR_OUT_EDGE = configStruct->triggerOutEdge;

compCtr.stcField.u1ENABLED = 1u;

savedIntrStatus = Cy_SysLib_EnterCriticalSection();

tempCounterValue = (uint64_t)Cy_Evtgen_GetCounterValue(base);

/* Setting active comparator value */
base->COMP_STRUCT[structNum].unCOMP0.stcField.u32INT32 = (uint32_t)(tempCounterValue + (uint64_t)configStruct->valueActiveComparator);

/* Setting deep sleep comparator value */
if(configStruct->functionalitySelection == CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY)
{
base->COMP_STRUCT[structNum].unCOMP1.stcField.u32INT32 = (uint32_t)(tempCounterValue + (uint64_t)configStruct->valueDeepSleepComparator);
}

Cy_SysLib_ExitCriticalSection(savedIntrStatus);

/* Setting comparator struct controll parameter */
base->COMP_STRUCT[structNum].unCOMP_CTL.u32Register = compCtr.u32Register;

Cy_Evtgen_SetInterruptMask(base, structNum);
if(configStruct->functionalitySelection == CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY)
{
Cy_Evtgen_SetInterruptDeepSleepMask(base, structNum);
}

return CY_EVTGEN_OK;
}
Code Listing 17 Cy_SysPm_DeepSleep() function​
    cy_en_syspm_status_t Cy_SysPm_DeepSleep(cy_en_syspm_waitfor_t waitFor)
{

/* Sets a CPU core to the DeepSleep mode */
uint32_t interruptState;
cy_en_syspm_status_t retVal = CY_SYSPM_SUCCESS;

/* Call the registered callback functions with
* the CY_SYSPM_CHECK_READY parameter.
*/
if(0u != currentRegisteredCallbacksNumber)
{
retVal = Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_CHECK_READY);
}

/* The device (core) can switch into the deep sleep power mode only when
* all executed registered callback functions with the CY_SYSPM_CHECK_READY
* parameter returned CY_SYSPM_SUCCESS.
*/
if(retVal == CY_SYSPM_SUCCESS)
{
/* Call the registered callback functions with the CY_SYSPM_BEFORE_TRANSITION
* parameter. The return value is ignored.
*/
interruptState = Cy_SysLib_EnterCriticalSection();
if(0u != currentRegisteredCallbacksNumber)
{
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_BEFORE_ENTER);
}

#if(0u != CY_CPU_CORTEX_M0P)

/* The CPU enters the deep sleep mode upon execution of WFI/WFE */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

if(waitFor != CY_SYSPM_WAIT_FOR_EVENT)
{
__WFI();
}
else
{
__WFE();
}
#else

/* Repeat WFI/WFE instructions if wake up was not intended.
* Cypress Ticket #272909
*/
do
{
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

if(waitFor != CY_SYSPM_WAIT_FOR_EVENT)
{
__WFI();
}
else
{
__WFE();
}
} while (0); //rmkn _FLD2VAL(CPUSS_CM4_PWR_CTL_PWR_MODE, CPUSS->unCM4_PWR_CTL.u32Register) == CY_SYSPM_CM4_PWR_CTL_PWR_MODE_RETAINED);

#endif /* (0u != CY_CPU_CORTEX_M0P) */

Cy_SysLib_ExitCriticalSection(interruptState);

/* Call the registered callback functions with the CY_SYSPM_AFTER_TRANSITION
* parameter. The return value is ignored.
*/
if(0u != currentRegisteredCallbacksNumber)
{
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_AFTER_EXIT);
}
}
else
{
/* Execute callback functions with the CY_SYSPM_CHECK_FAIL parameter to
* undo everything done in the callback with the CY_SYSPM_CHECK_READY
* parameter. The return value is ignored.
*/
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_CHECK_FAIL);
retVal = CY_SYSPM_FAIL;
}
return retVal;
}
Code Listing 18 C Cy_SysInt_SetSystemIrqVector() function​
    void  Cy_SysInt_SetSystemIrqVector(cy_en_intr_t sysIntSrc, cy_systemIntr_Handler userIsr)
{

/* Changes the User ISR vector for the System Interrupt */
if (Cy_SysInt_SystemIrqUserTableRamPointer != NULL)
{
Cy_SysInt_SystemIrqUserTableRamPointer[sysIntSrc] = userIsr;
}
}

Usage of smart I/O in cyclic wakeup​

This section describes the role of smart I/O in reducing the LPACTIVE period in cyclic wakeup operation.

As described in the beginning of the cyclic wakeup operation section, cyclic wakeup is intended to minimize the average power consumption in an application. This average consumption current is affected by the following:

  • DeepSleep current
  • LPACTIVE current
  • Percentage of LPACTIVE time in one period.

DeepSleep current and LPACTIVE current mostly depend on electrical specifications of HW, while the percentage of the LPACTIVE time in one period depends on the optimization of SW. Because the current consumption during LPACTIVE (several mA) is relatively much higher than in DeepSleep (several 10μA), from the SW point of view, reducing the LPACTIVE time plays an important factor in achieving a low average consumption current. To shorten the LPACTIVE period, use of Smart I/O is suggested.

In the flow of cyclic wakeup operation proposed in Figure 8, the MCU need to wake up and configure I/O ports to turn sensors on, and wait for the sensor’s stabilization before triggering ADC conversion. If a long sensor stabilization time is required, the MCU can optionally be put in Sleep/DeepSleep again to reduce the current consumption, but this approach may make program more complex. Additionally, you should consider the transition time between different power modes.

Figure 10 shows the system configuration of this use case. GPIO is activated by smart I/O, instead of CPU as demonstrated in Figure 7.

Figure 10. System configuration of cyclic wakeup with smart I/O​

Figure 10

Advantage of smart I/O implementation in cyclic wakeup​

Smart I/O can be used to manipulate I/O during DeepSleep mode. This can eliminate the unnecessary LPACTIVE time CPU spends to activate I/O especially when the CPU must wait for a long time for the sensor to stabilize.

The internal logic of smart I/O includes three-input lookup table (LUTs) and data unit (DU) among other components. DU acts as a counter with count up/down and reload function. By setting the data unit and LUTs properly, we can create a circuit that delays GPIO from outputting high with desired latency.

As shown in Figure 11, because smart I/O can operate in DeepSleep, you can use it to activate GPIO while the CPU is in DeepSleep mode.

Figure 11. Smart I/O-based cyclic wakeup operation​

Figure 11

Smart I/O configuration in cyclic wakeup​

The data unit (DU) can be used as a counter to delay “H” output. However, the DU is only 8-bit counter. During DeepSleep, because the source clock of smart I/O is ILO with frequency of 32 kHz, the DU can count for maximum interval as follows:

2 8 32 × 10 3 × 10 3 = 8 [ m s ]

Therefore, for applications that require cyclic wakeup period larger than 8 ms, you need extra bits for the counter.

Thus, for this example, an 11-bit timer equivalent circuitry by smart I/O called “sensor activation circuitry” is implemented. An 11-bit counter equivalent circuitry can generate delay up to 32 ms. Figure 12 shows the operation of the circuitry. Here, ‘DAT’ is the upper limit of the DU. DAT is configured by the SMARTIO_PRTx_DATA register. A single clock pulse is output at the data unit tr_out when the count value is equal to DAT.

Figure 12. Operation of sensor activation circuitry​

In this use case, the circuitry receives one signal from HSIOM named the “sensor_io_clr” signal, with active HIGH, which is used to clear the output of LUT3[1], i.e., the sensor activation output. The following I/O port and HSIOM signal are used:

  • smartio_data[1] = sensor_io (to I/O port, i.e., external sensor activation port)
  • chip_data[1] = sensor_io_clr (from HSIOM, manipulated by the CPU to clear ‘sensor_io’)

Figure 13 shows the connection and functional logic of each LUT3 and DU in this circuitry.

Figure 13. Logical example of a sensor activation circuitry​

The data unit operates in INCR_WRAP mode. This mode increments the data by 1 from an initial value (DATA 0) until it reaches a final value (DATA 1). When the count value matches the final value, it wraps around to DATA 0.

In this circuitry, the data unit carries the lower 8 bits of the 11-bit counter, LUT3[0], LUT3[1], LUT3[3] stands for the 9th, 10th, and 11th bit of the 11-bit counter. The output of LUT3[1], i.e., the 11th bit of the counter, is connected to the GPIO port to activate the external sensor. Figure 14 shows the signal path in this use case.

Figure 14. Signal path of sensor activation circuitry​

Figure 14

Table 9, Table 10, Table 11 and Table 12 show the truth table of each LUT3. The bold in the table indicate an invalid pattern.

Table 9. Lookup table LUT3 [0]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

LUT3[0] out

LUT3[0] out

DU tr_out

0

0

0

0

0

0

1

1

0

1

0

0

0

1

1

0

1

0

0

0

1

0

1

0

1

1

0

1

1

1

1

0

Table 10. Lookup table LUT3 [1]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

LUT3[1] out

LUT3[0] out

DU tr_out

0

0

0

0

0

0

1

0

0

1

0

1

0

1

1

0

1

0

0

1

1

0

1

0

1

1

0

1

1

1

1

0

Table 11. Lookup table LUT3 [2]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

LUT3[1] out

LUT3[0] out

DU tr_out

0

0

0

0

0

0

1

0

0

1

0

0

0

1

1

0

1

0

0

0

1

0

1

0

1

1

0

0

1

1

1

1

Table 12. Lookup table LUT3 [3]​

Tr0_in

Tr1_in

Tr2_in

Tr_out

LUT3[3] out

LUT3[2] out

CHIP_ DATA[0]

0

0

0

0

0

0

1

0

0

1

0

0

0

1

1

1

1

0

0

1

1

0

1

1

1

1

0

1

1

1

1

0

The H output delayed by the sensor activation circuitry can be calculated as follows:

delay=4×DAT1-DAT032=DAT1-DAT08[ms]

Therefore, you can configure DAT1 and DAT0 (usually set to ‘0’) to satisfy the sensor stabilization waiting time as in the rough estimation as follows:

delay= TCyclic Wakeup period-Tsensor stabilization wait

∴DAT1=8×(TCyclic Wakeup period-Tsensor stabilization wait)
Sensor activation circuitry in cyclic wakeup operation​

Using the sensor activation circuitry constructed in the previous section, the operation of cyclic wakeup can be enhanced as shown in Figure 15.

Figure 15. Cyclic wakeup operation with smart I/O usage​

Figure 15 Figure 15

Note: The gray box in the flowchart indicates a hardware operation. Therefore, processing with software is not required.

The GPIO is activated by smart I/O while the CPU is still in DeepSleep mode and the sensor’s stabilization time can be satisfied just by adjusting DAT0 and DAT1 properly. The behavior of the GPIO is now isolated from the operation of the CPU; this makes the software flow less complex.

For example, the CPU doesn’t need to go to Sleep mode after activating the GPIO to cut back the current consumption if a long sensor waiting time is required.

Configuration and example code​

Table 13 lists the parameters and Table 14 lists the functions of the configuration part in SDL for smart I/O in cyclic wakeup.

Table 13. List of smart I/O in cyclic wakeup configuration parameters​

Parameters

Description

Value

.sysIntSrc

Interrupt setting for event generator

evtgen_0_interrupt_dpslp_IRQn

.intIdx

CPUIntIdx4_IRQn

.isEnabled

true

.frequencyRef

clk_ref

8000000ul

.frequencyLf

clk_lf

32000ul

.frequencyTick

Event generator clock (clk_ref_div)

32000ul

.ratioControlMode

Event generator ratio control mode

CY_EVTGEN_RATIO_CONTROL_SW

.ratioValueDynamicMode

Event generator dynamic mode

CY_EVTGEN_RATIO_DYNAMIC_MODE0

.functionalitySelection

Event generator select functionality

CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY

.triggerOutEdge

Event generator trigger

CY_EVTGEN_EDGE_SENSITIVE

.valueDeepSleepComparator

Initializes comparator structure

DPSLP_COMP_VAL

.valueActiveComparator

Initializes comparator structure

ACTIVE_COMP_VAL

lutCfgLut0.opcode

Configures LUT3[0] operation mode setting

CY_SMARTIO_LUTOPC_GATED_OUT

lutCfgLut0.lutMap

Configures LUT3[0] output pattern setting

0x42ul

lutCfgLut0.tr0

Configures LUT3[0] tr0 input

CY_SMARTIO_LUTTR_DU_OUT

lutCfgLut0.tr1

Configures LUT3[0] tr1 input

CY_SMARTIO_LUTTR_LUT0_OUT

lutCfgLut0.tr2

Configures LUT3[0] tr2 input

CY_SMARTIO_LUTTR_LUT0_OUT

lutCfgLut3.opcode

Configures LUT3[3] operation mode setting

CY_SMARTIO_LUTOPC_GATED_OUT

lutCfgLut3.lutMap

Configures LUT3[3] output pattern setting

0x78ul

lutCfgLut3.tr0

Configures LUT3[3] tr0 input

CY_SMARTIO_LUTTR_DU_OUT

lutCfgLut3.tr1

Configures LUT3[3] tr1 input

CY_SMARTIO_LUTTR_LUT0_OUT

lutCfgLut3.tr2

Configures LUT3[3] tr2 input

CY_SMARTIO_LUTTR_LUT3_OUT

lutCfgLut2.opcode

Configures LUT3[2] operation mode setting

CY_SMARTIO_LUTOPC_COMB

lutCfgLut2.lutMap

Configures LUT3[2] output pattern setting

0x80ul

lutCfgLut2.tr0

Configures LUT3[2] tr0 input

CY_SMARTIO_LUTTR_DU_OUT

lutCfgLut2.tr1

Configures LUT3[2] tr1 input

CY_SMARTIO_LUTTR_LUT0_OUT

lutCfgLut2.tr2

Configures LUT3[2] tr2 input

CY_SMARTIO_LUTTR_LUT3_OUT

lutCfgLut1.opcode

Configures LUT3[1] operation mode setting

CY_SMARTIO_LUTOPC_GATED_OUT

lutCfgLut1.lutMap

Configures LUT3[1] output pattern setting

0x54ul

lutCfgLut1.tr0

Configures LUT3[1] tr0 input

CY_SMARTIO_LUTTR_CHIP1

lutCfgLut1.tr1

Configures LUT3[1] tr1 input

CY_SMARTIO_LUTTR_LUT1_OUT

lutCfgLut1.tr2

Configures LUT3[1] tr2 input

CY_SMARTIO_LUTTR_LUT2_OUT

lutCfgDu.tr0

Configures DU input trigger 0 source selection

CY_SMARTIO_DUTR_LUT1_OUT

lutCfgDu.tr1

Configures DU input trigger 1 source selection

CY_SMARTIO_DUTR_ONE

lutCfgDu.data0

DU input DATA0 source selection

CY_SMARTIO_DUDATA_ZERO

lutCfgDu.data1

DU input DATA1 source selection

CY_SMARTIO_DUDATA_DATAREG

lutCfgDu.opcode

DU opcode

CY_SMARTIO_DUOPC_INCR_WRAP

lutCfgDu.size

DU width size is 8

CY_SMARTIO_DUSIZE_8

lutCfgDu.dataReg

DU DATA register value

0xFCul

Table 14. List of smart I/O in cyclic wakeup configuration functions​

Functions

Description

Remarks

CyclicWakeUp_SystemUpdate()

SystemUpdate for cyclic wakeup

See Code Listing 21

CyclicWakeUp_Operation()

Cyclic wakeup function

See Code Listing 22

Init_SmartIO()

Smart I/O module initialization

See Code Listing 23

Cy_SmartIO_Enable()

Enables smart I/O

See Code Listing 24

Init_SmartIO_Cfg()

Configures smart I/O

See Code Listing 25

Cy_SmartIO_Deinit()

Resets the smart I/O to default values

See Code Listing 26

Cy_GPIO_Inv()

Sets a pin output logic state to the inverse of the current output logic state

See Code Listing 27

Code Listing 19 demonstrates an example program to smart I/O in cyclic wakeup operation. See the architecture TRM and application note for GPIO, ADC and smart I/O.

Code Listing 19 Example of usage of smart I/O in cyclic wakeup​
operation

int main(void)
{
:
CyclicWakeUp_SystemUpdate(); /* SystemUpdate for Cyclic wakeup See Code Listing 21 */

Init_SmartIO(); /* Smart IO module initialization See Code Listing 23 */

Cy_SmartIO_Enable(SMART_IO_PORT); /* Configures Smart I/O See Code Listing 24 */

while(1 /*g_flagContinueCWK*/){
Cy_GPIO_Inv(DPSLP_IDC_PRT, DPSLP_IDC_PIN); /* See Code Listing 27 */
CyclicWakeUp_Operation(); /* Cyclic WakeUp function. See (a) of Figure 15. See Code Listing 22 */
}


for(;;)
{
Cy_GPIO_Inv(DPSLP_IDC_PRT, DPSLP_IDC_PIN);
for(uint32_t idx = 0ul; idx < 1000000ul; idx++ ){}
}

}
Code Listing 20 Event generator configration​
    /**
* \var cy_stc_evtgen_config_t evtgenConfig
* \brief Evtgen configuration
*/
/* Eventgenerator Configuration */
const cy_stc_evtgen_config_t evtgenConfig =
{

.frequencyRef = 8000000ul, /**< clk_ref = clk_hf1 = CLK_PATH2 (IMO) -> 8,000,000 for silicon */
.frequencyLf = 32000ul, /**< clk_lf = 32,000 for silicon */

.frequencyTick = 32000ul, /**< Setting 1,000,000 Hz for event generator clock (clk_ref_div) */
.ratioControlMode = CY_EVTGEN_RATIO_CONTROL_SW,
.ratioValueDynamicMode = CY_EVTGEN_RATIO_DYNAMIC_MODE0,
};

/**
* \var cy_stc_evtgen_struct_config_t evtgenStructureConfig
* \brief Evtgen structure configuration
*/
const cy_stc_evtgen_struct_config_t evtgenStructureConfig =
{
.functionalitySelection = CY_EVTGEN_DEEPSLEEP_FUNCTIONALITY,
.triggerOutEdge = CY_EVTGEN_EDGE_SENSITIVE,
.valueDeepSleepComparator = DPSLP_COMP_VAL, /**< In active functionality, this value is used for making period of interrupts/triggers */
/**< 32,000 / 1,000,000 (clk_ref_div) = 32[ms] */
.valueActiveComparator = ACTIVE_COMP_VAL, /**< In active functionality, this value is used for making period of interrupts/triggers */
/**< 40,000 / 1,000,000 (clk_ref_div) = 4[ms] */
};
Code Listing 21 CyclicWakeUp_SystemUpdate() function​
    /* SystemUpdate for Cyclic wakeup */
void CyclicWakeUp_SystemUpdate(void)
{

SRSS->unPWR_CTL2.stcField.u1LINREG_DIS = 0ul;
SRSS->unPWR_CTL2.stcField.u1BGREF_LPMODE = 1ul;

/*********************/
/* Clock Setthings */
/*********************/
/*** FLL disabling ***/
/* Disable Fll */
SRSS->unCLK_FLL_CONFIG.stcField.u1FLL_ENABLE = 0ul; /* 0 = disable */
SRSS->unCLK_FLL_CONFIG4.stcField.u1CCO_ENABLE = 0ul; /* 0 = disable */

/*********** Setting wait state for ROM **********/
CPUSS->unROM_CTL.stcField.u2SLOW_WS = 0ul;
CPUSS->unROM_CTL.stcField.u2FAST_WS = 0ul;

/*********** Setting wait state for RAM **********/
CPUSS->unRAM0_CTL0.stcField.u2SLOW_WS = 0ul;
CPUSS->unRAM0_CTL0.stcField.u2FAST_WS = 0ul;

#if defined (CPUSS_RAMC1_PRESENT) && (CPUSS_RAMC1_PRESENT == 1UL)
CPUSS->unRAM1_CTL0.stcField.u2SLOW_WS = 0ul;
CPUSS->unRAM1_CTL0.stcField.u2FAST_WS = 0ul;
#endif /* defined (CPUSS_RAMC1_PRESENT) && (CPUSS_RAMC1_PRESENT == 1UL) */

#if defined (CPUSS_RAMC2_PRESENT) && (CPUSS_RAMC2_PRESENT == 1UL)
CPUSS->unRAM2_CTL0.stcField.u2SLOW_WS = 0ul;
CPUSS->unRAM2_CTL0.stcField.u2FAST_WS = 0ul;
#endif /* defined (CPUSS_RAMC2_PRESENT) && (CPUSS_RAMC2_PRESENT == 1UL) */

/*********** Setting wait state for FLASH **********/
FLASHC->unFLASH_CTL.stcField.u4MAIN_WS = 0ul;

/*** Set clock LF source ***/
SRSS->unCLK_SELECT.stcField.u3LFCLK_SEL = CY_SYSCLK_LFCLK_IN_ILO0;

/*******************************************/
/* Deinitialize peripherals */
/*******************************************/
Cy_Evtgen_DeinitializeCompStruct(EVTGEN0, EVTGEN_COMP_STRUCT_NO);
Cy_Evtgen_Deinitialize(EVTGEN0);

/*******************************************/
/* Initialize and start Event generator */
/*******************************************/
Cy_Evtgen_Initialize(EVTGEN0,&evtgenConfig);

/*******************************************/
/* Initialize comparator structure */
/*******************************************/
Cy_Evtgen_InitializeCompStruct(EVTGEN0, EVTGEN_COMP_STRUCT_NO, &evtgenStructureConfig, &evtgenStruct0Context);
}
Code Listing 22 CyclicWakeUp_Operation() function​
    /* Cyclic WakeUp function */
void CyclicWakeUp_Operation(void)
{
/* confirm that output of LUT1 has been cleared */
while((LUT1_OUT_LED_PORT->unIN.u32Register >> (LUT1_OUT_LED_PIN)) & CY_GPIO_IN_MASK){};

/* clear chip_data_out[1] before entering deepsleep*/
LUT1_OUT_LED_PORT->unOUT_CLR.u32Register = CY_GPIO_OUT_MASK << LUT1_OUT_LED_PIN; /* See (c) of Figure 15. */

/* Put the system to DeepSleep */
{
/* put mcu in deepsleep */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
// SCB->SCR; /* dummy read +/
WaitCoreCycle(1ul);
__WFI(); /* See (a) of Figure 15. Set to the DeepSleep mode */

/* Start ADC by software trigger*/
Cy_Adc_Channel_SoftwareTrigger(&CYCLIC_ADC_POT_MACRO->CH[ADC_GROUP_FIRST_LOGICAL_CHANNEL]);

/* Clear evtgen deepsleep interrput */
Cy_Evtgen_ClearStructInterruptDeepSleep(EVTGEN0,EVTGEN_COMP_STRUCT_NO);
NVIC_ClearPendingIRQ(irq_cfg_evtgen_dpslp.intIdx);
}

/* Reconfigure the event generator for the next wake-up */
/* See (b) of Figure 15. */
{
g_EvtgenCompareValue = (uint32_t)(g_EvtgenCompareValue + DPSLP_COMP_VAL);

/* Disable deep sleep comparator */
EVTGEN0->COMP_STRUCT[EVTGEN_COMP_STRUCT_NO].unCOMP_CTL.stcField.u1COMP1_EN = 0ul;

/* Setting deep sleep comparator value */
EVTGEN0->COMP_STRUCT[EVTGEN_COMP_STRUCT_NO].unCOMP1.stcField.u32INT32 = g_EvtgenCompareValue;

/* Enable deep sleep comparator */
EVTGEN0->COMP_STRUCT[EVTGEN_COMP_STRUCT_NO].unCOMP_CTL.stcField.u1COMP1_EN = 1ul;
}

/* wait for ADC completion */
while(!CYCLIC_ADC_POT_MACRO->CH[ADC_GROUP_LAST_LOGICAL_CHANNEL].unINTR.stcField.u1GRP_DONE){};

/* set chip_data_out[1] to clear lut1_trout */
LUT1_OUT_LED_PORT->unOUT_SET.u32Register = CY_GPIO_OUT_MASK << LUT1_OUT_LED_PIN;

/* In this sample software, only check range comparison result for first ADC channel */
if(CYCLIC_ADC_POT_MACRO->CH[ADC_GROUP_FIRST_LOGICAL_CHANNEL].unINTR.stcField.u1CH_RANGE == 1ul) {
g_flagContinueCWK = false;
}

for (uint8_t ch = ADC_GROUP_FIRST_LOGICAL_CHANNEL; ch < (ADC_GROUP_FIRST_LOGICAL_CHANNEL + ADC_GROUP_NUMBER_OF_CHANNELS); ch++)
{
/* Clear interrupt source */
CYCLIC_ADC_POT_MACRO->CH[ch].unINTR.u32Register = 0xFFFFFFFFul;
}
}
Code Listing 23 Init_SmartIO() function​
    /* Smart IO module initialization */
void Init_SmartIO(void)
{
Cy_SmartIO_Deinit(SMART_IO_PORT); /* See Code Listing 26 */
Init_SmartIO_Cfg(); /* See Code Listing 25 */
}
Code Listing 24 Cy_SmartIO_Enable() function​
    /* Enable Smart I/O */
void Cy_SmartIO_Enable(volatile stc_SMARTIO_PRT_t* base)
{
un_SMARTIO_PRT_CTL_t workCTL = base->unCTL;
workCTL.stcField.u1ENABLED = CY_SMARTIO_ENABLE;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_DISABLE;
base->unCTL.u32Register = workCTL.u32Register;
}
Code Listing 25 Init_SmartIO_Cfg() function​
    cy_en_smartio_status_t Init_SmartIO_Cfg(void)
{
/* Configures Smart I/O */
/* Configure smart io to output H in deepsleep
* Using data unit and LUT0,1,2,3 to create a 11bit counter
* Data uint acts as lower 8 bit, count up from 0 to value written in DATA, reset to 0 at overflow
* LUT0 acts as 9th bit, LUT3 acts as 10th bit and LUT 1 act as 11th bit
* output of LUT1 is smart io output, i.e. P15.1 or TP202 on the CPU board
*/

cy_stc_smartio_ducfg_t lutCfgDu;
cy_stc_smartio_lutcfg_t lutCfgLut0;
cy_stc_smartio_lutcfg_t lutCfgLut1;
cy_stc_smartio_lutcfg_t lutCfgLut2;
cy_stc_smartio_lutcfg_t lutCfgLut3;

cy_stc_smartio_config_t smart_io_cfg;
cy_en_smartio_status_t retStatus = (cy_en_smartio_status_t)0xFF;

/* initialize the Smart IO structure */
memset(&lutCfgDu, 0, sizeof(cy_stc_smartio_ducfg_t));
memset(&lutCfgLut0, 0, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut1, 0, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut2, 0, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut3, 0, sizeof(cy_stc_smartio_lutcfg_t));
memset(&smart_io_cfg, 0, sizeof(cy_stc_smartio_config_t));

/* Active clock source is selected */
smart_io_cfg.clkSrc = (cy_en_smartio_clksrc_t)CY_SMARTIO_CLK_LFCLK;

/* Bypass channel mask is 11111100 for Pin0 and Pin1 */
smart_io_cfg.bypassMask = SMARTIO_BYPASS_CH_MASK;

smart_io_cfg.hldOvr = true;

/*************************** LUT0 config ***************************/
/* Configure LUT3 [0] */
lutCfgLut0.opcode = CY_SMARTIO_LUTOPC_GATED_OUT;

lutCfgLut0.lutMap = 0x42ul;

lutCfgLut0.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_DU_OUT;
lutCfgLut0.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT0_OUT;
lutCfgLut0.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT0_OUT;
smart_io_cfg.lutCfg[0] = &lutCfgLut0;

/*************************** LUT3 config ***************************/
/* Configure LUT3 [3] */
lutCfgLut3.opcode = CY_SMARTIO_LUTOPC_GATED_OUT;

lutCfgLut3.lutMap = 0x78ul;

lutCfgLut3.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_DU_OUT;
lutCfgLut3.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT0_OUT;
lutCfgLut3.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT3_OUT;
smart_io_cfg.lutCfg[3] = &lutCfgLut3;

/*************************** Lut2 config ***************************/
/* Configure LUT3 [2] */
lutCfgLut2.opcode = CY_SMARTIO_LUTOPC_COMB;

lutCfgLut2.lutMap = 0x80ul;

lutCfgLut2.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_DU_OUT;
lutCfgLut2.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT0_OUT;
lutCfgLut2.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT3_OUT;
smart_io_cfg.lutCfg[2] = &lutCfgLut2;

/*************************** LUT1 config ***************************/
/* Configure LUT3 [1] */
lutCfgLut1.opcode = CY_SMARTIO_LUTOPC_GATED_OUT;

lutCfgLut1.lutMap = 0x54ul;

lutCfgLut1.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_CHIP1;
lutCfgLut1.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT1_OUT;
lutCfgLut1.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT2_OUT;
smart_io_cfg.lutCfg[1] = &lutCfgLut1;

/* Data Unit (DU) configuration structure */
/* Configure DU */
lutCfgDu.tr0 = CY_SMARTIO_DUTR_LUT1_OUT, /*CY_SMARTIO_DUTR_DU_OUT;*/ /**< DU input trigger 0 source selection */
lutCfgDu.tr1 = CY_SMARTIO_DUTR_ONE; /**< DU input trigger 1 source selection */
lutCfgDu.data0 = CY_SMARTIO_DUDATA_ZERO; /**< DU input DATA0 source selection */
lutCfgDu.data1 = CY_SMARTIO_DUDATA_DATAREG; /**< DU input DATA1 source selection */
lutCfgDu.opcode = CY_SMARTIO_DUOPC_INCR_WRAP; /**< DU op-code */
lutCfgDu.size = CY_SMARTIO_DUSIZE_8; /**< DU operation bit size */
lutCfgDu.dataReg = 0xFCul; /**< DU DATA register value */
smart_io_cfg.duCfg = &lutCfgDu;

}
Code Listing 26 Cy_SmartIO_De​
init() function

void Cy_SmartIO_Deinit(volatile stc_SMARTIO_PRT_t* base)
{
un_SMARTIO_PRT_CTL_t workCTL= {.u32Register = 0ul};
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE; /* Resets the Smart I/O to default values */
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = CY_SMARTIO_CLK_GATED;
workCTL.stcField.u8BYPASS = CY_SMARTIO_CHANNEL_ALL;
base->unCTL.u32Register = workCTL.u32Register;

base->unSYNC_CTL.u32Register = CY_SMARTIO_DEINIT;
for(uint8_t idx = CY_SMARTIO_LUTMIN; idx < CY_SMARTIO_LUTMAX; idx++)
{
base->unLUT_SEL[idx].u32Register = CY_SMARTIO_DEINIT;
base->unLUT_CTL[idx].u32Register = CY_SMARTIO_DEINIT;
}
base->unDU_SEL.u32Register = CY_SMARTIO_DEINIT;
base->unDU_CTL.u32Register = CY_SMARTIO_DEINIT;
base->unDATA.u32Register = CY_SMARTIO_DEINIT;
}
Code Listing 27 Cy_GPIO_Inv() function​
    __STATIC_INLINE void Cy_GPIO_Inv(volatile stc_GPIO_PRT_t* base, uint32_t pinNum)
{
base->unOUT_INV.u32Register = CY_GPIO_OUT_MASK << pinNum; /*Set a pin output logic state to the inverse of the current output logic state */
}

CAN wakeup operation​

As long as there is any communication on the CAN bus, the ECU is awake. If CAN communication occurs while the ECU is in low-power mode, ECU must wake up from low-power mode. This section describes an implementation example of the CAN wakeup operation by using TRAVEO™ T2G family MCUs.

TRAVEO™ T2G family MCUs have the following pins for wakeup:

  • Up to 4 pins to wake up from Hibernate mode

See the datasheet for the supported number of pins that can wake up the device from Hibernate mode.

  • GPIO pins to wake up from DeepSleep mode

See the datasheet for the supported number of GPIO that can wake up the device from DeepSleep mode.

The CAN block cannot detect a wakeup condition when the MCU is DeepSleep or Hibernate mode. To support CAN wakeup, MCU should use the function of GPIO interrupt or WAKEUP pin.

Figure 16 shows the example of CAN wakeup from DeepSleep.

Figure 16. CAN wakeup from DeepSleep mode​

Figure 16

The software sets the I/O port and GPIO interrupt before the MCU enters low- power mode. The CAN receive functionality is disabled. After that, when the MCU detects a wakeup signal while in low-power mode, the MCU wakes up from low-power mode. After that, software enables the CAN receive functionality and CAN communication starts. For more details on CAN and GPIO, see architecture TRM.

Configuration and example code​

Table 15 lists the functions of the configuration part in SDL for CAN wakeup operation. In this example, the GPIO and CAN RX pins are common.

Table 15. List of CAN wakeup operation configuration functions​

Functions

Description

Remarks

GpioIntHandler()

Handler for GPIO interrupts

See Code Listing 30

Cy_GPIO_Pin_Init()

Initialize all pin configuration setting for the pin

See Code Listing 30

Cy_SysPm_DeepSleep()

Puts the system to DeepSleep

See Code Listing 31

Code Listing 28 demonstrates an example program to CAN wakeup operation. See the architecture TRM and application note for CAN.

Code Listing 28 Example to CAN wakeup operation​
    int main(void)
{
/* Wakeup by GPIO interrupt. See (d) of Figure 16. See Code Listing 29 */

Cy_SysInt_SetSystemIrqVector(gpio_irq_cfg.sysIntSrc, GpioIntHandler);

for(;;)
{

/* Stop CAN */
/* CAN Clock stop request */
/* Stop CANFD. See (a) of Figure 16. */
CY_CANFD_UNIT->unCTL.stcField.u8STOP_REQ = CY_CANFD_STOP_REQ_BIT;
while(CY_CANFD_UNIT->unSTATUS.stcField.u8STOP_ACK != CY_CANFD_STOP_REQ_BIT);


/* Change CAN Rx Port to GPIO */
/* Change CAN RX to GPIO. See (b) of Figure 16. See Code Listing 30 */
Cy_GPIO_Pin_Init(CY_CANFD0_RX_PORT, CY_CANFD0_RX_PIN, &user_button_port_pin_cfg);

/* Put the system to DeepSleep */
/* Enter DeepSleep mode. See (c) of Figure 16. See Code Listing 31 */
Cy_SysPm_DeepSleep(CY_SYSPM_WAIT_FOR_INTERRUPT);

/* Change GPIO to CAN Rx Port */
/* Change GPIO to CAN RX. See (e) of Figure 16. See Code Listing 30 */
Cy_GPIO_Pin_Init(can_pin_cfg[0].portReg, can_pin_cfg[0].pinNum, &can_pin_cfg[0].cfg);

/* CAN Clock start request */
CY_CANFD_UNIT->unCTL.stcField.u8STOP_REQ = 0x00ul;
while(CY_CANFD_UNIT->unSTATUS.stcField.u8STOP_ACK != 0x00ul);

/* Start CAN */
CY_CANFD_TYPE->M_TTCAN.unCCCR.stcField.u1INIT = 0ul;

/* Start CANFD. See (f) of Figure 16 */
while(CY_CANFD_TYPE->M_TTCAN.unCCCR.stcField.u1INIT != 0ul);
}
}
}
Code Listing 29 GpioIntHandler() function​
    /* Handler for GPIO interrupts */
void GpioIntHandler(void)
{
uint32_t intStatus;

/* If falling edge detected */
intStatus = Cy_GPIO_GetInterruptStatusMasked(CY_CANFD0_RX_PORT, CY_CANFD0_RX_PIN);
if (intStatus != 0ul)
{
Cy_GPIO_ClearInterrupt(CY_CANFD0_RX_PORT, CY_CANFD0_RX_PIN);
}
}

Code Listing 30 Cy_GPIO_Init() function​
    cy_en_gpio_status_t Cy_GPIO_Pin_Init(volatile stc_GPIO_PRT_t *base, uint32_t pinNum, const cy_stc_gpio_pin_config_t *config)
{
/* Initialize all pin configuration setting for the pin */
cy_en_gpio_status_t status = CY_GPIO_SUCCESS;

if((NULL != base) && (NULL != config))
{
Cy_GPIO_Write(base, pinNum, config->outVal);
Cy_GPIO_SetHSIOM(base, pinNum, config->hsiom);
Cy_GPIO_SetVtrip(base, pinNum, config->vtrip);
Cy_GPIO_SetSlewRate(base, pinNum, config->slewRate);
Cy_GPIO_SetDriveSel(base, pinNum, config->driveSel);
Cy_GPIO_SetDrivemode(base, pinNum, config->driveMode);
Cy_GPIO_SetInterruptEdge(base, pinNum, config->intEdge);
Cy_GPIO_ClearInterrupt(base, pinNum);
Cy_GPIO_SetInterruptMask(base, pinNum, config->intMask);
}
else
{
status = CY_GPIO_BAD_PARAM;
}

return(status);
}
Code Listing 31 Cy_SysPm_DeepSleep() function​
    /* Sets a CPU core to the DeepSleep mode */
cy_en_syspm_status_t Cy_SysPm_DeepSleep(cy_en_syspm_waitfor_t waitFor)
{
uint32_t interruptState;
cy_en_syspm_status_t retVal = CY_SYSPM_SUCCESS;

/* Call the registered callback functions with
* the CY_SYSPM_CHECK_READY parameter.
*/
if(0u != currentRegisteredCallbacksNumber)
{
retVal = Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_CHECK_READY);
}

/* The device (core) can switch into the deep sleep power mode only when
* all executed registered callback functions with the CY_SYSPM_CHECK_READY
* parameter returned CY_SYSPM_SUCCESS.
*/
if(retVal == CY_SYSPM_SUCCESS)
{
/* Call the registered callback functions with the CY_SYSPM_BEFORE_TRANSITION
* parameter. The return value is ignored.
*/
interruptState = Cy_SysLib_EnterCriticalSection();
if(0u != currentRegisteredCallbacksNumber)
{
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_BEFORE_ENTER);
}

#if(0u != CY_CPU_CORTEX_M0P)

/* The CPU enters the deep sleep mode upon execution of WFI/WFE */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

if(waitFor != CY_SYSPM_WAIT_FOR_EVENT)
{
__WFI();
}
else
{
__WFE();
}
#else

/* Repeat WFI/WFE instructions if wake up was not intended.
* Cypress Ticket #272909
*/
do
{
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;

if(waitFor != CY_SYSPM_WAIT_FOR_EVENT)
{
__WFI();
}
else
{
__WFE();
}
} while (0); //rmkn _FLD2VAL(CPUSS_CM4_PWR_CTL_PWR_MODE, CPUSS->unCM4_PWR_CTL.u32Register) == CY_SYSPM_CM4_PWR_CTL_PWR_MODE_RETAINED);

#endif /* (0u != CY_CPU_CORTEX_M0P) */

Cy_SysLib_ExitCriticalSection(interruptState);

/* Call the registered callback functions with the CY_SYSPM_AFTER_TRANSITION
* parameter. The return value is ignored.
*/
if(0u != currentRegisteredCallbacksNumber)
{
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_AFTER_EXIT);
}
}
else
{
/* Execute callback functions with the CY_SYSPM_CHECK_FAIL parameter to
* undo everything done in the callback with the CY_SYSPM_CHECK_READY
* parameter. The return value is ignored.
*/
(void) Cy_SysPm_ExecuteCallback(CY_SYSPM_DEEPSLEEP, CY_SYSPM_CHECK_FAIL);
retVal = CY_SYSPM_FAIL;
}
return retVal;
}

2 Reset occurs when the counter value reaches UPPER_LIMIT or when the counter is cleared before LOWER_LIMIT.

3 Interrupt occurs when the counter value reaches WARN_LIMIT.

4 The fault manager converts this to a high-priority interrupt (such as non- mskable interrupt, NMI) that gives the processor an opportunity to return to a safe state, such as halting memory writes and releasing peripherals.

5 Interrupt occurs when the BIT specified by MCWDT2_CTR2_CONFIG [20:16] toggles.

Glossary​

Table 16. Glossary

Terms

Description

ADC

Analog-to-digital converter. See the “SAR ADC” chapter of the architecture TRM for details.

Basic WDT

Basic watchdog timer. See the “Watchdog Timer” chapter of the architecture TRM for details.

BOD

Brown-out detection. See the “Power supply and monitoring” chapter of the architecture TRM for details.

CPUSS

CPU subsystem. See the “CPU subsystem” section of the architecture TRM for details.

ECO

External crystal oscillator. See the “Clocking system” chapter of the architecture TRM for details.

EVTGEN

Event generator. See the “Event generator” chapter of the architecture TRM for details.

FLL

Frequency-locked loop. See the “Clocking system” chapter of the architecture TRM for details.

GPIO

General-purpose input/output. See the “I/O system” chapter of the architecture TRM for details.

HF

High-frequency clock. See the “Clocking system” chapter of the architecture TRMfor details.

ILO

Internal low-speed oscillators. See the “Clocking system” chapter of the architecture TRMfor details.

IMO

Internal main oscillator. See the “Clocking system” chapter of the architecture TRM for details.

LF

Low-frequency clock. See the “Clocking system” chapter of the architecture TRM for details

LPACTIVE

Low-power active. See the “Device power modes” chapter of the architecture TRM for details.

LV supplies

Low-voltage supplies.

LVD

Low-voltage detection. See the “Power supply and monitoring” chapter of the architecture TRM for details.

MCWDT

Multi-counter watchdog timer. See the “Watchdog timer” chapter of the architecture TRM for details.

Pending interrupt

Interrupt of pending state. See the “Interrupts” chapter of the architecture TRM for details.

PLL

Phase-locked loop. See the “Clocking system” chapter of the architecture TRM for details.

POR

Power-on reset. See the “Reset system” chapter of the architecture TRM for details.

RTC

Real-time clock. See the “Real-time clock” chapter of the architecture TRM for details.

SCB

Serial communication block. See the “Serial communication block (SCB)” chapter of the architecture TRM for details.

SRSS

System resources subsystem. See the “System resources subsystem” section of the architecture TRMfor details.

VDDD

Digital power supply.

WCO

Watch crystal oscillator. See the “Clocking system” chapter of the architecture TRM for details.

WDT

Watchdog timer reset. See the “Watchdog timer” chapter of the architecture TRM for details.

WFE

Wait for event instruction

WFI

Wait for interrupt instruction

WIC

Wakeup interrupt controller. See the “Interrupts” chapter of the architecture TRM for details.

XRES

External reset I/O pin. See the “Reset system” chapter of the architecture TRM for details.

The following are the TRAVEO™ T2G family series datasheets and technical reference manuals. Contact Technical Support to obtain these documents.

  1. Device datasheets:
  2. Technical reference manuals:
  3. Application notes:

Other references​

A sample driver library (SDL) including startup as sample software to access various peripherals is provided. SDL also serves as a reference, to customers, for drivers that are not covered by the official AUTOSAR products. The SDL cannot be used for production purposes as it does not qualify to any automotive standards. The code snippets in this application note are part of the SDL. Contact Technical Support to obtain the SDL.

Revision history​

Document version

Date of release

Description of changes

**

2019-02-28

New application note.

*A

2019-11-05

Updated Associated Part Family as “Traveo™ II Family CYT2B/CYT4B/CYT4D Series”.

Added target part numbers “CYT4D Series” related information in all instances across the document.

Updated Power Modes Transition:

Added “CAN wakeup operation”.

*B

2020-03-12

Updated associated part family as “TRAVEO™ T2G family CYT2/CYT3/CYT4 series”.

Changed target part numbers from “CYT2B/CYT4B/CYT4D series” to “CYT2/CYT4 Series” in all instances across the document.

Added target part numbers “CYT3 Series” related information in all instances across the document.

*C

2020-12-03

Updated power modes transition:

Updated cyclic wakeup Operation:

Added “Usage of smart I/O in cyclic wakeup”.

*D

2021-04-19

Updated to Infineon template.

*E

2021-10-21

Added example of SDL code and description in all instances.

*F

2023-11-13

Template update; no content update.

1 RTC (along with WCO) is supplied with VDDD and is available irrespective of the device power mode. RTC alarms can wake up the device from any power mode.

2 Reset occurs when the counter value reaches UPPER_LIMIT or when the counter is cleared before LOWER_LIMIT.

3 Interrupt occurs when the counter value reaches WARN_LIMIT.

4 The fault manager converts this to a high-priority interrupt (such as non- mskable interrupt, NMI) that gives the processor an opportunity to return to a safe state, such as halting memory writes and releasing peripherals.

5 Interrupt occurs when the BIT specified by MCWDT2_CTR2_CONFIG [20:16] toggles.