Skip to main content

AN220203 Smart I/O usage setup in TRAVEO™ T2G family

PDF File

About this document​

Scope and purpose​

AN220203 describes how to use Smart I/O in TRAVEO™ T2G MCUs. Smart I/O adds a programmable logic circuitry between a peripheral and a GPIO port, thereby integrating board-level glue logic.

Associated part family​

TRAVEO™ T2G family CYT2/CYT3/CYT4 series

Introduction​

This application note describes how to use and setup Smart I/O in Infineon TRAVEO™ T2G family CYT2/CYT3/CYT4 series MCUs.

Smart I/O adds programmable logic to an I/O port. Smart I/O integrates Boolean logic functionality such as AND, OR, and XOR into a port. It also pre- or post-processes the signals between high-speed I/O matrix (HSIOM) and I/O port. For example, Smart I/O can enable digital glue logic for input signals using multiple flip-flops without CPU intervention. HSIOM multiplexes GPIOs sharing multiple functions into peripheral devices selected by the user. See the Architecture Technical Reference Manual (TRM) for details of HSIOM.

To understand the functionality described and terminology used in this application note, see the Smart I/O chapter in the Architecture TRM. Figure 1 shows examples of typical signal paths.

Figure 1. Smart I/O interface​

Figure 1

Path 1: Implements self-contained logic functions that directly operate on I/O port signals

Path 2: Implements self-contained logic functions that operate on HSIOM signals

Path 3: Logic conversed HSIOM output signals route to I/O port

Path 4: Logic conversed I/O port input signals route to HSIOM

For each signal path, the Smart I/O function gives an option for a programmable output. This application note shows the example usage and configuration of the Smart I/O function.

Applications of Smart I/O​

Smart I/O can be used whenever simple logic operations and routing are required to be performed on signals to or from the I/O pins. Typical applications include the following:

  • Change routing to/from pins: This function allows rerouting signals from the fixed-function peripherals to non-dedicated pins on the same port.
  • Invert the polarity of signal: This function inverts the polarity of output signals, such as the SPI signal, before it goes out from a pin.
  • Clock or signal buffer: This function drives a GPIO input signal, which has to drive a heavier load for one pin, through two GPIO buffers.
  • Detect a pattern on pins: This function detects the patterns of several signal inputs and outputs the programmable signal depending on the result of detection.

These applications of Smart I/O can work in low-power mode (DeepSleep), therefore can be used as a wakeup interrupt.

Bypass of Smart I/O​

When the Smart I/O function is not used, it will be automatically bypassed by setting the SMARTIO_PRTx_CTL.ENABLE1 bit to “0”: Disabled. It is also possible to bypass any I/O pin in the Port group using the SMARTIO_PRTx_CTL.BYPASS bits. When BYPASS bits are set to “1”: Bypass, HSIOM and I/O port are connected directly.

Note that the bypass setting must be configured before enabling the Smart I/O. (SMARTIO_PRTx_CTL.ENABLE set to “1”: Enabled)

Table 1 shows the description of the SMARTIO_PRTx_CTL register for bypass setting. See the Registers TRM for details.

Table 1. Register for Bypass setting​

Register

Bit Field

Setting

SMARTIO_PRTx_CTL

BYPASS [7:0]

Bypass Smart I/O

‘0’: No bypass (Smart I/O is present in the signal path)

‘1’: Bypass (Smart I/O is absent in the signal path)

ENABLED [31]

Enable Smart I/O

0: Disabled (Signals are bypassed: default)

1: Enabled (Should only be set to ‘1’ when Smart I/O is completely configured.)

Structure of Smart I/O​

Figure 2 shows the block diagram of Smart I/O. Smart I/O is positioned in the signal path between the HSIOM and the I/O port.

Figure 2. Block Diagram of Smart I/O​

Figure 2

The Smart I/O consists of the following components:

  • Clock and reset
  • Synchronizer (Sync)
  • 3-input lookup tables (LUT3 [x]): x = 0 to 7
  • Data unit (DU)

Smart I/O is implemented for the specified I/O cell. Smart I/O can provide programmable signals to HSIOM and I/O port with a combination of these components. See the Package Pin List and Alternate Functions of Device Datasheet for details on the I/O port that can be used as Smart I/O.

The io_data_in [7:0] is the input signal from the I/O port, while the chip_data [7:0] is the input signal from HSIOM. These signals are input to Smart I/O via the Sync components (synchronizer). The smartio_data [7:0] is the output signal from Smart I/O. These signals are routed or modified by Smart I/O and output to the I/O port or HSIOM.

The clk_block is used for all components in Smart I/O. The clk_block can be selected from the I/O port input signals (io_data_in [7:0]), HSIOM input signals (chip_data [7:0]), clk_smartio, and clk_lf. The clk_smartio is derived from the system clock (clk_sys/CLK_HF) using a peripheral clock divider, and the clk_smartio is input in the Clock and Reset block. See the Clocking system chapter of Architecture TRM for details on clk_smartio and clk_lf.

Eight lookup tables (LUT3 [x]) are implemented for each Smart I/O unit. LUT3 [x] can provide the programmable output, and it can decide the connection of signals between HSIOM and the I/O port. This means that the eight lookup tables offer a flexible routing combination of input channel and output.

The data unit can provide enhanced functionality for the output signal. Clock and Reset block is used to synchronize the signals of HSIOM, I/O port, and each block in Smart I/O. Synchronizer controls the synchronization/asynchronization of the HSIOM input and the I/O port input.

Clock and Reset​

Smart I/O can provide reset signals and clock selection. Figure 3 shows the selection logic of the configuration of clock and reset.

Figure 3. Functional image of clock and reset setting​

Figure 3

When io_data_in [7:0] and chip_data [7:0] are selected as the clock source, the clocks have no associated reset. When clk_smartio is selected as the clock source, either rst_sys_act_n or rst_sys_dpslp_n can be used depending on the operating power mode: Active or DeepSleep. When clk_lf is selected as the clock source, rst_lf_dpslp_n can be used. The clock (clk_block) and reset (rst_block_n) can be set by the SMARTIO_PRTx_CTL.CLOCK_SRC [12:8] register.

The following clock sources are available for selection:

  • io_data_in [7:0]: These are I/O port input signals.
  • chip_data [7:0]: These are HSIOM input signals.
  • clk_smartio: This clock is derived from the system clock clk_sys/CLK_HF.
  • clk_lf: This clock is a low-frequency system clock. This clock is only available in DeepSleep mode.

The following reset sources are available for selection:

  • rst_sys_act_n: Smart I/O is active only in Active power mode with the clock from the peripheral divider.
  • rst_sys_dpslp_n: Smart I/O is active in all power modes except in DeepSleep mode with the clock from the peripheral divider.
  • rst_lf_dpslp_n: Smart I/O is active in all power modes with the clock from ILO.

Table 2 shows the configuration of the SMARTIO_PRTx_CTL.CLOCK_SRC [12:8] register. See the Registers TRM for details.

Table 2. Register for Clock and Reset setting​

Register

Bit Field

Setting

SMARTIO_PRTx_CTL

CLOCK_SRC [12:8]

Clock (clk_block)/Reset (rst_block_n) source selection:

  • 0 ... 7: io_data_in[0]/1 ... io_data_in[7]/’1’
  • 8... 15: chip_data[0]/1 ...chip_data[7]/’1’
  • 16: clk_smartio/rst_sys_act_n
  • 17: clk_smartio/rst_sys_dpslp_n
  • 19: clk_lf/rst_lf_dpslp_n
  • 20... 30: Clock source is a constant ‘0’.
  • 31: asynchronous mode/”1”. Select this when a clockless operation is configured.

Synchronizer​

Each input signal at the I/O port and HSIOM can be used either in synchronous or asynchronous mode. The synchronizer synchronizes the input signal with the Smart I/O clock (clk_block).

Table 3 shows synchronizer setting register and configuration. See the Registers TRM for details.

Table 3. Register for Synchronizer Setting​

Register

Bit Field

Setting

SMARTIO_PRTx_SYNC_CTL

IO_SYNC_EN [7:0]

Synchronization of the io_data_in [7:0] signals with clk_block

0: No synchronization

1: Synchronization

CHIP_SYNC_EN [15:8]

Synchronization of the chip_data [7:0] signals with clk_block

0: No synchronization

1: Synchronization

3-inputs lookup tables (LUT3 [x])​

Each LUT3 [x] has three inputs and one output. All inputs (Tr0_in, Tr1_in, Tr2_in) of each LUT3 [x] block should be selected. If there is only one input operation, provide the input to all three input sources (Tr0_in, Tr1_in, Tr2_in). Each LUT3 [x] takes three input signals and generates an output based on the configuration set in register. Figure 4 shows the basic block diagram of each LUT3 [x]. The output pattern can be set by the register.

Figure 4. LUT3 [x] Block Diagram​

Figure 4

LUT3 [x] output configuration​

Output signal (Tr_out) of LUT3 [x] can be programmed using SMARTIO_PRTx_LUT_CTLy.LUT[7:0]2 based on three input sources (Tr2_in, Tr1_in, Tr0_in). Table 4 shows example of setting each LUT3 [x].

Table 4. LUT3 [x] output setting​

Tr 2_in

Tr 1_in

Tr 0_in

Tr_out

Tr_out(Example 1)

Tr_out(Example 2)

0

0

0

A

0

0

0

0

1

B

0

0

0

1

0

C

0

1

0

1

1

D

0

0

1

0

0

E

1

1

1

0

1

F

1

0

1

1

0

G

1

0

1

1

1

H

1

0

Eight output patterns (A to H) are generated for three input signals. Each output from A to H is a Boolean value of 0 or 1. This output pattern value [H, G, F, E, D, C, B, A] is set in the LUT [7:0].

In case of example 1, the output pattern is [H, G, F, E, D, C, B, A] = [1, 1, 1, 1, 0, 0, 0, 0]. Therefore, the value "0xF0" is set to LUT [7:0]. Also, in the case of example 2, the output pattern is [H, G, F, E, D, C, B, A] = [0, 0, 0, 1, 0, 1, 0, 0]. Therefore, the set value is "0x14" to LUT [7:0].

Table 5 shows the SMARTIO_PRTx_LUT_CTLy.LUT [7:0] register for LUT3 [x] output setting. See the Registers TRM for details.

Table 5. Register for Setting the Output from LUT3 [x]​

Register

Bit Field

Setting

SMARTIO_PRTx_LUT_CTLy

LUT [7:0]

LUT3 [x] configuration. Depending on the LUT opcode (LUT_OPC), internal state and LUT3 [x] input signals tr0_in, tr1_in, and tr2_in, the LUT3 [x] configuration is used to determine the LUT3[x] output signal and the next sequential state.

LUT3 [x] input selection​

The input sources (Tr0_in, Tr1_in, Tr2_in) of each LUT3 [x] can be selected from the following:

  • Data unit output
  • Other LUT3 [x] output signal (Tr_out)
  • Input signal from HSIOM (chip_data [7:0])
  • Input signal from I/O port (io_data_in [7:0])

LUT3[7] to LUT3[4] operate on io_data/chip_data[7] to io_data/chip_data[4], whereas LUT3[3] to LUT3[0] operate on io_data/chip_data[3] to io_data/chip_data[0].

The input sources can be configured with LUT_TR0_SEL [3:0], LUT_TR1_SEL [11:8], and LUT_TR2_SEL [19:16] in the SMARTIO_PRTx_LUT_SELy register. Table 6 shows the SMARTIO_PRTx_LUT_SELy register and input selection setting. Note that Data Unit output can only be input to tr0_in. See the Registers TRM for details.

Table 6. Register for LUT3 [x] Input Source Setting​

Register

Bit Field

Setting

SMARTIO_PRTx_LUT_SELy

LUT_TR0_SEL [3:0]

LUT3 [x] input signal tr0_in source selection:

0: Data unit output

1: LUT3 [1] output

2: LUT3 [2] output

3: LUT3 [3] output

4: LUT3 [4] output

5: LUT3 [5] output

6: LUT3 [6] output

7: LUT3 [7] output

8: chip_data [0] (for LUT3 [0], [1], [2], [3]); chip_data [4] (for LUT3 [4], [5], [6], [7])

9: chip_data [1] (for LUT3 [0], [1], [2], [3]); chip_data [5] (for LUT3 [4], [5], [6], [7])

10: chip_data [2] (for LUT3 [0], [1], [2], [3]); chip_data [6] (for LUT3 [4], [5], [6], [7])

11: chip_data [3] (for LUT3 [0], [1], [2], [3]); chip_data [7] (for LUT3 [4], [5], [6], [7])

12: io_data_in [0] (for LUT3 [0], [1], [2], [3]); io_data_in [4] (for LUT3 [4], [5], [6], [7])

13: io_data_in [1] (for LUT3 [0], [1], [2], [3]); io_data_in [5] (for LUT3 [4], [5], [6], [7])

14: io_data_in [2] (for LUT3 [0], [1], [2], [3]); io_data_in [6] (for LUT3 [4], [5], [6], [7])

15: io_data_in [3] (for LUT3 [0], [1], [2], [3]); io_data_in [7] (for LUT3 [4], [5], [6], [7])

LUT_TR1_SEL [11:8] / LUT_TR2_SEL [19:16]

LUT3 [x] input signal tr1_in / tr2_in source selection:

0: LUT3 [0] output

1: LUT3 [1] output

2: LUT3 [2] output

3: LUT3 [3] output

4: LUT3 [4] output

5: LUT3 [5] output

6: LUT3 [6] output

7: LUT3 [7] output

8: chip_data [0] (for LUT3 [0], [1], [2], [3]); chip_data [4] (for LUT3 [4], [5], [6], [7])

9: chip_data [1] (for LUT3 [0], [1], [2], [3]); chip_data [5] (for LUT3 [4], [5], [6], [7])

10: chip_data [2] (for LUT3 [0], [1], [2], [3]); chip_data [6] (for LUT3 [4], [5], [6], [7])

11: chip_data [3] (for LUT3 [0], [1], [2], [3]); chip_data [7] (for LUT3 [4], [5], [6], [7])

12: io_data_in [0] (for LUT3 [0], [1], [2], [3]); io_data_in [4] (for LUT3 [4], [5], [6], [7])

13: io_data_in [1] (for LUT3 [0], [1], [2], [3]); io_data_in [5] (for LUT3 [4], [5], [6], [7])

14: io_data_in [2] (for LUT3 [0], [1], [2], [3]); io_data_in [6] (for LUT3 [4], [5], [6], [7])

15: io_data_in [3] (for LUT3 [0], [1], [2], [3]); io_data_in [7] (for LUT3 [4], [5], [6], [7])

Each LUT3 [x] has limited connections with input/output of HSIOM and I/O port signals. Sometimes, multiple LUT3 [x] are necessary for a complete flexible routing.

The LUT3 [x] and data unit do not include any combinatorial loops. However, when one LUT3 [x] interacts with the other or to the data unit, inadvertent combinatorial loops are possible. To overcome this limitation, the SMARTIO_PRTx_CTL.PIPELINE_EN bit is used. When set, all outputs (LUT3 [x] and data unit) are registered before branching out to other components. Table 7 shows PIPELINE_EN setting. This bit is set to “1” (Enabled) to ensure low power consumption, if Smart I/O is not used. See the Registers TRM for details.

Table 7. PIPELINE_EN Setting​

Register

Bit Field

Setting

SMARTIO_PRTx_CTL

PIPELINE_EN [25]

Enable for pipeline register:

0: Disabled (Register is bypassed)

1: Enabled (Default value)

LUT3 [x] operation​

Each LUT3 [x] has the following four operations selected by a 2-bit Op Code field. The four operations are:

Combinatorial

LUT3 [x] is purely combinatorial. Each LUT3 [x] output is the result of the LUT mapping truth table, and will only be delayed by the LUT3 [x] combinatorial path (Basic mode).

Figure 5. Combinatorial
Figure 5

Gated Input 2

LUT3 [x] input 2 is registered. Other inputs are directly connected to LUT3 [x]. The output is combinatorial (Input synchronization).

Figure 6. Gated Input2
Figure 6

Gated Output

Inputs are directly connected to LUT3 [x] and the output is registered (Output synchronization).

Figure 7. Gated output
Figure 7

Set/reset flip-flop

Input signals are used to control an S/R flip-flop.

Figure 8. S/R flip-flop enable
Figure 8

These four operations can be set with the register shown in Table 8. See the for details.

Table 8. Register for LUT3 [x] Mode Setting​

Register

Bit Field

Setting

SMARTIO_PRTx_LUT_CTLy

LUT_OPC [9:8]

0: Combinatorial

1: Gated Input 2

2: Gated Output

3: Set/reset flip-flop

Data Unit (DU)​

Each Smart I/O block includes a data unit (DU) component. DU consists of a simple 8-bit data path. It is capable of performing simple increment, decrement, increment/decrement, shift, and AND/OR operations. DU can generate a programmable output (Tr_out) signal based on two 8-bit data inputs that DATA0 (data0_in [7:0]) and DATA1 (data1_in [7:0]). The internal state is captured in flip-flops. The DU behavior can be controlled by up to three input signals (Tr0_in, Tr1_in, Tr2_in). Figure 9 shows the basic block diagram of Data Unit.

Figure 9. Data Unit Block Diagram​

Input selection​

DU has up to three control input signals. These signals can be selected as input from the following.

  • Constant “0”
  • Constant “1”
  • DU output
  • LUT3 [x] outputs

The number of control signals required depends on the DU operation code.

These inputs can be configured with the SMARTIO_PRTx_DU_SEL register. Table 9 shows the SMARTIO_PRTx_DU_SEL register and input selection setting. See the Registers TRM for details.

Table 9. Register for DU Inputs Source Setting​

Register

Bit Field

Setting

SMARTIO_PRTx_DU_SEL

DU_TR0_SEL [3:0] / DU_TR1_SEL [11:8] / DU_TR2_SEL [19:16]

Data unit input signal “tr0_in” / “tr1_in” / “tr2_in” source selection:

0: Constant ‘0’

1: Constant ‘1’

2: Data unit output

3- 10: LUT3 [x] outputs

Otherwise: Undefined

DATA 0 and DATA 1 use input data for DU logic to be initialized. These data can be selected from the following:

  • Constant 0x00
  • io_data_in [7:0]
  • chip_data_in [7:0]
  • DATA [7:0] bits of SMARTIO_PRTx_DATA register

The data width handled by the data unit can be changed between 1 bit and 8 bits. Table 10 shows the configuration registers for input data to DU.

Table 10. Register for DU Data Setting​

Register

Bit Field

Setting

SMARTIO_PRTx_DU_SEL

DU_DATA0_SEL [25:24] / DU_DATA1_SEL [29:28]

Data unit input data “data0_in” / “data1_in” source selection:

0: 0x00

1: chip_data [7:0].

2: io_data_in [7:0].

3: SMARTIO_PRTx_DATA.DATA [7:0] MMIO register field.

SMARTIO_PRTx_DATA

DATA [7:0]

Data unit input data source

SMARTIO_PRTx_DU_CTL

DU_SIZE [2:0]

Size/width of the data unit (in bits) is DU_SIZE+1.

Operation of data unit​

The DU operation is defined by SMARTIO_PRTx_DU_CTL.DU_OPC [11:8]. Table 11 shows the configuration registers for DU operation code setting. See the Registers TRM for details.

Table 11. DU Operation Code Configuration​

Register

Bit Field

Setting

SMARTIO_PRTx_DU_CTL

DU_OPC [11:8]

Data unit opcode specifies the data unit operation:

"1": INCR

"2": DECR

"3": INCR_WRAP

"4": DECR_WRAP

"5": INCR_DECR

"6": INCR_DECR_WRAP

"7": ROR

"8": SHR

"9": AND_OR

"10": SHR_MAJ3

"11": SHR_EQL

Otherwise: Undefined

Default Value: Undefined

Table 12 shows each DU operation.

The ‘Operation’ column in Table 12 shows the operation outline and the pseudo code. In the pseudo code, “Combinational:” indicates that the operations are independent of previous output states. "Registered:" indicates that data operates on inputs and previous output states (registered using flip-flops).

Table 12. DU Operation​

Operation code

Operation

DU_OPC [11:8] = 1:

INCR

INCR increments data by 1 from an initial value (DATA 0) until it reaches a final value (DATA 1).

    
du_size = Size - 1
mask = (1 << (DU_SIZE+1)) - 1
data_eql_data1 = (data & mask) == DATA1 &amp; mask

Combinational:

    Tr_out = data_eql_data1



Registered:

```c

data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in)
data <= data_eql_data1? data: (data + 1) & mask;

DU_OPC [11:8] = 2:

DECR

DECR decrements data from an initial value (DATA 0) until it reaches ‘0’.

    
du_size = Size - 1
mask = (1 << (DU_SIZE+1)) - 1
data_eql_0 = (data & mask) == 0

Combinational:

    Tr_out = data_eql_0

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in)
data <= data_eql_data1? data: (data + 1) & mask;

DU_OPC [11:8] = 3:

INCR_WRAP

INCR_WRAP operates similar to INCR, but instead of stopping at DATA 1, it wraps around to DATA 0.

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) - 1
data_eql_data1 = (data & mask) == DATA1 & mask

Combinational:

    Tr_out = data_eql_data1

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in)
data <= data_eql_data1? DATA0 & mask: (data + 1) & mask;

DU_OPC [11:8] = 4:

DECR_WRAP

DECR_WRAP works similar to DECR. Instead of stopping at ‘0’, it wraps around to DATA0.

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) - 1
data_eql_0 = (data & mask) == 0

Combinational:

    Tr_out = data_eql_0

Registered:

    
data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in)
data <= data_eql_0? DATA0 & mask: (data + 1) & mask;

DU_OPC [11:8] = 5:

INCR_DECR

INCR_DECR is a combination of INCR and DECR. Depending on the trigger signals, it either starts incrementing or decrementing. Increment stops at DATA 1 and decrement stops at ‘0’.

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1
data_eql_0 = (data & mask) == 0
data_eql_data1 = (data & mask) == DATA1 & mask

Combinational:

    Tr_out = data_eql_data1 | data_eql_0 

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in)
data <= data_eql_data1? data: (data + 1) & mask;
else if (Tr2_in)
data <= data_eql_0? data: (data - 1) & mask;

DU_OPC [11:8] = 6:

INCR_DECR_WRAP

INCR_DECR_WRAP has the same functionality as INCR_DECR with wrap around to DATA 0 on reaching the limits (DATA 1 or ‘0’).

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1
data_eql_0 = (data & mask) == 0
data_eql_data1 = (data & mask) == DATA1 & mask

Combinational:

    Tr_out = data_eql_data1 | data_eql_0

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in)
data <= data_eql_data1? DATA0 & mask: (data + 1) & mask;
else if (Tr2_in)
data <= data_eql_0 ? DATA0 & mask: (data - 1) & mask;

DU_OPC [11:8] = 7:

ROR

POR rotates the data right and the LSB is sent out. The data for rotation is taken from DATA 0.

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1

Combinational:

    Tr_out = data [0]

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in) {
data <= data [7:1] & mask;
data [du_size] <= data [0]
}

DU_OPC [11:8] = 8:

SHIR

SHIR performs the shift register operation. Initial data (DATA 0) is shifted out and data on tr2_in is shifted in.

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1

Combinational:

    Tr_out = data [0]

Registered

    
data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in) {
data <= data [7:1] & mask;
data [du_size] <= Tr2
}

DU_OPC [11:8] = 9:

AND_OR

ANDs data1 and data0 along with mask; then, ORs all bits of the ANDed output

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1

Combinational:

    Tr_out =| (data & DATA1 & mask)

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;

DU_OPC [11:8] = 10:

SHR_MAJ3 (Majority 3)

SHR_MAJ3 performs the same functionality as SHR. Instead of sending the shifted-out value, it sends a ‘1’, if at least two samples are high in the last three samples/shifted-out values of data [0]. Otherwise, it sends a ‘0’. This function sends out the majority of the last three samples.

    du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1

Combinational:

Tr_out = data == 0x03 | data == 0x05 | data == 0x06 | data == 0x07

Tr_out = data == 0x03 | data == 0x05 | data == 0x06 | data == 0x07

Registered:

    
data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in) {
data <= (0, data [7:1]) & mask;
data [du_size] <= Tr2_in
}

DU_OPC [11:8] = 11:

SHR_EQL (Match DATA1)

SHR_EQL performs the same operation as SHR. Instead of shift-out, the output is the comparison result (DATA 0 == DATA 1).

    
du_size = Size - 1
mask = (1 << (DU_SIZE+1)) – 1
data_eql_data1 = (data & mask) == DATA1 & mask

Combinational:

    Tr_out = data_eql_data1

Registered:

    data <= data;
if (Tr0_in)
data <= DATA0 & mask;
else if (Tr1_in) {
data <= (0, data [7:1]) & mask;
data [du_size] <= Tr2_in
}

Smart I/O configuration​

Figure 10 shows an example of the configuration flow of Smart I/O.

Figure 10. Smart I/O Configuration Flow​

When configuring Smart I/O, first initialize each component such as clock and reset, synchronizer, LUT3 [x] and DU. Before enabling Smart I/O (SMARTIO_PRTx_CTL.ENABLE set to “1”: Enabled), all components and routing should be configured.

If Smart I/O is not used, clock selection in clock and reset component should be set to a value between 20 to 30, and PIPELINE_EN should be set to “1”, to ensure low power consumption.

Note:

(*1) See Structure of Smart I/O for ports, source and clock setting, see 3-inputs lookup tables (LUT3 [x]) for LUT3 [x] setting, and see Data Unit (DU) for DU setting.

(*2) See Table 3 for Synchronization setting.

(*3) See Table 1 for bypass and Smart I/O enable setting.

(*4) See Table 7 for PIPELINE_EN setting.

Example configuration​

This section describes how to use Smart I/O using the Sample Driver Library (SDL). The code snippets in this application note are part of SDL. See Other references for the SDL.

SDL basically has a configuration part and a driver part. The configuration part mainly configures the parameter values for the desired operation. The driver part configures each register based on the parameter values in the configuration part. You can configure the configuration part according to your system.

Smart I/O can be useful for an application that involves simple logic operations for input/output signal, or the internal routing between internal HSIOM port and the I/O port. No CPU is required for these operations. This section explains how to use Smart I/O according to the use case.

In this example, CYT2B7 series is used.

Use case to change routing from I/O pins to HSIOM by inverting polarity​

This section explains an example of routing and simple logic operations by using Smart I/O.

In this use case, routing is changed to connect the input from pin 7 of Port 13 (io_data_in [7]) to pin 1 of HSIOM (smartio_data [1]). In addition, the polarity of io_data_in [7] is inverted, and the inverted io_data_in [7] signal is output to smartio_data [1]. See the Package Pin List and Alternate Functions of Device Datasheet for I/O port which can used Smart I/O.

Figure 11 shows the connection from the I/O port to HSIOM with signal inverting. LUT3 [1] and LUT3 [7] are used for this use case.

Figure 11. Signal Inverting Image​

Figure 12 shows the signal path of this example.

Figure 12. Example of the Overview of Routing​

Note that LUT3 [1] and LUT3 [7] are used. LUT3[7:4] that can use io_data [7] as input cannot be routed to smartio_data [1] directly. Therefore, output of LUT3 [7] must go through LTU3 [1] which can be routed to smartio_data [1]. In this use case, LUT3 [1] inverts the input signal from LUT3 [7] and outputs it to smartio_data [1].

Table 13 shows the truth table of LUT3 [7] and Table 14 shows the truth table of LUT3 [1]. The bold highlights in the tables indicate an invalid combination pattern.

Table 13. Look Up Table LUT3 [7]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

0

0

0

0

0

0

1

0

0

1

0

0

0

1

1

0

1

0

0

0

1

0

1

0

1

1

0

0

1

1

1

1

Table 14. Look Up Table LUT3 [1]​

Tr2_in

Tt1_in

Tr0_in

Tr_out

0

0

0

1

0

0

1

1

0

1

0

1

0

1

1

1

1

0

0

1

1

0

1

1

1

1

0

1

1

1

1

0

The three inputs of LUT3 [1] are input same signal, Similarly, LUT3 [7] are input same signal. Therefore, the input pattern of LTU3s is [Tr2_in, Tr1_in, Tr0_in] = [0, 0, 0] or [1, 1, 1].

LUT3 [7] does not change polarity. That is, Tr_out is “1”, when [Tr2_in, Tr1_in, Tr0_in] = [1, 1, 1], and otherwise, Tr_out = “0”.

LUT3 [1] reverses polarity. That is, Tr_out is “0”, when [Tr2_in, Tr1_in, Tr0_in] = [1, 1, 1], and otherwise, Tr_out = “1”.

Figure 13 shows the setting procedure for Smart I/O.

Figure 13. Setting procedure for Smart I/O​

(a) See the Table 14 for setting pattern.

(b) See the Table 13 for setting pattern.

Configuration and example code​

Table 15 lists the parameters and Table 16 lists the functions of the configuration part in SDL for Smart I/O.

Table 15. List of Smart I/O configuration Parameters​

Parameters

Description

Value

SMART_IO_CLK_ACTIVE

Defines Smart I/O clock source

1ul (Select Active clock source)

CY_SMARTIO_CLK_INV

Defines Smart I/O clock

PCLK_SMARTIO13_CLOCK

SMART_IO_PORT

Defines Smart IO port

SMARTIO_PRT13 (It is assigned to Smar I/O Port13)

SMARTIO_BYPASS_CH_MASK

Defines Bypass channel mask

io_data_in [7] to smartio_data [7]: No bypass

io_data_in [6] to smartio_data [6]: Bypass

io_data_in [5] to smartio_data [5]: Bypass

io_data_in [4] to smartio_data [4]: Bypass

io_data_in [3] to smartio_data [3]: Bypass

io_data_in [2] to smartio_data [2]: Bypass

io_data_in [1] to smartio_data [1]: No bypass

io_data_in [0] to smartio_data [0]: Bypass

0x7Dul (See Table 1)

No use Smart IO for io_data_in [6] to io_data_in [2] and io_data_in [0]

SMARTIO_IOSYNC_CH_MASK

Defines IO sync channel mask

0x00ul (See Table 3)

LUT_IP_BUTTON_PORT

Defines input port for LUT3[7] input

CY_BUTTON2_PORT (It is assigned to GPIO Port 13)

LUT_IP_BUTTON_PIN

Defines input port pin for LUT3[7] input

CY_BUTTON2_PIN (It is assigned to GPIO Port 7 pin)

LUT_IP_BUTTON_PIN_MUX

Configures input port pin function

CY_BUTTON2_PIN_MUX (It is assigned to GPIO)

CY_SMARTIO_LUTTR_IO

Selects LUT3[7] input

CY_SMARTIO_LUTTR_IO7

LUT_INV_OUT_PORT

Defines output port for LUT3[7] input

P13_1_PORT (It is assigned to GPIO Port 13)

LUT_INV_OUT_PIN

Defines output port pin for LUT3[7] input

P13_1_PIN (It is assigned to GPIO Port 1 pin)

LUT_INV_OUT_PIN_MUX

Configures output port pin function

P13_1_GPIO (It is assigned to GPIO)

LUTx_OUT_MAP

LUT3[7] output pattern

0x80ul (See Table 13.)

LUTx_INV_OUT_MAP

LUT3[1] output pattern

0x7Ful (See Table 14.)

LUTx_LOGIC_OPCODE

Select LUT3 Operation Mode

CY_SMARTIO_LUTOPC_COMB

(It is assigned to Combinatorial)

CY_SYSCLK_DIV_16_BIT

Selects Divider Type to 16-bit divider

1ul

CY_SMARTIO_ENABLE

Sets to Smart I/O and Pipeline enable

1ul

CY_SMARTIO_DISABLE

Sets to Smart I/O and Pipeline Disable

0ul

CY_SMARTIO_DEINIT

Resets the Smart I/O to default value

0ul

CY_SMARTIO_CHANNEL_ALL

Sets to all pin Smart I/O bypass

0xfful

CY_SMARTIO_CLK_DIVACT

Selects the source clock to clk_smartio/rst_sys_act_n. See Table 2.

16ul

CY_SMARTIO_CLK_GATED

Selects the source clock to Clock source is a constant ‘0’. See Table 2.

20ul

CY_SMARTIO_CLK_ASYNC

Selects the source clock to asynchronous mode/“1”. See Table 2.

31ul

CY_SMARTIO_LUTTR_LUT7_OUT

Selects LUT3[1] input

7ul (It is assigned to LUT3[7] output. See Table 6.)

CY_SMARTIO_LUTTR_IO7

Selects LUT3[7] input

15ul (It is assigned to io_data_in [7] output. See Table 6.)

smart_io_cfg.clkSrc

Source clock setting

CY_SMARTIO_CLK_DIVACT

smart_io_cfg.bypassMask

Configures bypass setting

SMARTIO_BYPASS_CH_MASK

smart_io_cfg.ioSyncEn

Configures Synchronizer setting

SMARTIO_IOSYNC_CH_MASK

lutCfgLut1.opcode

Configures LUT3[1] Operation Mode setting

LUTx_LOGIC_OPCODE

lutCfgLut1.lutMap

Configures LUT3[1] output pattern setting

LUTx_INV_OUT_MAP

lutCfgLut1.tr0

Configures LUT3[1] tr0 input

CY_SMARTIO_LUTTR_LUT7_OUT

lutCfgLut1.tr1

Configures LUT3[1] tr1 input

CY_SMARTIO_LUTTR_LUT7_OUT

lutCfgLut1.tr2

Configures LUT3[1] tr2 input

CY_SMARTIO_LUTTR_LUT7_OUT

lutCfgLut7.opcode

Configures LUT3[7] Operation Mode setting

LUTx_LOGIC_OPCODE

lutCfgLut7.lutMap

Configures LUT3[7] output pattern setting

CY_SMARTIO_LUTTR_IO

lutCfgLut7.tr0

Configures LUT3[7] tr0 input

CY_SMARTIO_LUTTR_IO

lutCfgLut7.tr1

Configures LUT3[7] tr1 input

CY_SMARTIO_LUTTR_IO

lutCfgLut7.tr2

Configures LUT3[7] tr2 input

CY_SMARTIO_LUTTR_IO

Table 16. List of Smart I/O Configuration Functions​

Functions

Description

Remarks

Init_IO_Pin()

Configures GPIO Port pin

–

Cy_SmartIO_Deinit()

Resets the Smart I/O to default values

Resets the Smart I/O registers; SMARTIO_PRTx_CTL, SMARTIO_PRTx_SYNC_CTL, SMARTIO_PRTx_LUT_SELy, SMARTIO_PRTx_LUT_CTLy, SMARTIO_PRTx_DU_SEL, SMARTIO_PRTx_DU_CTL and SMARTIO_PRTx_DATA

Init_SmartIO()

Configures and enables Smart I/O, Call for Init_SmartIO_Cfg() and Cy_SmartIO_Enable()

–

Init_SmartIO_Cfg()

Configures Smart I/O setting structure, Calls for Cy_SmartIO_Init()

–

Cy_SmartIO_Enable()

Enable Smart I/O

Write to PIPELINE_EN and ENABLED bit

Cy_SmartIO_Init()

Configure Smart I/O register

Write to the related registers for Source clock, Bypass, Synchronizer, LUT3, and DU.

Code Listing 1 demonstrates an example program to change routing from I/O Pins to HSIOM by Inverting Polarity. See the Architecture TRM and Application Note for GPIO and clock configuration.

The following description will help you understand the register notation of the driver part of SDL:

  • base signifies the pointer to the Smart I/O register base address.
  • base- >unLUT_SEL[idx].u32Register is the SMARTIO_PRTx_LUT_SEL[idx] register mentioned in the Registers TRM. Other registers are also described in the same manner. “ x ” signifies the port suffix number and “ idx ” signifies the register index number.
  • To improve the register setting performance, the SDL writes a complete 32-bit data to the register. Each bit field is generated and written to the register as the final 32-bit data.
    
un_SMARTIO_PRT_CTL_t workCTL= {.u32Register = 0ul};
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = CY_SMARTIO_CLK_GATED;
workCTL.stcField.u8BYPASS = CY_SMARTIO_CHANNEL_ALL;
base->unCTL.u32Register = workCTL.u32Register;
See cyip_smartio_v2.h under hdr/rev_x/ip for more information on the union and
structure representation of registers.

##### Code Listing 1 Example to Change Routing from I/O Pins to HSIOM by
Inverting Polarity
``` c


/* Smart IO clock source selection */
#define SMART_IO_CLK_ACTIVE 1ul /* Define Clock active */

/* Smart IO port selections macro */
#define SMART_IO_PORT SMARTIO_PRT13 /* Define Smart I/O port */

#define CY_SMARTIO_CLK_INV PCLK_SMARTIO13_CLOCK /* Define Smart I/O port */

/* Bypass channel mask */
#define SMARTIO_BYPASS_CH_MASK 0x7Dul /* Define Smart I/O bypass channel */

/* IO sync channel mask */
#define SMARTIO_IOSYNC_CH_MASK 0x00ul /* Define Smart I/O sync channel mask */

/* Lut input button pin configuration */
/* Define input port to LUT3[7] */
#define LUT_IP_BUTTON_PORT CY_BUTTON2_PORT /* GPIO_PRT3 */
#define LUT_IP_BUTTON_PIN CY_BUTTON2_PIN /* 7 */
#define LUT_IP_BUTTON_PIN_MUX CY_BUTTON2_PIN_MUX /* P13_7_GPIO */

#define CY_SMARTIO_LUTTR_IO CY_SMARTIO_LUTTR_IO7 /**< I/O signal 7 (for LUT 4,5,6,7) */

/* LUT output pin configuration */
/* Define output port from LUT3[1] */
#define LUT_INV_OUT_PORT P13_1_PORT
#define LUT_INV_OUT_PIN P13_1_PIN
#define LUT_INV_OUT_PIN_MUX P13_1_GPIO

/* LUT output map */
/* Define LUT3[1] and LUT3[7] output pattern */
#define LUTx_OUT_MAP 0x80ul
#define LUTx_INV_OUT_MAP 0x7Ful

/* LUT logic circuit type macro */
#define LUTx_LOGIC_OPCODE CY_SMARTIO_LUTOPC_COMB /* Define LUT logic circuit type */

#define CY_SMARTIO_ENABLE 1ul
#define CY_SMARTIO_DISABLE 0ul
#define CY_SMARTIO_DEINIT 0ul
#define CY_SMARTIO_CHANNEL_ALL 0xfful /**< All channels */


/* Button input configuration */
/* Configure Port for input (Port13 pin) */
cy_stc_gpio_pin_config_t button_cfg =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_HIGHZ,
.hsiom = LUT_IP_BUTTON_PIN_MUX,
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};

/* Configure Port for output (Port13 pin) */
cy_stc_gpio_pin_config_t inv_out_cfg =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_STRONG_IN_OFF,
.hsiom = LUT_INV_OUT_PIN_MUX,
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};


int main(void)
{
:
Init_IO_Pin(); /* (1) Configure GPIO pin. See Code Listing 2. */

/* Deinit before Init */
Cy_SmartIO_Deinit(SMART_IO_PORT); /* Disable all Smart I/O. See Code Listing 3 */

/* SmartIO peripheral clock divider setting */
{
/* (3) Configure peripheral Clock */
Cy_SysClk_PeriphAssignDivider(CY_SMARTIO_CLK_INV, CY_SYSCLK_DIV_16_BIT, 0ul);
uint32_t sourceFreq = 80000000ul;
uint32_t targetFreq = 12000000ul;
uint32_t divNum = (sourceFreq / targetFreq);

Cy_SysClk_PeriphSetDivider(CY_SYSCLK_DIV_16_BIT, 0ul, (divNum - 1ul));
Cy_SysClk_PeriphEnableDivider(CY_SYSCLK_DIV_16_BIT, 0ul);
}

/* Initialization call for the Smart IO */
Init_SmartIO(); /* Initialize Smart I/O. See Code Listing 4 */

for(;;);
}
Code Listing 2 Init_IO_Pin() Function​
    

void Init_IO_Pin(void)
{
/* Configure Port13 7pin. */
Cy_GPIO_Pin_Init(LUT_IP_BUTTON_PORT, LUT_IP_BUTTON_PIN, &button_cfg);

/* Configure Port13 1pin. */
Cy_GPIO_Pin_Init(LUT_INV_OUT_PORT, LUT_INV_OUT_PIN, &inv_out_cfg);
}
Code Listing 3 Cy_SmartIO_Deinit() Function​
   void Cy_SmartIO_Deinit(volatile stc_SMARTIO_PRT_t* base) 
{
un_SMARTIO_PRT_CTL_t workCTL= {.u32Register = 0ul};
/* (2) Disable all Smart I/O port */
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = CY_SMARTIO_CLK_GATED;
workCTL.stcField.u8BYPASS = CY_SMARTIO_CHANNEL_ALL;
base->unCTL.u32Register = workCTL.u32Register;

base->unSYNC_CTL.u32Register = CY_SMARTIO_DEINIT;
for(uint8_t idx = CY_SMARTIO_LUTMIN; idx < CY_SMARTIO_LUTMAX; idx++)
{
base->unLUT_SEL[idx].u32Register = CY_SMARTIO_DEINIT;
base->unLUT_CTL[idx].u32Register = CY_SMARTIO_DEINIT;
}
base->unDU_SEL.u32Register = CY_SMARTIO_DEINIT;
base->unDU_CTL.u32Register = CY_SMARTIO_DEINIT;
base->unDATA.u32Register = CY_SMARTIO_DEINIT;
}
Code Listing 4 Init_SmartIO() Function​
    
void Init_SmartIO(void)
{
cy_en_smartio_status_t retStatus = (cy_en_smartio_status_t)0xFF;

retStatus = Init_SmartIO_Cfg(); /* Configure Smart I/O. See Code Listing 5 */
if(retStatus == CY_SMARTIO_SUCCESS)
{
/* After all the configuration, enable SMART IO */
Cy_SmartIO_Enable(SMART_IO_PORT); /* Enable Smart I/O. See Code Listing 6 */
}
}
Code Listing 5 Init_SmartIO_Cfg() Function​
    
cy_en_smartio_status_t Init_SmartIO_Cfg(void)
{
cy_stc_smartio_lutcfg_t lutCfgLut1;
cy_stc_smartio_lutcfg_t lutCfgLut7;

cy_stc_smartio_config_t smart_io_cfg;
cy_en_smartio_status_t retStatus = (cy_en_smartio_status_t)0xFF;

/* initialize the Smart IO structure */
memset(&lutCfgLut1, 0, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut7, 0, sizeof(cy_stc_smartio_lutcfg_t));
/* Clear configuration structure */
memset(&smart_io_cfg, 0, sizeof(cy_stc_smartio_config_t));

#ifdef SMART_IO_CLK_ACTIVE
/* Active clock source is selected */
/* Configure Smart I/O clock source */
smart_io_cfg.clkSrc = (cy_en_smartio_clksrc_t)CY_SMARTIO_CLK_DIVACT;
#else
/* Asynchronous clock source is selected */
smart_io_cfg.clkSrc = (cy_en_smartio_clksrc_t)CY_SMARTIO_CLK_ASYNC;
#endif /* SMART_IO_CLK_ACTIVE */

/* Bypass channel mask for input and output pin */
/* Configure BYPASS setting */
smart_io_cfg.bypassMask = SMARTIO_BYPASS_CH_MASK;

/* IO channel sync mask for selected pin */
/* Configure Synchronizer setting */
smart_io_cfg.ioSyncEn = SMARTIO_IOSYNC_CH_MASK;

/* LUT3[1] setting */
/* Configure LUT3 [1] */
/****************************/
/* Lut configuration for output, check description above */
lutCfgLut1.opcode = LUTx_LOGIC_OPCODE;
lutCfgLut1.lutMap = LUTx_INV_OUT_MAP;

/* Lut configuration for input */
lutCfgLut1.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT7_OUT;
lutCfgLut1.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT7_OUT;
lutCfgLut1.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT7_OUT;
smart_io_cfg.lutCfg[LUT_INV_OUT_PIN] = &lutCfgLut1;

/* LUT3[7] setting */
/* Configure LUT3 [7] */
/****************************/
/* Lut configuration for output, check description above */
lutCfgLut7.opcode = LUTx_LOGIC_OPCODE;
lutCfgLut7.lutMap = LUTx_OUT_MAP;

/* Lut configuration for input (button) */
lutCfgLut7.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_IO;
lutCfgLut7.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_IO;
lutCfgLut7.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_IO;
smart_io_cfg.lutCfg[LUT_IP_BUTTON_PIN] = &lutCfgLut7;

/* Initialization of Smart IO structure */
/* Configure Smart I/O. See Code Listing 7. */
retStatus = Cy_SmartIO_Init(SMART_IO_PORT, &smart_io_cfg);
return retStatus;
}
Code Listing 6 Cy_SmartIO_Enable() Function​
    

void Cy_SmartIO_Enable(volatile stc_SMARTIO_PRT_t* base)
{
un_SMARTIO_PRT_CTL_t workCTL = base->unCTL;
workCTL.stcField.u1ENABLED = CY_SMARTIO_ENABLE;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_DISABLE;
base->unCTL.u32Register = workCTL.u32Register; /* (8) Enable Smart I/O. */
}
Code Listing 7 Cy_SmartIO_Init() Function​
    

cy_en_smartio_status_t Cy_SmartIO_Init(volatile stc_SMARTIO_PRT_t* base, const cy_stc_smartio_config_t* config)
{
cy_en_smartio_status_t status = CY_SMARTIO_SUCCESS;

if(NULL != config)
{
/* (4) Set clock source and bypass to Smart */
un_SMARTIO_PRT_CTL_t workCTL = {.u32Register = 0ul};
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE;
workCTL.stcField.u1HLD_OVR = config->hldOvr;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = config->clkSrc;
workCTL.stcField.u8BYPASS = config->bypassMask;
base->unCTL.u32Register = workCTL.u32Register;

/* (5) Set synchronizer to Smart IO */
un_SMARTIO_PRT_SYNC_CTL_t workSYNC_CTL = {.u32Register = 0ul};
workSYNC_CTL.stcField.u8IO_SYNC_EN = config->ioSyncEn;
workSYNC_CTL.stcField.u8CHIP_SYNC_EN = config->chipSyncEn;
base->unSYNC_CTL.u32Register = workSYNC_CTL.u32Register;

/* LUT configurations - skip if lutCfg is a NULL pointer */
/* (6), (7) Set LUT3 */
for(uint32_t i = CY_SMARTIO_LUTMIN; i < CY_SMARTIO_LUTMAX; i++)
{
if(NULL != config->lutCfg[i])
{
un_SMARTIO_PRT_LUT_SEL_t workLUT_SET = { .u32Register = 0ul };
workLUT_SET.stcField.u4LUT_TR0_SEL = config->lutCfg[i]->tr0;
workLUT_SET.stcField.u4LUT_TR1_SEL = config->lutCfg[i]->tr1;
workLUT_SET.stcField.u4LUT_TR2_SEL = config->lutCfg[i]->tr2;
base->unLUT_SEL[i].u32Register = workLUT_SET.u32Register;

un_SMARTIO_PRT_LUT_CTL_t workLUT_CTL = { .u32Register = 0ul };
workLUT_CTL.stcField.u2LUT_OPC = config->lutCfg[i]->opcode;
workLUT_CTL.stcField.u8LUT = config->lutCfg[i]->lutMap;
base->unLUT_CTL[i].u32Register = workLUT_CTL.u32Register;
}
}

/* DU Configuration - skip if duCfg is a NULL pointer */
/* Set DU. It is ignored in this use case. */
if(NULL != config->duCfg)
{
un_SMARTIO_PRT_DU_SEL_t workDU_SEL = {.u32Register = 0ul};
workDU_SEL.stcField.u4DU_TR0_SEL = config->duCfg->tr0;
workDU_SEL.stcField.u4DU_TR1_SEL = config->duCfg->tr1;
workDU_SEL.stcField.u4DU_TR2_SEL = config->duCfg->tr2;
workDU_SEL.stcField.u2DU_DATA0_SEL = config->duCfg->data0;
workDU_SEL.stcField.u2DU_DATA1_SEL = config->duCfg->data1;
base->unDU_SEL.u32Register = workDU_SEL.u32Register;

un_SMARTIO_PRT_DU_CTL_t workDU_CTL = {.u32Register = 0ul};
workDU_CTL.stcField.u3DU_SIZE = config->duCfg->size;
workDU_CTL.stcField.u4DU_OPC = config->duCfg->opcode;
base->unDU_CTL.u32Register = workDU_CTL.u32Register;

base->unDATA.stcField.u8DATA = config->duCfg->dataReg;
}
}
else
{
status = CY_SMARTIO_BAD_PARAM;
}

return(status);
}

Use case to reset detection/stability circuitry​

This section explains how to implement a reset detection/stability circuitry on the Smart I/O. Figure 14 shows the operation of reset detection/stability.

Figure 14. Operation of Reset Detection/Stability Circuity​

In this use case, circuitry has two enable signals; pin_rst_enable and gpio_rst_enable. The pin_rst_enable is an enable signal from external circuitry and the gpio_rst_enable is an enable control signal by software. When both signals are enabled, the circuitry is active.

The rst_in_n is an external reset input with active high, and rst_out_n is a reset output with active high. The circuitry monitors rst_in_n. When rst_in_n is activated for a specific number of continuous cycles, the rst_out_n is output. A reset will be activated or released, when the operation clock selected by CLOCK_SRC [12:8] is input continuously for 16 cycles. The source clock 80 MHz is divided by 6 to 13 MHz. Then, count 76 ns multiplied by 16 cycle, the time of reset activation or release is approximately 1.2 μs.

The following I/O port and HSIOM signals are used:

  • io_data_in [6] = pin_rst_enable; (from I/O port)
  • io_data_in [7] = rst_in_n; (from I/O port)
  • smartio_data [5] = rst_out_n; (to I/O port)
  • chip_data [4] = gpio_rst_enable; (from HSIOM)

Figure 15 shows the connection and functional logic of each LUT3 [3:0] and DU in this circuity.

Figure 15. Logical Example of a Reset Detection/Stability Circuitry​

In this use case, four LUT3s and one DU are used.

LUT3 [4] is used to generate the activation signal of this circuitry from two enable signals (pin_rst_enable and gpio_rst_en). LUT 3 [6] and LUT 3 [7] are used to monitor the rst_in_n state and to start the counter of the DU. LUT 3 [5] detects the stabilization wait completion and outputs rst_out_n.

DU is used to generate reset stability wait time, and the Tr_out of LUT3 [5] is output synchronously by gated output mode.

Figure 16 shows the signal path of this use case.

Figure 16. Signal Path of Reset Detection/Stability Circuitry​

In this use case, io_data_in [7:6], chip_data [4] and smartio_data [5] are used as input or output signals. Therefore, it can be configured with four LUT3s (LUT3 [7:4]). If smartio_data [3] is used for rst_out_n, it is necessary to go through LUT3 [3]. That is, five LUT3 [x] are required for this case.

Table 17, Table 18, Table 19, and Table 20 show truth table of each LUT3. The bold highlights in the tables indicate an invalid combination pattern.

Table 17. Look Up Table LUT3 [6]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

0

0

0

1

0

0

1

1

0

1

0

1

0

1

1

1

1

0

0

1

1

0

1

1

1

1

0

1

1

1

1

0

Table 18. Look Up Table LUT3 [7]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

0

0

0

0

0

0

1

0

0

1

0

0

0

1

1

1

1

0

0

0

1

0

1

1

1

1

0

0

1

1

1

0

Table 19. Look Up Table LUT3 [5]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

0

0

0

0

0

0

1

0

0

1

0

0

0

1

1

0

1

0

0

0

1

0

1

1

1

1

0

1

1

1

1

0

Table 20. Look Up Table LUT3 [4]​

Tr2_in

Tr1_in

Tr0_in

Tr_out

0

0

0

0

0

0

1

0

0

1

0

0

0

1

1

0

1

0

0

0

1

0

1

0

1

1

0

0

1

1

1

1

LUT3 [6] is an inverter circuit with one input and one output, and each input of Tr0_in, Tr1_in and Tr2_in is the same signal. Therefore, valid combination pattern of [Tr0_in, Tr1_in, Tr2_in, Tr_out] is [0, 0, 0, 1] or [1, 1, 1, 0]. If an invalid pattern occurs, the counter circuit is reset and rst_out_n keeps the current value.

LUT3 [7] has three different inputs. If the enable signal (Tr0_in) from LUT3 [4] is valid (=“1”) and the rst_in_n state (Tr2_in) is different from rst_out_n state (Tr1_in) from LUT3 [5], “1” is output.

LUT3 [5] generates rst_out_n signal. When the enable signal (Tr2_in) from LUT3 [4] is valid (=”1”) and the stability done signal (Tr0_in) from DU is detected (stabilization wait time has passed), the current rst_out_n signal (Tr1_in, Tr_out) of LUT3 [5] is reversed.

LUT3 [4] generates the enable signal for this circuitry. It has two inputs; pin_rst_enable and gpio_rst_enable. The pin_rst_enable is input to Tr2_in, and the gpio_rst_enable is input to Tr0_in and Tr1_in. Therefore, different value combination of Tr0_in and Tr1_in are invalid pattern. If an invalid pattern occurs, the circuitry is disabled (Tr_out = “0”).

DU operates in the INCR_WRAP mode. This mode increments data by 1 from an initial value (DATA 0) until it reaches a final value (DATA 1). When the count value matches the final value, it wraps around to DATA 0. If rst is “1”, the counter value is set to initial value.

In this mode, DU has two control signal inputs; count_en and count_rst. The count_en is the input to Tr1_in, and the count_rst is input to Tr0_in. DU has two counter control registers (DATA 0 and DATA 1) and one output signal (Tr_out). DATA0 register is the initial value of the counter, and DATA1 register is final counter value.

Table 21 shows DU configuration and input/output operation.

Table 21. DU operation​

Tr0_in (rst)

Tr1_in (en)

Operation

DATA 0 (Initial value)

DATA 1 (Final value)

Tr_out

1

0

INCR_WRAP:Increments data by 1 from an initial value (DATA 0) until it reaches a final value (DATA 1).

When count value matches the final value, it wraps around to DATA 0.

0

16

0 (It is the reset state)

0

1

A single clock pulse is output when the count value is equal to the final value.

Tr0_in operates as “rst” and Tr1_in operates as “en”. Tr0_in is connected to the output of LUT3 [6] and Tr1_in is connected to the input of LUT3 [6]. When "1" is input to en, the DU starts a counter. Then, outputs the single pulse, when counter value reaches the final value.

Figure 17 shows the setting procedure for Smart I/O.

Figure 17. Setting procedure for Smart I/O​

(1) See the Application Note for the GPIO configuration (AN220193).

(6) See the Table 20 for setting pattern.

(7) See the Table 19 for setting pattern.

(8) See the Table 17 for setting pattern.

(9) See the Table 18 for setting pattern.

Configuration and example code​

Table 22 lists the parameters and Table 23 lists the functions of the configuration part in SDL for Smart I/O.

Table 22. List of Smart I/O Configuration Parameters​

Parameters

Description

Value

SMART_IO_CLK_ACTIVE

Defines Smart I/O clock source

1ul (Select Active clock source)

CY_SMARTIO_CLK_INV

Defines Smart I/O clock

PCLK_SMARTIO13_CLOCK

SMART_IO_PORT

Defines Smart IO port

SMARTIO_PRT13 (It is assigned to Smar I/O Port13)

SMARTIO_BYPASS_CH_MASK

Defines Bypass channel mask

io_data_in [7] to smartio_data [7]: No bypass

io_data_in [6] to smartio_data [6]: No bypass

io_data_in [5] to smartio_data [5]: No bypass

io_data_in [4] to smartio_data [4]: No bypass

io_data_in [3] to smartio_data [3]: Bypass

io_data_in [2] to smartio_data [2]: Bypass

io_data_in [1] to smartio_data [1]: Bypass

io_data_in [0] to smartio_data [0]: Bypass

0x0Ful (See Table 1)

No use Smart IO for io_data_in [3] to io_data_in [0]

SMARTIO_IOSYNC_CH_MASK

Defines IO sync channel mask

0x00ul (See Table 3)

GPIO_RST_EN_PORT

Defines input port for LUT3[4] input

GPIO_PRT13 (It is assigned to GPIO Port13)

GPIO_RST_EN_PIN

Defines input port pin for LUT3[4] input

4ul (It is assigned to GPIO Port 4pin)

GPIO_RST_EN_PIN_MUX

Configures input port pin function

P13_4_GPIO (It is assigned to GPIO)

PIN_RST_EN_PORT

Defines input port for LUT3[6] input

GPIO_PRT13 (It is assigned to GPIO Port13)

PIN_RST_EN_PIN

Defines input port pin for LUT3[6] input

6ul (It is assigned to GPIO Port 6 pin)

PIN_RST_EN_PIN_MUX

Configures input port pin function

P13_6_GPIO (It is assigned to GPIO)

RST_IN_PORT

Defines input port for LUT3[7] input

GPIO_PRT13 (It is assigned to GPIO Port 13)

RST_IN_PIN

Defines input port pin for LUT3[7] input

7ul (It is assigned to GPIO Port 6 pin)

RST_IN_PIN_MUX

Configures input port pin function

P13_7_GPIO (It is assigned to GPIO)

RST_OUT_PORT

Defines input port for LUT3[5] output

GPIO_PRT13 (It is assigned to GPIO Port 13)

RST_OUT_PIN

Defines input port pin for LUT3[5] output

5ul (It is assigned to GPIO Port 6 pin)

RST_OUT_PIN_MUX

Configures input port pin function

P13_5_GPIO (It is assigned to GPIO)

LUT4_OUT_MAP

LUT3[4] output pattern

0x80ul (See Table 20)

LUT5_OUT_MAP

LUT3[5] output pattern

0x60ul (See Table 19)

LUT6_OUT_MAP

LUT3[6] output pattern

0x7Ful (See Table 17)

LUT7_OUT_MAP

LUT3[7] output pattern

0x28ul (See Table 18)

LUTx_LOGIC_OPCODE_COMB

Selects LUT3 Operation Mode

CY_SMARTIO_LUTOPC_COMB

(It is assigned to Combinatorial)

LUTx_LOGIC_OPCODE_GO

Selects LUT3 Operation Mode

CY_SMARTIO_LUTOPC_GATED_OUT

LUTx_LOGIC_OPCODE_GI2

Selects LUT3 Operation Mode

CY_SMARTIO_LUTOPC_GATED_TR2

CY_SYSCLK_DIV_16_BIT

Selects Divider Type to 16-bit divider

1ul

CY_SMARTIO_ENABLE

Sets to Smart I/O and Pipeline enable

1ul

CY_SMARTIO_DISABLE

Sets to Smart I/O and Pipeline Disable

0ul

CY_SMARTIO_DEINIT

Resets the Smart I/O to default value

0ul

CY_SMARTIO_CHANNEL_ALL

Sets to all pin Smart I/O bypass

0xfful

CY_SMARTIO_CLK_DIVACT

Selects the source clock to clk_smartio/rst_sys_act_n. See Table 2.

16ul

CY_SMARTIO_CLK_GATED

Selects the source clock to Clock source is a constant ‘0’. See Table 2.

20ul

CY_SMARTIO_CLK_ASYNC

Selects the source clock to asynchronous mode/“1”. See Table 2.

31ul

CY_SMARTIO_LUTTR_CHIP4

LUT3[4] Tr0/Tr1 input

4ul (It is assigned to LUT3[4]. See Table 6)

CY_SMARTIO_LUTTR_IO6

LUT3[4] Tr2 input

14ul (It is assigned to LUT3[4]. See Table 6)

CY_SMARTIO_LUTTR_DU_OUT

LUT3[5] Tr0 input

0ul (It is assigned to LUT3[5]. See Table 6)

CY_SMARTIO_LUTTR_LUT5_OUT

LUT3[5] Tr1 input/LUT3[7] Tr1 input

5ul (It is assigned to LUT3[5]. See Table 6)

CY_SMARTIO_LUTTR_LUT4_OUT

LUT3[5] Tr2 input/ LUT3[7] Tr2 input

4ul (It is assigned to LUT3[5]. See Table 6)

CY_SMARTIO_LUTTR_LUT7_OUT

LUT3[6] Tr0/Tr1/Tr2 input

7ul (It is assigned to LUT3[6]. See Table 6)

CY_SMARTIO_LUTTR_IO7

LUT3[7] Tr0 input

15ul (It is assigned to LUT3[7]. See Table 6)

CY_SMARTIO_DUTR_LUT6_OUT

DU Tr0 input trigger source

9ul (It is assigned to LUT6 output. See Table 9)

CY_SMARTIO_DUTR_LUT7_OUT

DU Tr1 input trigger source

10ul (It is assigned to LUT7 output. See Table 9)

CY_SMARTIO_DUTR_ZERO

DU Tr2 input trigger source

0ul (It is assigned to Constant 0. See Table 9)

CY_SMARTIO_DUDATA_ZERO

DU data0 input DATA source

0ul (It is assigned to Constant 0. See Table 10)

CY_SMARTIO_DUDATA_DATAREG

DU data1 input DATA source

3ul (It is assigned to SMARTIO.DATA register. See Table 10)

CY_SMARTIO_DUOPC_INCR_WRAP

DU opcode

3ul (It is assigned to Increment and wrap-around (Count up and wrap). See Table 11)

CY_SMARTIO_DUSIZE_8

DU operation bit size

7ul (It is assigned to 8-bits size/width operand. See Table 10)

smart_io_cfg.clkSrc

Source clock setting

CY_SMARTIO_CLK_DIVACT

smart_io_cfg.bypassMask

Configures bypass setting

SMARTIO_BYPASS_CH_MASK

smart_io_cfg.ioSyncEn

Configures Synchronizer setting

SMARTIO_IOSYNC_CH_MASK

lutCfgLut4.opcode

Configures LUT3[4] Operation Mode setting

LUTx_LOGIC_OPCODE_GI2

lutCfgLut4.lutMap

Configures LUT3[4] output pattern setting

LUT4_OUT_MAP

lutCfgLut4.tr0

Configures LUT3[4] tr0 input

CY_SMARTIO_LUTTR_CHIP4

lutCfgLut4.tr1

Configures LUT3[4] tr1 input

CY_SMARTIO_LUTTR_CHIP4

lutCfgLut4.tr2

Configures LUT3[4] tr2 input

CY_SMARTIO_LUTTR_IO6

lutCfgLut5.opcode

Configures LUT3[5] Operation Mode setting

LUTx_LOGIC_OPCODE_GO

lutCfgLut5.lutMap

Configures LUT3[5] output pattern setting

LUT5_OUT_MAP

lutCfgLut5.tr0

Configures LUT3[5] tr0 input

CY_SMARTIO_LUTTR_DU_OUT

lutCfgLut5.tr1

Configures LUT3[5] tr1 input

CY_SMARTIO_LUTTR_LUT5_OUT

lutCfgLut5.tr2

Configures LUT3[5] tr2 input

CY_SMARTIO_LUTTR_LUT4_OUT

lutCfgLut6.opcode

Configures LUT3[6] Operation Mode setting

LUTx_LOGIC_OPCODE_COMB

lutCfgLut6.lutMap

Configures LUT3[6] output pattern setting

LUT6_OUT_MAP

lutCfgLut6.tr0

Configures LUT3[6] tr0 input

CY_SMARTIO_LUTTR_LUT7_OUT

lutCfgLut6.tr1

Configures LUT3[6] tr1 input

CY_SMARTIO_LUTTR_LUT7_OUT

lutCfgLut6.tr2

Configures LUT3[6] tr2 input

CY_SMARTIO_LUTTR_LUT7_OUT

lutCfgLut7.opcode

Configures LUT3[7] Operation Mode setting

LUTx_LOGIC_OPCODE_GI2

lutCfgLut7.lutMap

Configures LUT3[7] output pattern setting

LUT7_OUT_MAP

lutCfgLut7.tr0

Configures LUT3[7] tr0 input

CY_SMARTIO_LUTTR_LUT4_OUT

lutCfgLut7.tr1

Configures LUT3[7] tr1 input

CY_SMARTIO_LUTTR_LUT5_OUT

lutCfgLut7.tr2

Configures LUT3[7] tr2 input

CY_SMARTIO_LUTTR_IO7

lutCfgDu.tr0

Configures DU input trigger 0 source selection - LUT[3]6 output

CY_SMARTIO_DUTR_LUT6_OUT

lutCfgDu.tr1

Configures DU input trigger 1 source selection - LUT[3]7 output

CY_SMARTIO_DUTR_LUT7_OUT

lutCfgDu.tr2

Configures DU input trigger 2 source selection - Constant 0

CY_SMARTIO_DUTR_ZERO

lutCfgDu.data0

DU input DATA0 source selection - Fixed 0

CY_SMARTIO_DUDATA_ZERO

lutCfgDu.data1

DU input DATA1 source selection - SMARTIO_PRTx_DATA.DATA [7:0]

CY_SMARTIO_DUDATA_DATAREG

lutCfgDu.opcode

DU op-code

CY_SMARTIO_DUOPC_INCR_WRAP

lutCfgDu.size

DU width size is 8

CY_SMARTIO_DUSIZE_8

lutCfgDu.dataReg

DU DATA register value = 16

10ul

sourceFreq

Source Frequency

80000000ul (80MHz)

targetFreq

Target Frequency

12000000ul (12MHz)

Table 23. List of Smart I/O configuration functions​

Functions

Description

Remarks

Init_IO_Pin()

Configures GPIO Port pin

–

Cy_SmartIO_Deinit()

Resets the Smart I/O to default values

Resets the Smart I/O registers; SMARTIO_PRTx_CTL, SMARTIO_PRTx_SYNC_CTL, SMARTIO_PRTx_LUT_SELy, SMARTIO_PRTx_LUT_CTLy, SMARTIO_PRTx_DU_SEL, SMARTIO_PRTx_DU_CTL and SMARTIO_PRTx_DATA

Init_SmartIO()

Configures and enables Smart I/O, Calls for Init_SmartIO_Cfg() and Cy_SmartIO_Enable()

–

Init_SmartIO_Cfg()

Configures Smart I/O setting structure, Calls for Cy_SmartIO_Init()

–

Cy_SmartIO_Enable()

Enable Smart I/O

Write to PIPELINE_EN and ENABLED bit

Cy_SmartIO_Init()

Configures Smart I/O register

Write to the related registers for Source clock, Bypass, Synchronizer, LUT3, and DU.

Code Listing 8 demonstrates an example program to reset detection/stability circuitry. See the Architecture TRM and Application Note for GPIO and clock configuration.

The following description will help you understand the register notation of the driver part of SDL:

  • base signifies the pointer to the Smart I/O register base address.
  • base- >unLUT_SEL[idx].u32Register is the SMARTIO_PRTx_LUT_SEL[idx] register mentioned in the Registers TRM. Other registers are also described in the same manner. “ x ” signifies the port suffix number and “ idx ” signifies the register index number.
  • To improve the register setting performance, the SDL writes a complete 32-bit data to the register. Each bit field is generated and written to the register as the final 32-bit data.
    
un_SMARTIO_PRT_CTL_t workCTL= {.u32Register = 0ul};
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = CY_SMARTIO_CLK_GATED;
workCTL.stcField.u8BYPASS = CY_SMARTIO_CHANNEL_ALL;
base->unCTL.u32Register = workCTL.u32Register;

See cyip_smartio_v2.h under hdr/rev_x/ip for more information on the union and structure representation of registers.

Code Listing 8 Example to Reset Detection/Stability Circuitry​
    

/* Smart IO clock source selection */
/* Define Clock active */
#define SMART_IO_CLK_ACTIVE 1ul

/* Smart IO port selections macro */
/* Define Smart I/O port */
#define SMART_IO_PORT SMARTIO_PRT13

/* Define Smart I/O Clock */
#define CY_SMARTIO_CLK_INV PCLK_SMARTIO13_CLOCK

/* Bypass channel mask */
/* Define Smart I/O bypass channel */
#define SMARTIO_BYPASS_CH_MASK 0x0Ful /* 00001111: 0000 means [7:4] are not bypassed i.e. programmable SMARTIO is exposed */

/* IO sync channel mask */
/* Define Smart I/O sync channel */
#define SMARTIO_IOSYNC_CH_MASK 0x00ul

/* Lut pin configuration */
/* Define input port to LUT3[4] */
#define GPIO_RST_EN_PORT GPIO_PRT13
#define GPIO_RST_EN_PIN 4ul
#define GPIO_RST_EN_PIN_MUX P13_4_GPIO /* Check signal at BB JP6.7 */

/* Define input port to LUT3[6] */
#define PIN_RST_EN_PORT GPIO_PRT13
#define PIN_RST_EN_PIN 6ul
#define PIN_RST_EN_PIN_MUX P13_6_GPIO /* Check signal at BB JP11.14 */

/* Define input port to LUT3[7] */
#define RST_IN_PORT GPIO_PRT13
#define RST_IN_PIN 7ul
#define RST_IN_PIN_MUX P13_7_GPIO /* Check signal at BB JP11.13 */

/* Define output port to LUT3[5] */
#define RST_OUT_PORT GPIO_PRT13
#define RST_OUT_PIN 5ul
#define RST_OUT_PIN_MUX P13_5_GPIO /* Check signal at BB JP6.6 */

/* LUT output map */
/* Define LUT3[4], LUT3[5], LUT3[6] and LUT3[7] output pattern */
#define LUT4_OUT_MAP 0x80ul
#define LUT5_OUT_MAP 0x28ul
#define LUT6_OUT_MAP 0x7Ful
#define LUT7_OUT_MAP 0x28ul

/* LUT logic circuit type macro */
/* Define LUT logic circuit type */
#define LUTx_LOGIC_OPCODE_COMB CY_SMARTIO_LUTOPC_COMB
#define LUTx_LOGIC_OPCODE_GO CY_SMARTIO_LUTOPC_GATED_OUT
#define LUTx_LOGIC_OPCODE_GI2 CY_SMARTIO_LUTOPC_GATED_TR2

#define CY_SMARTIO_ENABLE 1ul
#define CY_SMARTIO_DISABLE 0ul
#define CY_SMARTIO_DEINIT 0ul
#define CY_SMARTIO_CHANNEL_ALL 0xfful /**< All channels */

/* Port pin configuration */
/******************************************************************************/

/* Configure Port for output (Port13 pin) */
cy_stc_gpio_pin_config_t gpio_rst_cfg =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_STRONG_IN_OFF, /* SmartIO from CPU */
.hsiom = GPIO_RST_EN_PIN_MUX, /* P13_4_GPIO */
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};

/* Configure Port for input (Port13 pin) */
cy_stc_gpio_pin_config_t pin_rst_cfg =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_HIGHZ, /* CPU from SmartIO */
.hsiom = PIN_RST_EN_PIN_MUX, /* P13_6_GPIO */
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};

/* Configure Port for input (Port13 pin) */
cy_stc_gpio_pin_config_t rst_in_cfg =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_HIGHZ, /* CPU from SmartIO */
.hsiom = RST_IN_PIN_MUX, /* P13_7_GPIO */
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};

/* Configure Port for output (Port13 pin) */
cy_stc_gpio_pin_config_t rst_out_cfg =
{
.outVal = 0ul,
.driveMode = CY_GPIO_DM_STRONG_IN_OFF, /* CPU from SmartIO */
.hsiom = RST_OUT_PIN_MUX, /* P13_5_GPIO */
.intEdge = 0ul,
.intMask = 0ul,
.vtrip = 0ul,
.slewRate = 0ul,
.driveSel = 0ul,
};


int main(void)
{
:
Init_IO_Pin(); /* (1) Configure GPIO pin. See Code Listing 9. */

/* Deinit before Init */
Cy_SmartIO_Deinit(SMART_IO_PORT); /* Disable all Smart I/O. See Code Listing 10. */

/* SmartIO peripheral clock divider setting */
/* (3) Configure peripheral Clock */
{
Cy_SysClk_PeriphAssignDivider(CY_SMARTIO_CLK_INV, CY_SYSCLK_DIV_16_BIT, 0ul);
uint32_t sourceFreq = 80000000ul;
uint32_t targetFreq = 12000000ul;
uint32_t divNum = (sourceFreq / targetFreq);

Cy_SysClk_PeriphSetDivider(CY_SYSCLK_DIV_16_BIT, 0ul, (divNum - 1ul));
Cy_SysClk_PeriphEnableDivider(CY_SYSCLK_DIV_16_BIT, 0ul);
}

Init_SmartIO(); /* Initialize Smart I/O. See Code Listing 11. */

Cy_SysEnableApplCore(CY_CORTEX_M4_APPL_ADDR);

Cy_GPIO_Clr(GPIO_PRT13, 4ul);

while(1)
{

}
}
Code Listing 9 Init_IO_Pin() Function​
   
void Init_IO_Pin(void)
{
/* Please check ReadMe.txt for proper connection of Input and Output */
/* Configure Port13 4pin. */
Cy_GPIO_Pin_Init(GPIO_RST_EN_PORT, GPIO_RST_EN_PIN, &gpio_rst_cfg);

/* Configure Port13 pin */
Cy_GPIO_Pin_Init(PIN_RST_EN_PORT, PIN_RST_EN_PIN, &pin_rst_cfg);

/* Configure Port13 pin */
Cy_GPIO_Pin_Init(RST_IN_PORT, RST_IN_PIN, &rst_in_cfg);

/* Configure Port13 pin */
Cy_GPIO_Pin_Init(RST_OUT_PORT, RST_OUT_PIN, &rst_out_cfg);
}
Code Listing 10 Cy_SmartIO_Deinit() Function​
    

void Cy_SmartIO_Deinit(volatile stc_SMARTIO_PRT_t* base)
{
un_SMARTIO_PRT_CTL_t workCTL= {.u32Register = 0ul};
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE; /* (2) Disable all Smart I/O port */
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = CY_SMARTIO_CLK_GATED;
workCTL.stcField.u8BYPASS = CY_SMARTIO_CHANNEL_ALL;
base->unCTL.u32Register = workCTL.u32Register;

base->unSYNC_CTL.u32Register = CY_SMARTIO_DEINIT;
for(uint8_t idx = CY_SMARTIO_LUTMIN; idx < CY_SMARTIO_LUTMAX; idx++)
{
base->unLUT_SEL[idx].u32Register = CY_SMARTIO_DEINIT;
base->unLUT_CTL[idx].u32Register = CY_SMARTIO_DEINIT;
}
base->unDU_SEL.u32Register = CY_SMARTIO_DEINIT;
base->unDU_CTL.u32Register = CY_SMARTIO_DEINIT;
base->unDATA.u32Register = CY_SMARTIO_DEINIT;
}
Code Listing 11 Init_SmartIO() Function​
    

void Init_SmartIO(void)
{
cy_en_smartio_status_t retStatus = (cy_en_smartio_status_t)0xFF;

/* Configure Smart I/O. See Code Listing 12. */
retStatus = Init_SmartIO_Cfg();
if(retStatus == CY_SMARTIO_SUCCESS)
{
/* After all the configuration, enable SMART IO */
/* Enable Smart I/O. See Code Listing 13. */
Cy_SmartIO_Enable(SMART_IO_PORT);
}
}
Code Listing 12 Init_SmartIO_Cfg() Function​
   
cy_en_smartio_status_t Init_SmartIO_Cfg(void)
{
cy_stc_smartio_ducfg_t lutCfgDu;
cy_stc_smartio_lutcfg_t lutCfgLut4;
cy_stc_smartio_lutcfg_t lutCfgLut5;
cy_stc_smartio_lutcfg_t lutCfgLut6;
cy_stc_smartio_lutcfg_t lutCfgLut7;

cy_stc_smartio_config_t smart_io_cfg;
cy_en_smartio_status_t retStatus = (cy_en_smartio_status_t)0xFF;

/* initialize the Smart IO structure */
/* Clear configuration structure */
memset(&lutCfgDu, 0ul, sizeof(cy_stc_smartio_ducfg_t));
memset(&lutCfgLut4, 0ul, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut5, 0ul, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut6, 0ul, sizeof(cy_stc_smartio_lutcfg_t));
memset(&lutCfgLut7, 0ul, sizeof(cy_stc_smartio_lutcfg_t));
memset(&smart_io_cfg, 0ul, sizeof(cy_stc_smartio_config_t));

#ifdef SMART_IO_CLK_ACTIVE
/* Active clock source is selected */
/* Configure Smart I/O clock source */
smart_io_cfg.clkSrc = (cy_en_smartio_clksrc_t)CY_SMARTIO_CLK_DIVACT;
#else
/* Asynchronous clock source is selected */
smart_io_cfg.clkSrc = (cy_en_smartio_clksrc_t)CY_SMARTIO_CLK_ASYNC;
#endif /* SMART_IO_CLK_ACTIVE */

/* Bypass channel mask for input and output pin */
/* Configure BYPASS setting */
smart_io_cfg.bypassMask = SMARTIO_BYPASS_CH_MASK;

/* IO channel sync mask for selected pin */
/* Configure Synchronizer setting */
smart_io_cfg.ioSyncEn = SMARTIO_IOSYNC_CH_MASK;

/*************************** LUT3[4] setting ***************************/
/* Configure LUT3 [4] */
lutCfgLut4.opcode = LUTx_LOGIC_OPCODE_GI2;
lutCfgLut4.lutMap = LUT4_OUT_MAP;

/* Lut configuration for input */
lutCfgLut4.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_CHIP4;
lutCfgLut4.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_CHIP4;
lutCfgLut4.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_IO6;
smart_io_cfg.lutCfg[4] = &lutCfgLut4;

/*************************** LUT3[5] setting ***************************/
/* Configure LUT3 [5] */
/* Lut configuration for output, check description above */
lutCfgLut5.opcode = LUTx_LOGIC_OPCODE_GO;
lutCfgLut5.lutMap = LUT5_OUT_MAP;

/* Lut configuration for input (button) */
lutCfgLut5.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_DU_OUT;
lutCfgLut5.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT5_OUT;
lutCfgLut5.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT4_OUT;
smart_io_cfg.lutCfg[5] = &lutCfgLut5;

/*************************** LUT3[6] setting ***************************/
/* Configure LUT3 [6] */
lutCfgLut6.opcode = LUTx_LOGIC_OPCODE_COMB;
lutCfgLut6.lutMap = LUT6_OUT_MAP;

/* Lut configuration for input */
lutCfgLut6.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT7_OUT;
lutCfgLut6.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT7_OUT;
lutCfgLut6.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT7_OUT;
smart_io_cfg.lutCfg[6] = &lutCfgLut6;

/*************************** LUT3[7] setting ***************************/
/* Configure LUT3 [7] */
lutCfgLut7.opcode = LUTx_LOGIC_OPCODE_GI2;
lutCfgLut7.lutMap = LUT7_OUT_MAP;

/* Lut configuration for input */
lutCfgLut7.tr0 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT4_OUT;
lutCfgLut7.tr1 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_LUT5_OUT;
lutCfgLut7.tr2 = (cy_en_smartio_luttr_t)CY_SMARTIO_LUTTR_IO7;
smart_io_cfg.lutCfg[7] = &lutCfgLut7;

/*************************** DU setting ***************************/
/* Configure DU */
lutCfgDu.tr0 = CY_SMARTIO_DUTR_LUT6_OUT; /**< DU input trigger 0 source selection - LUT[3]6 output*/
lutCfgDu.tr1 = CY_SMARTIO_DUTR_LUT7_OUT; /**< DU input trigger 1 source selection - LUT[3]7 output*/
lutCfgDu.tr2 = CY_SMARTIO_DUTR_ZERO; /**< DU input trigger 2 source selection - Constant 0*/
lutCfgDu.data0 = CY_SMARTIO_DUDATA_ZERO; /**< DU input DATA0 source selection - Fixed 0*/
lutCfgDu.data1 = CY_SMARTIO_DUDATA_DATAREG; /**< DU input DATA1 source selection - SMARTIO_PRTx_DATA.DATA [7:0]*/
lutCfgDu.opcode = CY_SMARTIO_DUOPC_INCR_WRAP; /**< DU op-code */
lutCfgDu.size = CY_SMARTIO_DUSIZE_8; /**< DU width size is 8 */
lutCfgDu.dataReg = 0x10ul; /**< DU DATA register value = 16 */
smart_io_cfg.duCfg = &lutCfgDu;

/*****************************************************************/
/* Initialization of Smart IO structure */
/* Configure Smart I/O. See Code Listing 14. */
retStatus = Cy_SmartIO_Init(SMART_IO_PORT, &smart_io_cfg);
return retStatus;
}
Code Listing 13 Cy_SmartIO_Enable() Function​
    

void Cy_SmartIO_Enable(volatile stc_SMARTIO_PRT_t* base)
{
un_SMARTIO_PRT_CTL_t workCTL = base->unCTL;
workCTL.stcField.u1ENABLED = CY_SMARTIO_ENABLE;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_DISABLE;
base->unCTL.u32Register = workCTL.u32Register; /* (12) Enable Smart I/O. */
}
Code Listing 14 Cy_SmartIO_Init() Function​

cy_en_smartio_status_t Cy_SmartIO_Init(volatile stc_SMARTIO_PRT_t* base, const cy_stc_smartio_config_t* config)
{
cy_en_smartio_status_t status = CY_SMARTIO_SUCCESS;

if(NULL != config)
{
/* (4) Set clock source and bypass to Smart IO */
un_SMARTIO_PRT_CTL_t workCTL = {.u32Register = 0ul};
workCTL.stcField.u1ENABLED = CY_SMARTIO_DISABLE;
workCTL.stcField.u1HLD_OVR = config->hldOvr;
workCTL.stcField.u1PIPELINE_EN = CY_SMARTIO_ENABLE;
workCTL.stcField.u5CLOCK_SRC = config->clkSrc;
workCTL.stcField.u8BYPASS = config->bypassMask;
base->unCTL.u32Register = workCTL.u32Register;

/* (5) Set synchronizer to Smart IO */
un_SMARTIO_PRT_SYNC_CTL_t workSYNC_CTL = {.u32Register = 0ul};
workSYNC_CTL.stcField.u8IO_SYNC_EN = config->ioSyncEn;
workSYNC_CTL.stcField.u8CHIP_SYNC_EN = config->chipSyncEn;
base->unSYNC_CTL.u32Register = workSYNC_CTL.u32Register;

/* LUT configurations - skip if lutCfg is a NULL pointer */
/* (6), (7), (8), (9) Set LUT3 */
for(uint32_t i = CY_SMARTIO_LUTMIN; i < CY_SMARTIO_LUTMAX; i++)
{
if(NULL != config->lutCfg[i])
{
un_SMARTIO_PRT_LUT_SEL_t workLUT_SET = { .u32Register = 0ul };
workLUT_SET.stcField.u4LUT_TR0_SEL = config->lutCfg[i]->tr0;
workLUT_SET.stcField.u4LUT_TR1_SEL = config->lutCfg[i]->tr1;
workLUT_SET.stcField.u4LUT_TR2_SEL = config->lutCfg[i]->tr2;
base->unLUT_SEL[i].u32Register = workLUT_SET.u32Register;

un_SMARTIO_PRT_LUT_CTL_t workLUT_CTL = { .u32Register = 0ul };
workLUT_CTL.stcField.u2LUT_OPC = config->lutCfg[i]->opcode;
workLUT_CTL.stcField.u8LUT = config->lutCfg[i]->lutMap;
base->unLUT_CTL[i].u32Register = workLUT_CTL.u32Register;
}
}

/* DU Configuration - skip if duCfg is a NULL pointer */
/* (10) Set DU */
if(NULL != config->duCfg)
{
un_SMARTIO_PRT_DU_SEL_t workDU_SEL = {.u32Register = 0ul};
workDU_SEL.stcField.u4DU_TR0_SEL = config->duCfg->tr0;
workDU_SEL.stcField.u4DU_TR1_SEL = config->duCfg->tr1;
workDU_SEL.stcField.u4DU_TR2_SEL = config->duCfg->tr2;
workDU_SEL.stcField.u2DU_DATA0_SEL = config->duCfg->data0;
workDU_SEL.stcField.u2DU_DATA1_SEL = config->duCfg->data1;
base->unDU_SEL.u32Register = workDU_SEL.u32Register;

un_SMARTIO_PRT_DU_CTL_t workDU_CTL = {.u32Register = 0ul};
workDU_CTL.stcField.u3DU_SIZE = config->duCfg->size;
workDU_CTL.stcField.u4DU_OPC = config->duCfg->opcode;
base->unDU_CTL.u32Register = workDU_CTL.u32Register;

base->unDATA.stcField.u8DATA = config->duCfg->dataReg;
}
}
Else
{
status = CY_SMARTIO_BAD_PARAM;
}

return(status);
}

Glossary​

Table 24. Glossary

Terms

Description

chip_data

Input signals from HSIOM

Clk_sys/CLK_HF

This is derived from the system clock using a peripheral clock divider. See the Clocking System chapter of the Architecture TRM for details.

DeepSleep

Power mode that only low-frequency peripherals are available. See the DeepSleep Mode section in the Device Power Modes chapter of the Architecture TRM for details.

DU

Data Unit. DU performs simple increment, decrement, increment/decrement, shift, and AND/OR operations based on opcode configuration in register. See the Smart I/O - Data Unit section in the I/O System chapter of the Architecture TRM for details.

GPIO

General-purpose input/output

HSIOM

High Speed I/O Matrix. See the High-Speed I/O Matrix section in the I/O System chapter of the Architecture TRM for details.

io_data_in

Input signals from I/O port

I/O Port

I/O Port provides the interface between the CPU core and peripheral components to the outside world. See the I/O System chapter of the Architecture TRM for details.

LUT3 [x]

3-input Lookup Tables. LUT3 [x] block takes three input signals and generates an output based on the configuration set in register. See the Smart I/O - LUT3 section in the I/O System chapter of the Architecture TRM for details.

smartio_data

Output signals from Smart I/O

The following are the TRAVEO™ T2G family series datasheets and Technical Reference Manuals. Contact Technical Support to obtain these documents.

  • Device datasheet
    • CYT2B7 Datasheet 32-Bit Arm® Cortex®-M4F Microcontroller TRAVEO™ T2G family
    • CYT2B9 Datasheet 32-Bit Arm® Cortex®-M4F Microcontroller TRAVEO™ T2G family
    • CYT4BF Datasheet 32-Bit Arm® Cortex®-M7 Microcontroller TRAVEO™ T2G family
    • CYT4DN Datasheet 32-Bit Arm® Cortex®-M7 Microcontroller TRAVEO™ T2G family
    • CYT3BB/4BB Datasheet 32-Bit Arm® Cortex®-M7 Microcontroller TRAVEO™ T2G family
  • Body Controller Entry Family
    • TRAVEO™ T2G Automotive Body Controller Entry Family Architecture Technical Reference Manual (TRM)
    • TRAVEO™ T2G Automotive Body Controller Entry Registers Technical Reference Manual (TRM) for CYT2B7
    • TRAVEO™ T2G Automotive Body Controller Entry Registers Technical Reference Manual (TRM) for CYT2B9
  • Body Controller High Family
    • TRAVEO™ T2G Automotive Body Controller High Family Architecture Technical Reference Manual (TRM)
    • TRAVEO™ T2G Automotive Body Controller High Registers Technical Reference Manual (TRM) for CYT4BF
    • TRAVEO™ T2G Automotive Body Controller High Registers Technical Reference Manual (TRM) for CYT3BB/4BB
  • Cluster 2D Family
    • TRAVEO™ T2G Automotive Cluster 2d Family Architecture Technical Reference Manual (TRM)
    • TRAVEO™ T2G Automotive Cluster 2d Registers Technical Reference Manual (TRM)
  • Application Note
    • AN220193 - GPIO USAGE SETUP IN TRAVEO™ T2G FAMILY
    • AN220208 - CLOCK CONFIGURATION SETUP IN TRAVEO™ T2G BODY ENTRY FAMILY
    • AN224434 - CLOCK CONFIGURATION SETUP IN TRAVEO™ T2G FAMILY CYT4B SERIES
    • AN226071 - CLOCK CONFIGURATION SETUP IN TRAVEO™ T2G FAMILY CYT4D SERIES
    • AN229513 - CLOCK CONFIGURATION SETUP IN TRAVEO™ T2G FAMILY CYT2C SERIES

Other references​

A Sample Driver Library (SDL) including startup as sample software to access various peripherals is provided. SDL also serves as a reference, to customers, for drivers that are not covered by the official AUTOSAR products. The SDL cannot be used for production purposes as it does not qualify to any automotive standards. The code snippets in this application note are part of the SDL. Contact Technical Support to obtain the SDL.

Revision history​

Document version

Date of release

Description of changes

**

2018-09-27

New application note.

*A

2019-06-17

Updated Associated Part Family as “TRAVEO™ T2G family CYT2B/CYT4B Series”.

Added target part numbers “CYT4B Series” related information in all instances across the document.

*B

2019-11-20

Updated Associated Part Family as “TRAVEO™ T2G family CYT2B/CYT4B/CYT4D Series”.

Added target part numbers “CYT4D Series” related information in all instances across the document.

*C

2020-06-29

Updated Associated Part Family as “TRAVEO™ T2G family CYT2/CYT3/CYT4 Series”.

Changed target part numbers from “CYT2B/CYT4B/CYT4D Series” to “CYT2/CYT4 Series” in all instances across the document.

Added target part numbers “CYT3 Series” in all instances across the document.

*D

2021-04-16

Updated Example Configuration:

Added example of SDL Code and description in all instances.

Updated to Infineon template.

*E

2023-11-10

Template update; no content updated.

1 Subscripts x in register names used in this sentence are Port number

2 Subscripts y in register names used in this sentence are LUT3 number.