1. You can set the default debugger options for CMSIS-DAP or J-Link. See

    Program/Debug with KitProg3/MiniProg4 (CMSIS-DAP)

    or

    Program/Debug with J-Link

    .


    Note:

    If using J-Link with a PSOC™ 64 "Secure Boot" MCU, you must specify a special type of

    Reset

    "Core" under the

    J-Link > Setup

    tab, as shown:


    ../figures/image30.png

  2. Select

    Project > Download > Download file…

    and select the

    <project_name>.hex

    file in

    <project_root >\Debug\Exe

    .


    ../figures/image19.png

  3. Select

    Project > Debug without Downloading

    .