Download/install software
ModusToolbox™ software
Download the ModusToolbox™ Setup program from
https://softwaretools.infineon.com/tools/com.ifx.tb.tool.modustoolboxsetup
. Refer to the instructions in the
ModusToolbox™ software installation guide
for how to install the necessary ModusToolbox™ tools and packages.
Once installation of all the tools is complete, click
Run
to launch the Dashboard.

IAR Embedded Workbench (Windows only)
We recommend and have tested IAR Embedded Workbench version 9.60.3 or later for PSOC™ Control C3 devices. This version can be used with all ModusToolbox™ supported devices.
The default installation location for the IAR compiler is
C:\iar[version]\arm
. Set the
CY_COMPILER_IAR_DIR
environment variable to the correct installation path using forward slashes. Alternatively, you can set this variable in the
Makefile
for each application. Refer to the
ModusToolbox™ tools package user guide
for more details about build system variables.