About this document​

Scope and purpose​

This application note introduces you to

PSOC™ 4

, an Arm® Cortex®-M0/M0+ based programmable system-on-chip. It helps you explore the

PSOC™ 4

architecture and development tools and explains you how to create your first project using PSOC™ Creator and ModusToolbox™, the development tools for

PSOC™ 4

; also guides you to more resources to accelerate in-depth learning about

PSOC™ 4

.

Intended audience​

This application note is intended for engineers new to PSOC™ and ModusToolbox™, and those with experience in working with embedded microcontrollers.

Associated part family​

All

PSOC™  4

parts

Software version​

PSOC™  Creator

4.4 SP2 or higher,

ModusToolbox™

3.2 or higher.

More code examples? We heard you.​

To access an ever-growing list of

PSOC™ 4

code examples using ModusToolbox™, please visit the

GitHub

site

. You can also explore the

PSOC™

video library

.

Introduction​

PSOC™ 4

is a true programmable embedded system-on-chip integrating custom analog and digital peripheral functions, memory, and an Arm® Cortex®-M0 or Cortex®-M0+ microcontroller on a single chip. This type of system is different from most mixed-signal embedded systems, which use a combination of a microcontroller unit (MCU) and external analog and digital peripherals. These systems typically require many integrated circuits in addition to the MCU, such as opamps, ADCs, and Application-specific Integrated Circuit (ASICs).

PSOC™ 4

provides a low-cost alternative to the combination of MCU and external ICs. In addition to reducing overall system cost, the programmable analog and digital subsystems allow great flexibility, in-field tuning of the design, and speedy time to market.

The capacitive touch-sensing feature in

PSOC™ 4

, known as CAPSENSE™, offers unprecedented signal-to-noise ratio; best-in-class liquid tolerance and a wide variety of sensor types such as buttons, sliders, trackpads, and proximity sensors.

PSOC™ 4

offers a best-in-class current consumption of 150 nA while retaining SRAM, programmable logic, and the ability to wake up from an interrupt.

PSOC™ 4

consumes only 20 nA while maintaining wakeup capability in its non-retention power mode. The

PSOC™ 4

family of devices also contain

PSOC™ 4

Bluetooth® LE, which integrates a Bluetooth® Low Energy radio system. For more details on

PSOC™ 4

Bluetooth® LE, see

AN91267

.

Using this document

The next few pages describe

PSOC™ 4

and the advantages of designing with PSOC™, ModusToolbox™, and PSOC™ Creator. Or, you can jump right in and quickly build a simple design in ModusToolbox™ – go to

Getting started with PSOC 4000T design

. If you are using PSOC™ Creator – go to

My first

PSOC™ 4

design using PSOC™ Creator

.

Development ecosystem​

PSOC resources​

The wealth of information available on the

Infineon

webpage can help you select the right PSOC™ device and, additionally, integrate the device into your designs efficiently and effectively. The following is an abbreviated list for

PSOC™ 4

:

Firmware/application development​

There are two development platforms that you can use for application development with

PSOC™ 4000T

:

  • ModusToolbox™:

    This software includes configuration tools, low-level drivers, middleware libraries, and other packages that enable you to create MCU and wireless applications. All tools run on Windows, macOS, and Linux. ModusToolbox™ includes an Eclipse IDE, which provides an integrated flow with all the ModusToolbox™ tools. Other IDEs such as Visual Studio Code, IAR Embedded Workbench and Arm® MDK (μVision) are also supported.

    ModusToolbox™ software supports stand-alone device and middleware configurators. Use the configurators to set the configuration of different blocks in the device and generate code that can be used in firmware development.

    ModusToolbox™ supports all PSOC™ 6 MCU and the latest

    PSOC™ 4

    MCU devices.

    Table 1

    lists the supported

    PSOC™ 4

    devices. Infineon recommends you to use ModusToolbox™ for all application development for supported

    PSOC™ 4

    devices. For more information, see ModusToolbox™ tools package user guide.

    Table 1.List of PSOC™ 4 devices supported in ModusToolbox™

    Devices

    1

    ModusToolbox™

    PSOC™ Creator

    PSOC™ 4000S, PSOC™ 4100S, PSOC™ 4100S Plus, PSOC™ 4100S Plus 256K

    Yes

    Yes

    PSOC™ 4100S Max, PSOC™ 4000T, PSOC™ 4100T Plus

    Yes

    No

    All other

    PSOC™ 4

    devices

    No

    Yes

    The libraries and enablement software are available on

    GitHub

    .

    ModusToolbox™ tools and resources can also be used in the command line. For more information, see the “ModusToolbox™ build system” section in the

    ModusToolbox™ tools package user guide

    .

  • PSOC™ Creator:PSOC™ Creator is a free Windows-based IDE. It enables concurrent hardware and firmware design of PSOC™ 3,PSOC™ 4, PSOC™ 5LP, and PSOC™ 6 MCU systems. Applications are created using schematic capture and over 150 pre-verified, production-ready peripheral Components.

Choosing an IDE

Figure 1

helps you to choose an appropriate IDE.

Figure 1.

Choosing an IDE



ModusToolbox™ software, the latest-generation toolset, is supported across Windows, Linux, and macOS platforms. ModusToolbox™ software supports 3rd-party IDEs, including the Eclipse IDE, Visual Studio Code, Arm® MDK (μVision), and IAR Embedded Workbench. The tools package includes an implementation for all the supported IDEs. The tools support all

PSOC™ 4000T

s. The associated BSP and library configurators also work on all three host operating systems.

Figure 2.

ModusToolbox™ environment



Certain features of the

PSOC™ 4000T

, such as UDBs (Universal Digital Blocks) and USB are not supported in ModusToolbox™ version 2.x and earlier. Newer versions of ModusToolbox™ support the USB host feature and improve the user experience with true multi-core debug support.

It is recommended to use ModusToolbox™ if you want to build an IoT application using IoT devices or if you are using a

PSOC™ 4000T

not supported in PSOC™ Creator.

PSOC™ Creator is the long-standing proprietary tool that runs on Windows only. This mature IDE includes a graphical editor that supports schematic based design entry with the help of Components. PSOC™ Creator supports all

PSOC™

3,

PSOC™

4, and

PSOC™

5LP devices, and a subset of

PSOC™ 4000T

devices.

Choose PSOC™ Creator if you are using a graphical editor for design entry and code generation, and if the

PSOC™

MCU that you are planning to use is supported by the IDE.

ModusToolbox software

ModusToolbox™ software is a set of tools and software that enables an immersive development experience for creating converged MCU and wireless systems, and enables you to integrate our devices into your existing development methodology. These include configuration tools, low-level drivers, libraries, and operating system support, most of which are compatible with Linux-, macOS-, and Windows-hosted environments.

Figure 3

shows a high-level view of what is available as part of ModusToolbox™ software. For a more in-depth overview of the ModusToolbox™ software, see

ModusToolbox™ tools package user guide

.

Figure 3.

ModusToolbox™ software



The ModusToolbox™ tools package installer includes the design configurators and tools, and the build system infrastructure.

The build system infrastructure includes the new project creation wizard that can be run independent of the Eclipse IDE, the make infrastructure, and other tools.

This means you choose your compiler, IDE, RTOS, and ecosystem without compromising usability or access to our industry-leading CAPSENSE™ (Human-Machine Interface), AIROC™ Wi-Fi and Bluetooth®, security, and various other features.

One part of the ModusToolbox™ ecosystem is run-time software that helps you rapidly develop Wi-Fi and Bluetooth® applications using connectivity combo devices. See the

ModusToolbox™ run-time software reference guide

for details.

Design configurators are the tools that help you create the configurable code for your BSP/Middleware. Jump to

Configurators

to know more about it.

All the application-level development flows depend on the provided low-level resources. These include:

  • Board support packages (BSP) – A BSP is the layer of firmware containing board-specific drivers and other functions. The BSP is a set of libraries that provides APIs to initialize the board and access to board level peripherals. It includes low-level resources such as peripheral driver library (PDL) for PSOC™ 4000T and has macros for board peripherals. It uses the HAL to configure the board. Custom BSPs can be created to enable support for end-application boards. See BSP Assistant to create your BSP.

  • Hardware abstraction layer (HAL)– The hardware abstraction layer (HAL) provides a high-level interface to configure and use hardware blocks on MCUs. It is a generic interface that can be used across multiple product families. The focus on ease-of-use and portability means the HAL does not expose all the low-level peripheral functionality. The HAL wraps the lower level drivers (like PSOC™ 4000T PDL) and provides a high-level interface to the MCU. The interface is abstracted to work on any MCU. This helps you write application firmware independent of the target MCU.

    The HAL can be combined with platform-specific libraries (such as PSOC™ 4000T PDL) within a single application. You can leverage the HAL's simpler and more generic interface for most of an application, even if one portion requires lower-level control.

  • PSOC™ 4000Tperipheral driver library (PDL)– The PDL integrates device header files, start-up code, and peripheral drivers into a single package. The PDL supports the PSOC™ 4000T family. The drivers abstract the hardware functions into a set of easy-to-use APIs. These are fully documented in the PDL API Reference.

    The PDL reduces the need to understand register usage and bit structures, thus easing software development for the extensive set of peripherals in the PSOC™ 4000T series. You configure the driver for your application, and then use API calls to initialize and use the peripheral.

  • Middleware (MW) – Extensive middleware libraries that provide specific capabilities to an application. The available middleware spans across connectivity (OTA, Bluetooth®, AWS IoT, Bluetooth® LE, Secure Sockets) to PSOC™ 4000T-specific functionality (CAPSENSE™, USB, device firmware upgrade (DFU), emWin). All the middleware is delivered as libraries and via GitHub repositories.

ModusToolbox applications

With the release of ModusToolbox™ v3.x, multi-core support is introduced, which has altered the folder structure slightly from the previous version of ModusToolbox™, but

PSOC™ 4

has single core only.

Figure 4.

Application type



The following shows the new folder structure for an example single-core application:

Figure 5.

Folder structure for single-core applications



PSOC 4

software resources

The software for

PSOC™ 4000T

s includes configurators, drivers, libraries, middleware, as well as various utilities, makefiles, and scripts. It also includes relevant drivers, middleware, and examples for use with IoT devices and connectivity solutions. You can use any or all tools in any environment you prefer.

Configurators

ModusToolbox™ software provides graphical applications called configurators that make it easier to configure a hardware block. For example, instead of having to search through all the documentation to configure a serial communication block as a UART with a desired configuration, open the appropriate configurator and set the baud rate, parity, and stop bits. Upon saving the hardware configuration, the tool generates the "C" code to initialize the hardware with the desired configuration.

There are two types of configurators: BSP configurators that configure items that are specific to the MCU hardware and library configurators that configure options for middleware libraries.

Configurators are independent of each other, but they can be used together to provide flexible configuration options. They can be used stand alone, in conjunction with other tools, or within a complete IDE. Configurators are used for:

  • Setting options and generating code to configure drivers

  • Setting up connections such as pins and clocks for a peripheral

  • Setting options and generating code to configure middleware

For

PSOC™ 4

applications, the available Configurators include:

  • Device Configurator: Sets up the system (platform) functions and the basic peripherals (for example, UART, Timer, PWM).

  • CAPSENSE™ Configurator and Tuner: Configures CAPSENSE™ and generates the required code.

  • Smart I/O Configurator: Configures the Smart I/O.

Each of the above configurators create their own files (For example,

design.cycapsense

for CAPSENSE™). BSP configurator files (For example,

design.modus

or

design.cycapsense

) are provided as part of the BSP with default configurations while library configurators (e.g. design.cybt) are provided by the application. When an application is created based on Infineon BSP, the application makes use of BSP configurator files from the Infineon BSP repo. You can customize/create all the configurator files as per your application requirement using ModusToolbox™ software. See

BSP Assistant

to create your custom BSP. See

ModusToolbox™ help

for more details.

Library management for

PSOC 4000T

The application can have shared/local libraries for the projects. If needed, different projects can use different versions of the same library. The shared libraries are downloaded under the

mtb_shared

directory. The application should use the

deps

folder to add library dependencies. The

deps

folder contains files with the

.mtb

file extension, which is used by ModusToolbox™ to download its git repository. These libraries are direct dependencies of the ModusToolbox™ project.

The Library Manager helps to add/remove/update the libraries of your projects. It also identifies whether particular library has a direct dependency on any other library using the manifest repository available on GitHub, and fetches all its dependencies. These dependency libraries are indirect dependencies of the ModusToolbox™ project. These dependencies can be seen under the

libs

folder. For more information, see the

Library Manager user guide

located at

<install_dir> /ModusToolbox/tools_<version>/library-manager/docs/library-manager.pdf

.

Software development for

PSOC 4000T

The ModusToolbox™ ecosystem provides significant source code and tools to enable software development for

PSOC™ 4000T

s. You use tools to:

  • Specify how you want to configure the hardware.

  • Generate code for that purpose, which you use in your firmware.

  • Include various middleware libraries for additional functionality, like Bluetooth® LE connectivity or FreeRTOS.

This source code makes it easier to develop the firmware for supported devices. It helps you quickly customize and build firmware without the need to understand the register set.

In the ModusToolbox™ environment, you use configurators to configure either the device, or a middleware library, like the Bluetooth® LE stack or CAPSENSE™. The BSP configurator files are used to configure device peripherals, pins, and memory using peripheral driver library code. The middleware is delivered as separate libraries for each feature/function such that it can be used across multiple platforms. For example, abstractionrtos, lwip, usb, etc.

Firmware developers who wish to work at the register level should refer to the driver source code from the PDL. The PDL includes all the device-specific header files and startup code you need for your project. It also serves as a reference for each driver. Because the PDL is provided as source code, you can see how it accesses the hardware at the register level.

Some devices do not support particular peripherals. The PDL is a superset of all the drivers for any supported device. This superset design means:

  • All API elements needed to initialize, configure, and use a peripheral are available.

  • The PDL is useful across various PSOC™ 4000Ts, regardless of available peripherals.

  • The PDL includes error checking to ensure that the targeted peripheral is present on the selected device.

This enables the code to maintain compatibility across products of the

PSOC™ 4000T

family, as long as the peripherals are available. A device header file specifies the peripherals that are available for a device. If you write code that attempts to use an unsupported peripheral, you will get an error at compile time. Before writing code to use a peripheral, consult the datasheet for the particular device to confirm support for that peripheral.

As the following figure shows, with the ModusToolbox™ software, you can:

  1. Choose a BSP (Project Creator).

  2. Create a new application based on a list of starter applications, filtered by the BSPs that each application supports (Project Creator).

  3. Add BSP or middleware libraries (Library Manager).

  4. Develop your application firmware using

    the HAL or

    PDL for

    PSOC™ 4000T

    (IDE of choice or command line).

Figure 6.

ModusToolbox™ resources and middleware



ModusToolbox help

The ModusToolbox™ ecosystem provides documentation and training. One way to access it is launching the Eclipse IDE for ModusToolbox™ software and navigating to the following

Help

menu items:

Choose

Help

>

ModusToolbox™ General Documentation

:

  • ModusToolbox™ Documentation Index:

    Provides brief descriptions and links to various types of documentation included as part the ModusToolbox™ software.

  • ModusToolbox™ Installation Guide:

    Provides instructions for installing the ModusToolbox™ software.

  • ModusToolbox™ User Guide:

    This guide primarily covers the ModusToolbox™ aspects of building, programming and debugging applications. It also covers various aspects of the tools installed along with the IDE.

  • ModusToolbox™ Training Material: Links to the training material available at https://github.com/Infineon/training-modustoolbox.

  • Release Notes

For documentation on Eclipse IDE for ModusToolbox™, choose

Help

>

Eclipse IDE for ModusToolbox™ Documentation

:

  • User Guide:

    Provides descriptions about creating applications as well as building, programming, and debugging them using Eclipse IDE

  • Eclipse IDE Survival Guide

1

PSOC™ 4 feature set

for complete PSOC™ 4 portfolio.

Support for other IDEs​

You can develop firmware for

PSOC™ 4000T

s using your preferred IDE such as Eclipse IDE,

IAR Embedded Workbench

,

Keil µVision 5

, or

Visual Studio Code

.

ModusToolbox™ Configurators are stand-alone tools that can be used to set up and configure

PSOC™ 4000T

resources and other middleware components without using the Eclipse IDE. The Device Configurator and middleware configurators use the

design.x

files within the application workspace. You can then point to the generated source code and continue developing firmware in your IDE.

If there is a change in the device configuration, edit the

design.x

files using the configurators and regenerate the code. It is recommended that you generate resource configurations using the configuration tools provided with ModusToolbox™ software.

See

ModusToolbox™ tools package user guide

for details.

PSOC Creator​

PSOC™ Creator

is an IDE that enables concurrent hardware and firmware editing, compiling, and debugging of PSOC™ systems. Do the following to browse through PSOC™ Creator, as shown in

Figure 7

:

  1. Drag and drop Components to build your hardware system design

  2. Co-design your application firmware with the PSOC™ hardware

  3. Configure Components with config tools

  4. Explore the library of more than 100 Components

  5. Review Component datasheets

Figure 7.

Features of PSOC™ Creator features



PSOC Creator help

Download the PSOC™ Creator’s latest version from the

PSOC™ Creator

home page, launch the PSOC™ Creator, and navigate to the following:

  • Quick Start Guide: Choose Help > Documentation > Quick Start Guide. This guide gives you the basics for developing PSOC™ Creator projects.

  • Simple Component example projects: Choose File > Open > Example projects. These example projects demonstrate how to configure and use PSOC™ Creator Components.

  • System Reference Guide: Choose Help > System Reference > System Reference Guide. This guide lists and describes the system functions provided by PSOC™ Creator.

  • Component datasheets: Right-click a Component and select Open Datasheet. Visit the PSOC™  4 Component datasheets page for a list of all PSOC™ 4 Component datasheets.

  • PSOC™ Creator training videos: These videos provide step-by-step instructions on how to get started with PSOC™ Creator.

  • Document Manager: PSOC™ Creator provides a document manager to help you to find and review document resources easily. To open the document manager, choose the menu item Help > Document Manager.

Technical support​

If you have any questions, our technical support team is happy to assist you. You can create a support request on the

Technical support

page. The support team monitors and responds to your questions, issues, and bug reports posted on the

GitHub

repositories.

1

PSOC™ 4 feature set

for complete PSOC™ 4 portfolio.

PSOC 4 feature set​

PSOC™ 4

has an extensive set of features, which include a CPU and memory subsystem, a digital subsystem, an analog subsystem, and system resources, as shown in

Figure 8

. The following sections describe each feature. For more information, see the

PSOC™ 4

family device datasheets, technical reference manuals (TRMs), and application notes listed in

PSOC™ resources

.

Figure 8.

PSOC™ 4000T architecture



The

PSOC™ 4

portfolio consists of several families of Arm® CM0 and CM0+ microcontrollers. Most devices in the portfolio have CAPSENSE™ technology for capacitive-sensing applications. Other key features of the

PSOC™ 4

portfolio include a customizable analog front end through programmable analog blocks and wired and wireless connectivity options such as USB, Controller Area Network (CAN), and Bluetooth® LE. These unique features make

PSOC™ 4

the industry’s most flexible and scalable low-power mixed-signal architecture. The

PSOC™ 4

devices are classified as different families, as shown in

Table 2

, based on different features.

Table 2.

PSOC™ 4

families

Classification

Family

Features

Details

Entry level

PSOC™ 4

000 family

CAPSENSE™

Table 3

Intelligent analog

PSOC™ 4

100 family

CAPSENSE™ + Programmable Analog

Table 4

Programmable digital

PSOC™ 4

200 family

CAPSENSE™ + Programmable Analog + Programmable Digital Blocks

Table 5

Application specific

PSOC™ 4

500 family

CAPSENSE™ + Motor Control

Table 6

PSOC™ 4

700 family

CAPSENSE™ + Inductive Sensing

Analog coprocessor

2

PSOC™ 4

A00 family

CAPSENSE™ + Programmable Analog Blocks

AN211293

Note:

In

Table 3

and

Table 4

, the columns highlighted in green indicate that the device family is supported in ModusToolbox™.

Table 3.

PSOC™ 4000 family features

Features

PSOC™ 4000

PSOC™ 4000S

PSOC™ 4000T

CPU

16-MHz Cortex®-M0

48-MHz Cortex®-M0+

48-MHz Cortex®-M0+

Flash memory

16 KB

32 KB

64 KB

SRAM

2 KB

4 KB

8 KB

GPIOs

20

36

21

CAPSENSE™

Sense pins

16

35

19

Ultra-Low Power Wake on Touch (WoT)

No

No

Yes

CAPSENSE™ IP Generation

Fourth-generation

Fifth-generation

Fifth-generation Low Power

Single-slope ADC (10-bit 46-ksps)

None

1

None

Comparators

1 CSD comparator with a fixed threshold (1.2 V)

Two low-power comparators with wakeup feature

None

IDACs

3

One 7-bit and one 8-bit

Two 7-bits

None

Smart I/O ports

None

2

None

Power supply range

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

Low-power modes

Deep Sleep at 2.5 µA

Deep Sleep at 2.5 µA

Deep Sleep at 2.5 µA

Segment LCD drive

None

4 COM segment LCD drive

None

Serial communication

One I2C

Two SCBs with programmable I2C, SPI, or UART

1 SCB with programmable I2C, SPI, or UART. 1 SCB having I

2

C only

Timer Counter Pulse-Width Modulator (TCPWM)

1

5

2

Clocks

Internal main oscillator (IMO)

24 MHz/32 MHz

24 MHz to 48 MHz

24 MHz to 48 MHz

Internal low-speed oscillator (ILO)

32-kHz internal ILO

40 kHz

40 kHz

Watch crystal oscillator (WCO)

None

32-kHZ

None

Power supply monitoring

Power-on reset (POR)Brown-out detection (BOD)

POR, BOD

POR, BOD

Supported kit

CY8CKIT-040 pioneer kit

CY8CKIT-040T PSOC™ 4000T CAPSENSE™ Evaluation Kit

,

CY8CPROTO-040T PSOC™ 4000T CAPSENSE™ Prototyping Kit

, and

CY8CPROTO-040T-MS Multi-Sense Prototyping Kit

Supported IDE

PSOC™ Creator

PSOC™ Creator

,

ModusToolbox™

ModusToolbox™

Table 4.

PSOC™ 4100 family features

Features

PSOC™

4100

PSOC™

4100S

PSOC™

4100S

Plus

PSOC™

4100S Plus

256K

PSOC™

4100PS

PSOC™

4100M

PSOC™

4100 BL

4

PSOC™

4100S

Max

PSOC™

4100T

Plus

CPU

24-MHz Cortex®-M0

48-MHz Cortex®-M0+

48-MHz Cortex®-M0+

48-MHz Cortex®-M0+

48-MHz Cortex®-M0+

24-MHz Cortex®-M0

24-MHz Cortex®-M0

48-MHz Cortex®-M0+

48-MHz Cortex®-M0+

DMA

N/A

N/A

8 channels

8 channels

8 channels

8 channels

8 channels

16 channels

8 channels

Flash memory

32 KB

64 KB

128 KB

256 KB

32 KB

128 KB

256 KB

384 KB

128 KB

SRAM

4 KB

8 KB

16 KB

32 KB

4 KB

16 KB

32 kB

32 KB

32 KB

GPIOs

36

36

54

54

38

55

36

84

53

CAPSENSE™

1 channel, 35 sensors

1 channel,

35 sensors

1 channel,

53 sensors

1 channel,

53 sensors

1 channel,

33 sensors

2 channels,

54 sensors

1 channel,

35 sensors

2 channels,

80 sensors (32 control mux)

1 channel,

32 sensors

12-bit SAR ADC with sequencer

806-KSPS

1-MSPS

1-MSPS

1-MSPS

1-MSPS

806-KSPS

806-KSPS

1-MSPS

1-MSPS

Opamps (programmable)

2

2

2

2

4/PGA

4

2

2

None

Programmable Voltage Reference (PVref)

None

None

None

None

Four channels

None

None

None

None

Voltage DAC (VDAC)

None

None

None

None

Two 13-bit VDAC

None

None

None

None

Comparators (low power with wakeup feature)

2

2

2

2

2

2

2

2

None

IDACs

5

One 7-bit and one 8-bit

Two 7-bits

Two 7-bits

Two 7-bits

Two 7-bits

Two 7-bits and two 8-bits

One 7-bit and one 8-bit

None

None

Smart I/O ports

None

2

3

2

1

None

None

3

1

Power supply range

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 2.5 µA

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

Low-power modes

Deepsleep

1.3 µA

2.5 µA

2.5 µA

2.5 µA

2.5 µA

1.35 µA

2.5 µA

2.5 µA

2.5 µA

Hibernate

150 nA

NA

NA

NA

NA

150 nA

NA

NA

None

Stop

20 nA

NA

NA

NA

NA

35 nA

NA

NA

None

Segment LCD drive

4 COM

4 COM

4 COM

4 COM

4 COM

4 COM

4 COM

4 COM

None

SCBs with programmable I2C, SPI, or UART

2

3

5

5

3

4

2

5

5 (2 SCB, 3 UART)

TCPWM

4

5

8

8

8

8

4

8

6

CAN

None

None

1

None

None

None

None

1

None

BLE

None

None

None

None

None

None

4.1/4.2

None

None

Clocks

IMO

3 MHz to 24 MHz

24 MHz to 48 MHz

24 MHz to 48 MHz

24 MHz to 48 MHz

24 MHz to 48 MHz

3 MHz to

48 MHz

24 MHz to 48 MHz

24 MHz to 48 MHz

24 MHz to 48 MHz

ILO

32 kHz

40 kHz

40 kHz

40 kHz

40 kHz

32 kHz

40 kHz

40 kHz

40 kHz

WCO

Nil

32 kHz

32 kHz

32 kHz

32 kHz

32 kHz

32 kHz

32 kHz

32 kHz

Power supply monitoring

POR, BOD, Low-voltage detection (LVD)

POR, BOD

POR, BOD

POR, BOD

POR, BOD

POR, BOD, LVD

POR, BOD, LVD

POR, BOD

POR, BOD

Supported kit

CY8CKIT-149 prototyping kit

CY8CKIT-147 prototyping kit

CY8CKIT-044 pioneer kit

CY8CKIT-042 BLE pioneer kit

CY8CKIT-041S-MAX pioneer kit

PSOC™ 4100T Plus CAPSENSE™ prototyping kit

Supported IDE

PSOC™ Creator

PSOC™ Creator

,

ModusToolbox™

PSOC™ Creator

,

ModusToolbox™

PSOC™ Creator

,

ModusToolbox™

PSOC™ Creator

PSOC™ Creator

PSOC™ Creator

ModusToolbox™

ModusToolbox™

Table 5.

PSOC™ 4200 family features

Features

PSOC™ 4200

PSOC™ 4200DS

PSOC™ 4200M

PSOC™ 4200L

PSOC™ 4200 BL

6

CM0 CPU

48 MHz Cortex®-M0

48 MHz Cortex®-M0

48 MHz Cortex®-M0

48 MHz Cortex®-M0

48 MHz Cortex®-M0

DMA

None

8 channels

8 channels

32 channels

None

Flash memory

32 KB

64 KB

128 KB

256 KB

256 KB

SRAM

4 KB

8 KB

16 KB

32 KB

32 KB

GPIOs

36

21

55

96

36

CAPSENSE™

1 channel, 35 sensors

None

2 channels, 54 sensors

2 channels, 94 sensors

1 channel, 35 sensors

ADC (12-bit, 1-MSPS SAR ADC with sequencer)

1

None

1

1

1

Opamps (programmable)

2

None

2

4

2

Comparators (low power with wakeup feature)

2

2

2

2

2

IDACs

7

One 7-bits and one 8-bit

None

Two 7-bits and two 8-bits

Two 7-bits and two 8-bits

One 7-bit and one 8-bit

Programmable logic blocks (UDBs)

4

4

4

8

4

Smart I/O ports

None

1

None

None

None

Power supply range

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

1.71 V to 5.5 V

Low-power modes

Deep Sleep

1.3 µA

2 µA

1.3 µA

1.3 µA

1.5 µA

Hibernate

150 nA

NA

150 nA

150 nA

150 nA

Stop

20 nA

NA

20 nA

20 nA

20 nA

Segment LCD drive

4 COM

None

4 COM

8 COM

4 COM

SCBs with programmable I2C, SPI, or UART

2

3

4

4

2

TCPWM

4

4

8

8

4

CAN

None

None

2

2

None

BLE

None

None

None

None

4.1/4.2

USB Full Speed Device Controller (USB)

None

None

None

Yes

None

Clocks

IMO

3 MHz to 48 MHz

3 MHz to 48 MHz

3 MHz to 48 MHz

3 MHz to 48 MHz

3 MHz to 48 MHz

ILO

32 kHz

40 kHz

32 kHz

32 kHz

32 kHz

WCO

None

None

32 kHz

32 kHz

32 kHz

External crystal oscillator (ECO)

None

None

4 MHz to 33 MHz

None

None

Power supply monitoring

POR, BOD, LVD

POR, BOD

POR, BOD, LVD

POR, BOD, LVD

POR, BOD, LVD

Supported kit

CY8CKIT-042 pioneer kit

CY8CKIT-146 prototyping kit

CY8CKIT-044 pioneer kit

CY8CKIT-046 pioneer kit

CY8CKIT-042 Bluetooth® LE pioneer kit

Supported IDE

PSOC™ Creator

PSOC™ Creator

PSOC™ Creator

PSOC™ Creator

PSOC™ Creator

Table 6.

PSOC™ 4500 and PSOC™ 4700 family features

Features

PSOC™ 4500S

PSOC™ 4700S

CM0+ CPU

48 MHz Cortex®-M0+

48 MHz Cortex®-M0+

DMA

8 channels

None

Flash memory

256 KB

32 KB

SRAM

32 KB

4 KB

GPIOs

53

36

CAPSENSE™

1 channel, 52 sensors

1 channel, 35 sensors

MagSense

None

1 channel

ADC

Two 12-bits, 1-MSPS SAR ADCs with sequencer

10-bit, 16.8-ksps Single slope ADC

Opamps (programmable)

4

None

Comparators (low power with wakeup feature)

2

2

IDACs

8

Two 7-bits

Two 7-bits

Smart I/O ports

2

2

Power supply range

1.71 V to 5.5 V

1.71 V to 5.5 V

Low-power modes

Deep Sleep

1.3 µA

2.5 µA

Hibernate

150 nA

NA

Stop

20 nA

NA

Segment LCD drive

4 COM

8 COM

SCBs with programmable I2C, SPI, or UART

5

2

TCPWM

8

5

Motor Control Acceleration (MCA)

2

None

Clocks

IMO

24 MHz to 48 MHz

24 MHz to 48 MHz

ILO

40 kHz

40 kHz

WCO

32 kHz

32 kHz

ECO

4 MHz to 33 MHz

None

Power supply monitoring

POR, BOD

POR, BOD

Supported kit

CY8CKIT-045S pioneer kit

CY8CKIT-148 evaluation kit

Supported IDE

PSOC™ Creator

PSOC™ Creator

2

See

AN211293

for getting started with PSOC™ 4 analog coprocessor family devices.

3

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM for more details.

4

See

AN91267

for getting started with PSOC™ 4 Bluetooth® LE Family devices.

5

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM more details.

6

See

AN91267

for getting started with PSOC™ 4 Bluetooth® LE family devices.

7

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM for more details.

8

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM for more details.

PSOC is more than an MCU​

Figure 9

shows that a typical MCU contains a CPU (such as 8051 or an Arm® Cortex®) with a set of peripheral functions such as ADCs, DACs, UARTs, SPIs, and general I/O, all linked to the CPU’s register interface. Within the MCU, the CPU is the “heart” of the device – the CPU manages everything from setup to data movement to timing. Without the CPU, the MCU cannot function.

Figure 10

shows that PSOC™ is quite different. With PSOC™, the CPU, analog, digital, and I/O are equally important resources in a programmable system. It is the system’s interconnect and programmability that is the heart of PSOC™ – not the CPU. The peripheral analog and digital are interconnected with a highly configurable matrix of signal and data bus meshing that allows you to create custom designs that meet your application requirements. You can program PSOC™ to emulate an MCU, but you cannot program an MCU to emulate PSOC™.

Figure 9.

Typical MCU block diagram



Figure 10.

PSOC™ block diagram



A typical MCU requires CPU firmware to process state machines, use a timer for timing, and drive an output pin. Therefore, the functional path is always through the CPU. However, with PSOC™, asynchronous parallel processing is possible. You can configure a PSOC™ to have elements that operate independently from the CPU. The projects included with this application note demonstrate this concept. The PSOC™ is configured to make an LED blink without writing any code for the CPU as mentioned in section

Part 1: Create the design

.

The concept of PSOC Creator Components​

One other important thing about PSOC™ is the availability of PSOC™ Creator IDE. In PSOC™ Creator, different PSOC™ resources are organized as graphical elements called Components, which can be dragged and dropped onto a schematic to quickly build designs. Every peripheral in PSOC™ is available as a pre-validated PSOC™ Creator Component – PWM Component, ADC Component, DAC Component, CAPSENSE™ Component, UART Component and so on. The availability of pre-validated Components in the PSOC™ Creator significantly reduces the development time. It also allows you to quickly make changes in the design using graphical options.

For example, configuring a PWM to blink an LED in a typical microcontroller involves the following:

  1. Locate the registers corresponding to the PWM block.

  2. Calculate the values to be written to the PWM registers based on the required PWM period and duty cycle.

  3. Write many lines of code to configure the PWM registers, set the pin drive mode, and to connect the PWM output to the pin. Many MCUs do not offer alternate pins to connect to the internal blocks.

To implement the same functionality in PSOC™ is a trivial exercise, as you will find out later in this application note. Later, if you need to reconfigure the same PWM block to a Timer, you do not need anything more than a few mouse clicks in PSOC™ Creator.

The PSOC™ also has programmable digital blocks known as Universal Digital Blocks (UDBs). PSOC™ Creator also provides several Components made of UDBs such as UART, SPI, I2C, Timer, PWM, Counter, Digital Gates (AND, OR, NOT, XOR, and so on), and many more. You can even create your own custom state machines and digital logic using the UDBs in PSOC™ Creator. The method to create your own custom PSOC™ Creator Components is provided in the

PSOC™ Creator Component author guide

.

Getting started with PSOC 4000T design​

This section

provides

the following:

  • Demonstrate how to build a simple PSOC™ 4000T-based design and program it on to the development kit

  • Makes it easy to learn PSOC™ 4000T design techniques and how to use the ModusToolbox™ software with different IDEs.

    Note:

    You can use any supported IDE, but this section uses the Eclipse IDE as an example.

Prerequisites​

Before you get started, make sure that you have the appropriate development kit for your

PSOC™ 4000T

product line and have installed the required software. You also need internet to access the GitHub repositories during project creation.

Hardware

Testing this design requires one of the kits listed in

Table 7

, which has an integrated programmer.

Table 7.

List of

PSOC™ 4

pioneer kits, prototyping kits, and supported devices

Kit name

Kit type

Supported device family

Part number

CY8CKIT-145

Prototyping kit

PSOC™ 4

000S

CY8C4045AZI-S413

CY8CKIT-149

Prototyping kit

PSOC™ 4

100S Plus

CY8C4147AZI-S475

CY8CKIT-041S-Max

Pioneer kit

PSOC™ 4

100S Max

CY8C4149AZI-S598

CY8CKIT-040T

Evaluation kit

PSOC™ 4000T

CY8C4046LQI-T452

CY8CPROTO-040T

Prototyping kit

PSOC™ 4

000T

CY8C4046LQI-T452

CY8CPROTO-041TP

Prototyping kit

PSOC™ 4100T Plus

CY8C4147AZQ-T495

CY8CPROTO-040T-MS

Prototyping kit

PSOC™ 4000T

CY8C4046LQI-T452

Using these instructions​

These instructions are grouped into several sections. Each section is dedicated to a phase of the application development workflow. The major sections are:

  1. Create a BSP for your board

  2. Create a new application

  3. View and modify the design configuration

  4. Write firmware

  5. Build the application

  6. Program the device

  7. Test your design

If you are familiar with developing projects using ModusToolbox™, you can use one of the supported starter applications for your kit, such as

Hello World

or

Blinky

directly. This starter application is a complete project, which can run on supported kits without any additional code or configuration. This design is developed for the kits listed in

Table 7

. You can test this example by selecting the appropriate kit while creating the application. You can go through the instructions in the README.md file and observe how the steps are implemented in the code example.

Even if you are creating a different application from scratch following the instructions in this application note, you can use this code example as a reference.

About the design​

This design uses the

PSOC™ 4

MCU to blink an LED. On kits that support UART, the “Hello World” message is printed to the serial port stream.

Create a BSP for your board​

All ModusToolbox™ applications require a target BSP. Infineon provides BSPs for all of our kits (including the kits mentioned in

Table 7

) and for each chip architecture to use as a starting point. When working with your own hardware, you can modify an Infineon BSP to match the hardware. The BSP Assistant helps to simplify the process. If you are developing for your own hardware, create a custom BSP by following the steps given in

ModusToolbox™ BSP Assistant user guide

. Section

Opening the Device Configurator

describes how the configuration of the custom BSP can be edited.

Create a new application​

This section takes you on a step-by-step guided tour of the new application process. It uses the

Empty App

Empty App

Empty PSOC4 App

starter application and manually adds the functionality from the

Hello World

starter application. The Eclipse IDE for ModusToolbox™ is used in the instructions, but you can use any IDE or the command line if you prefer.

If you are familiar with developing projects with ModusToolbox™ software, you can use the

Hello World

starter application directly. It is a complete design, with all the firmware written for the supported kits. You can walk through the instructions and observe how the steps are implemented in the code example.

If you start from scratch and follow all the instructions in this application note, you can use the

Hello World

code example as a reference while following the instructions.

Launch the

Dashboard 3.2

application to get started.

Note:

Dashboard 3.2

application needs access to the internet to successfully clone the starter application onto your machine.

The

Dashboard 3.2

application helps you get started using the various tools with easy access to documentation and training material, a simple path for creating applications and creating and editing BSPs.

  1. Open the

    Dashboard 3.2

    application.

    To open the

    Dashboard 3.2

    application, do one of these:

    • Windows: Navigate to [ModusToolbox installation path]/tools_3.2/dashboard/dashboard.exe [ModusToolbox installation path]/tools_3.3/dashboard/dashboard.exe or you can also select the "

      dashboard

      ModusToolbox™ Dashboard 3.3

      " item from the Windows Start menu.

    • Linux:

      [ModusToolbox installation path]/tools_3.2/dashboard and run the executable

      [ModusToolbox installation path]/tools_3.3/dashboard and run the executable

    • macOS:

      Run the "dashboard" app

  2. On the

    Dashboard 3.2

    window, in the right pane, in the

    Target IDE

    drop-down list, select

    Eclipse IDE for ModusToolbox™

    , and click

    Launch Eclipse IDE for ModusToolbox™

    .

    Figure 11.

    Dashboard 3.2

    application





  3. Select a new workspace

    .

    At launch, Eclipse IDE for ModusToolbox™ displays a dialog to choose a directory for use as the workspace directory. The workspace directory is used to store workspace preferences and development artifacts. You can choose an existing empty directory by clicking the

    Browse

    button, as shown in the following figure. Alternatively, you can type in a directory name to be used as the workspace directory along with the complete path, and the IDE will create the directory for you.

    Figure 12.

    Select a directory as the workspace





  4. Create a new ModusToolbox™ application

    .

    1. Click New Application in the Start group of the Quick Panel.

    2. Alternatively, you can choose

      File

      >

      New

      >

      ModusToolbox™ Application

      , as shown in the following figure.

      The Project Creator opens.

      Figure 13.

      Create a new ModusToolbox™ application



  5. Select a target

    PSOC™ 4000T

    development kit

    ModusToolbox™ speeds up the development process by providing BSPs that set various workspace/project options for the specified development kit in the new application dialog.

    1. In the

      Choose Board Support Package (BSP)

      dialog, choose the

      Kit Name

      that you have. The steps that follow use

      CY8CPROTO-040T

      . See

      Figure 14

      for help with this step

    2. Click

      Next

      Figure 14.

      Choose target hardware



    3. In the

      Select Application

      dialog, select

      Empty App

      starter application, as shown in the following figure.

    4. In the

      Name

      field, type in a name for the application, such as

      Hello_World

      . You can choose to leave the default name if you prefer.

      Note:

      Try to use a short name without spaces in between.

    5. Click

      Create

      to create the application, as shown in the following figure, wait for the Project Creator to automatically close once the project is successfully created.

    Figure 15.

    Choose starter application



You have successfully created a new ModusToolbox™ application for a

PSOC™ 4000T

.

The BSP uses

CY8C4046LQI-T452

as the default device that is mounted on the

PSOC™ 4 CY8CPROTO-040T Prototyping Kit

.

If you are using custom hardware based on

PSOC™ 4000T

, or a different

PSOC™ 4000T

part number, please refer to the

Create a BSP for your board

or the

BSP Assistant user guide

.

View and modify the design configuration​

Figure 16

shows the ModusToolbox™ Project Explorer displaying the structure of the application project.

Figure 16.

Project explorer view



For understanding the files and folders in detail, see Section 2.4.2 in

ModusToolbox™ tools package user guide.

Opening the Device Configurator

You can modify the device configurations which is loaded by the selected BSP. For example, default kit BSPs do not have UART enabled. Below steps show how to enable UART peripheral for “Hello World” printing operation and how to enable User LED for

PSOC™ 4

kits.

  1. As shown in

    Figure 17

    , click

    Device configurator

    in the

    Quick Panel

    under the

    BSP Configurators

    section. This opens the Device Configurator dialog(

    Figure 18

    ). You can also open the other configurators and configure as required.

    Figure 17.

    Opening the Device Configurator



    Figure 18.

    Overview of design.modus



    From the

    Resource Categories Pane

    of the

    Device Configurator

    dialog, you can choose different resources to configure, such as peripherals, pins, and clocks.

    The

    Peripherals

    tab shows a list of available peripherals in the device. The configuration in the

    Personality

    column defines the behavior of the resource. For example, a

    Serial Communication Block (SCB)

    resource can have

    EZI2C, I2C, SPI,

    or

    UART

    as personalities. The

    Name(s)

    field is the user-defined name of the resource, which is used in firmware development. You can specify one or more names for each pin, as ModusToolbox™ provides the ability to assign different aliases to the pins, corresponding to different run-time configurations. Note that the listed names must be separated by commas with no space.

    In the

    Parameters

    pane, you can enter the configuration parameters for each enabled resource and the selected personality. The

    Code Preview

    pane shows the configuration code generated for the selected configuration parameters. This code is populated in the

    cycfg_

    files in the

    GeneratedSource

    folder. Any errors, warnings, and information messages, caused by the configuration, are displayed in the

    Notice List

    pane.

  2. Enable UART peripheral and configure the corresponding clocks as explained in the following steps:

    Note:

    For the CY8CKIT-040T kit skip these steps because UART is not supported on this kit.

    1. Go to the

      Peripherals

      tab in

      Resources Categories

      pane and enable

      Serial Communication Block (SCB) 0

      , set personality as UART-1.0 and the name as "CYBSP_UART". In

      Figure 19

      , SCB instance

      0

      is selected based on Rx/Tx pin required for the kit. As shown in

      Figure 20

      , the drop-down of Rx and Tx configuration parameters shows pins supported by SCB

      0

      . See the

      device datasheet

      for the pins available for each SCB instance.

      Figure 19.

      Enabling SCB as UART



    2. Set the required configuration parameters such as

      Clock

      ,

      Rx

      , and

      Tx

      in the

      Parameter

      pane. Retain the default values for other parameters.

      Figure 20.

      Setting UART configuration parameter



    3. Go to the

      Peripheral-Clocks

      tab in

      Resource Categories

      pane to configure the clock for UART peripheral.

      Figure 21.

      Configuring clock



      Tip:

      Go to the

      Code Preview

      pane to preview the generated code.

      Figure 22.

      Code preview pane



  3. Go to the

    Pins

    tab in

    Resource Categories

    pane to configure the GPIO connected to the user LED on the kit. See

    Table 8

    if you are using a different

    PSOC™ 4

    kit. Configure the GPIO as shown in

    Figure 23

    .

    Figure 23.

    Configuring GPIO



    Table 8.

    Pin mapping table across PSOC™ 4 kits

    Function

    CY8CKIT-145

    (

    PSOC™ 4

    000S)

    CY8CKIT-149

    (

    PSOC™ 4

    100S Plus)

    CY8CKIT-041S-MAX

    (

    PSOC™ 4

    100S Max)

    CY8CKIT-040T

    PSOC™ 4

    000T

    CAPSENSE™

    Evaluation Kit

    CY8CPROTO-040T

    PSOC™ 4

    000T CAPSENSE™ Prototyping Kit

    CY8CPROTO-040T-MS

    PSOC™ 4

    000T

    Multi-Sense

    Prototyping Kit

    CY8CPROTO-041TP

    CAPSENSE™

    Prototyping Kit

    User LED

    P2[5]

    P3[4]

    P7[3]

    P4[0]

    1[0], 3[0]

    1[0], 3[0]

    5[4], 5[5], 6[0], 6[2]

  4. Disable (i.e., uncheck) any other peripherals and pins that may have been enabled by default for the kit.

  5. Other resources like power, frequency and clock can be configured in the System tab of the Resource Categories Pane. Default Power settings are shown in

    Figure 24

    . For this design, no further changes are required.

    Figure 24.

    Configuring System Settings



  6. Go to

    File

    >

    Save

    or press

    [Ctrl]+[S]

    to save the configuration and to generate the source code in the

    GeneratedSource

    folder.

Write firmware​

This design uses the CM0+ CPU of the

PSOC™ 4

to execute two tasks: UART communication and LED control. The CM0+ CPU uses the UART to print the “Hello World” message to the serial port stream and to make the user LED on the kit blink.

If you are using the

Empty

PSOC™ 4

starter application, you can copy the code snippet provided in this section, to the main.c file of the application project. If you are using the

Hello World

code example, the required files are already in the application.

Firmware flow

This section explains the code in the

main.c

file of the application.

In this example, the CM0+ CPU comes out of reset and performs resource initialization. It configures the system clocks, pins, clock to peripheral connections, and other platform resources.

The clocks and system resources are initialized by the BSP initialization function. PDL functions are used to configure and enable the UART peripheral. The UART prints “Hello World” message on the terminal emulator – the onboard KitProg3 acts as the USB-UART bridge to create the virtual COM port. An infinite FOR loop, with a software delay, is used to toggle the user LED periodically.

Note that the application code uses BSP/PDL functions to execute the intended functionality.

  • cybsp_init()

    • This BSP function initializes the system resources of the device including but not limited to the system clocks and power regulators.
  • Cy_SCB_UART_Init()

    • This PDL function initializes the SCB block for UART operation. A configuration structure,

    CYBSP_UART_config

    , is used as a parameter for this function to configure the UART. This structure is autogenerated by

    design.modus

    based on the applied configuration.

  • Cy_SCB_UART_Enable()

    • This PDL function enables the SCB block for UART operation.
  • Cy_SCB_UART_PutString()

    • This PDL function places a NULL terminated string in the UART TX FIFO.
  • Cy_GPIO_Inv()

    • This PDL function sets a pin output logic state to the inverse of the current output logic state.
  • Cy_SysLib_Delay()

    • This PDL function inserts a delay (specified in milliseconds).

Copy

Code Listing 1

or

Code Listing 2

, as applicable, to the

main.c

of your application project.

Code Listing 1 Code snippet with UART communication (main.c) (Use for all kits other than CY8CKIT-040T)

/*******************************************************************************
* Include header files
******************************************************************************/
#include "cy_pdl.h"
#include "cybsp.h"

/*******************************************************************************
* Macros
*******************************************************************************/
#define LED_DELAY_MS (500u)
#define CY_ASSERT_FAILED (0u)
/*******************************************************************************
* Function Name: main
********************************************************************************
* Summary:
* System entrance point. This function performs
* - initial setup of device
* - configure the SCB block as UART interface
* - prints out "Hello World" via UART interface
* - Blinks an LED under firmware control at 1 Hz
*
* Parameters:
* none
*
* Return:
* int
*
*******************************************************************************/
int main(void)
{
cy_rslt_t result;

cy_stc_scb_uart_context_t CYBSP_UART_context;


/* Initialize the device and board peripherals */
result = cybsp_init();

/* Board init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(CY_ASSERT_FAILED);
}

/* Configure and enable the UART peripheral */
Cy_SCB_UART_Init(CYBSP_UART_HW, &CYBSP_UART_config, &CYBSP_UART_context);
Cy_SCB_UART_Enable(CYBSP_UART_HW);

/* Enable global interrupts */
__enable_irq();

/* Send a string over serial terminal */
Cy_SCB_UART_PutString(CYBSP_UART_HW, "Hello world\r\n");

for(;;)
{
/* Toggle the user LED state */
Cy_GPIO_Inv(CYBSP_USER_LED1_PORT, CYBSP_USER_LED1_PIN);

/* Wait for 0.5 seconds */
Cy_SysLib_Delay(LED_DELAY_MS);
}
}

Figure 25.

Firmware flowchart



Code Listing 2 Code snippet without UART communication (main.c) (Use for any kit including CY8CKIT-040T)

/*******************************************************************************
* Include header files
******************************************************************************/
#include "cy_pdl.h"
#include "cybsp.h"

/*******************************************************************************
* Macros
*******************************************************************************/
#define LED_DELAY_MS (500u)
#define CY_ASSERT_FAILED (0u)

/*******************************************************************************
* Function Name: main
********************************************************************************
* Summary:
* System entrance point. This function performs
* - initial setup of device
* - Blinks an LED under firmware control at 1 Hz
*
* Parameters:
* none
*
* Return:
* int
*
*******************************************************************************/
int main(void)
{
cy_rslt_t result;

/* Initialize the device and board peripherals */
result = cybsp_init();

/* Board init failed. Stop program execution */
if (result != CY_RSLT_SUCCESS)
{
CY_ASSERT(CY_ASSERT_FAILED);
}

/* Enable global interrupts */
__enable_irq();

for(;;)
{
/* Toggle the user LED state */
Cy_GPIO_Inv(CYBSP_USER_LED1_PORT, CYBSP_USER_LED1_PIN);

/* Wait for 0.5 seconds */
Cy_SysLib_Delay(LED_DELAY_MS);
}
}

This summarizes how the firmware works in the code example. For details, explore the source files.

Build the application​

This section explains how to build the application.

  1. Select the application project in the Project Explorer window and click the Build <name> Application shortcut under the <name> group in the Quick Panel. It uses the selected build configuration and compiles/links all projects that constitute the application.

  2. The Console view lists the results of the build operation.

Figure 26.

Build the application



If there are any errors, check the steps and make sure that you complete all required tasks.

Note:

You can also use the CLI to build the application. See the "3.5.3 Use command line" section in the

ModusToolbox™ user guide

. This document is located in the

/ide_3.2/docs/

folder in the ModusToolbox™ installation directory.

Program the device​

This section explains how to program the

PSOC™ 4

device.

ModusToolbox™ uses the SWD protocol to program and debug applications on PSOC™ 4 devices. For ModusToolbox™ to identify the device on the kit, the kit must be running KitProg3. Some kits are shipped with KitProg2 firmware instead of KitProg3. ModusToolbox™ includes the fw-loader command-line tool to switch the KitProg firmware from KitProg2 to KitProg3. See section 5.1.10 KitProg Firmware Loader in the

ModusToolbox™ IDE user guide

for more details.

If you are developing hardware on your own, you may need a hardware programmer/debugger; for example,

CY8CKIT-005 MiniProg4

.

  1. Connect the kit to the USB port of your computer

  2. Select the application project and click the <application name> Program (KitProg3_MiniProg4) shortcut under the Launches group in the Quick Panel. The IDE will select and run the appropriate run configuration. Note that this step will also perform a build if any files have been modified since the last build.

Figure 27.

Programming an application to a device



The Console view lists the results of the programming operation.

Figure 28.

Console – programming results



Test your design​

This section describes how to test your design.

Once the programming is done, reset the kit and observe the LED blinking.

For kits having UART enabled, follow these steps to observe the "Hello world" being printed. This application note uses Tera Term as the UART terminal emulator to view the results. You can use any terminal to view the output. Skip these steps for CY8CKIT-040T kit as UART is not supported for this kit.

  1. Select the serial port

    Launch Tera Term and select the USB-UART COM port as shown in

    Figure 29

    . Note that your COM port number may be different.

    Figure 29.

    Selecting the KitProg3 COM port in Tera Term


    ../figures/image34.png
  2. Set the baud rate

    Go to Setup > Serial port. Set the baud rate to 115200.

    Figure 30.

    Configuring the baud rate in Tera Term



  3. Reset the device

    Press the reset switch on the (See

    Table 9

    )

    PSOC™ 4

    kit. A "Hello world" message appears on the terminal. The user LED on the kit will start blinking.

    Table 9.

    Pin mapping table across PSOC™ 4 kits for reset switch

    Function

    CY8CKIT-145(PSOC™ 4000S)

    CY8CKIT-149(PSOC™ 4100S Plus)

    CY8CKIT-041S-MAX(PSOC™ 4100S Max)

    CY8CKIT-040T PSOC™ 4000T CAPSENSE™ Evaluation Kit

    CY8CPROTO-040T

    PSOC™ 4

    000T CAPSENSE™ Prototyping Kit

    CY8CPROTO-040T-MS

    PSOC™ 4

    000T Multi-Sense Prototyping Kit

    CY8CPROTO-041TP CAPSENSE™ Prototyping Kit

    RESET

    SW1

    SW2

    SW1

    SW1

    SW1

    SW1

    SW1

    Figure 31.

    UART message printed from

    PSOC™ 4



My first​

PSOC 4 design using PSOC Creator

This section:

  • Demonstrates how PSOC™ can be programmed to do more than a traditional MCU

  • Shows how to build a simple PSOC™ design and install it in a development kit.

  • Provides detailed steps that make it easy to learn PSOC™ design techniques and how to use PSOC™ Creator.

Before you begin​

Have you installed PSOC Creator?

Download and install PSOC™ Creator from the

PSOC™ Creator

home page. Note that the installation of the toolset may take a long time – see the PSOC™ Creator Release Notes for more information.

Do you have a development kit or prototyping kit?

Testing this design requires one of the kits listed in

Table 10

, which has an integrated programmer.

Table 10.

List of

PSOC™ 4

pioneer kits, prototyping kits, and supported Devices

Kit name

Kit type

Supported device family

Part number

CY8CKIT-040

Pioneer kit

PSOC™ 4000

CY8C4014LQI-422

CY8CKIT-042

Pioneer kit

PSOC™ 4200

CY8C4245AXI-483

CY8CKIT-044

Pioneer kit

PSOC™ 4200M

CY8C4247AZI-M485

CY8CKIT-046

Pioneer kit

PSOC™ 4200L

CY8C4248BZI-L489

CY8CKIT-042-BLE

Pioneer kit

PSOC™ 4200 Bluetooth® LE

CY8C4247LQI-BL483

CY8CKIT-045S

Pioneer kit

PSOC™ 4500S

CY8C4548AZI-S485

CY8CKIT-043

Prototyping kit

PSOC™ 4200M

CY8C4247AZI-M485

CY8CKIT-145

Prototyping kit

PSOC™ 4000S

CY8C4045AZI-S413

CY8CKIT-147

Prototyping kit

PSOC™ 4100PS

CY8C4145LQI-PS433

CY8CKIT-149

Prototyping kit

PSOC™ 4100S Plus

CY8C4147AZI-S475

Want to see the project in action?

If you do not want to go through the design process, you can get the completed PSOC™ Creator project using

Find Code Example

in PSOC™ Creator (

File

>

Code Example…

>

CE230991_My_First_Project

). You can then jump to the

Build

and

Program

steps.

About the design​

This design simply blinks two LEDs using a TCPWM Component, as shown in

Figure 32

. The TCPWM is configured in PWM mode. The two complementary outputs of this PWM control the LEDs. The PWM operates at a very low frequency and 50 percent duty cycle so that the toggling of the LEDs is visible. If you use a dual-color LED instead of two separate LEDs, this project can toggle the color of the dual-color LED.

Figure 32.

My first

PSOC™ 4

design



Part 1: Create the design​

This section takes you on a step-by-step guided tour of the design process. It starts with creating an empty project and guides you through hardware and firmware design entry.

  1. Start PSOC™ Creator, and from the

    File

    menu choose

    New

    >

    Project

    , as shown in

    Figure 33

    .

    Figure 33.

    Creating a new project



  2. Select your development kit in the pop-up window. For example, if you have a CY8CKIT-149, select

    Kit: CY8CKIT-149 (PSOC™ 4100S Plus)

    and click

    Next

    . If you do not see your

    PSOC™ 4

    development kit listed in the menu, download and install the kit setup for your kit from the website.

    Alternately, you can also select the target device radio button instead of the target hardware and select the appropriate device and click

    Next

    .

    Figure 34.

    Create a new empty

    PSOC™ 4

    project



  3. Select the option

    Empty Schematic

    from the next window and click

    Next

    .

    Figure 35.

    Select empty schematic



  4. Provide a project name (for example, "My_First_Project") and Workspace Name as shown in

    Figure 36

    . Choose an appropriate location for your new project, and click

    Finish

    .

    Figure 36.

    Selecting project name and location



  5. Creating a new project generates a project folder with a baseline set of files shown in the

    Workspace Explorer

    (see

    Figure 37

    ). To open the project schematic file, double-click

    TopDesign.cysch

    .

    Figure 37.

    Opening TopDesign schematic



  6. Drag one PWM (TCPWM mode) Component from the Component Catalog onto the schematic, as shown in

    Figure 38

    .

    Figure 38.

    Location of the PWM Component



  7. Double-click the PWM Component on the schematic to configure the Component properties, as shown in

    Figure 39

    . Click the

    PWM

    tab, and set the

    Period

    value to 254 and the

    Compare

    value to 127 to generate a PWM signal with a 50 percent duty cycle.

    Set the

    Prescaler

    to 8x, to divide the input clock frequency by 8.

    Figure 39.

    Configuring the PWM Component



  8. A PWM Component requires an input clock for its operation. Drag and drop a

    Clock

    Component onto the schematic, and configure the

    Frequency

    to 800 Hz by double-clicking on the Component, as shown in

    Figure 40

    and

    Figure 41

    . Because the Prescaler value set in PWM Component is 8, the effective input clock of the PWM is only 100 Hz. Therefore, the PWM period of 254 results in a PWM output time period of 2.54 seconds.

    Figure 40.

    Location of the clock Component



    Figure 41.

    Configuring the clock Component



  9. Drag and drop a

    Digital Output Pin

    Component. Change the name to LED_1 as shown in

    Figure 42

    and

    Figure 43

    . Add another Digital Output Pin Component and change its name to LED_2.

    Figure 42.

    Location of the digital output pin Component



    Figure 43.

    Renaming a pin Component


    ../figures/image48.png
  10. In the schematic window, select the wire tool as shown in

    Figure 44

    , or press

    W

    .

    Figure 44.

    Selecting the wire tool


    ../figures/image49.png
  11. Wire the Components together, as shown in

    Figure 45

    .

    Figure 45.

    Wiring the schematic



  12. Most Components are disabled at device reset (the major exception being the Clock Component, which is automatically started as a default), and you must add code to the project to enable them. Open main.c from Workspace Explorer and add code to the main() function, as provided in Code Listing 3.


    Code Listing 3 Enabling the PWM Component

     int main(void)
    {
    /* Enable and start the PWM */
    PWM_1_Start();

    for(;;)
    {

    }
    }
  13. Select Build My_First_Project from the Build menu. Note that PSOC™ Creator automatically generates source code files in the Workspace Explorer window for the PWM, Clock, and Digital Output Pin Components, as shown in

    Figure 46

    .

    Figure 46.

    Generated source files



  14. Open the file

    My_First_Project.cydwr

    (Design-Wide Resource file) from

    Workspace Explorer

    and click the

    Pins

    tab. You can use this tab to select the device pins for the outputs LED_1 and LED_2.

    Figure 47

    shows the pin configuration to connect the LED_1 and LED_2 pins to the LEDs in the

    CY8CKIT-149 PSOC™ 4 prototyping kit

    . See

    Table 11

    if you are using a different

    PSOC™ 4

    pioneer kit, or

    Table 12

    if you are using a

    PSOC™ 4

    prototyping kit.

    Figure 47.

    Pin selection



    Table 11.

    Pin mapping table across pioneer kits

    Function

    CY8CKIT-040 (

    PSOC™ 4

    CY8CKIT-041(

    PSOC™ 4

    100S)

    CY8CKIT-042(

    PSOC™ 4

    CY8CKIT-042-BLE(

    PSOC™ 4

    200 BLE)

    CY8CKIT-044(

    PSOC™ 4

    200M)

    CY8CKIT-046(

    PSOC™ 4

    200L)

    CY8CKIT-045S(

    PSOC™ 4

    500S)

    Green LED (Active LOW)

    P1[1]

    P2[6]

    P0[2]

    P3[6]

    P2[6]

    P5[3]

    P0[0]

    Red LED (Active LOW)

    P3[2]

    9

    P3[4]

    10

    P1[6]

    P2[6]

    P0[6]

    P5[2]

    P1[6]

    Table 12.

    Pin mapping table across prototyping kits

    Function

    CY8CKIT-145 (

    PSOC™ 4

    000S)

    CY8CKIT-149 (

    PSOC™ 4

    100S Plus)

    Green LED - LED 1 (Active LOW)

    P3[4]

    P1[6]

    Green LED - LED 2 (Active LOW)

    P3[5]

    P5[7]

  15. Finally, rebuild the project as explained in

    Step 13

    .

9

PSOC™ 4000 parts have fixed pins for complementary PWM outputs – P1[1] and P1[6]. You cannot use any other pins for PWM outputs. See the device datasheet for more details. If you are using the

CY8CKIT-040

, you can use the green LED connected to P1[1], as LED1. To use the red LED as LED2, connect P3[2] from header J4 to P1[6] from header J3, using a wire. Alternately, you can connect an external LED to P1[6] as LED2.

10

Similar to the note above, if you are using the

CY8CKIT-041

, you can use the green LED connected to P2[6], as LED1 and the complementary PWM output P2[7] for LED2. To use the red LED as LED2, connect P3[4] from header J2 to P2[7] from header J3, using a wire. Alternately, you can connect an external LED to P2[7] as LED2.

Part 2: Program the device​

This section explains how to program the device. Connect the kit board to your computer using the USB cable.

  1. Select the PSOC™ Creator menu item

    Debug

    >

    Select Debug Target

    , as shown in

    Figure 48

    .

    Figure 48.

    Selecting debug target



  2. In the

    Select Debug Target

    dialog box, click

    Port Acquire

    , and then click

    Connect

    , as shown in

    Figure 49

    . Click

    OK

    to close the dialog box.

    Figure 49.

    Connecting to a device



  3. Choose the menu item

    Debug

    >

    Program

    to program the device with the project, as shown in

    Figure 50

    .

    Figure 50.

    Programming the device



  4. You can view the programming status on the status bar (lower-left corner of the window), as shown in

    Figure 51

    .

    Figure 51.

    Programming status



  5. After the device is programmed, ensure that the LEDs toggle, and confirm the working operation of the project.

9

PSOC™ 4000 parts have fixed pins for complementary PWM outputs – P1[1] and P1[6]. You cannot use any other pins for PWM outputs. See the device datasheet for more details. If you are using the

CY8CKIT-040

, you can use the green LED connected to P1[1], as LED1. To use the red LED as LED2, connect P3[2] from header J4 to P1[6] from header J3, using a wire. Alternately, you can connect an external LED to P1[6] as LED2.

10

Similar to the note above, if you are using the

CY8CKIT-041

, you can use the green LED connected to P2[6], as LED1 and the complementary PWM output P2[7] for LED2. To use the red LED as LED2, connect P3[4] from header J2 to P2[7] from header J3, using a wire. Alternately, you can connect an external LED to P2[7] as LED2.

Summary​

This application note explored the

PSOC™ 4

architecture and development tools.

PSOC™ 4

is a truly programmable embedded system-on-chip, integrating configurable analog and digital peripheral functions, memory, and an Arm® Cortex®-M0/M0+ microcontroller on a single chip. Because of the integrated features and low-leakage power modes,

PSOC™ 4

is an ideal choice for low-power and cost-effective embedded systems.

This application note also guided you to a comprehensive collection of resources to accelerate in-depth learning about

PSOC™ 4

.

References​

  1. Infineon Technologies AG:

    001-54181: Getting started with PSOC™ 3

    ;

    Available online

  2. Infineon Technologies AG:

    001-77759: Getting started with PSOC™ 5LP

    ;

    Available online

Revision history​

Document revision

Date

Description of changes

**

2013-01-24

New Application Note

*A

2013-04-11

Demo project changed to leverage Pioneer kit.

Added architecture introduction.

*B

2013-05-09

Reformatted graphics. Updated links.

*C

2013-12-19

Updated attached Associated Project files.

Updated content across the entire document.

Updated in new template.

*G

2014-04-10

Updated the projects and the respective section in the AN to support PSOC™ Creator 3.0 SP1 and PSOC™ 4000 device.

*H

2014-09-25

Added Code Examples section.

Minor edits and format changes throughout the document.

*I

2015-03-17

Added More Information section.

Removed detailed feature descriptions.

Updated for PSOC™ 4200M family of devices.

*J

2015-09-10

Added the following sections: Convert Project to Bootloadable for CY8CKIT-049, Bootload Your CY8CKIT-049, and More PSOC™ 4 Code Examples.

Updated

Figure 8

.

*K

2015-09-16

Updated for PSOC™ 4200L.

Updated the example projects to PSOC™ Creator 3.3.

*L

2015-12-30

Updated the example projects to PSOC™ Creator 3.3 SP1.

*M

2016-02-05

Updated for PSOC™ 4000S and PSOC™ 4100S.

Updated the example projects to PSOC™ Creator 3.3 SP2.

Updated

Table 10

,

Table 11

to add PSOC™ 4200 BLE.

*N

2017-04-19

Updated logo and copyright

*O

2017-10-06

Added references to PSOC™ 4100S Plus throughout the document.

Updated Table 1 to add PSOC™ 4100S Plus.

*P

2017-11-03

Updated the example projects to PSOC™ Creator 4.2

Updated Table 1 to add supported kit

Updated

Table 10

to add CY8CKIT-49, CY8CKIT-145 and CY8CKIT-149

Added

Table 11

to include CY8CKIT-145 and CY8CKIT-149 pin mapping

Updated Figure 7.

Added example project of CY8CKIT-145 and CY8CKIT-149 as a part of the

AN79953.zip

file in this application note landing page.

*Q

2018-03-06

Updated template

Updated for PSOC™ 4100PS

Minor edits and format changes throughout the document

Added example project of CY8CKIT-147 as a part of the

AN79953.zip

file

*R

2018-05-04

Updated template

Corrected the link to PSOC™ 4100S Plus in

PSOC™ resources

*S

2019-09-06

Updated Table 1 to add PSOC™ 4500 and update the specifications of PSOC™ 4100S Plus device family.

Added Motor Control Accelerator feature.

*T

2020-11-09

Updated for ModusToolbox™ support for some of the PSOC™ 4 devices.

Corrected the links in

PSOC™ resources

.

PSOC™ 4 families are recategorized in

Local sales office locations PSOC™ 4 feature set

Added new section My first PSOC™ 4 design using ModusToolbox™

Removed sections : Convert Project to Bootloadable for CY8CKIT-049, Bootload Your CY8CKIT-049, and More PSOC™ 4 Code Examples

*U

2021-07-08

Updated to Infineon template

Updated Figure 2, Figure 3, Figure 4, and Figure 5 to the latest MTB 2.3 version

Updated document with PSOC™ 4100S Max device

Changed the default device to PSOC™ 4100S Max and updated

Figure 8

Updated Modify the design section

*V

2022-06-15

Updated document with PSOC™ 4000T device

Updated with the latest release version of ModusToolbox™ (version-3.0)

*W

2023-02-13

Updated Folder structure with the latest release version of ModusToolbox™(VERSION-3.0)

*X

2023-07-21

Updated the pin changes for PSOC™ 4000T device

Updated content with the latest release of ModusToolbox™ 3.1

*Y

2024-02-05

Fixed broken links

*Z

2024-02-26

Updated content with the latest release of ModusToolbox™ 3.2

AA

2024-09-18

Changed the default device to CY8CPROTO-040T kit

AB

2025-01-13

Updated the document with CY8CPROTO-040T-MS PSOC™ 4000T Multi-Sense Prototyping Kit

AC

2025-03-27

Updated document with PSOC™ 4100T Plus device

Trademarks​

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc., and any use of such marks by Infineon is under license.

PSOC™, formerly known as PSoC™, is a trademark of Infineon Technologies. Any references to PSoC™ in this document or others shall be deemed to refer to PSOC™.

1

PSOC™ 4 feature set

for complete PSOC™ 4 portfolio.

2

See

AN211293

for getting started with PSOC™ 4 analog coprocessor family devices.

3

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM for more details.

4

See

AN91267

for getting started with PSOC™ 4 Bluetooth® LE Family devices.

5

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM more details.

6

See

AN91267

for getting started with PSOC™ 4 Bluetooth® LE family devices.

7

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM for more details.

8

IDACs are available only when CAPSENSE™ is not in use. See the respective PSOC™ 4 architecture TRM for more details.

9

PSOC™ 4000 parts have fixed pins for complementary PWM outputs – P1[1] and P1[6]. You cannot use any other pins for PWM outputs. See the device datasheet for more details. If you are using the

CY8CKIT-040

, you can use the green LED connected to P1[1], as LED1. To use the red LED as LED2, connect P3[2] from header J4 to P1[6] from header J3, using a wire. Alternately, you can connect an external LED to P1[6] as LED2.

10

Similar to the note above, if you are using the

CY8CKIT-041

, you can use the green LED connected to P2[6], as LED1 and the complementary PWM output P2[7] for LED2. To use the red LED as LED2, connect P3[4] from header J2 to P2[7] from header J3, using a wire. Alternately, you can connect an external LED to P2[7] as LED2.