PSOC™ 4000T reference manuals
A reference manual (RM) provides detailed technical information on a device family. It also provides a functional description of the various sub-blocks in the device including block features, architecture, and use cases. In addition to that, it includes register level description of the user accessible registers in the device.
The reference manuals for the PSOC™ 4000T device families are listed below.
Device family | Architecture RM | Registers RM |
|---|---|---|
PSOC™ 4000T |