To set various build options, use the sections on the IAR Embedded Workbench Project Options dialog where you can enter command-line options:

  • C / C++ Compiler > Extra Options

  • Assembler > Extra Options

  • Linker > Extra Options

Prebuild and postbuild steps from a ModusToolbox application are not included in the export process by default for most devices at this time. If your original application has these steps, you must include them in the IAR Embedded Workbench manually as follows:

  1. In IAR Embedded Workbench, open the Options dialog, go to the

    Build Actions

    category.

  2. Click the

    New

    button to open the New Build Action dialog.

  3. On the New Build Action dialog, enter a command-line argument, output and/or input files, the working directory, and the build order.

  4. If using a postbuild script that works with .elf files, switch to the

    Linker > Output

    tab and change the file extension from ".out" to ".elf" in the

    Output filename

    field:


    ../figures/image20.png

  5. Click

    OK

    to close the Options dialog.

    Refer to the IAR Embedded Workbench Help for more details.

  6. On the IAR main menu, select

    Project > Make

    to build the application. You should see the following:

    Hello_World.elf

    Total number of errors: 0
    Total number of warnings: 0
    Resolving dependencies...
    Build succeeded