Skip to main content

Quick start

This section provides a simple workflow for how to use the QSPI Configurator.

  1. Launch the QSPI Configurator .

  2. Open an existing or create a new configuration file.

  3. Specify the configuration file location.

    Note: The device database (device-db) is loaded before the configuration. If device-db is not present on the disk, it will be downloaded automatically. Observe the notification on the status bar.

  4. Select a memory from the Memory Part Number list.

    • If your memory device supports SFDP, select Auto detect SFDP .

      ../figures/image7.png

    • If your memory device does not support SFDP, or for manual configuration, select a memory from the Memory Part Number list, and specify the configuration parameters as required (for example, memory mapped, write enable, etc.). See QSPI Configuration Fields .

      ../figures/image8.png

    Note: If the required memory part number is not present in the list, you can add it. Select [Browse]…, navigate to the memory file location, and select it.

  5. Save the Configuration file to generate source code. See Code generation .

  6. Use the generated structures as input parameters for QSPI functions in your application.