Launch the QSPI Configurator
There are numerous ways to launch the QSPI Configurator, and those ways depend on how you use the various tools in ModusToolbox™ software.
make command
As described in the tools package user guide build system chapter, you can run numerous make commands in the application directory, such as launching the QSPI Configurator. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:
make qspi-configurator
This command opens the QSPI Configurator GUI for the specific application in which you are working.
VS Code and Eclipse
VS Code and Eclipse have tools to launch the QSPI Configurator from within an open application. Refer to the applicable user guide for more details:
From the Device Configurator
You can also launch the QSPI Configurator from the Device Configurator:
-
Open the Device Configurator. See the Device Configurator user guide for details.
-
On the Peripherals tab, enable the QSPI resource.
-
Optionally, review and resolve the tasks in the Notice List pane. These can be resolved later.
-
On the Parameters tab, click the Launch QSPI Configurator button.

Executable (GUI)
If you don't have an application or if you just want to see what the configurator looks like, you can launch the QSPI Configurator GUI by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows Start menu). By default, it is installed here:
[Install_dir]/ModusToolbox/tools_[version]/qspi-configurator-[version]
When launched this way, the QSPI Configurator opens without any memories configured.

You can either open a specific Configuration file or create a new one. See Menus for more information.