Skip to main content

Overview

The QSPI Configurator is intended to create and configure QSPI configuration for external memory chips and generate code to control the application firmware.

../figures/image4.png

Some devices allow you to extend the default RAM and flash with external memory chips of the following types: flash, non-volatile FRAM, or RAM. Use the SPI to connect a chip to the device. You can attach up to four external memory parts and configure them with the QSPI Configurator.

The QSPI Configurator bears information about the set of default memory parts. However, if your specific memory part is not present, you can create a new one. In the QSPI Configurator, you can select an attached memory part or Serial Flash Discoverable Parameter (SFDP), which is a standard to query the information about attached memory parts at run-time, for each slot and configure the slot parameters.

The QSPI Configurator saves configuration information in a *.cyqspi file, which contains all the required information about the device and the application. When you save changes, the QSPI Configurator generates/updates firmware in the BSP’s "GeneratedSource" folder.

Supported software

NameLink
Peripheral Driver LibraryGitHub repo: https://github.com/Infineon/mtb-pdl-cat1
SMIF Driver Documentation: https://Infineon.github.io/mtb-pdl-cat1/pdl_api_reference_manual/html/group__group__smif.html