Skip to main content

ModusToolbox™ CAPSENSE™ Configurator user guide

A newer revision of this document may be available on the web here.

Scope and purpose

The CAPSENSE™ Configurator is used to create and configure CAPSENSE™ widgets and generate code to control the application firmware.

Intended audience

This document helps application developers understand how to use the CAPSENSE™ Configurator as part of creating a ModusToolbox™ application.

Conventions used

The following are the conventions used in this guide:

ConventionExplanation
BoldEmphasizes heading levels, column headings, menus and sub-menus.
ItalicsDenotes file names and paths.
MonospaceDenotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets.
File > NewIndicates that a cascading sub-menu opens when you select a menu item.

Abbreviations and definitions

  • Application – One or more projects related to each other.

  • BIST – Built-In Self-Test

  • CAPDAC – capacitive digital-to-analog converter

  • CAPSENSE – capacitive sensing

  • Configurator – A GUI-based tool used to configure a resource.

  • CSD – CAPSENSE™ sigma-delta – self-capacitance sensing method

  • CSX – CAPSENSE™ Transmit/Receive (CAPSENSE™ with two electrodes: Tx and Rx) – mutual capacitance sensing method

  • EFS – external frame start

  • IDAC – current-output digital-to-analog converter

  • IDE – integrated development environment

  • IIR filter – infinite-impulse response filter

  • CSD HW – CAPSENSE™ Sigma Delta – 4 th generation hardware (HW) block

  • ISX – inductive sensing method

  • LFSR – linear-feedback shift register

  • MFS – multi-frequency scan

  • MSC HW – multi-sense converter – 5 th generation hardware (HW) block

  • MSCLP HW – multi-sense converter low power – 5 th generation LP hardware (HW) block

  • Peripheral – Any external analog or digital device that provides input and output for the computer.

  • PRS – pseudo-random sequencer

  • PSOC™ – programmable system-on-chip

  • SNR – signal-to-noise ratio

  • SSC - spread spectrum clock

  • Widget – This CAPSENSE™ functional unit consists of one sensor or a group of similar sensors that implement(s) a specific higher-level functionality such as a Button, Proximity, Linear Slider, Radial Slider, Matrix Buttons, Touchpad, Low Power, Liquid Level, and Liquid Presence widget.

Reference documents

Refer to the following documents for more information as needed: