ModusToolbox™ CAPSENSE™ Tuner user guide
A newer revision of this document may be available on the web here.
Scope and purpose
The CAPSENSE™ Tuner is used to tune CAPSENSE™ applications.
Intended audience
This document helps application developers understand how to use the CAPSENSE™ Tuner as part of creating a ModusToolbox™ application.
Document conventions
| Convention | Explanation |
|---|---|
| Bold | Emphasizes heading levels, column headings, menus and sub-menus |
| Italics | Denotes file names and paths. |
Monospace | Denotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets |
| File > New | Indicates that a cascading sub-menu opens when you select a menu item |
Abbreviations and definitions
The following define the abbreviations and terms used in this document:
-
Application – One or more projects related to each other.
-
CAPSENSE – capacitive sensing
-
Configurator – A GUI-based tool used to configure a resource.
-
CSD – self-capacitance sensing method
-
CSX – CAPSENSE™ Transmit/Receive (CAPSENSE™ with two electrodes: Tx and Rx), mutual capacitance sensing method
-
ISX – inductive sensing method
-
IDE – integrated development environment
-
CSD HW – CAPSENSE™ Sigma Delta – 4 th generation hardware (HW) block
-
MSC HW – multi-sensing converter – 5 th generation hardware (HW) block
-
MSCLP HW – multi-sensing converter low power – 5 th generation LP hardware (HW) block
-
Peripheral – Any external analog or digital device that provides an input and output for the computer.
-
PSOC™ – programmable system-on-chip
-
RTT – real-time transfer
-
SMARTSENSE – Auto-tuning process used for proper functionality and optimized performance of the CAPSENSE™ system.
-
SNR – signal-to-noise ratio
-
Widget – A CAPSENSE™ functional unit consisting of one sensor or a group of similar sensors, implementing a specific higher-level functionality such as Button, Proximity Sensor, Linear Slider, Radial Slider, Matrix Buttons, Touchpad, Low Power, and Liquid Level widget.
Reference documents
Refer to the following documents for more information as needed:
- ModusToolbox™ tools package user guide
- Eclipse IDE for ModusToolbox™ user guide
- VS Code for ModusToolbox™ user guide
- CAPSENSE™ Configurator user guide
- Device Configurator user guide
- MTB CAT1 Peripheral driver library
- MTB CAT2 Peripheral driver library
- Liquid-level sensing with PSOC™ 4 CAPSENSE™
- Device datasheets
- Device technical reference manuals