Skip to main content

ModusToolbox™ Segment LCD Configurator user guide

A newer version of this document may be available on the web here.

Scope and purpose

The Segment LCD Configurator is used to generate display structures for the Segment LCD Driver.

Intended audience

This document helps application developers understand how to use the Segment LCD Configurator as part of creating a ModusToolbox™ application.

Document conventions

ConventionExplanation
BoldEmphasizes heading levels, column headings, menus and sub-menus
ItalicsDenotes file names and paths.
MonospaceDenotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets
File > NewIndicates that a cascading sub-menu opens when you select a menu item

Abbreviations and definitions

The following define the abbreviations and terms used in this document:

  • Application – One or more projects related to each other

  • Configurator – A GUI-based tool used to configure a resource

  • LCD – liquid crystal display

  • Glass – An LCD glass with one or more displays (for example, one 7-segment display and one bar-graph display).

  • Display – A block of symbols that have the same type on an LCD glass to indicate a multi-digital number or character string

  • Symbol – A block of pixels on an LCD glass to indicate a single digit or character.

  • Pixel – A basic displaying item; can be a segment of a 7-segment symbol (thus called a "segment"), a pixel of a dot-matrix display, or a stand-alone arbitrarily-shaped display element; each pixel has a unique set of common and segment lines within one LCD glass.

  • Common line (Com/COM for short) – A common wire/signal from the PSoC™ MCU to the LCD glass. In the Segment LCD Configurator, this is represented as a column in the Mapping table .

  • Segment line (Seg/SEG for short) – A segment wire/signal from the PSoC™ MCU to the LCD glass represented as a row in the Mapping table .

Reference documents

Refer to the following documents for more information as needed: