Display view
The Display view contains one or more tabs that show display types configured in the Display Editor.

A display symbol contains a set of pixels named A, B, C… (or 00, 01, 02 for the matrix display type) by default. The pixel names correspond to cell names in the Mapping table (for a pixel placed on the mapping table). The pixels have colors showing the connectivity status:
- Light Green – The pixel is connected, and the symbol is currently selected.
- Dark Green – The pixel is connected, and the symbol is currently not selected.
- Blue – The pixel is currently selected (connected or not).
- White – The pixel is not connected, and the symbol is currently selected.
- Grey – The pixel is not connected, and the symbol is not currently selected.
note
The same colors are used for pixels in the mapping table, when applicable.
note
In this document, symbol segments for displays (for example, 7-segment, 14-segment, etc.), are called “pixels” so that they are not confused with segment LCD connections (physical wires) represented as rows of the mapping table (see Abbreviations and definitions under About this document).