Overview
The Segment LCD Configurator is a stand-alone tool included with the ModusToolbox™ software and used to generate display structures for the Segment LCD Driver. Section "Supported software" provides details on the PDL libraries. The tool is supported on Windows, Linux, and macOS.

The Segment LCD Configurator supports the following types of displays:
- bar graph (1 pixel per symbol)
- 7-segment
- 14-segment
- 16-segment
- 5x8 dot matrix (40 pixels per symbol)
See the Display Editor section for more information about display types.
Supported software
| Name | Version | Link |
|---|---|---|
| PSoC™ 6 Peripheral Driver Library | 1.3.1 and later | https://github.com/Infineon/psoc6pdl |
| MTB CAT1 Peripheral Driver Library | 2.0.0 and later | https://github.com/Infineon/mtb-pdl-cat1 |
| MTB CAT2 Peripheral Driver Library | 1.3.0 and later | https://github.com/Infineon/mtb-pdl-cat2 |