Recommended Values for __Reset_Finish_Delay
Proper device operation may require adjusting the
__Reset_Finish_Delay
parameter, depending on the device's configuration. The following show the recommended values for this parameter when using KitProg3/MiniProg4 or ULINK2 debuggers/programmers.
KitProg3/MiniProg4 – 20 000 - 100 000
ULINK2 – 10 000 - 100 000
For example: