The VS Code GUI shows these launch configurations by default:

  • Launch : This builds the associated project, programs project-specific output file, and then starts a debugging session.

  • Attach : This starts a debugging session attaching to a running a target without programming or reset.

  • Erase Device : This erases all internal memories.

  • Erase All : If present, erases all internal and external memories.

  • Program : This builds the associated project, programs project-specific output file, and then runs the program.

Program

Open the main menu, select

Terminal > Run Task

. On the selection menu, select the "program" task.

If needed, VS Code builds the application and messages display in the Terminal. If the build is successful, device programming starts immediately. If there are build errors, then error messages will indicate as such. When programming completes successfully, the LED will start blinking.



Debug

Select the

Run and Debug

icon in the VS Code Activity Bar, select the

Launch PSoC C3 CM33 (KitProg3_Miniprog4)

or

Launch PSoC C3 CM33 (JLink)

Launch Configuration, and click

Start Debugging

icon or press

F5

.

If needed, VS Code builds the application and messages display in the Console. If the build is successful, VS Code switches to debug mode automatically. If there are build errors, then error messages will indicate as such.



Changing programming interface SWD/JTAG

To change the target interface, update the application’s

bsp.mk

file by adding a make variable as shown (possible values are ‘swd’ and ‘jtag’).

MTB_PROBE_INTERFACE=swd

Then, regenerate launch configurations:

Update debugger serial number

If there are two or more debugger probes connected to your computer, the first detected probe will be used by default. There should not be more than one probe with the same serial number. Use this method if you want to use only one specific device. Use OS-specific tools to determine the serial number of connected USB devices.

Update application's

bsp.mk

file by adding variable below with the serial number specified, and regenerate launch configurations:

MTB_PROBE_SERIAL=0B0B0F9701047400

Add Live Watch

While debugging an application in VS Code, it is possible to add a Live Watch variable. This topic provides an example using the Hello World application.

Note:

Live Watch is not supported for multi-core applications.

  1. Open the application's

    launch.json

    file, and locate the launch configuration. In this case "Launch PSoC C3 CM33 (KitProg3_MiniProg4)".

  2. Scroll to the end of the configuration and add the following:

    "liveWatch": {
    "enabled": true,
    "samplesPerSecond": 4
    }
  3. Open the

    main.c

    file and declare a global variable:

    volatile int count = 0;
  4. Add the code to increment the variable every time the LED is blinking:

    count++;
  5. Launch a serial terminal such as PuTTY to monitor the output.

    Note:

    This step may only be required for applications that have output, such as Hello World.

  6. Start the debugger. When it stops at

    main()

    , add the

    count

    variable to the

    CORTEX LIVE WATCH

    section and press the [

    Enter

    ] key.



  7. Check that the variable was added to the list and click on

    Run/Continue

    to proceed with debugging.

  8. Observe that the variable's value increments as the code is running.



Add SEGGER SWO/RTT Grapher

You can use the SEGGER real-time transfer (RTT) to visualize the output of the target performed via the SWO pin. This section provides an example:

  1. Start by adding the live watch described in the previous topic.

  2. In the main.c file, add an include for the SEGGER RTT header file:

    #include "SEGGER_RTT.h"
  3. Also, change the "count" global variable to

    uint32_t

    :

    static uint32_t count = 0;
  4. Next, locate the main "for" loop. Insert these two lines directly before the loop:

    SEGGER_RTT_Init();
    SEGGER_RTT_ConfigUpBuffer(0, NULL, NULL, 0, SEGGER_RTT_MODE_BLOCK_IF_FIFO_FULL);
  5. Then, inside the loop, update the

    count=count+1;

    line to add

    CySysLib_Delay();

    and

    SEGGER_RTT_Write();

    commands, as follows:

        for (;;)
    {
    Cy_SysLib_Delay(100);
    count=count+1;
    if(count%256==0)
    {
    count=0;
    }
    SEGGER_RTT_Write(0, &count, sizeof(count));

    /* code continues */

    }
  6. Manually add a new file in the deps directory named, segger-rtt.mtb, with the following content:

    https://github.com/SEGGERMicro/RTT#master#$$ASSET_REPO$$/RTT/master
  7. Edit the

    .

    cyignore

    file with the following content:

    # Segger RTT
    $(SEARCH_RTT)/Examples
    $(SEARCH_RTT)/Syscalls/SEGGER_RTT_Syscalls_IAR.c
  8. Open the Library Manager and click

    Update

    , or run

    make getlibs

    to update the application and acquire the RTT library.

  9. Open the

    launch.json

    file and, in the same "Launch" configuration where you added the live watch, and add the

    rttConfig

    configuration, as follows:

       "liveWatch": {
    "enabled": true,
    },
    "rttConfig": {
    "enabled": true,
    "address": "auto",
    "decoders": [
    {
    "label": "",
    "port": 0,
    "type": "graph",
    "encoding": "unsigned",
    "graphId": "count",
    "scale": 1
    }
    ]
    },

  10. Then, add the

    graphConfig

    configuration:

     "graphConfig": [
    {
    "label": "RTT variable test",
    "timespan": 20,
    "type": "realtime",
    "annotate": true,
    "maximum": 255,
    "minimum": 0,
    "plots": [
    {
    "graphId": "count",
    "label": "value of count",
    "color": "#FF0000"
    }
    ]
    }
    ]
  11. Save all files, start the debugger, and then click Continue.


    VS Code will display the RTT grapher.