About this document​

Scope and purpose​

This application note introduces you to the analog system block of PSOC™ HV mixed signal (MS) family MCUs. This application note also guides you to develop hardware and firmware design for human-machine interface (HMI), body, and powertrain applications.

Intended audience​

This document is intended for hardware and firmware design engineers.

Introduction​

PSOC™ HV MS is a fully-integrated programmable embedded system for several automotive HMI, body, and powertrain applications. The system features an Arm® Cortex® M0+ processor with programmable and reconfigurable analog and digital blocks. It is a combination of a microcontroller with a 12-bit SAR ADC, 5

th

-generation multi-sense converter (MSC) block supporting capacitive sensing (CAPSENSE™), digital peripherals such as PWMs and serial communication interfaces along with a LIN interface with integrated PHY, and a high-voltage subsystem to operate directly off the 12-V car battery.

PSOC™ HV MS is available in a 32-/48-/56-/64-QFN package with wettable flanks. To get a better understanding of the functionality described and terminology used in this application note, it is a good idea to read the “Section A: Overview” chapter of the architecture technical reference manual (architecture TRM) and AN85951 - PSOC™ 4 and PSOC™ 6 MCU CAPSENSE™ design guide. For more details, see References.

Analog system overview​

The analog system (see

Figure 1

) in PSOC™ HV MS includes a successive approximation register analog-to-digital converter (SAR ADC), low-power comparator (LPCOMP), continuous-time block mini (CTBm), and CAPSENSE™ block.

Note: This document does not describe the CAPSENSE™ block in detail. For more details, see AN0005 - CAPSENSE™ (multi-sense converter) block in PSOC™ HV MS family in References.

Figure 1. Analog system block diagram


SAR ADC​

PSOC™ HV MS has a SAR ADC, which is designed for applications that require moderate resolution and high data rate. It consists of the following blocks (see

Figure 2

):

Figure 2. SAR ADC block diagram


Before the SAR ADC, there are three multiplexers to route to the 16 internal channels (MS-64K) or 24 internal channels (MS-128K) of the SAR ADC. The DIAGMUX/ EXPMUX also has broken wire detection to check for broken wires from IO to the ADC.

  • SARMUX: Routes external pins and internal signals (AMUXBUS-A/-B, CTBm, temperature sensor output)

  • DIAGMUX: Configurable to measure various supply voltages, reference voltages and grounds on-chip

  • EXPMUX (for MS-128K): Expansion analog inputs from 8x GPIO

  • SAR ADC core: Fast 12-bit ADC with 1 Msps sampling rate

  • SARREF: Used for multiple reference selection

  • SARSEQ: The sequencer controller (SARSEQ) is used to control SARMUX, DIAGMUX, EXPMUX and SAR ADC to do an automatic scan on all enabled channels without CPU intervention and for pre-processing, such as averaging the output data

The result from each channel is double-buffered; a complete scan may be configured to generate an interrupt at the end of the scan. The sequencer may also be configured to flag overflow, collision, and saturation errors that can be configured to assert an interrupt.

For more flexibility, it is also possible to control most analog switches, including those in SARMUX/DIAGMUX/EXPMUX with the firmware. This makes it possible to implement an alternative sequencer with the firmware.

The SAR ADC block provides the following features:

  • Operates across the entire device power supply range

  • Sample rate up to 1 Msps

  • 16x(MS-64K)/24x (MS-128K) individually configurable channels that can scan various input sources and one injection channel

  • Each channel has the following features:

    • Input from an external pin (only for eight channels in single-ended mode and four channels in differential mode) or internal signal (AMUXBUS/CTBm/temperature sensor/diagnostic inputs)

    • Programmable acquisition times

    • Selectable 8-, 10-, and 12-bit resolution

    • Single-ended or differential measurement

    • Averaging

    • Results are double-buffered

    • Result may be left- or right-aligned

  • Diagnostic current sources and sinks (DIAG current SRC/SINK) to check for broken wires

  • Scan triggered by firmware, timer, low-power comparator, and by the SAR end-of-conversion signal

    • Hardware/firmware trigger (one-shot), and free-running (continuous conversion) modes

  • Hardware averaging support

    • First-order accumulate

    • Samples averaging from 2 to 256 (powers of 2)

  • Results represented in 16-bit sign-extended values

  • Selectable voltage references

    • Internal VDDA and VDDA/2 references

    • Internal 1.2 V reference with buffer

    • External reference

  • Interrupt generation

    • Finished scan conversion

    • Saturation detection and over-range (configurable) detection for every channel

    • Scan results overflow

    • Collision detection

  • Configurable injection channel

    • Triggered by firmware

    • Can be interleaved between two scan sequences (tailgating)

    • Selectable sample time, resolution, single-ended, or differential averaging

  • Low-power modes

    • ADC core and reference voltage have dedicated low-power modes

  • Internal AHB bridge and decoder used to communicate with the CPU

Low-power comparator​

PSOC™ HV MS devices have low-power comparators that can perform fast analog signal comparison in all system power modes. The positive and negative inputs can be connected to dedicated GPIO pins or to AMUXBUS-A/AMUXBUS-B. The comparator output can be read by the CPU through a status register, used as an interrupt or wakeup source, or routed to a GPIO.

PSOC™ HV MS comparators have the following features:

  • Configurable positive and negative inputs

  • Programmable power and speed

  • Ultra-low-power mode support (<4 µA)

  • Optional 10 mV input hysteresis

  • Low-input offset voltage (<4 mV after trim)

  • Wakeup source in deep sleep mode

Figure 3

shows the block diagram for the low-power comparator.

Figure 3. Low-power comparator block diagram


Continuous-time block mini (CTBm)​

The continuous-time block mini (CTBm) provides discrete operational amplifiers (opamps) inside the chip to use continuous-time signal chains. Each CTBm block includes a switch matrix for input/output configuration, two identical opamps, which are also configurable as two comparators, a charge pump inside each opamp, and a digital interface for comparator output routing, switch controls, and interrupts. PSOC™ HV MS-128K devices have one CTBm block, which can be operational in deep sleep power mode.

Note: PSOC™ HV MS-64K does not have the CTBm block.

The opamps in the PSOC™ HV MS-128K CTBm block have the following features:

  • Discrete, high-performance, and highly configurable on-chip amplifiers

  • Programmable power, bandwidth, compensation, and output drive strength

  • 1 mA or 10 mA selectable output current drive capability

  • 6 MHz gain bandwidth for 20 pF load

  • Less than 1 mV offset with trim

  • Support for opamp follower mode

  • Comparator mode with optional 10 mV hysteresis

  • Buffer/preamplifier for SAR inputs

  • Support in deep sleep device power mode

Figure 4

shows the block diagram for the CTBm block available in the PSOC™ HV MS-128K device.

Figure 4. CTBm block diagram


Schematic and layout example​

Schematic example​

Figure 5

shows the general schematic of the external circuit for the analog system block of the PSOC™ HV MS MCU. The external components for each analog interface (I/F) depend on the application. Therefore, this example only shows the power block of the PSOC™ HV MS MCU, which is very important to operate the analog system. For more information about the power block and pin assignment, see AN234116 - Hardware design guide and PSOC™ HV MS datasheet in

References.

Figure 5. General schematic for the analog system block

../figures/unsupported.svg

Table 1

shows an example of external components.

Note: See AN234116 for details of external components of the power block.

Table 1. External component example for CAPSENSE™ buttons

Symbol

Overview

Parameter

Value 1

Value 2

Value 3

C10

SAR ADC bypass capacitor

1 μF or 0.1 μF

X7R or more

> 10 V

SAR ADC bypass capacitor​

The internal references (1.2 V from bandgap or VDDA/2) are buffered with the reference buffer. This reference may be routed to the Ext Vref/SAR bypass pin where an external capacitor can be used to filter internal noise that may exist on the reference signal. The SAR ADC sample rate is limited to 100 ksps (at 12-bit sample rate) without an external reference bypass capacitor.

For example, without a bypass capacitor and with the 1.2 V internal Vref, the maximum SAR ADC clock frequency is 1.6 MHz. When using an external reference, it is recommended that an external capacitor is used.

Table 2

lists different reference modes and its maximum frequency/sample rate for 12-bit continuous mode operation.

Table 2. SAR ADC reference mode

Reference mode

Bypass capacitor

Buffer

Max frequency

Max sample rate (12-bit)

1.2 V internal Vref

No

Yes

1.6 MHz

100 ksps

Yes

Yes

18 MHz

1 Msps

VDDA/2

No

Yes

1.6 MHz

100 ksps

Yes

Yes

18 MHz

1 Msps

VDDA

No

No

9 MHz

500 ksps

External Vref (low-impedance path)

No

No

18 MHz

1 Msps

The startup time of the 1.2 V internal Vref varies with the bypass capacitor size;

Table 3

lists two common values for the bypass capacitor and the corresponding startup time specification for the internal Vref. If the reference selection is changed between scans or when scanning after sleep/deep sleep, make sure that the 1.2 V internal Vref is settled when the SAR ADC starts sampling. The worst-case settling time (when Vref is completely discharged) is the same as the startup time.

Table 3. Bypass capacitor values

Internal Vref startup time

Maximum specification

Startup time for reference with external capacitor (1 µF)

2 ms

Startup time for reference with external capacitor (0.1 µF)

200 µs

Startup time without external capacitor

10 µs

Layout example​

Figure 6

shows an example of the power supply block layout.

Figure 6. Analog system block layout

image9.svg

Follow these guidelines for the PSOC™ HV MS analog system circuit on the PCB:

Note: See AN234116 for detailed layout guidelines for the power block.

  • Place C10 (SAR ADC bypass capacitor) as close as possible to the pin. If the board has a GND plane, provide a through hole (via) near this capacitor.

  • If C10 is placed on the bottom side, provide a through hole (via) near the pin. Place C10 as close as possible to the through hole on the bottom side.

AutoPDL firmware configuration​

Infineon provides an evaluation license of the Automotive Peripheral Driver Library (AutoPDL) including startup code as sample firmware. AutoPDL provides low-level drivers for all PSOC™ HV peripherals and is ISO 26262 compliant. AutoPDL has the following features:

  • Drivers and middleware

    • Low-level drivers for all peripherals

    • Middleware for complex peripherals such as CAPSENSE™

  • Qualified for ASPICE Level 2

    • MISRA 2012 AMD1, CERT C “Rules” (L1, L2, L3) are applied, Deviations/Warnings documented

    • Traceability

  • Safety ASIL-B

    • Safety documentation reduces customers’ effort for safety qualification

    • Safety features based on safety element out of context (SEooC)

  • Compiler version

    • IAR Embedded Workbench for Arm®, Functional Safety, version 8.50

Note: These examples are created based on AutoPDL version 1.3.1.


Analog system Peripheral Driver Library​

The Peripheral Driver Library is a set of firmware drivers that provide APIs for accessing the hardware. These APIs perform initialization and control activities of each peripheral.

Table 4

lists and describes the interface to each analog system function. The peripheral drivers of analog system are located in the AutoPDL path of:

<user path>\source\drivers\ sar, lpcomp, ctb

For more detailed information, see UsersGuide_xxxx _x_x_PSoC4HV_PDL.pdf in

<user path>\doc folder

.

Table 4. Analog system functions

Function

Description

SAR ADC (cy_sar.h)

Cy_SAR_Init()

Initializes SAR ADC global control registers

Cy_SAR_DeInit()

Deinitializes SAR ADC global control registers

Cy_Sar_Enable()

Enables the SAR hardware

Cy_Sar_Disable()

Disables the SAR hardware

Cy_Sar_StartConvert()

Starts conversion immediately

Cy_Sar_StopConvert()

Stops continuous conversion

Cy_Sar_SetConvertMode()

Sets the registers SAMPLE_CTRL.DSI_TRIGGER_EN and DSI_TRIGGER_LEVEL

Cy_Sar_GetInterruptStatusMasked()

Gets the INTR_MASKED register value

Cy_Sar_GetResult16()

Gets the CHAN_RESULT.RESULT register value

Cy_Sar_SetLowLimit()

Sets the RANGE_THRES.RANGE_LOW register value

Cy_Sar_SetHighLimit()

Sets the RANGE_THRES.RANGE_HIGH register value

Cy_Sar_SetAnalogSwitch()

Sets the MUX_SWITCH0 register value

Cy_Sar_SetSwitchSarSeqCtrl()

Sets the MUX_SWITCH_HW_CTRL register value

Cy_Sar_GetChanResultUpdated()

Gets the CHAN_RESULT_UPDATED register value

Cy_Sar_EnableInjection

Sets the INJ_CHAN_CONFIG.INJ_START_EN register value

Cy_Sar_SetRangeCond()

Sets the RANGE_COND register value

Cy_Sar_SetDiagSwitch()

Sets the MUX_SWITCH2 register value

Cy_Sar_SetDiagHwCtrl()

Sets the MUX_SWITCH_HW_CTRL2 register value

Cy_Sar_GetInterruptStatus()

Gets the INTR register value

Cy_Sar_ClearInterrupt()

Clears the INTR register value

Cy_Sar_SetInterruptMask()

Sets the INTR_MASK register value

Cy_Sar_GetRangeInterruptStatus()

Gets the RANGE_INTR register value

Cy_Sar_ClearRangeInterrupt()

Clears the RANGE_INTR register value

Cy_Sar_SetRangeInterruptMask()

Sets the RANGE_INTR_MASK register value

Cy_Sar_GetRangeInterruptStatusMasked()

Gets the RANGE_INTR_MASKED register value

Cy_Sar_GetSatInterruptStatus()

Gets the SATURATE_INTR register value

Cy_Sar_ClearSatInterrupt()

Clears the SATURATE_INTR register value

Cy_Sar_SetSatInterruptMask()

Sets the SATURATE_INTR_MASK register value

Cy_Sar_GetSatInterruptStatusMasked()

Gets the SATURATE_INTR_MASKED register value

Cy_Sar_GetInterruptCause()

Gets the INTR_CAUSE register value

Cy_Sar_EnablePump()

Sets the PUMP_CTRL.ENABLED register value

Cy_Sar_DisablePump()

Clears the PUMP_CTRL.ENABLED register value

Cy_Sar_SetPumpClk()

Sets the PASS_CTRL register value

Cy_Sar_InitChannel()

Sets the CHAN_CONFIG and CHAN_EN register value

Cy_Sar_DeinitChannel()

Sets the initial value to CHAN_CONFIG and CHAN_EN register value

Cy_Sar_EnableChannel()

Sets the CHAN_EN register value

Cy_Sar_DisableChannel()

Clears the CHAN_EN register value

Cy_Sar_GetInterruptMask()

Gets the INTR_MASK register value

Cy_Sar_GetSatInterruptMask()

Gets the SATURATE_INTR_MASK register value

Cy_Sar_GetRangeInterruptMask()

Gets the RANGE_INTR_MASK register value

Cy_Sar_IsBusy()

Gets the SAR conversion status

Cy_Sar_CalcDieTemp()

Converts the die temp measurement to degrees Celsius

LPCOMP (cy_lpcomp.h)

Cy_Lpcomp_Init()

Initializes the low-power comparator

Cy_Lpcomp_DeInit()

Deinitializes the low-power comparator

Cy_Lpcomp_Start()

Enables the low-power comparator and sets the interrupt mode

Cy_Lpcomp_Stop()

Disables the low-power comparator and sets the interrupt mode to disabled

Cy_Lpcomp_ClearInterrupt()

Clears LPCOMP interrupts by setting each bit

Cy_Lpcomp_GetInterruptSource()

Returns the status of two different LPCOMP interrupt requests

Cy_Lpcomp_GetInterruptSourceMasked()

Returns an interrupt request register masked by an interrupt mask

Cy_Lpcomp_GetCompare()

Returns a non-zero value when the voltage connected to the positive input is greater than the negative input voltage

Cy_Lpcomp_SetInterruptMask()

Sets the LPCOMP interrupt mask by setting each bit

Cy_Lpcomp_GetInterruptMask()

Returns an interrupt mask

Cy_Lpcomp_SetSpeed()

Sets the drive power mode and speed configuration

CTBm (cy_ctb.h)

Cy_Ctb_InitOpamp()

Initializes the opamp(s)

Cy_Ctb_DeInit()

Resets the CTB registers back to power on reset defaults

Cy_Ctb_Enable()

Powers up the CTB hardware block

Cy_Ctb_Disable()

Powers down the CTB hardware block

Cy_Ctb_SetDeepSleepMode()

Enables or disables the entire CTB (not per opamp) in deep sleep mode

Cy_Ctb_SetPower()

Configures the power level and charge pump for the specific opamp(s)

Cy_Ctb_SetCompInterruptEdgeType()

Sets the comparator edge detect for interrupt and output trigger

Cy_Ctb_GetCompStatus()

Returns the comparator status

Cy_Ctb_GetInterruptStatus()

Returns the status of the specified edge detect interrupt request

Cy_Ctb_ClearInterrupt()

Clears the CTB comparator interrupt

Cy_Ctb_SetInterruptMask()

Sets the specified interrupt mask value

Cy_Ctb_GetInterruptMask()

Returns the specified interrupt mask value

Cy_Ctb_GetInterruptStatusMasked()

Returns the CTB comparator edge output interrupt state after being masked

Cy_Ctb_SetAnalogSwitch()

Open or close a set of the CTB switches

Cy_Ctb_GetAnalogSwitch()

Returns the open or closed state of the specified analog switch(es)

Cy_Ctb_OpenAllSwitches()

Opens all the switches and disables all hardware control of the switches

Cy_Ctb_EnableSarSeqCtrl()

Enables the SAR sequencer control for the specified switches

Cy_Ctb_DisableSarSeqCtrl()

Disables the SAR sequencer control for the specified switches

Cy_Ctb_SetDsabSource()

Sets the DSAB bias current sources

AutoPDL code example​

To successfully execute the analog system examples, you need the following:

  • Evaluation kit (CYHVMS-64K-56-001 or KIT_PSOC4-HVMS-64K_LITE)

  • IAR EWARM 8.50.9 (or FS 8.50.10)

  • AutoPDL evaluation license or source code

SAR ADC example​

This example demonstrates the SAR ADC single-channel measurement with single-ended input and averaging mode. The code example is located in the AutoPDL path of

<user path>\examples\sar

.

SAR ADC example configuration:

  • Channel: CH0 as single-ended (unsigned)

  • Resolution: maximum resolution (12-bit)

  • Target sample rate: 50 ksps (SAR clock 1 MHz, 18 clock cycles)

  • Acquisition time: 4 or 302 clock cycles

  • Averaging: enable (32 samples)

  • Diagnostic current sources and sink: Disable

  • Positive terminal: P5.3 (external temperature sensor)

  • Negative terminal: VSSA

  • Vref connection: VDDA

Code Listing 1

shows an example of SAR ADC configuration. For more details, see the architecture and register TRM in

References

.

Note: You should compare the code example with the flowchart and learn how to use the SAR ADC functions. You cannot copy/paste the code and expect it to work. This applies to all code examples provided in this document.


Code Listing 1​

1 /* SAR channel configuration to use unsigned format. */
2 cy_stc_sar_channel_config_t config0_chan0_config =
3 {
4 .sampleTimeSel = CY_SAR_SAMPLE_TIME_SEL1,
5 .posPinPortAddr = CY_SAR_POS_ADDR_SARMUX_3,
6 .avgEn = TRUE,
7 .negPinPortAddr = CY_SAR_NEG_ADDR_DIAG_VSSA,
8 .resolution = CY_SAR_MAXRESOLUTION,
9 .differentialEn = FALSE,
10 .negAddrEn = FALSE,
11 .diagVplusSource = FALSE,
12 .diagVplusSink = FALSE,
13 .diagVminusSoure = FALSE,
14 .diagVminusSink = FALSE,
15 };
16
17 /* SAR control configuration */
18 cy_stc_sar_control_config_t config0_ctrl0_config =
19 {
20
21 /* SAMPLE_TIME01 register */
22 /* Set the aperture times to target a 50 ksps scan rate.
23 * Recall that the SAR clock is 1 MHz.
24 * Sample Time 0 is set to 302 clock cycles.
25 * Sample Time 1 is set to 4 clock cycles. */
26 .sampleTime0 = 302,
27 .sampleTime1 = 4,
28
29 /* SAMPLE_TIME23 register */
30 /* Set the unused sample times 2 and 3 to be 4 clock cycles.
31 * Note that these two sample times are not used by any channels and only shown for reference */
32 .sampleTime2 = 4,
33 .sampleTime3 = 4,
34 .rangeCond = CY_SAR_RANGE_COND_BELOW,
35
36 /* Set the initial state of switches.
37 * Close the switch between Pin 3 of the SARMUX to the positive terminal of the SAR (used by channel 3).
38 * Close the switch between VSSA and the negative terminal of the SAR (VSSA_VMINUS). */
39 .sarmuxFirmwareSwitches = CY_SAR_MUX_FW_P3_VPLUS_MSK | CY_SAR_MUX_FW_VSSA_VMINUS_MSK,
40
41 .singleEndedSigned = FALSE,
42 .vrefSel = CY_SAR_VREF_SEL_VDDA,
43 .negSel = CY_SAR_NEG_SEL_VSSA_KELVIN,
44 .sarHwCtrlNegvref = CY_SAR_NEGVREF_FW_ONLY,
45 .pwrCtrlvref = CY_SAR_NORMAL_PWR,
46 .icontLv = CY_SAR_LV_NORMAL_PWR,
47 .subResolution = CY_SAR_SUB_RESOLUTION_10B,
48 .avgCnt = CY_SAR_AVG_CNT_32,
49 .avgMode = CY_SAR_ACCUNDUMP,
50 .trigMode = CY_SAR_TRIGGER_MODE_FW_ONLY,
51 .vrefBypCapEn = TRUE ,
52 .boostpumpEn = FALSE,
53 .refbufEn = TRUE,
54 .switchDisable = TRUE,
55 .leftAlign = FALSE,
56 .differentialSigned = FALSE,
57 .avgShift = TRUE,
58 .dsiSyncTrigger = FALSE,
59 .eosDsiOutEn = FALSE,
60 };

Figure 7

shows the flowchart for SAR ADC design;

Code Listing 2

shows the main function.

Figure 7. Flowchart for SAR ADC example


Code Listing 2​

1	/* Function Name: main */
2 int main(void)
3 {
4 SystemInit();
5
6 __enable_interrupt(); /* Enable global interrupts. */
7
8 /* Initialize Port and Clock */
9 Peripheral_Initialization();
10
11 /* Opening UART Comment */
12 TERM_PRINT_H("SAR ADC Code example \n\r");
13
14 /* Initialize the SAR positive port */
15 Cy_Gpio_SetDriveMode(CY_USER_PORT, CY_USER_PIN, CY_GPIO_DRIVE_MODE_ANALOG);
16
17 /* Configure the clock for the SAR for a 1 MHz clock frequency. */
18 Cy_SysClk_Periph_AssignDivider(CY_PCLK_PASS0_CLOCK_SAR, CY_SYSCLK_DIV_16_BIT, 1u);
19 Cy_SysClk_Periph_SetDivider(CY_SYSCLK_DIV_16_BIT, 1u, SAR_TARGET_CLK_DIVIDER - 1u);
20 Cy_SysClk_Periph_EnableDivider(CY_SYSCLK_DIV_16_BIT, 1u);
21
22 /* Interrrupt Configuration for WDT */
23 Cy_SysInt_SetVector(pass_0_interrupt_sar_IRQn, SAR_Interrupt);
24 Cy_SysInt_ClearPendingIRQ(pass_0_interrupt_sar_IRQn);
25 Cy_SysInt_EnableIRQ(pass_0_interrupt_sar_IRQn);
26
27 /* De-initialize and enable the SAR to Config0. */
28 Cy_Sar_DeInit(CY_SAR0);
29
30 /* Initialize the SAR block to Config0. */
31 Cy_Sar_Init(CY_SAR0, &config0_ctrl0_config);
32
33 /* Set interrupt mask for the SAR sources */
34 Cy_Sar_SetInterruptMask(CY_SAR0, CY_SAR_INTR_EOS_INTR_MSK);
35
36 /* Enable the SAR block to Config0. */
37 Cy_Sar_Enable(CY_SAR0);
38 // Wait 2 [ms]
39 Cy_SysLib_DelayUs(2000);
40
41 /* Initialize and enable the SAR channel to Config0 channel 0. */
42 Cy_Sar_InitChannel(CY_SAR0, 0, &config0_chan0_config);
43 Cy_Sar_EnableChannel(CY_SAR0, CONFIG0_CHAN_EN);
44
45 /* Initiate continuous conversions. */
46 Cy_Sar_StartConvert(CY_SAR0, CY_SAR_CONVERT_MODE_CONTINUOUS);
47
48 for(;;)
49 {
50 // Wait 0.5 [s]
51 Cy_SysLib_Delay(500);
52
53 /* Printing SAR(ADC) values in UART terminal */
54 Term_Printf("ADC conversion value for Potentiometer : %d \n\r", chanResult);
55 }
56 }
57
58 /* Function Name: SAR_Interrupt */
59 void SAR_Interrupt(void)
60 {
61 uint32 intrStatus = 0u;
62
63 /* Read interrupt status register. */
64 intrStatus = Cy_Sar_GetInterruptStatus(CY_SAR0);
65
66 /* Check for the EOS interrupt. */
67 if ((intrStatus & CY_SAR_INTR_EOS_INTR_MSK) == CY_SAR_INTR_EOS_INTR_MSK)
68 {
69 /* Clear handled interrupt. */
70 Cy_Sar_ClearInterrupt(CY_SAR0, intrStatus);
71
72 /* Get the ADC results for connected channel in Config0. */
73 chanResult = Cy_Sar_GetResult16(CY_SAR0, 0);
74 }
75 }

Low-power comparator example​

This example demonstrates the LPCOMP0_CH0 single-channel measurement with differential input on +ve (P1.1) and -ve (P1.2) terminals. The comparator value of LPCOMP is available in the

lpcompCmpValue

variable; the signal can be output to any GPIO. The code example is located in AutoPDL path of

<user path>\examples\lpcomp

.

Note: Pin assignment differs between this example and the AutoPDL example file.

LPCOMP example configuration:

  • Channel: LPCOMP[0]CH0 as single-channel measurement

  • Power mode: Slow operating mode (uses less power, <50 µA)

  • Hysteresis: Enable (add 10 mV hysteresis)

  • Interrupt type: Both rising and falling edges

  • Comparator DSI (trigger) out: Synchronize and level

Code Listing 3

shows the example of LPCOMP configuration. For more details, see the architecture and register TRMs in

References

.

Code Listing 3​

1	/* Configuration structure for channel of low-power comparator */
2 cy_stc_lpcomp_config_t user_lpcomp_ch_cfg =
3 {
4 .outputMode = CY_LPCOMP_OUT_SYNC, // CY_LPCOMP_OUT_DIRECT,
5 .hysteresis = CY_LPCOMP_HYST_ENABLE,
6 .speed = CY_LPCOMP_MODE_SLOW,
7 };

Figure 8

shows the flow chart for LPCOMP design, and

Code Listing 4

shows the code example of main function.

Figure 8. Flowchart for LPCOMP example


Code Listing 4​

1	/* Function Name: main */
2 int main(void)
3 {
4 SystemInit();
5
6 __enable_interrupt(); /* Enable global interrupts. */
7
8 /* Initialisation of User Led */
9 Cy_Gpio_SetPinMode(CY_USER_LED1_PORT_IDX, CY_USER_LED1_PIN, CY_USER_LED1_MUX);
10 Cy_Gpio_SetDriveMode(CY_USER_LED1_PORT_IDX, CY_USER_LED1_PIN, CY_GPIO_DRIVE_MODE_OD_DRIVE_HIGH);
11
12 /* Initialisation of low-power comparator input */
13 Cy_Gpio_SetPinMode(USER_LPCOMP_POS_IN_PORT, USER_LPCOMP_POS_IN_PIN, USER_LPCOMP_POS_IN_PIN_MUX);
14 Cy_Gpio_SetDriveMode(USER_LPCOMP_POS_IN_PORT, USER_LPCOMP_POS_IN_PIN, CY_GPIO_DRIVE_MODE_ANALOG);
15
16 Cy_Gpio_SetPinMode(USER_LPCOMP_NEG_IN_PORT, USER_LPCOMP_NEG_IN_PIN, USER_LPCOMP_NEG_IN_PIN_MUX);
17 Cy_Gpio_SetDriveMode(USER_LPCOMP_NEG_IN_PORT, USER_LPCOMP_NEG_IN_PIN, CY_GPIO_DRIVE_MODE_ANALOG);
18
19 /* Initialisation of low-power comparator output */
20 Cy_Gpio_SetPinMode(USER_LPCOMP_OUT_PORT, USER_LPCOMP_OUT_PIN, USER_LPCOMP_OUT_PIN_MUX);
21 Cy_Gpio_SetDriveMode(USER_LPCOMP_OUT_PORT, USER_LPCOMP_OUT_PIN, CY_GPIO_DRIVE_MODE_PULLUP);
22
23 /* De-initializes the low-power comparator */
24 Cy_Lpcomp_DeInit(LPCOMP_INSTANCE, LPCOMP_CHANNEL);
25
26 /* Initializes the low-power comparator */
27 Cy_Lpcomp_Init(LPCOMP_INSTANCE, LPCOMP_CHANNEL, &user_lpcomp_ch_cfg);
28
29 /* Enable low-power comparator */
30 Cy_Lpcomp_Start(LPCOMP_INSTANCE, LPCOMP_CHANNEL, LPCOMP_INTERRUPT);
31
32 /* Set irq for low-power comparator interrupt */
33 Cy_SysInt_SetVector(LPCOMP_IRQ, LpcompEventHandler);
34 Cy_SysInt_ClearPendingIRQ(LPCOMP_IRQ);
35 Cy_SysInt_EnableIRQ(LPCOMP_IRQ);
36
37 /* Set interrupt mask for the lpcomp sources */
38 Cy_Lpcomp_ClearInterrupt(LPCOMP_INSTANCE, LPCOMP_INTR_MASK);
39 Cy_Lpcomp_SetInterruptMask(LPCOMP_INSTANCE, LPCOMP_INTR_MASK);
40
41 /* Check blinking rate of RED Led */
42 for(;;)
43 {
44 // Wait 0.05 [s]
45 Cy_SysLib_DelayUs(50000);
46 Cy_Gpio_Inv(CY_USER_LED1_PORT_IDX, CY_USER_LED1_PIN);
47 }
48 }
49
50 /* Function Name: intrupput */
51 void LpcompEventHandler(void)
52 {
53 uint32 intStatus;
54
55 /* Get the current status of LPCOMP interrupts */
56 intStatus = Cy_Lpcomp_GetInterruptSource(LPCOMP_INSTANCE);
57
58 if(intStatus & LPCOMP_INTR_MASK)
59 {
60 /* Get the LPCOMP channel compare value */
61 lpcompCmpValue = Cy_Lpcomp_GetCompare(LPCOMP_INSTANCE, LPCOMP_CHANNEL);
62 }
63
64 /* Clear the LPCOMP interrupt */
65 Cy_Lpcomp_ClearInterrupt(LPCOMP_INSTANCE, intStatus);
66 }

Continuous-time block mini example​

This example demonstrates the comparator and amplifier functions of continuous-time block mini (CTBm) by using AutoPDL. The comparator compares the input voltage of P1.1 and P1.6. The amplifier amplifies the input voltage at P1.7 with 2x magnification.

Note: There is no code example in the AutoPDL package.

CTBm example configuration:

  • Comparator

    • Power level: High-power mode

    • Opamp output mode: Comparator mode

    • Comparator edge detection: Both edge detection

    • Comparator trigger mode: Output pulse

    • Trigger output: Synchronize

    • Comparator hysteresis: Enable 10 mV hysteresis

    • Opamp charge pump: Enable

    • Deep sleep mode: Disable

  • Amplifier

    • Power level: High-power mode

    • Opamp output mode: Amplifier mode

    • Opamp charge pump: Enable

    • Deep sleep mode: Disable

    • Other comparator settings: Default

Code Listing 5

shows the example of CTBm configuration. For more details, see the architecture and register TRMs in

References

.

Code Listing 5​

67	/* Comparator configuration structure */
68 cy_stc_ctb_opamp_config_t Ctb_Control_Config = {
69 .switchCtrl = TEST_CTB_COMPARATOR0_SWITCH_MASK,
70 .power = CY_CTB_POWER_HIGH,
71 .outputMode = CY_CTB_MODE_COMP,
72 .compEdge = CY_CTB_COMP_EDGE_BOTH,
73 .compLevel = CY_CTB_COMP_TRIGGER_OUT_PULSE,
74 .compBypass = FALSE,
75 .compHyst = TRUE,
76 .pump = TRUE,
77 };
78
79 /* Amplifier configuration structure */
80 cy_stc_ctb_opamp_config_t Ctb_Control_Config = {
81 .switchCtrl = TEST_CTB_AMPLIFIER1_SWITCH_MASK,
82 .power = CY_CTB_POWER_HIGH,
83 .outputMode = CY_CTB_MODE_OPAMP_INTERNAL,
84 .compEdge = CY_CTB_COMP_EDGE_DISABLE,
85 .compLevel = CY_CTB_COMP_TRIGGER_OUT_PULSE,
86 .compBypass = FALSE,
87 .compHyst = FALSE,
88 .pump = TRUE,
89 };

Figure 9

shows the flow chart for CTBm design, and

Code Listing 6

shows the code example of main function.

Figure 9. Flowchart for CTBm example


Code Listing 6​

90	/* Function Name: main */
91 int main(void)
92 {
93 SystemInit();
94
95 /* Enable global interrupts. */
96 __enable_interrupt();
97
98 Peripheral_Setup();
99
100 Comparator0_Sequence(); /* Configure opamp0 as comparator */
101 Amplifier1_Sequence(); /* Configure opamp1 as amplifier */
102
103 Cy_Ctb_SetDsabSource(CY_PASS0, CY_CTB_DSAB_ACTIVE); /* Active mode */
104 Cy_Ctb_SetDeepSleepMode(CY_CTBM0, FALSE); /* Disable deep sleep mode */
105
106 Cy_Ctb_Enable(CY_CTBM0); /* Enable CTB */
107 Cy_SysLib_Delay(1u); /* Wake-up time from Enabled to Usable */
108
109 /* Enable comparator0 interrupt */
110 Cy_Ctb_ClearInterrupt(CY_CTBM0, CY_CTB_OPAMP_0); /* Clear comparator0 interrupt */
111 Cy_Ctb_SetInterruptMask(CY_CTBM0, CY_CTB_OPAMP_0); /* Enable comparator0 interrupt mask */
112
113 for(;;)
114 {
115 Cy_SysLib_Delay(1000);
116 }
117 }
118
119 /* Function Name: intrupput */
120 void DEFAULT_CTB_HANDLER(void)
121 {
122 uint32 intrStatus = Cy_Ctb_GetInterruptStatus(CY_CTBM0, CY_CTB_OPAMP_BOTH);
123
124 /* OpAmp0 comparator edge detect interrupt */
125 if (CY_CTB_INTR_COMP0_MSK == (CY_CTB_INTR_COMP0_MSK & intrStatus))
126 {
127 Cy_Ctb_ClearInterrupt(CY_CTBM0, CY_CTB_OPAMP_0); /* Clear interrupt */
128 }40 }

CTBm connects to SAR ADC​

The SAR ADC inputs are from the external pin (only for eight channels in single-ended mode and four channels in differential mode) or an internal signal (AMUXBUS/CTBm/temperature sensor/diagnostic inputs).

This example demonstrates how to connect the CTBm output via the sarbus0/1 input of SARMUX, which is a programmable analog multiplexer (see

Figure 10

).

Note: CTBm sampling time is not fast enough to sample at 1 Msps.See the architecture TRM for more detailed SARMUX information.

Figure 10. SARMUX block diagram


Code Listing 7

shows an example of the SAR ADC channel configuration and amplifier switch mask definition. See Section

SAR ADC example

for SAR ADC configuration details and Section

Continuous-time block mini example

for CTBm configuration details.

Code Listing 7​

1	/* SAR ADC channel configuration*/
2 static cy_stc_sar_channel_config_t Sar_channel_config =
3 {
4 .posPinPortAddr = CY_SAR_POS_ADDR_CTB0_OA1, /* POS select CTB0 opamp1 */
5 .resolution = CY_SAR_MAXRESOLUTION, /* 12-Bit resolution */
6 .sampleTimeSel = CY_SAR_SAMPLE_TIME_SEL0, /* Sample time 0 */
7 .negPinPortAddr = CY_SAR_NEG_ADDR_SARMUX_0, /* Default negative port/pin address */
8 .differentialEn = FALSE, /* Disable differential */
9 .avgEn = TRUE, /* Enable average */
10 .negAddrEn = FALSE, /* Disable negative port/pin address */
11 .diagVplusSource = FALSE, /* Disable VPLUS pullup */
12 .diagVplusSink = FALSE, /* Disable VPLUS pulldown */
13 .diagVminusSoure = FALSE, /* Disable VMINUS pullup */
14 .diagVminusSink = FALSE, /* Disable VMINUS pulldown */
15 };
16
17 /* amplifier1SwitchMask */
18 #define TEST_CTB_AMPLIFIER1_SWITCH_MASK (CY_CTB_OA1_SW_OA1P_A43_MSK | \
19 CY_CTB_OA1_SW_OA1M_A22_MSK | \
20 CY_CTB_OA1_SW_OA1O_D52_MSK | \
21 CY_CTB_OA1_SW_OA1O_D82_MSK)
22
23 #define TEST_CTB_AMPLIFIER1_SEQ_SWITCH_MASK (CY_CTB_SW_HW_CTRL_P2_MSK | CY_CTB_SW_HW_CTRL_P3_MSK)

posPinPortAddr = CY_SAR_POS_ADDR_CTB0_OA1

sets the positive port of the SAR ADC (select CTB0 opamp1).

TEST_CTB_AMPLIFIER1_SWITCH_MASK

controls the CTBm internal switches as shown below (0=open, 1=close switch).

  • CY_CTB_OA1_SW_OA1P_A43_MSK

    : Opamp1 positive terminal ctbbus1

  • CY_CTB_OA1_SW_OA1M_A22_MSK

    : Opamp1 negative terminal P4

  • CY_CTB_OA1_SW_OA1O_D52_MSK

    : Opamp1 output sarbus0 (ctbbus2 in CTB)

  • CY_CTB_OA1_SW_OA1O_D82_MSK: Opamp1 output switch to short 1x with 10x drive

Figure 11

shows the internal switches setting of this example.

Note: The negative port is connected to Vref by the SAR ADC configuration.See Section SAR ADC example to learn how to get the SAR ADC results.

Figure 11. Internal switches setting


Summary​

This application note described the details of the analog system block of PSOC™ HV MS MCU. By using the analog system block, human-machine interface (HMI), body, and powertrain applications can be achieved with higher quality.

Infineon provides an evaluation board and wealth of sample software to help you get started with PSOC™ HV MS family MCUs. To use the evaluation board, contact your sales representative or Infineon Technical Support.

Glossary​

Table 5. Glossary

Terms

Description

ADC

analog-to-digital converter

AHB

Advanced High-performance Bus

AMUX

analog multiplexer

API

application programming interface

AutoPDL

Automotive Peripheral Driver Library

ASIL-B

Automotive Safety Integrity Level – B

ASPICE

Automotive Software Process Improvement and Capability Determination

CERT

Computer Emergency Response Team

CPU

central processing unit

CTBm

Continuous-time block mini

CTRL

Control

CTRLMUX

control multiplexer

DIAGMUX

diagnostic multiplexer

DIAG cur SRC/SINK

diagnostic current sources and sinks

DMA

direct memory access

EXPMUX

expansion multiplexer

FW

firmware

GND

Ground

GPIO

general-purpose I/O

GUI

graphical user interface

HFCLK

high-frequency clock

HMI

human-machine interface

HV

high-voltage

HW

hardware

I/O

input or output

I/F

Interface

IAR

IAR Systems (company name)

IAR EARM

IAR Embedded Workbench for Arm® (software name)

IC

integrated circuit

ISO

International Organization for Standardization

LED

light-emitting diode

LIN

Local Interconnect Network

LPCOMP

Low-power comparator

MUX

Multiplexer

MW

middleware

MSC

multi-sense converter

MCU

microcontroller unit

MISRA

Motor Industry Software Reliability Association

MS

mixed signal

PCB

printed circuit board

PELI

peripheral

pF

picofarad

PHY

physical layer

PWM

pulse width modulation

QFN

quad flat non-leaded

RX

receiver

SAR

successive approximation register

SARMUX

SAR multiplexer

SARREF

SAR reference

SARSEQ

SAR sequencer

SEooC

safety element out of context

SW

switch

TRM

technical reference manual

TX

transmitter

References​

Application notes​

  1. Infineon Technologies AG:

    AN185951 PSOC™ 4 and PSOC™ 6 MCU CAPSENSE™ design guide

    ; Available online

  2. Infineon Technologies AG:

    AN234115 - Getting started with PSOC™ HV MS family

    ; Available online

  3. Infineon Technologies AG:

    AN234116 - Hardware design guide for PSOC™ HV MS family

    ; Available online

  4. Infineon Technologies AG:

    AN0003 - High voltage subsystem (HVSS) in PSOC™ HV MS family

    ; Available online

  5. Infineon Technologies AG:

    AN0005 - CAPSENSE™ (multi-sense converter) block in PSOC™ HV MS family

    ; Available online

Device datasheet​

  1. Infineon Technologies AG:

    PSOC™ High Voltage (HV) Mixed Signal (MS) Automotive MCU datasheet

    ; Available online

Architecture reference manual​

  1. Infineon Technologies AG:

    PSOC™ high voltage (HV) mixed signal (MS) MCU architecture technical reference manual (TRM)

    ; Available online

Registers reference manual​

  1. Infineon Technologies AG:

    PSOC™ high-voltage (HV) mixed signal (MS): PSOC(TM) HVMS-64K registers TRM

    ; Available online

  2. Infineon Technologies AG:

    PSOC™ high-voltage (HV) mixed signal (MS): PSOC(TM) HVMS-128K registers TRM

    ; Available online

Evaluation board user guide​

  1. Infineon Technologies AG:

    CYHVMS-64K-56-001 PSOC™ high-voltage (HV) mixed signal (MS) evaluation kit user guide

    ; Available online

Automotive peripheral driver library (AutoPDL)​

  1. Infineon Technologies AG:

    PSOC™ HV MS AutoPDL

    ; Available online

Revision history​

Document version

Date of release

Description of changes

V1.0

2025-06-26

Initial release

Trademarks​

PSOC™, formerly known as PSoC™, is a trademark of Infineon Technologies. Any references to PSoC™ in this document or others shall be deemed to refer to PSOC™.