About this document​

Scope and purpose​

This application note introduces the CAPSENSE™ multi-sense converter (MSC) block of PSOC™ HV mixed signal (MS) family MCUs. This application note also describes how to develop hardware and firmware design for human machine interface (HMI), body, and powertrain applications.

Intended audience​

The intended audience for this document is design engineers, technicians, and developers of electronic systems.

Introduction​

PSOC™ HVMS is a fully integrated programmable embedded system for several automotive HMI, body, and powertrain applications. The system features an Arm® Cortex® M0+ processor with programmable and reconfigurable analog and digital blocks. It is a combination of a microcontroller with a 12-bit SAR ADC, 5th-generation multi-sense converter (MSC) block supporting capacitive sensing (CAPSENSE™), digital peripherals such as PWMs and serial communication interfaces along with a LIN interface with integrated PHY, and a high-voltage subsystem to operate directly off the 12 V car battery.

PSOC™ HVMS is available in a 32-/48-/56-/64-QFN package with wettable flanks. To understand the functionality described and terminology used in this application note, see the Overview section of the architecture reference manual and

AN185951 - PSOC™ 4 and PSOC™ 6 MCU CAPSENSE™ design guide

. See

References

in this application note for more details.

Multi-sense converter overview​

The multi-sense converter (MSC) is supported on all pins in PSOC™ HV MS via MSC CAPSENSE™ block that can be connected to any pin via the analog MUX buses that any GPIO pin can be connected to. The MSC block in the PSOC™ HVMS can be used to scan sense inputs autonomously (without CPU sequencing and intervention) with support for DMA or can operate via CPU firmware-driven switch sequencing via the analog MUX buses that any GPIO pin can be connected to. The CAPSENSE™ function can thus be provided on any pin or group of pins in a system under software control.

The MSC block supports the following;

  • One MSC converter

  • Both self-capacitance (CSD) and mutual-capacitance (CSX) sensing

  • Multi-sense (capacitive, resistive, impedance, and current sensing)

  • Support 5:1 or more signal-to-noise ratio (SNR) and water tolerance

  • Autonomous scanning (scan multiple sensors without CPU involvement)

  • Improved water tolerance (uses both passive and active shields)

  • Improved linearity

  • Higher sensitivity (system level chopping, SINC2 filter, baseline compensation)

  • 14-bit resolution

  • Ratio-metric sensing

  • Capacitance sensing up to 200 pF

  • 70 dB CMRR and SINC2 filter for noise reduction

The CAPSENSE™ blocks provide both self as well as mutual capacitance sensing. Shield drive can be either active (with an opamp) or passive (less power, for shield loads less than 20 pF).

Figure 1

shows the MSC CAPSENSE™ block diagram. The main features include ratio-metric sensing, differential mode of operation without the need of reference voltage, use of capacitor DACs (CDAC) in place of current DACs (IDAC) which improves noise performance.

Figure 1. MSC CAPSENSE™ block diagram


GPIO cell capacitance to charge converter​

In the MSC architecture, the sensor is either interfaced to the AMUX or a new control MUX matrix, which supports autonomous scanning (limited number of pins supported). The GPIO cells are configured as switched-capacitance circuits that convert sensor capacitances into equivalent charge transfer.

Figure 2

shows the GPIO cell structure.

Figure 2. GPIO cell structure


Four non-overlapping, out-of-phase clocks of frequency FSW control the switches (SW1, SW2, SW3, and SW4) as

Figure 3

shows.

Figure 3. Voltage across sensor capacitance


See

AN85951 - PSOC™ 4 and PSOC™ 6 MCU CAPSENSE™ design guide

in for a more detailed MSC overview.

Schematic and layout example​

Figure 3

shows a general schematic of an external circuit (2x CSD buttons, 2x CSX buttons, and 1x touchpad) for the MSC block of the PSOC™ HVMS MCU. See AN234116 - Hardware design guide in

References

for more information of the power block.

Figure 4. General schematic for MSC block

Series resistors on CAPSENSE™ pins​

Every CAPSENSE™ controller pin has some parasitic capacitance (C

P

) associated with it. As

Figure 5

shows, adding an external resistor forms a low-pass RC filter that attenuates the RF noise amplitude coupled to the pin. This resistance also forms a low-pass filter with the parasitic capacitance of the CAPSENSE™ sensor that significantly reduces the RF emissions.

Figure 5. RC filter


Series resistors should be placed close to the device pins so that the radiated noise picked by the traces gets filtered at the input of the device. Thus, it is recommended to place series resistors within 10 mm of the pins.

For CAPSENSE™ designs using copper on PCBs, the recommended series resistance for CAPSENSE™ input lines are 560 Ω. Adding resistance increases the time constant of the switched-capacitor circuit that converts C

P

into an equivalent resistor. If the series resistance value is larger than 560 Ω, the slower time constant of the switching circuit suppresses the emissions and interference but limits the amount of charge that can transfer. This lowers the signal level, which in turn lowers the SNR. Smaller values are better in terms of SNR, but are less effective at blocking RF.

CAPSENSE™ buttons​

Schematic example​

This example (

Figure 6

) is using 2x CSD buttons (round solid) and 2x CSX buttons (fishbone patterns). The feature of each button is:

  • CSD button: Simple design, low cost, 1 button for 1 GPIO

  • CSX button: High sensitivity, high noise tolerance, and allow multiple buttons without ghost effect

B0 and B1 are connected to P4.7 and P4.6 GPIOs. CSB1 is connected to P7.1 (TX) and P4.4 (RX) GPIOs, and CSB2 is connected to P7.0 (TX) and P4.5 (RX) GPIOs.

Note: The MSC block of PSOC™ HVMS can be connected to all GPIO pins via the analog MUX buses.

Figure 6. Schematic example of CAPSENSE™ buttons


Table 1

shows an example of external components.

Table 1. External component example for CAPSENSE™ buttons

Symbol

Overview

Parameter

Value 1

Value 2

Value 3

B0, B1

CSD button

round solid

9 mm

_

CSB1, CSB2

CSX button

fishbone pattern

10 x 10 mm

_

R26, R28, R30, R32, R37, R39

Series resistor

560 Ω

+/- 1%

> 1/10 W

Layout example​

Figure 7

shows an example of CSD and CSX button layout.

Note: PSOC™ HVMS silicon is placed on top side in this example. Red lines mean the bottom side.

Figure 7. Layout example of CSD and CSX buttons


Follow these guidelines for the design of the CAPSENSE™ button circuit on the PSOC™ HV MS:

  • Place the external series resistors near the IC terminal

  • Draw the CAPSENSE™ lines on the bottom side (If possible, also place the PSOC™ HV MS silicon on the bottom side)

  • Create the hatch ground around CAPSENSE™ buttons (See AN85951 for more detailed hatch ground)

  • Divide the ground plane between shape ground and hatch ground using one-point connection (GND or shield pin)

  • To avoid a cross-talk, each CAPSENSE™ line has to follow the 3 W rule states that “to reduce cross talk from adjacent traces, a minimum spacing of two trace widths should be maintained from edge to edge”

  • For CSX buttons, use different GPIO ports for Tx and Rx pins (e.g., TX: port 7, Rx: port 4)

  • Provide a through-hole (via) for the CAPSENSE™ button on the edge of each button

  • Recommend that the final finish is electroless nickel/immersion gold (ENIG)

CMOD capacitors​

Schematic example​

The sigma-delta converter in MSC block uses an external integrating capacitor, called a modulator capacitor CMOD.

Figure 8

shows the CMOD capacitor connection for the PSOC™ HV MS family.

Note: The CMOD value of PSOC™ HV MS supports up to 10 nF and typical is 2.2 nF. Increasing CMOD have the adverse effect of increasing the noise, initialization time, and minimum signal required to detect. MSC method requires two external integration capacitors, CMOD1 and CMOD2. C13 and C14 are typically used. C11 and C12 are optional. See PSOC™ HV MS datasheet for each CMOD pin assignment.

Figure 8. Schematic example of CMOD capacitors


Table 2

shows an example of external components.

Table 2. External component example for CMOD capacitors

Symbol

Overview

Parameter

Value 1

Value 2

Value 3

C13, C14

Typical use CMOD

2.2 nF

C0G

> 10 V

C11, C12

Optional CMOD

Any value

C0G

> 10 V

Layout example​

Figure 9

shows an example of CMOD layout.

Figure 9. Layout example of a CMOD capacitor


Follow these guidelines for the design of the CMOD capacitor circuit on the PSOC™ HV MS:

  • Place the CMOD capacitors near the IC terminal

  • If the CMOD capacitors are placed in a different layer of PCB, provide a through-hole (via) near the IC terminal

  • Provide a ground through-hole near this capacitor to minimize the current loop

  • Place the GND layer under the CMOD capacitors

CAPSENSE™ touchpad​

Schematic example​

This example (

Figure 10

) is using a 9 × 8 touchpad (also known as trackpad). The touchpad has two linear sliders arranged in an X and Y pattern, enabling it to locate a finger’s position in both X and Y dimensions. The touchpads can be sensed using either CSD or CSX sensing method.

  • CSD-based touchpads suffer from ghost touches, so it supports only single-point touch applications.

  • CSX touchpads can support multi-point touch applications, but these may need more scanning time compared to the CSD touchpad because this method scans each intersection rather than rows and columns.

Figure 10. Schematic example of CAPSENSE™ touchpad


Table 3

shows an example of external components.

Table 3. External component example for CAPSENSE™ touch

Symbol

Overview

Parameter

Value 1

Value 2

Value 3

CST1

Touchpad

Typical design

Column 9

Row 8

R12-14, R16-20, R21-25, R27, R29, R31, R33

Series resistor

560 Ω

+/- 1%

> 1/10 W

Layout example​

Figure 11

shows an example of touchpad layout.

Note: PSOC™ HV MS silicon is placed on top side in this example. Blue color is the top layer and red color is the bottom layer.

Figure 11. Layout example of touchpad


Follow these guidelines for the design of the touchpad circuit on the PSOC™ HV MS:

  • Place the external series resistors near the IC terminal

  • Draw the touchpad lines on the bottom side (If possible, also place the PSOC™ HV MS silicon on the bottom side)

  • Create the hatch ground around the touchpad (See AN85951 for more detailed hatch ground)

  • Divide the ground plane between shape ground and hatch ground using one-point connection (GND or shield pin)

  • To avoid a cross-talk, each trackpad line has to follow 3 W rule states

  • If possible, enter a ground guard into each trackpad line

  • Connect the lines to the edge of the touchpad shape using the through-hole

  • Recommend of final finish is electroless nickel/immersion gold (ENIG)

AutoPDL firmware configuration​

Infineon provides an evaluation license of the Automotive Peripheral Driver Library (AutoPDL) including startup code as sample firmware. The AutoPDL provides the low-level drivers for all PSOC™ HV peripherals with ISO 26262 compliant. The following features of AutoPDL are available.

  • Drivers and middleware

    • Low-level drivers for all peripherals

    • Middleware for complex peripherals such as CAPSENSE™

  • Quality ASPICE Level 2

    • MISRA 2012 AMD1, CERT C “Rules” (L1, L2, L3) are applied, Deviations/Warnings documented.

    • Traceability

  • Safety ASIL-B

    • Safety documentation reduces customers’ effort for safety qualification.

    • Safety features based on SEooC.

  • Compiler version

    • IAR Embedded Workbench for Arm®, Functional Safety, version 8.50

Note: CAPSENSE™ firmware configuration is created based on AutoPDL version 1.3.1.


CAPSENSE™ middleware​

The middleware is a set of firmware drivers that provide APIs for accessing the hardware. These APIs perform the initialization and control activities of each peripheral.

Table 4

lists and describes the interface to each CAPSENSE™ function. The peripheral drivers of CAPSENSE™ are located in the AutoPDL path of:

<user path>\source\middlewares\capsense\src

Note: The CAPSENSE™ has many registers to configure it (provide the hardware drivers as a binary file). Table 4 is simplified to only expose the controls the customer should be using. For more detailed information, see UsersGuide_Capsense _x_x_PSoC4HV_PDL.pdf in <user path>\doc folder.

Table 4. CAPSENSE™ functions

Function

Description

cy_cs_functions.h

Cy_Cs_Init()

Captures MSC HW block for CAPSENSE™ operations and configures it to the default state.

Cy_Cs_DeInit()

Stops the CAPSENSE™ middleware operation, releases the captured MSC hardware block, and resets all assigned GPIO sensing pins to the HI-Z analog driving mode.

Cy_Cs_Enable()

Enables the MSC HW block and its interrupt.

Cy_Cs_Disable()

Disables the MSC hardware block, its assigned clock divider, and interrupt.

Cy_Cs_InitAllWidgets()

Calibrates widgets that have Cref = Cfine = 0 values in the configuration, initializes baselines for all widgets, and executes the BIST.

Cy_Cs_CalibrateWidget()

Executes CapDAC auto-calibration for the specified widget.

Cy_Cs_CalibrateAllWidgets()

Executes CapDAC auto-calibration for all widgets.

Cy_Cs_GetWidgetCalAcc()

For the specified widget, calculates the maximum deviation of the sensor scan data from the calibration target in percent.

Cy_Cs_InitWidgetBaselines()

Executes a full scan and initializes baselines for the specified widget.

Cy_Cs_InitAllBaselines()

Executes a full scan and initializes baselines for all the widgets.

Cy_Cs_ScanWidget()

Initiates the scanning of all sensors in the specified widget. All supported by the widget scan types, i.e., CSD, CSX, and Listening will be performed. Scanning is initiated only if no scan is in progress. Scan finishing can be checked by the Cy_Cs_IsBusy() function.

Cy_Cs_BlockingScanWidget()

Initiates the scanning of all sensors in the specified widget and waits until the scan is done. All supported by the widget scan types, i.e., CSD, CSX, and listening will be performed. Scanning is initiated only if no scan is in progress.

Cy_Cs_ScanAllWidgets

Initiates the scanning of all widgets. All supported by each widget scan types, i.e., CSD, CSX, and Listening will be performed. Scanning is initiated only if no scan is in progress. Scan finishing can be checked by the Cy_Cs_IsBusy() function.

Cy_Cs_IsBusy()

This function returns the status of the CAPSENSE™ middleware whether a scan is currently in progress or not.

Cy_Cs_GetScanStatus()

Returns the error code of the latest scan.

Cy_Cs_ProcessWidget()

Performs full data processing of the specified widget.

Cy_Cs_ProcessAllWidgets()

Performs full data processing of all the widgets.

Cy_Cs_GetWidgetTouchStatus

Reports whether the specified widget detected touch on any of its sensors.

Cy_Cs_GetTouchReport()

Returns a pointer to the touch report structure.

Cy_Cs_SetTimeStamp()

This function writes the specified value into the middleware internal timestamp register that is used for gesture detection.

Cy_Cs_IncrementTimeStamp()

Increments the timestamp register by the preconfigured CY_CS_CFG_TIMESTAMP_INTERVAL value.

Cy_Cs_DecodeWidgetGestures()

Performs decoding of all enabled gestures for the specified widget.

Cy_Cs_GetWidgetNoiseLevel()

Returns normalized noise level for the specified widget. The noise level is expressed in percent, 100% corresponds to the noise data equal to the CY_CS_CFG_WDx_NOISE_THRESHOLD configuration parameter.

Cy_Cs_GetMaxNoiseLevel()

Returns the maximum normalized noise level of all widgets. The noise level is expressed in percent.

Cy_Cs_RunSelfTest()

Runs built-in self-tests that are specified by the test enable mask parameter.

Cy_Cs_GetCpValue()

Calculates the self-capacitance (CSD) value for the specified sensor.

Cy_Cs_GetCmValue()

Calculates the mutual capacitance (CSX) value for the specified Tx/Rx sensors crossing.

Cy_Cs_GetBistData()

Returns a pointer to the built-in self-test results structure.

Cy_Cs_SetCallbackTunerSendData()

Registers a user's callback function for data transmission. The registered function will be called by the CAPSENSE™ middleware to initialize a data transmission to the tuning application. This function must be called prior to Cy_Cs_InitTuner() call.

Cy_Cs_SetCallbackTunerRdCmplt()

Registers a user's callback function for checking if the previous report transmission is finished. The registered function will be called by the CAPSENSE™ middleware before sending a new report to the tuning application. If the previous data transmission is not finished, the new reports will be delayed or skipped. This function must be called prior to Cy_Cs_InitTuner() call.

Cy_Cs_InitTuner()

Initializes the tuner.

Cy_Cs_ProcessTunerReport()

Creates and transmits the tuning reports. It should be called after processing all the widgets. This function can be blocked if the previous report transmission is not finished or the report size is bigger than the communication buffer. Otherwise, the report transmission is done in the background.

Cy_Cs_GetContext()

Returns a pointer to the middleware context structure. It can be used to access all available data structures.

AutoPDL code example​

The following items are required to successfully execute the CAPSENSE™ examples.

  • Evaluation kit (CYHVMS-64K-56-001 or KIT_PSOC4-HVMS-64K_LITE)

  • IAR EWARM 8.50.9 (or FS 8.50.10)

  • AutoPDL evaluation lisence or source code

  • PSoCAutomotiveConfigurationTool software GUI tool

AutoPDL comes with three examples for using these different types of widgets (sliders, buttons, and touch pad). The user can either select one of these three CAPSENSE™ configuration files that are already made part of the “ <user path>\examples\capsense\usercfg ” and its corresponding .csproject file.

Note: KIT_PSOC4-HVMS-64K_LITE kit only supports “CSX_buttons.csproject”.


CAPSENSE™ MW demo application​

  1. Before starting the demo application, connect the power supply and any cables to the evaluation kit. See the relevant user guides for more details.

  2. CAPSENSE™ middleware demo application is in the following AutoPDL folder.

    <user path>\examples\capsense

  3. Go to the CAPSENSE™ example folder and copy the following files.

    • main_cm0plus.c

    • project_config.c

    • project_config.h

  4. Navigate to the following path and replace/paste the copied files into the folder as shown in

    Figure 12

    .

    <user path>\examples\Tools\psoc4hvms64k(or 128k)

    Figure 12. Replacing the header and code files


  5. Run the IAR EWARM 8.50.xx tool.

  6. Open the IAR project file of

    psoc4hvms64k (or 128k)_flash_cm0plus_template.eww

    in the

    examples\Tools\psoc4hvms64k(or 128k)

    folder.

  7. Click

    psoc4hvms64k (or 128k)_flash_cm0plus_template.eww

    on the Debug window, right-click, select

    Add > Add Files

    and select the pasted

    project_config.c

    and

    project_config.h

    files from the

    examples\Tools\psoc4hvms64k(or 128k)

    folder.

    Figure 13. Debug window preview


  8. Select

    Project > Rebuild All

    .

  9. The build is completed when the following message is displayed.

    Figure 14. Build complete preview


  10. Download the application (

    Project > Download > Download active application

    ) and push the reset switch on the evaluation board.

  11. For the CYHVMS-64K-56-001 evaluation board, touch the CSB1 or CSB2 buttons to confirm the CAPSENSE™ operation and observe the corresponding LED (D12 or D13) lights up.

    Figure 15. CYHVMS-64K-56-001 Evaluation Board


PSOC™ Automotive configuration tool​

  1. Open

    PSoCAutomotiveConfigurationTool.exe

    (Windows

    Start menu > Infineon Technologies

    ).

  2. Click

    Open Project

    in the upper left toolbar.

    Figure 16. Click Open Project in the toolbar


  3. Select the

    CSX_buttons.csproject

    file from the following path.

    <user path>\examples\capsense\usercfg

  4. Select the

    Widgets Tuning

    tab. One of the following windows appears.

    Figure 17. Widgets Tuning tab


  5. Select the

    Widget Display Settings

    tab that is located on the bottom side of the tool. Ensure that the

    Sensor Type = Mutual

    .

    Figure 18. Widget Display Settings tab


  6. Click

    Connect

    , and then click

    Run

    .

    If the connection is not working, disconnect and reconnect the wall adapter and USB cable.

    Figure 19. Click Connect, and then click Run


  7. Touch the CAPSENSE™ CSB1 or CSB2 buttons.

    You can observe the touching status on the tool.

    Figure 20. Touching status on the tool


  8. Click the white circle to show the waveform of the sensor. Select the

    Data

    drop down menu and unselect

    Scan Data

    . You can observe the CAPSENSE™ waveform in the

    Sensor Monitor

    window.

    Figure 21. Sensor Monitor window


CAPSENSE™ slider and touchpad demo application​

Note: For the KIT_PSOC4-HVMS-64K_LITE kit, the slider and touchpad board are not included in the kit. Skip these steps when you use the kit.

  1. Close and open

    PSoCAutomotiveConfigurationTool.exe

    (windows

    start menu > Infineon Technologies

    ).

  2. Click

    Open Project

    .

  3. Select

    Slider_Btn.csproject

    or

    9x8_touchpad.csproject

    .

  4. Click

    Save Project

    to generate the

    cy_cs_cfg.h

    file in the same folder as the

    xxx.csproject

    path.

    Figure 22. Click Save Project in Widgets Creation tab


  5. Confirm the

    cy_cs_cfg.h

    file with updated Date modified.

    Figure 23. Update Date modified


  6. Connect either extension board (slider or touchpad) to CYHVMS-64K-56-001 evaluation board. Note that KIT_PSOC4-HVMS-64K_LITE is not included in the extension board.

  7. Open IAR project file of

    psoc4hvms64k(or 128k)_flash_cm0plus_template.eww

    .

  8. Select

    Project > Rebuild All

    .

  9. Download the application (

    Project > Download > Download active application

    ) and push the reset switch on the evaluation board.

  10. Touch extension board buttons, slider, or touchpad. The location you are touching is displayed on the PSoCAutomotiveConfigurationTool.

Note: To show the wave form of each data, select the Widget Display Settings tab that is located on the bottom side of the tool. Change the Sensor Type = Self.

Figure 24. Slider extension board (a), Touchpad extension board (b)


CAPSENSE™ performance tuning​

After the sensor layout is complete (see

Schematic and layout example

and PCB layout guidelines of

AN85951

), the next step is to implement the firmware and tune the CAPSENSE™ parameters for the sensor to achieve optimum performance. The CAPSENSE™ sensing method is a combination of hardware and firmware techniques. Therefore, it has several hardware and firmware parameters required for proper operation. These parameters should be tuned to optimum values for reliable touch detection and fast response. Most of the capacitive touch solutions in the market must be manually tuned.

Figure 25

shows a general manual tuning procedure.

Figure 25. Manual tuning process overview


Signal-to-noise ratio (SNR)​

In practice, the raw counts (equivalent digital counts) vary due to inherent noise in the system. CAPSENSE™ noise is the peak-to-peak variation in raw counts in the absence of a touch, as

Figure 26

shows.

A well-tuned CAPSENSE™ system reliably discriminates between the ON and OFF states of the sensors. To achieve good performance, the CAPSENSE™ signal must be significantly larger than the CAPSENSE™ noise. SNR is defined as the ratio of CAPSENSE™ signal to CAPSENSE™ noise is the most important performance parameter of a CAPSENSE™ sensor.

Figure 26. Signal-to-noise ratio (SNR)


In this example, the average level of raw count in the absence of a touch is 5925 counts. When a finger is placed on the sensor, the average raw count increases to 6060 counts, which means the signal is 6060 – 5925 = 135 counts. The minimum value of the raw count in the OFF state is 5912 and the maximum value is 5938 counts. Therefore, the CAPSENSE™ noise is 5938 – 5912 = 26 counts. This results in an SNR of 135 / 26 = 5.2.

The minimum SNR recommended for a CAPSENSE™ sensor is 5. This 5:1 ratio comes from best practice threshold settings, which enable enough margin between signal and noise to provide reliable ON/OFF operation.

Note: Typical application requires a minimum 5:1 SNR, but better to have above 10:1 if EMC and temperature variation issues are expected.


CSD button tuning​

This section explains how to tune the self-capacitance-based button manually for optimum performance with respect to parameters such as reliability, power consumption, response time, and linearity using the CSD-RM sensing technique and PSoCAutomotiveConfigurationTool. Here, capacitive sigma-delta (CSD) represents the self-capacitance sensing technique and RM represents the ratio-metric method.

Note: For the KIT_PSOC4-HVMS-64K_LITE kit, the CSD-RM board is not included in the kit. Skip the CSD button-tuning section when you use the kit.


Measure the parasitic capacitance (CP)​

The capacitance of the sensor in the absence of a touch is called the parasitic capacitance, C

P

. C

P

results from the electric field between the sensor (including the sensor pad, traces, and vias) and other conductors in the system such as the ground planes, traces, and any metal in the product’s chassis or enclosure. The GPIO and internal capacitances of PSOC™ also contribute to the parasitic capacitance. However, these internal capacitances are typically very small when compared to the sensor capacitance.

  1. Connect the

    CSD liner slider

    extension board to the CYHVMS-64K-56-001 evaluation board. Note that KIT_PSOC4-HVMS-64K_LITE is not included in the extension board.

  2. Open

    1x_CSD_button.csproject

    on

    PSoCAutomotiveConfigurationTool.exe

    .

  3. Click

    Save Project

    button to generate

    cy_cs_cfg.h

    file in the same folder as the

    xxx.csproject

    path.

  4. Download the application on IAR EARM.

  5. Estimate the C

    P

    of the sensor electrode using the Cy_Cs_GetCpValue() function in the firmware. The measured capacitance value is in femtofarad (fF).

  6. Add the following code in

    main_cm0plus.c

    and add the breakpoint into code line of Cy_Cs_GetCpValue() function.

    Figure 27. uint32_t CpValue (a), Cy_Cs_GetCpValue(0, 0, &CpValue) (b)


  7. Click Download and Debug button.

    Figure 28. Download and Debug button


  8. Double-click the CpValue, and right-click to show the menu. Select Add to Watch: ‘CpValue’.

    Figure 29. Add to Watch: ‘CpValue’ preview


  9. Click

    Go

    to run the debugging.

    Figure 30. Run debugging


  10. Monitor C

    P

    value in fF.

    Figure 31. Monitor C

    P

    value in fF


Calculate the sense clock frequency​

The sense clock frequency is a measure of how fast the PSOC™ takes to scan a group of CAPSENSE™ sensors (the adjustment of sense clock frequency can be done to reduce EMI in systems).

  1. Calculate the maximum sense clock frequencies using the following equations.

    Fs(maximum) =14×5×RSeriesTotalCpRSeriesTotal⁢  =REXT+Rinternal

    Figure 32. Equations for maximum sense clock frequencies

    where,

    • C P = Sensor parasitic capacitance. This value is obtained from Measure the parasitic capacitance (CP) .

    • R

      SeriesTotal

      = Total series-resistance, including the R

      internal

      resistance of the internal switches, the recommended external series resistance of 560 Ω: R

      EXT

      (connected on PCB trace connecting sensor pad to the device pin), and trace resistance if using highly resistive materials (example ITO or conductive ink).

    • R

      internal

      = Internal resistance, this varies based on scan and shield modes, see

      Table 5

      .

    Table 5. Internal resistance for sensor

    Scan mode

    R

    internal

    CTRLMUX

    525 Ω

    AMUXBUS

    425 Ω

  2. The sense clock divider value, as given by the following equation, is obtained by dividing HFCLK (F

    MOD

    : e.g., 48 MHz) by Maximum sense clock frequency (kHz): F

    SW

    calculated and choosing the nearest ceiling sense clock divider option in the configurator.

    Sense⁢ clock⁢ ⁢divider⁢  =FMODFSW

    Figure 33. Equation for sense clock divider value

    Table 6. Sense clock frequency settings for CYHVMS-64K-56-001 from C

    P

    Development Kit

    C

    P

    of Sensor electrode

    RSeriesTotal (ohm)

    Maximum sense clock frequency (kHz)

    Sense clock divider

    CYHVMS-64K-56-001 (Pin P3.0)

    23140 fF

    23.140 pF

    560 (external) + 525 (internal) + e.g. 200 (trace) = 1285

    1681.52

    28.54

    32 (divisible by 4)

Note: The actual sense clock divider value is chosen such that the divider is divisible by 4, to have all the four scan phases for equal durations.


SNR measurement using PSOC™ Automotive configuration tool​

See Section

Signal-to-noise ratio (SNR)

for more SNR information.

  1. Open PSOC™ Automotive configuration tool GUI tool, select the

    Widgets Display Settings

    tab (bottom side), change/confirm

    Sensor Type = Self

    , click

    S0

    (gray color), select the

    Raw Data

    and

    Baseline

    . You can observe the raw data waveform in Sensor Monitor window.

    Figure 34. Sensor Monitor window


  2. The following values are used in this example:

    • Average level of raw data in the OFF state = 206

    • Minimum value of raw data in the OFF state = 195

    • Maximum value of raw data in the OFF state = 213

    • Average level of raw data when the finger is placed = 580

  3. Calculate the SNR value:

    • Signal data = 580 - 206 = 374

    • OFF noise = 213 – 195 = 18

    • SNR = 374 / 18 = 20.77

  4. In the IAR EARM tool, open the

    cy_cs_cfg.h

    file on IAR EARM, and update the two sense clock divider parameters to the calculated value of the sense clock divider (See

    Table 6

    ).

    • CY_CS_CFG_WD0_SC_SNS_CLK_DIV

    • CY_CS_CFG_WD0_SC_CCOMP_DIV

    Figure 35. Sense clock divider parameteres


  5. Download the application on IAR EARM.

  6. Open PSoCAutomotiveConfigurationTool GUI tool, click run button and confirm the raw data waveform.

    Figure 36. Raw data waveform


    • Average level of raw data in the OFF state = 0

    • Minimum value of raw data in the OFF state = 0

    • Maximum value of raw data in the OFF state = 0

    • Average level of raw data when the finger is placed = 325

    • Signal data = 325 - 0 = 325

    • OFF noise = 0

    • SNR = ∞

Set number of sub-conversions and scan time​

The number of sub-conversions decides the sensitivity of the sensor and sensor scan time. Increasing the number of sub-conversions (N

Sub

) increases the signal and SNR. However, increasing the number of sub-conversions also increases the scan time of the sensor per the following equation.

Figure 37. Number of sub-conversions and scan time

TSCAN=NSUBFSW

where,

  • T SCAN = Sensor scan time

  • N SUB = Number of sub-conversions

  • F SW = Sense clock frequency

  1. Update the number of sub-conversions (CY_CS_CFG_WD0_SC_SUBCONV_COUNT) on IAR EARM. Increase or decrease the number of sub-conversions by (e.g. 5) and load the parameters to the device. The signal level is directly proportional to the number of sub-conversions.

    Figure 38. Update the number of sub-conversions on IAR EARM


    Note: The sense clock divider and the number of sub-conversions should be the same for both the sensors scanned in the same slot. Use the values corresponding to the sensor with the highest CP.

  2. Measure SNR as mentioned in Section

    SNR measurement using PSOC™ Automotive configuration tool

    and tune until the minimum SNR of 10:1 and a raw data count greater than 50 are achieved.

  3. Skip this step if the following conditions are met:

    • Measured SNR from the previous stage is greater than 10:1.

    • Raw data count > 50.

    If your system is very noisy (e.g. counts < 20), set the scaling factor (CY_CS_CFG_WD0_SC_SCAL_FACTOR). It can be used to change the number of counts per 1 pF of signal. The default 100% scaling factor provides a signal of approximately 150 counts per pF. Setting this to 200% will provide 300 counts of signal per pF.

Tune threshold parameters​

CAPSENSE™ threshold parameters govern the sensor status based on the raw count of a sensor.

Table 7

provides a list of CAPSENSE™ threshold parameters. These parameters apply to both CSD and CSX sensing methods. This section defines these parameters with the help of Baseline.

Table 7

also shows the recommended values for the threshold parameters and they are applicable for most of the designs. However, if there is any external noise present in the end system, you must modify these thresholds accordingly to avoid any sensor false trigger.

Table 7. CAPSENSE™ component widget threshold parameters

No.

Parameter name

cy_cs_cfg.h

Recommended value

1

Finger touch detection threshold

CY_CS_CFG_WD0_SC_FINGER_THRESHOLD_HI

80% signal

2

Finger liftoff detection threshold

CY_CS_CFG_WD0_SC_FINGER_THRESHOLD_LO

60% signal

3

Noise threshold

CY_CS_CFG_WD0_NOISE_THRESHOLD

2x noise or 20% signal (highest of both)

4

IIR filter threshold

CY_CS_CFG_WD0_SC_IIR_THRESHOLD

Same as noise threshold

5

Baseline update threshold

CY_CS_CFG_WD0_SC_BASELINE_THRESHOLD

Same as noise threshold

CSX button tuning​

This section explains how to manually tune the mutual-capacitance-based button for optimum performance with respect to parameters such as reliability, power consumption, response time, and linearity using the CSX-RM sensing technique and PSoCAutomotiveConfigurationTool. Here, the crosspoint (CSX) represents the mutual-capacitance between the Tx electrode and Rx electrode and RM represents the ratio-metric method.

Measure the parasitic capacitance (Cp)​

  1. Use on-board CSX buttons to measure the C

    p

    value. Both CYHVMS-64K-56-001 and KIT_PSOC4-HVMS-64K_LITE boards can support the CSX buttons.

  2. Take a back-up of the

    cy_cs_cfg.h

    file of the tuned CSD setting if necessary.

  3. Open

    CSX_buttons.csproject

    on PSoCAutomotiveConfigurationTool.exe.

  4. Click

    Save Project

    button to generate the

    cy_cs_cfg.h

    file in same folder as the

    xxx.csproject

    path.

  5. Download the application on IAR EARM.

  6. Estimate the Cp of the sensor electrode using the Cy_Cs_GetCpValue() function in firmware. The measured capacitance value is in femtofarad (fF).

    See

    Measure the parasitic capacitance (Cp)

    for how to measure the Cp value using the Cy_Cs_GetCpValue() function.

Figure 39. Measure capacitance value


Calculate the Tx clock frequency​

The Tx clock frequency determines the duration of each sub-conversion. The Tx clock signal must completely charge and discharge the sensor parasitic capacitance.

  1. Calculate maximum Tx clock frequencies using the following equation.

    FTX<12×5×RSeriesTxCPTx

    Figure 40. Tx clock frequency

    where,

    • C

      pTx

      = Tx electrode parasitic capacitance. This value is obtained from

      Measure the parasitic capacitance (Cp)

      .

    • R

      SeriesTx

      = Total series-resistance, including the R

      internal

      resistance of the internal switches, the recommended external series resistance of 560 Ω (connected on PCB trace, connecting sensor pad to the device pin), and trace resistance if using highly resistive materials (example ITO or conductive ink).

    • R

      internal

      = Internal resistance, this varies based on scan modes, see

      Table 8

      .

    Table 8. Internal resistance for sensor

    Scan mode

    Rinternal

    CTRLMUX

    950 Ω

    AMUXBUS

    500 Ω

  2. The Tx clock divider value, as given by the following equation, is obtained by dividing HFCLK (F

    MOD

    : e.g., 48 MHz) by Maximum Tx clock frequency (kHz): F

    TX

    calculated and choosing the nearest ceiling Tx clock divider option in the configurator.

    TxClkDiv=FModFTx

    Figure 41. Tx clock divider value

    Table 9. Tx clock frequency settings for CYHVMS-64K-56-001 from Cp

    Development Kit

    Cp of Sensor electrode

    RSeriesTotal (ohm)

    Maximum Tx clock frequency (kHz)

    Tx clock divider

    CYHVMS-64K-56-001 (TX: P7.1, RX: P4.4)

    9968 fF

    9.968 pF

    560 (external) + 950 (internal) + e.g., 200 (trace) = 1710

    5866.72

    8.18

    12 (divisible by 4)

    Note: The actual sense clock divider value is chosen such that the divider is divisible by 4, to have all the four scan phases for equal durations.

SNR measurement using PSOC™ Automotive configuration tool​

  1. Open PSOC™ Automotive configuration tool, select

    Widgets Display Settings

    tab (bottom side), change/confirm

    Sensor Type = Mutual

    , click

    B0 button

    , select the

    Raw Data

    and

    Baseline

    . You can observe the raw data waveform in the Sensor Monitor window.

    Figure 42. Sensor Monitor window preview


  2. The following values are used in this example:

    • Average level of raw data in the OFF state = -2

    • Minimum value of raw data in the OFF state = -4

    • Maximum value of raw data in the OFF state = 1

    • Average level of raw data when the finger is placed = 310

  3. Calculate the SNR value:

    • Signal data = 310 – (-2) = 312

    • OFF noise = 1 – (-4) = 5

    • SNR = 312 / 5 = 62.4

  4. Open the IAR EARM tool, open

    cy_cs_cfg.h

    file on IAR EARM and update the two sense clock divider parameters.

    • CY_CS_CFG_WD0_MC_SNS_CLK_DIV

    • CY_CS_CFG_WD0_MC_CCOMP_DIV

    Figure 43. Update the two sense clock divider parameters in the IAR EARM tool



  5. Download the application on IAR EARM.

  6. Open the PSoCAutomotiveConfigurationTool tool, rerun and confirm the raw data waveform.

    Figure 44. PSoCAutomotiveConfigurationTool tool



    • Average level of raw data in the OFF state = -20

    • Minimum value of raw data in the OFF state = -50

    • Maximum value of raw data in the OFF state = 5

    • Average level of raw data when the finger is placed = 250

    • Signal data = 250 – (-20) = 270

    • OFF noise = 5 – (-50) = 55

    • SNR = 270 / 55 = 4.90

Note: In the case of this example, the SNR of 10:1 condition is not satisfied due to two CSX buttons used. It needs to increase the value of Tx clock divider (e.g. Tx clock divider uses 24 or more, double of 12) to satisfy the condition.


Set number of sub-conversions and scan time​

The number of sub-conversions decides the sensitivity of the sensor and sensor scan time. Increasing the number of sub-conversions (N

Sub

) increases the signal and SNR. However, increasing the number of sub-conversions also increases the scan time of the sensor per the following equation.

TCSX=NSubFTx

Figure 45. Setting number of sub-conversions and scan time

  1. Update the number of sub-conversions (CY_CS_CFG_WD0_MC_SUBCONV_COUNT) on IAR EARM. Increase or decrease the number of sub-conversions by (e.g. 5) and load the parameters to the device. The signal level is directly proportional to the number of sub-conversions.

    Figure 46. Update the number of sub-conversions on IAR EARM



    Note: The Tx clock divider and the number of sub-conversions should be the same for both the sensors scanned in the same slot. Use the values corresponding to the sensor with the highest CP.

  2. Measure SNR as mentioned in Section

    SNR measurement using PSOC™ Automotive configuration tool

    and tune until the minimum SNR of 10:1 and a raw data count greater than 50 are achieved.

  3. Skip this step if the following conditions are met:

    • Measured SNR from the previous stage is greater than 10:1.

    • Raw data count > 50.

    If your system is very noisy (e.g. counts < 20), set Scaling factor (CY_CS_CFG_WDx_MC_SCAL_FACTOR). It can be used to change the number of counts per 1 pF of signal. The default 100% scaling factor provide a signal of approximately 150 counts per pF. Setting this 200% will provide 300 counts of signal per pF.

Tune threshold parameters​

The tuning of threshold parameters is the same value as CSD button tuning. See

Tune threshold parameters

for more details.

Touchpad tuning​

This section explains how to manually tune the mutual-capacitance-based touchpad for optimum performance with respect to parameters such as reliability, power consumption, response time, and linearity using the CSX-RM sensing technique and PSoCAutomotiveConfigurationTool.

Measure the parasitic capacitance (Cp)​

  1. Connect

    Trackpad

    extension board to CYHVMS-64K-56-001 evaluation board. Note that KIT_PSOC4-HVMS-64K_LITE is not included in the extension board.

  2. Take a back-up of the

    cy_cs_cfg.h

    file of tuned CSD or CSX setting if necessary.

  3. Open

    9x8_touchpad.csproject

    on

    PSoCAutomotiveConfigurationTool.exe

    .

  4. Click

    Save Project

    button to generate

    cy_cs_cfg.h

    file in same folder as

    xxx.csproject

    path.

  5. Download the application on IAR EARM.

  6. Estimate the C

    P

    of the sensor electrode using the Cy_Cs_GetCpValue() function in firmware. The measured capacitance value is in femtofarad (fF).

    See

    Measure the parasitic capacitance (CP)

    for how to measure the C

    P

    value using the Cy_Cs_GetCpValue() function.

Figure 47. Estimating the C

P

of the sensor electrode in firmware


Calculate the Tx clock frequency​

The Tx clock frequency is the same equation as CSX button tuning. See

Calculate the Tx clock frequency

for more details.

Table 10. Tx clock frequency settings for CYHVMS-64K-56-001 from C

P

Development Kit

C

P

of Sensor electrode

RSeriesTotal (ohm)

Maximum Tx clock frequency (kHz)

Tx clock divider

CYHVMS-64K-56-001 (TX0: P3.2, RX0: P0.2)

14476 fF

14.476 pF

560 (external) + 950 (internal) + e.g. 200 (trace) = 1710

4039.75

11.88

12 (divisible by 4)

Note: In this example, 8x-TX and 9x-Rx pins are used. Therefore, the Tx clock divider uses 108 (9 × 12).


SNR measurement using PSOC™ Automotive configuration tool​

  1. Open the PSOC™ Automotive configuration tool GUI tool, select

    Widgets Display Settings

    tab (bottom side), change/confirm

    Sensor Type = Mutual

    , change the Display Mode to

    Heat map

    . You can observe the signal data value on each sensor element of the touchpad.

    Figure 48. Change Display Mode to Heat map


  2. Capture and note the highest/lowest noise of the sensor element (peak-to-peak noise), without placing a finger (recommend observing the noise value for 3–5 seconds).

  3. In this example:

    • Minimum value of signal data in the OFF state = –4

    • Maximum value of signal data in the OFF state = 5

    • Maximum peak-to-peak noise = 5 – (–4) = 9

  4. Firmly hold the finger on the touchpad in the least touch intensity (LTI) position (at the intersection of four nodes) as shown in the following figure. See

    AN85951

    for more details on the LTI position.

    Note: Finger movement during the test can artificially increase the noise level. The LTI signal is measured at the farthest point of the trackpad from the sensor pin connection, where the sensors have the worst-case RC-time constant.

    Figure 49. Touchpad preview


  5. Calculate the LTI Signal:

    • LTI Signal = (269 + 266 + 232 + 269) / 4 = 259

  6. Calculate the SNR value using the following equation:

    SNR=LTISignalPk−Pknoise

    Figure 50. SNR value

    • SNR = 259 / 9 = 28.77

  7. Open the IAR EARM tool, open

    cy_cs_cfg.h

    file on IAR EARM, and update two Tx clock divider parameters (See

    Table 10

    ).

    • CY_CS_CFG_WD0_MC_SNS_CLK_DIV

    • CY_CS_CFG_WD0_MC_CCOMP_DIV

    Figure 51. Updating Tx clock divider parameters


  8. Download the application on IAR EARM.

  9. Open PSoCAutomotiveConfigurationTool GUI tool, rerun and confirm the SNR.

    • Minimum value of signal data in the OFF state = -2

    • Maximum value of signal data in the OFF state = 4

    • Maximum peak-to-peak noise = 4 – (-2) = 6

    • LTI Signal = (260 + 258 + 225 + 263)/4 = 251.5

    • SNR = 251.5/6 = 41.91

Summary​

This application note has described details of the CAPSENSE™ (multi-sense converter) block of PSOC™ HV MS MCU. By using the CAPSENSE™ (multi-sense converter) block, human machine interface (HMI), body, and power-train applications can be achieved with higher quality. Infineon provides an evaluation board and a wealth of sample software to help you get started with PSOC™ HV MS family MCUs. To evaluate the evaluation board, contact your sales representative or Infineon Technical Support.

Glossary​

Table 11. Glossary

Terms

Description

3W

3 width

ADC

analog to digital converter

AMD

Advanced Micro Devices, Inc. (company name)

AMUX

analog multiplexer

API

application programming interface

AutoPDL

automotive peripheral driver library

Arm®

Advanced RISC Machine (company name)

ASIL-B

automotive safety integrity level - B

ASPICE

automotive software process improvement and capability determination

BIST

built in self-test

CAPDAC

capacitor digital to analog converter

CAPSENSE™

capacitive sensing

CDAC

capacitor digital to analog converter

CERT

computer emergency response team

CM0+

Arm® Cortex®-M0+ (processor core name)

CLK

clock

CMOD

modulator capacitor

CMRR

common mode rejection ratio

CP

parasitic capacitance

CPU

central processing unit

CSB

CAPSENSE™ button

CST

CAPSENSE™ touchpad

CSD

CAPSENSE™ sigma delta (self-capacitance)

CSX

CAPSENSE™ crosspoint (mutual-capacitance)

CTRL

control

CTRLMUX

control multiplexer

DMA

direct memory access

ENIG

electroless nickel/immersion gold

fF

femtofarad

FW

firmware

GND

ground

GPIO

general purpose I/O

GUI

graphical user interface

HFCLK

high frequency clock

HMI

human machine interface

HV

high-voltage

HW

hardware

I/O

input or output

IAR

IAR Systems (company name)

IAR EARM

IAR Embedded Workbench for Arm® (software name)

IC

integrated circuit

IDAC

current digital to analog converter

ISO

international organization for standardization

ITO

indium tin oxide

LED

light emitting diode

LIN

local interconnect network

LTI

least touch intensity

MUX

multiplexer

MW

middleware

MSC

multi-sense converter

MCU

microcontroller unit

MISRA

motor industry software reliability association

MS

mixed signal

PCB

printed circuit board

PELI

peripheral

pF

picofarad

PHY

physical layer

PSOC™

programmable system on chip

PWM

pulse width modulation

QFN

quad flat non-leaded

RF

radio frequency

RM

ratiometric method

RX

receiver

SAR

successive approximation register

SEooC

safety element out of context

SNR

signal-to-noise ratio

SW

switch

TX

transmitter

References​

The following documents are PSOC™ HV MS family series application notes, datasheets, and reference manuals. Contact

Technical Support

to obtain these documents and a sample driver library.

Application notes

  1. Infineon Technologies –

    AN85951 - PSOC™ 4 and PSOC™ 6 MCU CAPSENSE™ design guide

  2. Infineon Technologies – AN234115 - Getting started with PSOC™ HV MS family

  3. Infineon Technologies – AN234116 - Hardware design guide for PSOC™ HV MS family

  4. Infineon Technologies – AN0003 - High voltage subsystem (HVSS) in PSOC™ HV MS family

  5. Infineon Technologies – AN0006 - Analog system block in PSOC™ HV MS family

Device datasheet

  1. Infineon Technologies – PSOC™ High Voltage (HV) Mixed Signal (MS) Automotive MCU datasheet

Architecture reference manual

  1. Infineon Technologies – PSOC™ high voltage (HV) mixed signal (MS) MCU architecture technical reference manual (TRM)

Registers reference manual

  1. Infineon Technologies – PSOC™ high-voltage (HV) mixed signal (MS): PSOC™ HVMS-64K registers reference manual

  2. Infineon Technologies – PSOC™ high-voltage (HV) mixed signal (MS): PSOC™ HVMS-128K registers reference manual

Evaluation board user guide

  1. Infineon Technologies – CYHVMS-64K-56-001 PSOC™ high-voltage (HV) mixed signal (MS) evaluation kit user guide

Automotive peripheral driver library (AutoPDL)

  1. Infineon Technologies – PSOC™ HV MS AutoPDL

Revision history​

Document revision

Date

Description of changes

V1.0

2024-01-29

Initial release

V1.1

2025-06-26

Template update

Updated PSoC™ to PSOC™

Trademarks​

PSOC™, formerly known as PSoC™, is a trademark of Infineon Technologies. Any references to PSoC™ in this document or others shall be deemed to refer to PSOC™.