About this document​

Scope and purpose​

This application note introduces you to the high-voltage subsystem (HVSS) of PSOC™ 4 HV precision analog (PA) family. This application note also guides you to develop HVSS hardware and firmware design for battery monitoring application.

Intended audience​

This document is intended for hardware and firmware design engineers.

Introduction​

This application note provides an overview of the high-voltage subsystem (HVSS) with the CY8C41xxLCE-HV4xx series from the PSOC™ 4 high voltage (HV) precision analog (PA) family. PSOC™ 4 HV PA is a fully integrated programmable embedded system for battery monitoring and management. The system features an Arm® Cortex® M0+ processor and programmable and reconfigurable analog and digital blocks. To get a better understanding of the HVSS functionality described and terminology used in this application note, it is a good idea to read the "Section 22: High-voltage subsystem" chapter of the

architecture reference manual

.

HVSS overview​

The PSOC™ 4 HV PA high-voltage subsystem (HVSS) contains a series of analog circuits used in battery monitoring and management applications. The applications are directly connected to an automotive battery and operates up to 42 V. The HVSS has the following features:

  • HVSS circuits operate directly off 12 V/24 V automotive battery (tolerates up to 42 V)

  • A linear regulator powered by the automotive battery voltage producing 3.3 V (HVREG)

    • Output voltage accuracy: 2.7 V to 3.6 V

    • Input voltage range: 3.6 V to 42 V

    • Output current capability: 30 mA

    • Low current consumption for always on: 20 µA maximum

    • Power good function

  • A LIN physical interface transceiver (LIN PHY)

    • Data rates up to 20 kbps with high EM noise immunity

    • Positive/negative DC tolerance for LIN pin: –27 V to 42 V

    • Sleep mode current consumption: IVBAT + IVDDD = 10 µA maximum

    • Programmable slew rate control: 1.0/1.5/2.0 V/us at VBAT = 12 V

    • Dominant timeout and LIN wakeup interrupt timers

  • A set of input voltage dividers (VDIVIDER) providing attenuated signals to ADCs

    • Dividers attenuate the input by a factor of 16x or 24x

    • 1.2 V full-scale outputs from an input of 19.2 V (16x) or 28.8 V (24x)

  • An AHB bus interface and control/status registers

  • Interrupt logic

Figure 1

shows the block diagram for the HVSS.

Figure 1. HVSS block diagram


  • HV regulator (HVREG)

The HVREG is the high-voltage regulator with self-startup from the battery without a reference voltage; it provides 3.3 V to VDDD and VDDA as the chip supply. It also contains a power good function and Zener diode on the output pin for overvoltage protection. The HVREG operates with stability against automotive battery voltage transient events, keeping the output voltage between 2.7 V to 3.6 V even if the VBAT pin drops down to 3.6 V in cold cranking or rises up to 42 V in a load dump surge.

  • LIN PHY

The LIN PHY is the interface between the local interconnect network (LIN) protocol controller and the physical bus in a LIN, which meets the requirements of LIN standard 2.2 A and is backward compatible with LIN 2.0. It supports data rates of 1 to 20 kbps. Non-LIN fast slew rates are available providing 100 kbps data rates for fast downloads, for factory and field flash program updates using the LIN pin.

  • HV ADC voltage dividers (VDIVIDER)

The VDIVIDER is a voltage divider used on the VSENSE and VDIAG pins to scale the battery voltage to levels compatible with on-chip ADCs so that battery voltages can be measured. In typical battery monitoring and management applications, the VSENSE input is normally connected directly to the battery with a series 2.2 kΩ resistor to measure battery voltage. VDIAG can be used to measure the voltage at other locations such as the ECU or other loads where monitoring is desired. The external 2.2 kΩ resistors in series with voltage sources limit the current during ESD and transient voltage events.

HVREG​

Block description​

Figure 2

shows the HVREG block architecture and function diagram. The HVREG generates a nominal 3.3 V output voltage with loads up to 30 mA from an external supply voltage input of 3.6 V to 42 V. The regulator maintains the output voltage from 3 V to 3.6 V when the supply voltage is greater than 4 V and may drop to 2.7 V when the supply is between 3.6 V to 4 V. In normal operation, the external automotive battery voltage is typically 12 V or higher but can drop as low as 4.5 V during cold cranking. However, the voltage at the V

BAT

pin can go as low as 3.6 V due to a reverse polarity protection diode and an EMI filter resistor.

This regulator provides 3.3 V

V

DDD

(and 3.3 V

V

DDA

), which are used to power the chip, including the digital regulators which then generate

V

CCD

(1.8 V) supplies. This regulator is always powered on.

Figure 2. HVREG block architecture and function diagram


HVREG input pins​

vddd_in is an analog input signal pin to monitor the

V

DDD

voltage level with the power good circuit (PG). This pin is connected to the output

V

DDD

at the appropriate place in the chip to monitor the drop in

V

DDD

.

HVREG output pins​

vddd is the output pin of this regulator, a nominal 3.3 V regulated voltage with loads up to 30 mA. This output drives the device’s

V

DDD

and

V

DDA

, and through the GPIO can drive external loads. The vddd pin is always ON after startup.

pg_hv

is the output pin of the power good circuit in HVREG. HVREG monitors the

V

DDD

output voltage through the

vddd_in

pin. When

V

DDD

is lower than 2 V,

pg_hv

provides a LOW. Thus, this output signal can work as the reset signal of the entire device in the voltage range lower than Vddd = 2.0 V.

Operating voltage​

Table 1

and

Table 2

show the HVREG absolute maximum ratings and operating conditions. See

PSOC™ 4 HV PA datasheet

for more information.

Table 1. HVREG absolute maximum ratings

Parameter

Description

Min.

Typ.

Max.

Units

Details/conditions

V

BAT

Supply voltage

V

BAT

−0.3

–

42

V

I

BAT

V

BAT

supply current

–

–

160

mA

I

BATABSDC

V

BAT

supply current, long-term average

–

–

40

mA

Table 2. HVREG operating conditions

Parameter

Description

Min

Typ

Max

Units

Details/conditions

V

BAT

Battery supply voltage

V

BAT

3.6

–

28

V

V

DDA

Analog regulator voltage

3

3.3

3.6

V

I

DDA

Analog regulator current

–

N/A

–

–

Not to be used off-chip

V

DDD

Digital regulator voltage,

V

BAT

> 4 V

3

3.3

3.6

V

V

DDD

Digital regulator voltage, 4 V≥

V

BAT

≥3.6 V

2.7

–

3.6

V

I

DD

Digital regulator current

–

–

30

mA

Core, GPIO, and external loads

VDIVIDER​

Block description​

VDIVIDER is used to scale the high-voltage analog inputs down to levels compatible with the ADC full-scale input voltage (1.2 V). These programmable dividers support two voltage scales – 16x (19.2 V full scale) or 24x (28.8 V full scale). Each divider can be independently enabled or disabled. The divider generates a differential signal for the ADC with the bottom of the divider referenced to vdiv_ret.

Figure 3

shows the block diagram of the VDIVIDER.

Figure 3. VDIVIDER block diagram


VDIVIDER input pins​

pg_hv

is the reset signal input pin. While this pin is LOW, the level shift circuit is in reset;

vs_div0/vs_div1

outputs "L" regardless of the

rdiv_en<1:0>

voltage level. The voltage level of this bus signals is

V

DDD

.

rdiv_en<1:0>

is an input bus for enabling the resistor dividers of the vsense and

vdiag

inputs. When either signal is set to "L", the corresponding resistor ladder is opened and its output becomes low. The voltage level of this bus signals is

V

CCD

.

rdiv_scale<1:0>

is an input bus to set the voltage attenuator ratio to either 1/16 or 1/24. The voltage level of this bus is

V

CCD

.

VDIVIDER output pins​

vs_div0/vs_div1

are output pins of the divided

vsense/vdiag

signals. The voltage level of this bus is

V

DDD

.

Operating voltage​

Table 3

and

Table 4

show the VDIVIDER absolute maximum ratings and operating conditions. See

PSOC™ 4 HV PA datasheet

for more information.

Table 3. VDIVIDER absolute maximum ratings

Parameter

Description

Min.

Typ.

Max.

Units

Details/conditions

V

SHV

V

SENSE

/V

DIAG

ADC sense voltage

−0.3

–

42

V

V

SHV

V

SENSE

/V

DIAG

ADC sense voltage

−40

–

42

V

With external 2.2 kΩ resistor

I

SH

V

SENSE

/V

DIAG

current

−20

–

1

mA

Forced externally

Table 4. VDIVIDER operating conditions

Parameter

Description

Min.

Typ.

Max.

Units

Details/conditions

V

SENSE

V

BAT

sense voltage

3.6

–

28

V

V

DIAG

V

DIAG

sense voltage

3.6

–

28

V

I

SENSE

V

SENSE

/V

DIAG

current

5

20

μA

V

RMEAS

HV measurement range

0

–

28

V

With HVATTEN = 24

V

RMEASLV

LV measurement range

0

–

1.2

V

V

RES

Resolution

–

0.293

–

mV

0 V to 18 V input range (Rdiv=16)

V

RES

Resolution

–

0.4

–

mV

0 V to 28 V input range (Rdiv=24)

LIN PHY​

Block description​

The LIN driver includes slew control to maintain a consistent duty cycle over a range of loads. It also includes turn-on/turn-off control to round the edges and minimize the EMI. Large amounts of RF energy can be present on the LIN bus; the driver must remain functional in the presence of this energy, which requires special attention to the design of the feedback circuits so they do not saturate in the presence of RF energy.

LIN receiver thresholds are specified in relation to the supply voltage, VBAT. A comparator with voltage dividers sets the receiver threshold and scales the bus voltages to appropriate levels. Noise filtering is needed to prevent the RF energy and brief transients from disturbing the communication.

The LIN specification has certain isolation requirements to ensure that the LIN bus is not compromised by certain faults, and that the loss of supply voltage or the ground of a slave node does not affect the LIN communication between other nodes. To address this requirement, the following are introduced:

  • Reverse protection diodes in series with pull-up resistors

  • A diode in series with the open-drain pull-down resistor to prevent powering the components from the LIN bus and/or excessively loading the LIN bus and disrupting the communication

Figure 4

shows the LIN PHY transceiver block diagram.

Figure 4. LIN PHY block diagram


LIN PHY input pins​

Pin

Description

lin_mode<2:0>

Input to change the LIN PHY function mode

txd

Data input signal, giving the drive state intended at the LIN pin in LIN PHY transmit mode

txd_en

Input signal to mask the

txd

signal. When

txd_en

is "L", the transmitter is controlled so that the

txd

input is ignored and the LIN pin becomes "recessive" (weak pull-up).

sl_round

Input configuration signal to tune the falling slew rate of LIN waveform. When the rounding mode is selected, the falling slope of the LIN bus waveform will be more moderate for lower EMI emission.

LIN PHY output pins​

Pin

Description

Lin

Input/output pin for LIN PHY transceiver. The block's transmitter can drive this pin. The receiver uses it as an input. This pin requires a positive/negative tolerance from −27 V to 42 V (to account for a "lost ground" mode that can give negative inputs, and battery surge cases for the high positive voltages).

rxd

Output of the LIN PHY receiver. The voltage level of this signal is

V

CCD

and reflects the state of the LIN pin.

Operating conditions​

Table 5

and

Table 6

show the LIN PHY absolute maximum ratings and operating conditions. See

PSOC™ 4 HV PA datasheet

for more information.

Table 5. LIN PHY absolute maximum ratings

Parameter

Description

Min.

Typ.

Max.

Units

Details/conditions

V

LIN

LIN pin voltage

−27

–

42

V

I

LIN

LIN pin current

–

–

200

mA

t

SCLIN

Short circuit tolerance: LIN

–

–

60

min

V

BAT

= LIN: 3.6 V to 28 V

–

–

500

ms

V

BAT

= LIN: 28 V to 42 V

Table 6. LIN PHY operating conditions

Parameter

Description

Min.

Typ.

Max.

Units

Details/conditions

V

BAT_LIN

V

BAT

range for LIN communications

7

–

28

V

LIN2.2 A parameter 10

V

LIN

LIN output voltage

6

–

28

V

R

LIN,PU

LIN pull-up resistor

20

30

47

kΩ

I

BUS_LIM

LIN output current

40

–

200

mA

Param 12

V

BUSdom

Receiver dominant state

–

–

0.4

V

BAT

Param 17

V

BUSrec

Receiver recessive state

0.6

–

–

V

BAT

Param 18

V

BUScnt

Receiver center voltage

0.475

0.5

0.525

V

BAT

Param 19

V

BUShys

Receiver hysteresis

–

–

0.175

V

BAT

Param 20

V

OH

Bus transmitter recessive

output voltage

V

BAT

-2

–

V

BAT

V

Not a LIN 2.2 A specification

V

OL

Bus transmitter dominant

output voltage

(

V

BAT

=

V

BUS

=7 V)

–

–

1.2

V

RL = 500 Ω (IOL<12 mA)

V

OL

Bus transmitter dominant

output voltage

(

V

BAT

=

V

BUS

=18 V)

–

–

2

V

RL = 500 Ω (IOL<32 mA)

V

SerDiode

Voltage drop at external series

Diodes

0.4

0.7

1

V

Param 21

R

LIN,PU

Internal slave pull-up

Resistor

20

30

47

kΩ

Param 26 (RSLAVE)

R

LIN,PD

Internal pull-down resistor for

Diagnosis

20

30

47

kΩ

Not a LIN 2.2 A specification

LIN physical layer specification overview​

LIN is a low-cost serial communication protocol, which has been standardized by the LIN consortium. The main properties of LIN are:

  • Single master with one or more slaves

  • Speeds up to 20 kbps

  • Single-wire implementation

  • Low cost silicon implementation based on common UART/SCI interface hardware or equivalent software/hardware state machine

The physical interface is a single-wire (not including ground) using a physical layer interface (PHY). The LIN PHY has two states: the recessive state where the LIN bus is pulled up close to the vehicle battery voltage (a reverse protection diode causes a small voltage drop) and a dominant state, which is essentially 0 V.

Figure 5

shows an overview of a LIN network.

Figure 5. LIN overview


Each node on the LIN network uses a LIN PHY (transceiver) to communicate over the network. The LIN physical layer is independent of the higher LIN protocol layers including master and slave operation. There are no differences between master and slave transceivers. Each LIN network can have up to 16 nodes. The PHY has a transmitter section, which includes the open-drain pull-down transistor and gate driver circuitry, a receiver, and a small pull-up resistor.

The master node includes a termination resistor that ranges from 500 to 1000 Ω depending on network speed and bus length (up to 40 m). The LIN PHY specification specifies network loads of 1000 Ω pull-up with 1 nF bus load capacitance, 680 Ω with 6.8 nF, and 500 Ω with 10 nF. All nodes include a nominal 30 kΩ nominal pull-up resistor; this is intended to compensate for increasing node capacitance (typically ~270 pF/node) to maintain approximately the same pull-up resistor to load capacitance (R × C) time constant as nodes are added. Typically used network speeds are either 10 kbps or 20 kbps.

HVSS firmware configuration​

Infineon provides the sample driver library (SDL) including startup code as sample firmware. The SDL provides a simple interface to access various peripherals and is used for system validation, hardware bring-up, benchmarks, feasibility studies, and demos. The SDL integrates device header files, startup code, and peripheral drivers. The SDL contains a set of firmware drivers that provide APIs for accessing device-specific resources and example for each peripheral. See AN230264 - Getting started with PSOC™ 4 HV PA family

[1]

for detailed SDL information.

The SDL should not be used for production purposes because it is not qualified with any automotive standards.

The following sections explain the details of the API and code examples for HVSS.

Peripheral drivers​

Peripheral drivers are a set of firmware drivers that provide APIs for accessing the hardware. These APIs perform initialization and control activities of each peripheral.

Table 7

lists and describes the interface to each HVSS function. The peripheral drivers of HVSS are located in the following SDL path:

C:/<user path>
PSoC_Sample_Driver_Library_x.x.x\psoc4hvXXXk\src\drivers\hvss

See

API details

for more information.

Table 7. HVSS functions

Function

Description

cy_hvss.c

Cy_Hvss_Init

Configures the HVSS module, which includes RDIV (resistor attenuation) and LIN-PHY configuration. This function should be called before using the LIN communication functions.

Cy_Hvss_DeInit

De-initializes both the LIN module and the RDIV

cy_hvss.h

Cy_Hvss_Hvreg_GetStatus

Gets the status of the HVSS regulator

Cy_Hvss_Rvid_EnableVS0

Enables VS0 in resistor attenuator control (RDIV)

Cy_Hvss_Rvid_DisableVS0

Disables VS0 in RDIV

Cy_Hvss_Rvid_EnableVS1

Enables VS1 in RDIV

Cy_Hvss_Rvid_DisableVS1

Disables VS1 in resistor attenuator control (RDIV)

Cy_Hvss_Rvid_SetPowerMode

Sets the power domain mode in RDIV

Cy_Hvss_Rvid_GetPowerMode

Gets the power domain mode of RDIV

Cy_Hvss_Rvid_SetAttenuationVS0

Gets VS0 attenuation of RDIV

Cy_Hvss_Rvid_GetAttenuationVS0

Gets VS0 attenuation of RDIV

Cy_Hvss_Rvid_SetAttenuationVS1

Gets VS1 attenuation of RDIV

Cy_Hvss_Rvid_GetAttenuationVS1

Gets VS1 attenuation of RDIV

Cy_Hvss_LinPhy_SetRxdPin

Sets the status of the LIN-PHY RxD pin

Cy_Hvss_LinPhy_GetRxdPin

Gets the status of the LIN-PHY; this will give the current status of the LIN RxD pin

Cy_Hvss_LinPhy_EnableWakeupTimer

Enables the LIN-PHY wake-up timer; required LIN compatibility in DS mode.

Cy_Hvss_LinPhy_DisableWakeupTimer

Disables the LIN-PHY wake-up timer

Cy_Hvss_LinPhy_GetWakeupTimerStatus

Gets the status of the LIN-PHY wakeup timer; will give the timer count if running

Cy_Hvss_LinPhy_EnableFaultTimer

Enables the LIN-PHY fault timer; required LIN compatibility in DS mode

Cy_Hvss_LinPhy_DisableFaultTimer

Disables the LIN-PHY fault timer

Cy_Hvss_LinPhy_GetFaultTimerStatus

Gets the status of the LIN-PHY fault timer; will give the timer count if running.

Cy_Hvss_LinPhy_SetPhyMode

Sets the LIN-PHY mode

Cy_Hvss_LinPhy_GetPhyMode

Gets the current LIN-PHY mode

Cy_Hvss_LinPhy_SetPhySlRound

Sets the SL round value of the LIN-PHY for lower EMI

Cy_Hvss_LinPhy_GetPhySlRound

Gets the SL round mode of the LIN-PHY

Cy_Hvss_LinPhy_SetPhyInterface

Sets the internal or GPIO connection of the LIN-PHY through the HSIOM

Cy_Hvss_LinPhy_GetPhyInterface

Gets the connection interface of the LIN-PHY through internal or GPIO

Cy_Hvss_LinPhy_EnablePhy

Enables the LIN-PHY

Cy_Hvss_LinPhy_DisablePhy

Disables the LIN-PHY

Cy_Hvss_LinPhy_GetPhyStatus

Gets the LIN-PHY status:

1- enabled

0 - reset (RxD pin is High-Z)

Cy_Hvss_LinPhy_ClearInterrupt

Clears the interrupt from the

LIN_INTR

register

Cy_Hvss_LinPhy_SetInterrupt

Sets the interrupt in the

LIN_INTR

register

Cy_Hvss_LinPhy_GetInterruptMask

Returns the interrupt mask from the

LIN_INTR_MASK

register

Cy_Hvss_LinPhy_SetInterruptMask

Sets the interrupt mask in the

LIN_INTR_MASK

register

Cy_Hvss_LinPhy_GetInterruptStatusMasked

Returns the masked status from the

LIN_INTR_MASKED

register

Cy_Hvss_LinPhy_SetWakeupInterruptMask

Sets the wakeup interrupt status masked the in

LIN_INTR_MASK

register

Cy_Hvss_LinPhy_ClearWakeupInterruptMask

Clears the wakeup interrupt status masked in the

LIN_INTR_MASK

register

Cy_Hvss_LinPhy_SetFaultInterruptMask

Sets the fault interrupt status masked in the

LIN_INTR_MASK

register

Cy_Hvss_LinPhy_ClearFaultInterruptMask

Clears the fault interrupt status masked in the

LIN_INTR_MASK

register

Startup/initialization sequence​

Figure 6

shows the flowchart for HVSS settings.

Figure 6. HVSS startup flowchart


The

Table 8

and

Table 10

steps are recommended when using HVSS:

Table 8. HVSS initialization steps

Step number

Step

Description

Values

1

RDIV enable

Enable the resistor dividers of the vsense and vdiag inputs.

Block: VDIVIDER

Pin name:

rdiv_en<1:0>

Function:

Cy_Hvss_Rvid_EnableVSx

2

RDIV active enable

Select power modes where RDIV is enabled:

0=Enable in Active and Deep-Sleep modes

1=Enable in Active mode only

Block: VDIVIDER

Pin name: none

Function:

Cy_Hvss_Rvid_SetPowerMode

3

RDIV scale enable

Set the voltage attenuator ratio to either 1/16 or 1/24:

0=16X attenuation

1=24X attenuation

Block: VDIVIDER

Pin name:

rdiv_scale<1:0>

Function:

Cy_Hvss_Rvid_SetAttenuationVSx

4

LIN mode set

Change the LIN PHY function mode (See

Table 9

)

Block: LIN PHY

Pin name:

lin_mode<2:0>

Function:

Cy_Hvss_LinPhy_SetPhyMode

5

LIN EMI value set

Set the SL round value of the LIN-PHY for lower EMI:

0=Normal

1=More moderate (rounded) for lower EMI

Block: LIN PHY

Pin name:

rdiv_scale<1:0>

Function:

Cy_Hvss_LinPhy_SetPhySlRound

6

LIN PHY interface set

Set the internal or GPIO connection of the LIN-PHY through the HSIOM:

0= Primary interface (connected to the internal LIN controller through HSIOM)

1= Alternate interface (connected to GPIOs through HSIOM)

Block: LIN PHY

Pin name: none

Function:

Cy_Hvss_LinPhy_SetPhyInterface

7

LIN enable

Enable the

LIN-PHY

.

enable function:

Cy_Hvss_LinPhy_EnablePhy

disable function:

Cy_Hvss_LinPhy_DisablePhy

Block: LIN PHY

Pin name:

txd_en

Function:

Cy_Hvss_LinPhy_EnablePhy

or

Cy_Hvss_LinPhy_DisablePhy

8

LIN wakeup timer enable (if applicable)

a. Enable the

LIN-PHY

wake-up timer

b. Set the value of the

LIN-PHY

wake-up timer (Number of

LF_CLK

edges before wakeup interrupt is triggered)

Block: LIN PHY

Pin name: none

Function:

Cy_Hvss_LinPhy_EnableWakeupTimer

9

LIN fault timer enable (if applicable)

a. Enable the

LIN-PHY

fault timer.

b. Set the value of the

LIN-PHY

fault timer (number of

LF_CLK

edges before a fault interrupt is triggered)

Block: LIN PHY

Pin name: none

Function:

Cy_Hvss_LinPhy_EnableFaultTimer

Table 9. LIN PHY function mode

Input

Output (driver)

State No.

LIN transceiver function

LIN_MODE[2:0]

Receiver

Slew control

Slew rate setting

txd = 1

txd = 0

Pull-up

0

Disable

000

Off

No

_

High-Z

High-Z

Off

1

Sleep

001

On (Low power)

No

_

Recessive

Recessive

On

2

Standby

010

On

No

_

Recessive

Recessive

On

3

Diagnosis

011

On

No

_

Recessive

Low (weak)

On/Off

4

Normal mode

100

On

Yes

1.0 V/µs

Recessive

Low (dominant)

On

5

101

On

Yes

1.5 V/µs

Recessive

Low (dominant)

On

6

110

On

Yes

2.0 V/µs

Recessive

Low (dominant)

On

7

Fast mode

111

On

No

_

Recessive

Low (dominant)

On

Table 10. HVSS deinitialization steps

Step

Description

1

RDIV control register to default

Set all bits of register to 0 "RDIV enable", "RDIV active enable" and "RDIV scale enable"

2

LIN PHY control register to default

Set all bits of register to 0 "LIN enable", "LIN PHY interface", "SL round" and "LIN mode"

3

LIN PHY timers to default

Set all bits of register to 0 "Wakeup timer" and "Fault timer"

4

LIN interrupt request register to default

Set all bits of register to 0 "Wakeup interrupt" and "Fault interrupt"

5

LIN interrupt set register to default

Set all bits of register to 0 "Wakeup interrupt" and "Fault interrupt"

6

LIN interrupt mask register to default

Set all bits of register to 0 "Wakeup interrupt" and "Fault interrupt"

Selecting the external components​

HVREG​

Schematic example​

Figure 7

shows an example HVREG schematic;

Table 11

shows an example of external components.

Figure 7. HVREG schematic example


Table 11. HVREG external component example

Symbol

Overview

Parameter

Value 1

Value 2

Remark

C4

Decoupling/smoothing capacitor for the high-voltage domain

2.2 μF X7R

> 50 V

C5

Decoupling capacitor for the high-voltage domain

0.1 μF X7R

> 50 V

C6

Capacitor for the external noise filter

47 pF C0G

> 50 V

C11

Decoupling capacitor for the VDDA domain

0.15 μF X7R

> 6.3 V

C12

Decoupling capacitor for the VDDD domain

0.15 μF X7R

> 6.3 V

C13

Decoupling/smoothing capacitor for the VDDD domain

3.3 μF X7R

> 6.3 V

C18

Decoupling capacitor for the VCCD domain

0.15 μF X7R

> 6.3 V

C21

Reference capacitor for the VREF domain

0.47 μF X7R

> 6.3 V

R2

Input filter resistor for the high-voltage domain

Typ 15 Ω

(7.5~15 Ω)

> 0.25 W

Layout example​

Figure 8

shows an example of the HVREG layout.

Figure 8. HVREG layout example


Follow these guidelines for the PCB power supply circuit on the PSOC™ 4 HV PA device:

  • Place the V BAT input capacitors C4, C5, and C6 as close as possible to the VBATpin. Place C6 closer to the VBAT pin, followed by C5 and C4. Place the R2 resistor for the input filter next to C4 and draw the layout as linear as possible. If the board has a GND plane, provide a through hole (via) near this capacitor

  • Place the VDDA capacitor (C11) as close as possible to the VDDA pin and the VSSA pin to minimize the current loop from VDDA to VSSA. If the board has a GND plane, provide a through hole near the VSSA pin of this capacitor.

  • Place the VDDD capacitors (C12 and C13) as close as possible to the VDDD pin to minimize the current loop from VDDD to VSSD. Place C12 closest to VDDD, followed by C13. If the board has a GND plane, provide a through hole connecting to the GND plane, near this capacitor.

  • Place the VCCD capacitor (C18) as close as possible to the VCCD pin to minimize the current loop from VCCD to VSSD. If the board has a GND plane, provide a through hole connecting to the GND plane, near this capacitor.

  • Place the reference voltage capacitor (C21) as close as possible to the VREFH and VREFL terminals. It is recommended to place the VREFH and VREFL traces diagonally, so that they have the same length. Place this capacitor on the same PCB layer as the device and avoid using through holes.

    • Provide a through hole for GND plane connection near each GND pin (VSSD, VSSA, VSSL).

    • When using LIN, place the LIN capacitor near the LIN and VSSL pins.

  • Provide a GND plane on the mounting surface of this IC. To effectively dissipate the heat from the QFN-32 package, it is recommended to provide a thermal via in the footprint of the thermal pad

See

AN230370

for schematic and layout examples of each sensor input (current/voltage/temperature).

VDIVIDER​

Schematic example​

Figure 9

shows an example of the VDIVIDER schematic;

Table 12

shows an example of external components.

Figure 9. Schematic example of voltage sensor line


Table 12. VDIVIDER external component example

Symbol

Overview

Parameter

Value 1

Value 2

Remark

R5, R7

Resistor for the external noise filter

2.2 kΩ

> 1/10 W

D3, D4

Transient voltage suppressor (TVS)

Bidirectional

Clamping voltage 44 V

Optional

C9, C19

Capacitor for the external noise filter

3.3 nF X7R

> 50 V

C10, C20

Capacitor for the external noise filter

47 pF C0G

> 50 V

Note: Resistor values for the voltage path (R5/R7): Note that any deviation from the nominal 2.2 kΩ is associated with a reduction in accuracy.


Layout example​

Figure 10

shows an example of the LIN layout.

Figure 10. VDIVIDER layout example


Follow these guidelines for the design of the voltage sensor line circuit on the PSOC™ 4 HV PA device:

  • Keep the wiring lengths of VSENSE and VDIAG as equal as possible

  • Wire the VSENSE and VDIAG sensor lines from each VBAT point

  • Keep the wiring width in the range of 0.127 mm to the IC terminal width

  • Guard the entire pattern by GND

  • Place the GND layer under the sensor line

LIN PHY​

Schematic example​

Figure 11

shows an example of LIN schematic;

Table 13

shows an example of external components.

Figure 11. LIN schematic example


Table 13. LIN external components

Symbol

Overview

Parameter

Value 1

Value 2

Remark

C25

Decoupling capacitor for the LIN domain

220 pF C0G

> 50 V

R16

Input filter resistance for the high-voltage domain

50 mΩ

> 1/3 W

D7

Transient voltage suppressor (TVS) diode

Bidirectional

Clamping voltage 44 V

Layout example​

Figure 12

shows an example of the LIN layout.

Figure 12. LIN layout example


Follow these guidelines for the PCB HVSS circuit:

  • Place capacitor (C25) near the LIN and VSSL terminals

  • Place the TVS diode (D7) for ESD protection near the LIN connector

  • Connect the LIN wiring as straight as possible

  • Change the optional filter element (R16) per your application

  • Place GND vias near the C25 and D7 terminals

  • Do not connect VSSL to the EP pad

  • Place a guard under the LIN wiring with a GND layer

  • Place a guard around LIN with GND

ESD protection​

Electro-static discharge (ESD) events generate high voltages and high currents depending on the path the charge takes to go to ground. If not properly bypassed, the voltages cause immediate oxide dielectric breakdown, especially in advanced geometry technologies with thin gate oxides, creating a weak spot in the oxide which allows the current flow and localized heating.

Depending on the current flow, this could cause permanent damage. A high current flow can cause overheating and melt the silicon, which results in creating a permanent short or high-leakage sites. High currents can also cause junction or metal failure. In summary, ESD failures can be caused by oxide breakdown, junction burnout, or metallization failure.

The following sections describe the ESD protection mechanism for each HVSS block.

HVREG protection​

Figure 13

shows the detailed block diagram for HVREG ESD protection. HVREG includes the cascode ESD transistors and two pads for the VBAT pin. The cascode ESD transistors are used to bypass the charge to the ground. Two pads for the VBAT pin reduce the impact by oxide breakdown, junction burnout, or metallization failure due to excess current.

Figure 13. HVREG ESD protection


VDIVIDER protection​

Figure 14

shows the detailed block diagram for VDIVIDER ESD protection.

VDIVIDER includes the cascode ESD transistors for

V

SENSE

and

V

DIAG

pins, which are used to bypass the charge to ground. The external 2.2 kΩ resistors in series with the voltage sources limit the current during ESD and transient voltage events.

Figure 14. VDIVIDER ESD protection


LIN PHY protection​

Figure 15

shows the detailed block diagram for LIN PHY ESD protection.

LIN PHY includes an HVPMOS diode, cascode ESD transistors, and two pads for the LIN and VSSL pins. The cascode ESD transistors are used to bypass the charge to VSSL. The two pads for the LIN and VSSL pins reduce the impact by oxide breakdown, junction burnout, or metallization failure due to excess current.

Figure 15. LIN PHY ESD protection


ESD events in an uncontrolled environment​

Despite the protection element inside the silicon, ESD events in an uncontrolled environment (end-user, retail customer, etc.) can be much more damaging. System design must take ESD protection on the PCB into account to prevent ESD events in the uncontrolled environment. This is usually done through techniques such as ESD protection devices (external devices), PCB layout techniques that attempt to control ESD, and appropriate grounding and shielding techniques.

PSOC™ 4 HV PA requires sufficient protection to withstand high voltage ESD on specific pins. ESD on LIN,

V

BAT

,

V

SENSE

, and

V

DIAG

pins is rated at ±8 kV, and is required to be protected by external devices as shown in

Figure 16

.

Figure 16. External device ESD protection


API details​

This chapter describes the APIs in shown

Table 7

. See the

SDL_psoc4hvpaXXXk.chm

file in the

SDL

path below for more information of all PSOC™ 4 HV PA APIs:

C:/<user path>\ PSoC_Sample_Driver_Library_x.x.x\docs

Cy_Hvss_Init()

cy_en_hvss_status_t Cy_Hvss_Init(cy_stc_hvss_config_t *config)

Description:

This function configures the HVSS module, which includes RDIV (resistor attenuation) and LIN-PHY configuration. This function should be called before using LIN communication functions.

Parameters:

config \ref cy_stc_hvss_config_t

Returns:

CY_HVSS_SUCCESS

– HVSS configuration completed successfully

CY_HVSS_BAD_PARAM

– One or more invalid parameters

CY_HVSS_ERROR

– Error occurred while configuring

Cy_Hvss_DeInit()

cy_en_hvss_status_t Cy_Hvss_DeInit(void)

Description:

This function deinitializes both the LIN module and the RDIV.

Parameters:

None.

Returns:

CY_HVSS_SUCCESS

– HVSS configuration completed successfully

CY_HVSS_BAD_PARAM

– One or more invalid parameters

CY_HVSS_ERROR

– Error occurred while configuring

Cy_Hvss_Hvreg_GetStatus()

__STATIC_INLINE uint8_t Cy_Hvss_Hvreg_GetStatus(void)

Description:

This function gets the status of the HVSS regulator.

Parameters:

None.

Returns:

PWR_GOOD

– Status bit.

Cy_Hvss_Rvid_EnableVS0()

__STATIC_INLINE void Cy_Hvss_Rvid_EnableVS0(void)

Description:

This function enables VS0 in RDIV.

Parameters:

None.

Returns:

None.

Cy_Hvss_Rvid_DisableVS0()

__STATIC_INLINE void Cy_Hvss_Rvid_DisableVS0(void)

Description:

This function disables VS0 in resistor attenuator control (RDIV).

Parameters:

None.

Returns:

None.

Cy_Hvss_Rvid_EnableVS1()

__STATIC_INLINE void Cy_Hvss_Rvid_EnableVS1(void)

Description:

This function enables VS1 in resistor attenuator control (RDIV).

Parameters:

None.

Returns:

None.

Cy_Hvss_Rvid_DisableVS1()

__STATIC_INLINE void Cy_Hvss_Rvid_DisableVS1(void)

Description:

This function disables VS1 in resistor attenuator control (RDIV).

Parameters:

None.

Returns:

None.

Cy_Hvss_Rvid_SetPowerMode ()

__STATIC_INLINE void Cy_Hvss_Rvid_SetPowerMode(cy_en_hvss_rdiv_power_mode_type_t mode)

Description:

This function sets the power domain mode in resistor attenuator control (RDIV).

Parameters:

mode \ref cy_en_hvss_rdiv_power_mode_type_t

  • CY_HVSS_RDIV_MODE_ACTIVE_DEEPSLEEP              = 0
  • CY_HVSS_RDIV_MODE_ACTIVE_ONLY             = 1

Returns:

None.

Cy_Hvss_Rvid_GetPowerMode

__STATIC_INLINE cy_en_hvss_rdiv_power_mode_type_t Cy_Hvss_Rvid_GetPowerMode(void)

Description:

This function gets then power domain mode of resistor attenuator control (RDIV).

Parameters:

None.

Returns:

\ref cy_en_hvss_rdiv_power_mode_type_t

  • CY_HVSS_RDIV_MODE_ACTIVE_DEEPSLEEP              = 0
  • CY_HVSS_RDIV_MODE_ACTIVE_ONLY             = 1

Cy_Hvss_Rvid_SetAttenuationVS0

__STATIC_INLINE void Cy_Hvss_Rvid_SetAttenuationVS0(cy_en_hvss_rdiv_attenuation_type_t attenuation)

Description:

This function gets the VS0 attenuation of resistor attenuator control (RDIV).

Parameters:

mode \ref cy_en_hvss_rdiv_attenuation_type_t

  • CY_HVSS_RDIV_ATTENUATION_16X               = 0
  • CY_HVSS_RDIV_ATTENUATION_24X               = 1

Returns:

None.

Cy_Hvss_Rvid_GetAttenuationVS0

__STATIC_INLINE cy_en_hvss_rdiv_attenuation_type_t Cy_Hvss_Rvid_GetAttenuationVS0(void)

Description:

This function gets the VS0 attenuation of resistor attenuator control (RDIV).

Parameters:

None.

Returns:

\ref cy_en_hvss_rdiv_attenuation_type_t

  • CY_HVSS_RDIV_ATTENUATION_16X               = 0
  • CY_HVSS_RDIV_ATTENUATION_24X               = 1

Cy_Hvss_Rvid_SetAttenuationVS1

__STATIC_INLINE void Cy_Hvss_Rvid_SetAttenuationVS1(cy_en_hvss_rdiv_attenuation_type_t attenuation)

Description:

This function gets the VS1 attenuation of resistor attenuator control (RDIV).

Parameters:

mode \ref cy_en_hvss_rdiv_attenuation_type_t

  • CY_HVSS_RDIV_ATTENUATION_16X               = 0
  • CY_HVSS_RDIV_ATTENUATION_24X               = 1

Returns:

None.

Cy_Hvss_Rvid_GetAttenuationVS1

__STATIC_INLINE cy_en_hvss_rdiv_attenuation_type_t Cy_Hvss_Rvid_GetAttenuationVS1(void)

Description:

This function gets the VS1 attenuation of resistor attenuator control (RDIV).

Parameters:

None.

Returns:

\ref cy_en_hvss_rdiv_attenuation_type_t

  • CY_HVSS_RDIV_ATTENUATION_16X               = 0
  • CY_HVSS_RDIV_ATTENUATION_24X               = 1

Cy_Hvss_LinPhy_SetRxdPin

__STATIC_INLINE void Cy_Hvss_LinPhy_SetRxdPin(uint8_t status)

Description:

This function sets the status of the LIN-PHY RxD pin.

Parameters:

status lin

– RxD pin status (HIGH or LOW).

Returns:

None.

Cy_Hvss_LinPhy_GetRxdPin

__STATIC_INLINE uint8_t Cy_Hvss_LinPhy_GetRxdPin(void)

Description:

This function gets the status of the LIN-PHY, which indicates the current status of the LIN RxD pin.

Parameters:

None.

Returns:

uint8_t

– Status of the LIN-PHY.

Cy_Hvss_LinPhy_EnableWakeupTimer

__STATIC_INLINE void Cy_Hvss_LinPhy_EnableWakeupTimer(void)

Description:

This function enables the LIN-PHY wake-up timer, which is required in DS mode for LIN compatibility.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_DisableWakeupTimer

__STATIC_INLINE void Cy_Hvss_LinPhy_DisableWakeupTimer(void)

Description:

This function disables the LIN-PHY wake-up timer.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_GetWakeupTimerStatus

__STATIC_INLINE uint16_t Cy_Hvss_LinPhy_GetWakeupTimerStatus(void)

Description:

This function gets the status of the LIN-PHY wakeup timer, which indicates the timer count if running.

Parameters:

None.

Returns:

uint16_t

– Status of the LIN-PHY wakeup timer.

Cy_Hvss_LinPhy_EnableFaultTimer

__STATIC_INLINE void Cy_Hvss_LinPhy_EnableFaultTimer(void)

Description:

This function enables the LIN-PHY fault timer, which is required LIN for compatibility in DS mode.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_DisableFaultTimer

__STATIC_INLINE void Cy_Hvss_LinPhy_DisableFaultTimer(void)

Description:

This function disables the LIN-PHY fault timer.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_GetFaultTimerStatus

__STATIC_INLINE uint16_t Cy_Hvss_LinPhy_GetFaultTimerStatus(void)

Description:

This function gets the status of the LIN-PHY fault timer, which provides the timer count if running.

Parameters:

None.

Returns:

uint16_t

– Status of the LIN-PHY fault timer.

Cy_Hvss_LinPhy_SetPhyMode

__STATIC_INLINE void Cy_Hvss_LinPhy_SetPhyMode(cy_en_hvss_lin_phy_mode_type_t mode)

Description:

This function sets the mode of the LIN-PHY.

Parameters:

mode /ref cy_en_hvss_lin_phy_mode_type_t

  • CY_HVSS_LIN_PHY_MODE_DISABLED           = 0
  • CY_HVSS_LIN_PHY_MODE_SLEEP              = 1
  • CY_HVSS_LIN_PHY_MODE_STANDBY            = 2
  • CY_HVSS_LIN_PHY_MODE_DIAGNOSIS          = 3
  • CY_HVSS_LIN_PHY_MODE_NORMAL_1_0        = 4
  • CY_HVSS_LIN_PHY_MODE_NORMAL_1_5        = 5
  • CY_HVSS_LIN_PHY_MODE_NORMAL_2_0        = 6
  • CY_HVSS_LIN_PHY_MODE_FAST               = 7

Returns:

None

Cy_Hvss_LinPhy_GetPhyMode

__STATIC_INLINE cy_en_hvss_lin_phy_mode_type_t Cy_Hvss_LinPhy_GetPhyMode(void)

Description:

This function gets the current mode of the LIN-PHY.

Parameters:

None.

Returns:

/ref cy_en_hvss_lin_phy_mode_type_t

  • CY_HVSS_LIN_PHY_MODE_DISABLED           = 0
  • CY_HVSS_LIN_PHY_MODE_SLEEP              = 1
  • CY_HVSS_LIN_PHY_MODE_STANDBY            = 2
  • CY_HVSS_LIN_PHY_MODE_DIAGNOSIS          = 3
  • CY_HVSS_LIN_PHY_MODE_NORMAL_1_0        = 4
  • CY_HVSS_LIN_PHY_MODE_NORMAL_1_5        = 5
  • CY_HVSS_LIN_PHY_MODE_NORMAL_2_0        = 6
  • CY_HVSS_LIN_PHY_MODE_FAST               = 7

Cy_Hvss_LinPhy_SetPhySlRound

__STATIC_INLINE void Cy_Hvss_LinPhy_SetPhySlRound(cy_en_hvss_lin_phy_emi_type_t mode)

Description:

This function sets the SL round value of the LIN-PHY for lower EMI.

Parameters:

mode /ref cy_en_hvss_LinPhy_emi_type_t

  • CY_HVSS_LIN_PHY_SL_ROUND_NORMAL             = 0
  • CY_HVSS_LIN_PHY_SL_ROUND_MODERATE              = 1

Returns:

None.

Cy_Hvss_LinPhy_GetPhySlRound

__STATIC_INLINE cy_en_hvss_lin_phy_emi_type_t Cy_Hvss_LinPhy_GetPhySlRound(void)

Description:

This function gets the SL round mode of the LIN-PHY.

Parameters:

None.

Returns:

/ref cy_en_hvss_LinPhy_emi_type_t

  • CY_HVSS_LIN_PHY_SL_ROUND_NORMAL             = 0
  • CY_HVSS_LIN_PHY_SL_ROUND_MODERATE              = 1

Cy_Hvss_LinPhy_SetPhyInterface

__STATIC_INLINE void Cy_Hvss_LinPhy_SetPhyInterface(cy_en_hvss_lin_phy_interface_type_t mode)

Description:

This function sets the internal or GPIO connection of the LIN-PHY through the HSIOM.

Parameters:

/ref cy_en_hvss_LinPhy_interface_type_t

  • CY_HVSS_LIN_PHY_INTERFACE_PRIMARY        = 0
  • CY_HVSS_LIN_PHY_INTERFACE_SECONDARY       = 1

Returns:

None.

Cy_Hvss_LinPhy_GetPhyInterface

__STATIC_INLINE cy_en_hvss_lin_phy_interface_type_t Cy_Hvss_LinPhy_GetPhyInterface(void)

Description:

This function gets the connection interface of the LIN-PHY through internal or GPIO.

Parameters:

None.

Returns:

/ref cy_en_hvss_LinPhy_interface_type_t

  • CY_HVSS_LIN_PHY_INTERFACE_PRIMARY        = 0
  • CY_HVSS_LIN_PHY_INTERFACE_SECONDARY       = 1

Cy_Hvss_LinPhy_EnablePhy

__STATIC_INLINE void Cy_Hvss_LinPhy_EnablePhy(void)

Description:

This function enables the LIN-PHY.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_DisablePhy

__STATIC_INLINE void Cy_Hvss_LinPhy_DisablePhy(void)

Description:

This function disables the LIN-PHY.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_GetPhyStatus

__STATIC_INLINE uint8_t Cy_Hvss_LinPhy_GetPhyStatus(void)

Description:

This function gets the status of the LIN-PHY.

1: Enabled

0: Reset (RxD pin is High-Z)

Parameters:

None.

Returns:

uint8_t

– Status of the LIN-PHY.

Cy_Hvss_LinPhy_ClearInterrupt

__STATIC_INLINE void Cy_Hvss_LinPhy_ClearInterrupt(uint32_t interrupt)

Description:

This function clears the interrupt from the LIN_INTR register.

Parameters:

interrupt – Interrupt mask for the interrupt.

Returns:

None.

Cy_Hvss_LinPhy_SetInterrupt

__STATIC_INLINE void Cy_Hvss_LinPhy_SetInterrupt(uint32_t interrupt)

Description:

This function sets the interrupt in the LIN_INTR register.

Parameters:

interrupt

– Interrupt mask for the interrupt.

Returns:

None.

Cy_Hvss_LinPhy_GetInterruptMask

__STATIC_INLINE uint32_t Cy_Hvss_LinPhy_GetInterruptMask(void)

Description:

This function returns the interrupt mask from the LIN_INTR_MASK register.

Parameters:

None.

Returns:

uint32_t

–Interrupt bit mask.

Cy_Hvss_LinPhy_SetInterruptMask

__STATIC_INLINE void Cy_Hvss_LinPhy_SetInterruptMask(uint32_t interrupt)

Description:

This function sets the interrupt mask in the LIN_INTR_MASK register.

Parameters:

interrupt

– Interrupt mask for the interrupt.

Returns:

None.

Cy_Hvss_LinPhy_GetInterruptStatusMasked

__STATIC_INLINE uint32_t Cy_Hvss_LinPhy_GetInterruptStatusMasked(void)

Description:

This function returns the masked status from the LIN_INTR_MASKED register.

Parameters:

None.

Returns:

Interrupt bit mask(s).

Cy_Hvss_LinPhy_SetWakeupInterruptMask

__STATIC_INLINE void Cy_Hvss_LinPhy_SetWakeupInterruptMask(void)

Description:

This function sets the wakeup interrupt status masked in the LIN_INTR_MASK register.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_ClearWakeupInterruptMask

__STATIC_INLINE void Cy_Hvss_LinPhy_ClearWakeupInterruptMask(void)

Description:

This function clears the wakeup interrupt status masked in the LIN_INTR_MASK register.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_SetFaultInterruptMask

__STATIC_INLINE void Cy_Hvss_LinPhy_SetFaultInterruptMask(void)

Description:

This function sets the fault interrupt status masked in the

LIN_INTR_MASK

register.

Parameters:

None.

Returns:

None.

Cy_Hvss_LinPhy_ClearFaultInterruptMask

__STATIC_INLINE void Cy_Hvss_LinPhy_ClearFaultInterruptMask(void)

Description:

This function clears the fault interrupt status masked in the

LIN_INTR_MASK

register.

Parameters:

None.

Returns:

None.

Summary​

This application note guides you through the details of the high-voltage subsystem of PSOC™ 4 HV PA, enabling you to connect automotive batteries directly and achieve battery monitoring and management applications with a minimal number of external components. Infineon provides evaluation boards and a wealth of sample software to help you get started with the PSOC™ 4 HV PA family. To access the evaluation board, contact your sales representative or reach out to

Infineon Technical Support

.

Glossary​

Table 14. Glossary

Terms

Description

A/D converter

analog to digital converter

ADC

analog to digital converter

AHB

advanced high-performance bus

API

application programming interface

BOD

brown-out detectors

CPU

central processing unit

CPUSS

CPU sub-system

DAP

debug access port

DC

direct current

DMA

direct memory access

DMAC

DMA controller

DW

data wire

ECC

error correction code (safety)

ECU

electronic control unit

EM

electro-magnetic

EMI

electro-magnetic interference

ESD

electro-static discharge

GPIO

general purpose I/O

HSIOM

high-speed I/O matrix

HVREG

high-voltage regulator

HVSS

high-voltage subsystem

I/O

input or output

IOSS

I/O subsystem

IRC

interrupt controller

IRQ

interrupt request

ISR

interrupt service routine

LIN

local interconnect network

MCU

microcontroller unit

MPU

memory protection unit

NMI

non-maskable interrupt

PA

precision analog

PACSS

precision analog channel subsystem

PCB

printed circuit board

PG

power good

PHY

physical interface transceiver

POR

power on reset

PWM

pulse width modulation

RAM

random access memory

RDIV

resistor attenuator control

RF

radio frequency

ROM

read-only memory

SCB

serial communication block

SDL

sample driver library

SPI

serial peripheral interface

SRAM

static RAM

SRSS

system resource sub-system

TCPWM

timer, counter and PWM

TRM

technical reference manual

TVS

transient voltage suppressor

VDIVIDER

voltage divider

WDT

watchdog timer

References​

The following are the PSOC™ 4 HV PA family series application notes, datasheets and technical reference manuals. Contact

Technical Support

to obtain these documents and sample driver library.

Application notes

  1. AN230264 - Getting started with PSOC™ 4 HV PA family

  2. AN230265 - Hardware design guide for PSOC™ 4 HV PA family

  3. AN230370 - Precision analog channel subsystem in PSOC™ 4 HV PA family

Device datasheet

  1. PSOC™ 4 HV precision analog datasheet

Architecture reference manual

  1. PSOC™ 4 HV PA architecture reference manual (RM)

Registers reference manual

  1. PSOC™ 4 HV PA registers reference manual (RM)

Evaluation board user guide

  1. PSOC™ 4 HV PA evaluation board user guide

Sample driver library (SDL)

  1. PSOC™ 4 HV PA sample driver library

Revision history​

Document revision

Date

Description of changes

**

2021-11-22

Initial release

*A

2023-04-19

Template update; no content updated.

*B

2024-11-20

Updated to the latest branding guidelines

Sunset review complete