After running a tool or configurator to change some part of your application, you will need to update the application using the

make ewarm

command with the modus-shell terminal.

Attention:

It's very important to pay attention to the name of your ipcf file(s). The name is always the one you specified when creating the project. However, if you exported from another IDE

without

using the

CY_IDE_PRJNAME

variable, the name will come from the project Makefile, which might be different than the ipcf file name..

The basic command is as follows:

make ewarm CY_IDE_PRJNAME=[existing-cprj-name] TOOLCHAIN=IAR

After running the command, verify the

ipcf

file(s) is(are) updated. When you view the project in IAR Embedded Workbench, you will see the updated file structure.