General LE tab (Option2, Option3)
The
General LE (Option2, Option3)
tab allows general configuration of the Bluetooth® resource:
for Option2

for Option3

The following chapters describe the
General LE tab
tab settings for
Option2
and
Option3
.
Enable GATT database
This parameter enables the GATT database. When not enabled, the
GATT Settings
tab hides and the files
cycfg_gatt_db.h
and
cycfg_gatt_db.c
are not generated.
Maximum remote clients/servers connections
These parameters display the maximum number of clients/servers that a local server can connect to.
Maximum attribute length
This value is the maximum length of an attribute in the design. The valid range is 23 - 512 bytes.
Note:
This parameter is used in BTSTACK 3.0 or earlier.
Attribute MTU size
This value is the Maximum Transmission Unit size (bytes) of an attribute in the design. The valid range is 23 - 517 bytes. This value is used to respond to an Exchange MTU request from the GATT Client.
Note:
This parameter is used in BTSTACK 3.0 or earlier.
RX PDU size
This value is the maximum size allowed for any received L2CAP PDU. The valid range is 65 - 65535 bytes.
Note:
This parameter is used in BTSTACK 3.0 or earlier.
GAP role
See
GAP role.