The

General

tab for

Option4

allows general configuration of the Bluetooth® resource. The tab displays as follows, depending on the mode selected.


../figures/image11.png

The following chapters describe the

General

tab settings for

Option4

.

Complete Bluetooth LE Protocol

The

Complete Bluetooth LE Protocol

mode enables both Bluetooth® Host and Controller. All GAP roles are exposed for configuration.

Maximum number of Bluetooth® LE connections

This parameter displays how many Bluetooth® LE connections (both Central and Peripheral) are allowed. The valid range is 1 - 4.

GAP role

The

GAP role

parameter can take the following values:

  • Peripheral – Defines the device to advertise using connectable advertising packets in order to establish connection. Peripheral devices need a Central device, because the Central device initiates connection. A Peripheral device can broadcast general information about the device through the advertisement data.

  • Central – Defines the device to initiate connection. Peripheral devices need a Central device, because the Central device initiates connection.

  • Broadcaster – Defines the device to send advertising data – similar to the Peripheral role. However, the Broadcaster does not support connection, it sends data but does not receive it.

  • Observer – Defines the device to scan for a Broadcaster and reports the received information to an application. The Observer role does not allow transmission.

Bluetooth LE Controller only (HCI)

HCI

mode enables the use of the device as

Bluetooth LE Controller

. Selecting this mode makes all other tabs unavailable.

../figures/image12.png