Skip to main content

Control parameters

The Control parameters group provides options to enter the required values.

ParameterDescriptionRangeDefault
Number of phasesNumber of converter's interleaving phases1 - 41
Switching freqTarget switching frequency of power switch operation50000 - 1000000Hz300000Hz
Control loop dividerFast control loop frequency divider1 - 51
Time delayTime expressed in fraction of PWM period to account for the inherent delay introduced by digital implementation: from analog sensing to duty cycle update. Such a delay is taken into account in the phase margin determination.0 - 10.02.00Ts
Control loop freqConverter sampling frequency10000 - 1000000Hz300000Hz
Crossover freq*Target crossover frequency2000 - 200000 Hz10000 Hz
Phase margin*Target phase margin10 - 9050
note

*The calculated valid range for the Crossover frequency and maximum valid value for Phase margin depend on the set of entered parameters. They display in the respective parameter tooltip.