Skip to main content

Version changes

This section lists and describes the changes for each version of this tool.

VersionChange DescriptionsNotes
1.0New tool.
1.1Added support for WICED Bluetooth® devices.
2.0Changed the Platform tab to System tab.This affects the file name generated during code generation. Older versions of the Device Configurator generated cycfg_platform.(c/h) files; it now generates cycfg_system.(c/h) files. If you are updating a design from a previous version, manually remove the old cycfg_platform.(c/h) files and update any references you created to use the new file names.
Moved the Analog-Routing Editor to a tab.
Updated the File menu for library settings.
Added Update All Personalities menu item.
Added the ability to enter multiple resource Names using comma-separated list.
2.1Added Open System Explorer menu item.
Added Change Devices menu item and dialog.
Added Undo/Redo operations to the Edit menu.
Added major/minor version number to the title bar.
2.20Added Copy feature to the Notice List.
Added ability to see documentation links without enabling a resource.
Added frequencies to clock diagram.
Added feature to support incremental patch updates.
2.21Added Search feature to Code Preview.
Implemented various performance improvements.
Fixed an issue with multiple font sizes in the GUI.
Fixed the PDL display name when using the MTB flow.
Updated to allow analog routing from the SAR to any analog resource or pin.
3.0Removed Change Devices dialog.
Updated the tool to recognize obsolete devices.
Added path to files in the Code Preview Pane.
Use command line tools instead.
Displays an error in the Notice List instead of blocking the file from being opened.
3.10Fixed the name conflict warning notices when the selected device is changed to not check against non-existent chip locations.
Added a ‘Fix’ to name conflict warnings in the notice list.
Locked down number entry to the English format (decimal place is always a period).
Made various performance improvements.
Added a search filter to the dialog that allows for the selection of multiple signals.
Added additional MPN consistency checking preprocessor macros to cyf_notices.h.
Added a log file that can be accessed from the About box. Debug messages are redirected to it.
Added back the ‘Fix’ to the MPN consistency notice.
Fixed error message displayed when the same *.modus file is opened in multiple instances of the Device-Configurator and mpn checking command line arguments are provided.
4.0Updated back-end to support multi-core applications.
Updated Create Design dialog.
Changed device library file from xml to props.json.
4.10Added Settings menu and items.
Improved parameter view sizing.
4.20Removed the Save As and Change Libraries menu items.
Removed New Design dialog and menu items.
Added a Filter button to the Parameters pane to toggle off and on non-editable parameters.
Deeper grouping is supported in the parameter view.
Added the use of the back-end server, meaning that multiple editors can be open for the same design file at once.
Added support for dynamically displayed resources. Used by some virtual locations to get a better user experience.
Supports multiple "configurator_support" libraries being found by default to be included for a single design (i.e. personalities can be split across PDL and middleware libraries).
5.0Renamed to Infineon Device Configurator.
Added section for stand-alone operation.
5.10Various bug fixes and back-end updates.
Updates for future device support.
5.20Update to the Settings menu; back-end changes.
5.30Added HTML documentation in the tool.
Created How to topics for memory configuration.
Moved subtabs to the top of the Memory tab and renamed Summary to Address View.
Added Delete All regions command to the Memory tab.
5.40Minor GUI updates for tooltips and improved display; minor back-end changes.
5.50Updates to the Memory tab; minor back-end changes.
5.60Added Notes pane and Toggle Word Wrap feature, minor back-end changes.