Skip to main content

Resources tabs

For some device families, the Device Configurator contains several tabs, each of which provides access to specific resources. Different devices have different resources tabs. However, for some device families, there are no separate tabs; resources are shown in a single pane, sometimes under collapsible trees.

When you enable a resource, or select an enabled resource, the Parameters pane displays various configuration options. As described under Icons, some enabled resources may contain errors, warnings, tasks, or infos that indicate some action might be required to resolve the issue. See Notice List for more details.

note

Only the tabs relevant for a selected device are displayed, so some of the tabs may not be included for some devices.

  • Tab features

  • Solutions tab – Options to configure multiple hardware blocks.

  • Peripherals – Options to enable any of the analog (if available), digital, system, and communication hardware capabilities of the chip that are not related to the platform.

  • Analog – For newer devices, options to enable and configure analog resources

  • Pins – Options for all the pin related resources.

  • Clocks tab – Clocks settings for newer devices.

  • Analog-Routing tab – For older devices, this tab shows all the analog resources, whether enabled or not, and how they connect. It also allows you to edit routes.

  • System tab – Options for chip-wide configuration settings such as power management and debug interfaces.

  • Memory tab – Options to allocate memory to various cores.

  • MMIO-Clocks tab – Options for all the MMIO clocks.

  • Peripheral-Clocks tab – Options for all the peripheral clocks.

  • DMA tab – Provides configuration of the DMA channel and transaction descriptors.

Tab features

Sections with diagrams, such as Pins, Analog-Routing, and System, include Zoom and Fit to size commands to resize the diagram as needed. You can also press and hold the [Ctrl] key and use the mouse scroll wheel to zoom in and out.

If you zoom the image larger than the frame area, scroll bars appear to move to different area of the diagram. You can also press and hold the [Alt] key with the mouse button to use the pan tool.

Each of the tabs (except the Analog-Routing tab) also has the following features:

Filter

The Resource column shows all available resources in an expandable tree. The filter box above the list of peripherals allows you to limit the peripherals shown in the tree as well as a Hide disabled resources filter button. There are also Expand and Collapse commands.

Cut, Copy, Paste

Use these commands to move and copy settings from one resource of the same type to another.

  • When you use Cut , the settings will be copied to the clipboard, and the selected resource will be disabled.

  • When you use Copy , the settings will just be copied to the clipboard.

  • When you use Paste , the selected resource will be enabled if needed. The selected resource must support the same Personality name and version as the cut/copied resource.

Name(s)

This displays the current resource name(s). This is an editable field where you can specify optional, alternate names for this resource. This is also used in generated code.

Personality

Each resource has a "Personality" file that contains the information for the given resource.

  • Some peripherals, such as Serial Communication Block (SCB) and Timer, Counter, Pulse Width Modulator (TCPWM), have a pull-down menu to select a specific personality, such as UART, SPI, or I 2 C.

  • Some peripherals have multiple personality versions from which you can select.

  • Some peripherals have a read-only field that only shows the name of this resource’s personality file.

Solutions tab

The Solutions tab displays for supported devices that provide configurations for a multi-resource solution. This tab provides configurable elements that generally consist of multiple hardware blocks. These elements pre-configure many of the low-level details and just present a higher-level interface to configure the solution-level element itself. All hardware that makes up the solution is configured in one Parameters pane, instead of having individual blocks on different panes. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

Peripherals

The Peripherals tab/tree is where you enable various analog, digital, system, and communication peripherals for the device to include in your application. The filter box and the hide disabled button above the list of peripherals allows you to limit the resources shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

Device families with tabs

Device families without tabs

Analog tab

For newer devices, the Analog tab allows you to enable and configure the various analog resources in your application. The filter box and the hide disabled button above the list of resources allows you to limit the items shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

The interactive diagram changes based on the enabled resource you have selected in the tree. You can double-click on certain areas of a diagram to enable/disable a resource.

Pins

The Pins tab/tree is where you enable all the pin related resources. All available pins are shown in an expandable tree, arranged by port number. The filter box and the hide disabled button above the list of pins allows you to limit the pins shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

The interactive pin package diagram shows the different states of the pins; there is a legend on the diagram. You can enable/disable a pin by double-clicking it in the diagram.

Pin states are shown in different colors:

  • Black – No connect
  • White – Disabled
  • Green – Enabled
  • Grey – Power/ground pins
  • Orange – Fixed function pins
  • Red – Error state
  • Semi-transparent – The hardware resource’s enabled state has been locked.

Device families with tabs

Device families without tabs

Clocks tab

For supported devices, the Clocks tab lists all the clocks in a design. All available clocks are shown in an expandable tree. The filter box and the hide disabled button above the list of resources allows you to limit the items shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

The interactive clock diagram shows all the system clocks and how they connect to each other. You can enable/disable a clock by double-clicking it in the diagram. Enabled clocks are green, disabled clocks are white, and clocks in error state are red.

note

The semi-transparent (faded) elements in the diagram indicate that their enabled state is locked.

Analog-Routing tab

For older devices, the** Analog-Routing** tab shows the various analog resources in your application. Enabled resources are green.

The Edit ../figures/image20.png command opens the Analog Route Editor.

Analog Route Editor

The Analog Route Editor allows you to manually edit the routing of analog resources in your application. It also provides the ability to lock-down all or some of the results.

note

The Analog Editor can some times be unresponsive during route recalculation. Please wait for it to finish algorithm execution.

note

If there are configuration errors, complete routing results will not be available; only locked resources. If you open the Analog Editor in this error state, a warning message will display. You can still lock and unlock switches, but you won’t get complete routing results as long as the configuration has errors.

Select a resource

To select an analog resource, click on it. Any enabled (green) element in the tree can be selected. The resource and the associated route(s) become blue. Also, the Edit Route command appears on the toolbar. See Edit Route.

At the same time, the selected analog resource(s) is highlighted in the Nets tree.

You can also select items in the tree to highlight them in the diagram.

Edit Route

With an editable analog resource selected, click the Edit Route command to enable edit mode. If multiple routes are selected, a pull-down menu displays to select the route to edit. You cannot edit multiple routes at the same time.

In edit mode, the net tree shows only the applicable route entries, and you cannot select resources using the tree. However, the lock/unlock check boxes remain enabled for use. The inactive switches change color to indicate they can be selected to use for the route being edited.

Route changes are live with updates applied automatically as you make changes. Selecting a switch adds it to the current route in a locked state and the route tree is updated to reflect the modifications.

If a change results in an error, a message displays. The routes are automatically rolled back to the previous state, so you will lose at most the last invalid change.

The toolbar shows the Finish edit command to return the editor to selection mode.

note

If a route is edited so that it uses switches associated with a location where no personalities are instantiated, you must manually power on the containing block at startup in order for the switches to function. Refer to the PDL API Reference Guide and the Device Technical Reference Manual for more details.

System tab

Depending on the device, the System tab provides access to system-level items, such as power management, debug interfaces, and system clocks (for older devices). All available resources are shown in an expandable tree. The filter box and the hide disabled button above the list of resources allows you to limit the items shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

Newer devices

Newer devices only show system-level resources, such as protection, debug, power, etc.

Older devices

Older devices show various clocks and the clock diagram.

The interactive clock diagram shows all the system clocks and how they connect to each other. You can enable/disable a clock by double-clicking it in the diagram. Enabled clocks are green, disabled clocks are white, and clocks in error state are red.

note

The semi-transparent (faded) elements in the diagram indicate that their enabled state is locked.

Memory tab

The Memory tab becomes visible for supported devices to configure and visualize memory regions for each core in the device. Similar to other tabs, there is a Resource section to enable/disable the Memory, as well as the Protection section for the Memory Protection Controllers (MPC), Memory Protection Units (MPU), and Security Attribution Units (SAU). This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

The main section of this tab contains various subtabs: Memory Regions, Memory Address View, Peripheral Address View, and Read Me

note

The Parameters pane for this tab is similar to other tabs, except this area contains mostly information, as well as a button to launch the QSPI Configurator.

Memory Regions subtab

The Memory Regions subtab displays if the Memory resource has been enabled. It consists of a toolbar, table, and legend. The toolbar allows you to expand and collapse the available memory bars in the table area, as well as Show/Hide Detailed View of the memories, Delete All memory regions, and Autocorrect All Overlaps.

Each memory shows as a usage bar that when expanded displays the details of how it is being used. The bar itself shows the display name of the memory along with its overall size. Hover the cursor over a used section to displays a tooltip that corresponds to the same information provided in the rows under the memory.

The rows show allocated and unallocated ranges of the memory. The final row shows the end offset of the memory along with a summary of used/free space. If the ending offset is outside the allowed range, the text becomes red and displays the maximum allowed offset along with the currently set offset that is in violation of the max. If more size is allocated then is available, that text will be in red as well.

Show/hide detailed view

Click the Hide Detailed View button to toggle it off and on to show/hide detailed address maps. If any of the addresses do not apply (that is, the core that uses that map is not selected), the values will be stricken out.

Add/edit memory allocations

To edit allocations, double-click an allocated row to open Edit Memory Region dialog.

To add an allocation, double-click an unallocated row to open the Add New Memory Region dialog.

Once the dialog is open, enter values:

  1. As needed, type the name of the Region id .

  2. Select a Domain from the pull-down menu.

  3. Enter the Offset and Size .

The Size entry allows for hex or decimal entry. It also accepts specifying units, which will always be converted to bytes. Units are case insensitive and can be entered as follows:

  • bytes or b = byte

  • kb or k = kilobyte (1 KB = 1,024 Bytes)

  • mb or m = megabyte (1 MB = 1024KB = 1,048,576 Bytes)

  • gb or g = gigabyte (1 GB = 1024MB = 1,048,576 KB = 1,073,741,824 Bytes)

  • tb or t = terabyte (1 TB = 1024 GB = 1,048,576 MB = 8,388,608 KB = 1,099,511,627,776 Bytes)

  • pb or p = petabyte (1 PB = 1024 TB = 1,048,576 GB = 1,073,741,824 MB = 1,099,511,627,776 KB = 1,125,899,906,842,624 Bytes)

  • eb or e = exabyte (1 EB = 1024 PB = 1,048,576 TB = 1,073,741,824 GB = 1,099,511,627,776 MB = 1,125,899,906,842,624 KB = 1,152,921,504,606,846,976 Bytes)

  • zb or z = zettabyte (1 ZB = 1024 EB = 1,048,576 PB = 1,073,741,824 TB = 1,099,511,627,776 GB = 1,125,899,906,842,624 MB = 1,152,921,504,606,846,976 KB = 1,180,591,620,717,411,303,424 Bytes)

  • yb or y = yottabyte (1 YB = 1024 ZB = 1,048,576 EB = 1,073,741,824 PB = 1,099,511,627,776 TB = 1,125,899,906,842,624 GB = 1,152,921,504,606,846,976 MB = 1,180,591,620,717,411,303,424 KB = 1,208,925,819,614,629,174,706,176 Bytes)

If there are obvious errors, the dialog will not allow you to click OK. There may also be an error message.

You can also open the dialog using the drop-down button at the beginning of a row or right-clicking on a row. Unallocated regions will start with an Add region option while allocated regions will have the Edit region option. Both options launch the same edit dialog.

If you prefer, use the keyboard shortcuts defined on the menus.

Rearrange memory regions

On the context menu, there are various options to move regions, as well as cut, copy, and paste regions.

When moving a region, there are two options: After existing regions and Specify offset.

When you select Specify offset, this dialog displays to enter the offset.

Use the Legend

The legend shows you the color for each core. You can change the color associated with a used combination of cores. Just click on any of the colors in the legend to open the color picker.

How to find out which region the main goes in from the main ld

Code that doesn't have an explicit section name goes in .text (or .text.function_name when using -ffunction-sections). Search for .text in the linker script or search the .map file for the function name.

How to read the build output and associate it with the regions defined in the tool

For each project in an application, “make build” will display a summary of the output sections:

Memory region             Used Size  Region Size  %age Used
m55_data_INTERNAL: 3796 B 256 KB 1.45%
m55_code_INTERNAL: 12024 B 256 KB 4.59%
user_nvm_C: 0 GB 32 KB 0.00%
m55_nvm: 24900 B 2816 KB 0.86%
m55_trailer: 0 GB 256 KB 0.00%
m55_code_secondary: 0 GB 256 KB 0.00%
m55_data_secondary: 2800 KB 2800 KB 100.00%
m33_m55_shared: 256 KB 256 KB 100.00%

gfx_mem: 0 GB 1808 KB 0.00%

m33_data: 0 GB 256 KB 0.00%

m33s_allocatable_shared: 0 GB 4 KB 0.00%

m33_allocatable_shared: 0 GB 4 KB 0.00%

m55_allocatable_shared: 1088 B 4 KB 26.56%

The “.map” file generated by the linker contains details about which input sections the linker placed into each output section. To find the memory region corresponding to each output section, search for the memory region that contains the section's address.

Example of “.map” file from GNU ld:

.appText_1      0x60580400     0x1f70
...
.text.main 0x6058094c 0x14 build/APP_KIT_PSE84_EVAL/Debug/main.o
0x6058094c main
.text.Cy_PDL_Init
0x60580960 0xc build/APP_KIT_PSE84_EVAL/.../cy_device.o
0x60580960 Cy_PDL_Init
  • .appText_1 is the output section name. It is followed by the output section start address (0x60580400) and the output section total size (0x1f70).

  • .text.main is the input section name. It is followed by its address (0x6058094c) and size (0x14).

Initialized data in volatile memory also consumes space in a non-volatile memory.

.data           0x20000000       0x24 load address 0x60582658

The .data section consumes 0x24 bytes at both its writable address 0x20000000 and its non-volatile address 0x60582658.

How to define a new region for some data buffer variable

For uninitialized data:
  1. In the memory tab, add a new region named “CUSTOM_DATA” in a writable memory such as SRAM.

  2. In the linker script, add a section for the region:

    GNU ld or LLVM lld

    .custom_data :
{
*(.custom_data*)
} >CUSTOM_DATA

armlink

    LOAD_CUSTOM_DATA CYMEM_CM55_0_CUSTOM_DATA_START CYMEM_CM55_0_CUSTOM_DATA_SIZE
{
EXEC_CUSTOM_DATA CYMEM_CM55_0_CUSTOM_DATA_START UNINIT CYMEM_CM55_0_CUSTOM_DATA_SIZE
{
*(.custom_data*)
}
}

ilinkarm

    do not initialize { section .custom_data* }
place in CUSTOM_DATA { section .custom_data* }
  1. In the source code, assign the variable to the section (GCC, armclang, or iccarm)
    __attribute__((section ".custom_data"))
uint32_t data_buffer[DATA_BUFFER_COUNT];
For data in volatile memory

For data in volatile memory that requires run-time initialization, the linker script must configure a non-volatile location to initialize the data. For this example, create a region named “CUSTOM_CODE” in a non-volatile memory.

GNU ld or LLVM lld

.custom_data :
{
*(.custom_data*)
} >CUSTOM_DATA AT>CUSTOM_CODE

.copy.table :
{
/* ... */
LONG(LOADADDR(.custom_data))
LONG(ADDR(.custom_data))
LONG(SIZEOF(.custom_data)/4)
/* ... */
}
note

If ADDR(.custom_data) is read-only, the .copy.table entry must use a writable address.

armlink

LOAD_CUSTOM_CODE CYMEM_CM55_0_CUSTOM_CODE_START CYMEM_CM55_0_CUSTOM_CODE_SIZE
{
EXEC_CUSTOM_DATA CYMEM_CM55_0_CUSTOM_DATA_START CYMEM_CM55_0_CUSTOM_DATA_SIZE
{
*(.custom_data*)
}
}

ilinkarm

initialize by copy { section .custom_data* }
place in CUSTOM_DATA { rw section .custom_data* }
place in CUSTOM_CODE { ro section .custom_data* }

How to define a new region for the code and then assign code to the particular region

  1. In the memory tab, add a new region named “CUSTOM_CODE” in a non-volatile memory such as RRAM.

  2. In the linker script, add a section for the region:

    GNU ld or LLVM lld

    a.	.custom_code :
{
*(.custom_code*)
} >CUSTOM_CODE

armlink

    LOAD_CUSTOM_CODE CYMEM_CM55_0_CUSTOM_CODE_START CYMEM_CM55_0_CUSTOM_CODE_SIZE
{
EXEC_CUSTOM_CODE +0
{
*(.custom_code*)
}
}

ilinkarm

    place in CUSTOM_CODE { section .custom_code* }
  1. In the source code, assign the variable to the section (GCC, armclang, or iccarm)
    __attribute__((section ".custom_code"))
void custom_code_function1(void);

How to assign a function or variable into a custom memory section

Variables and functions may be assigned to a section using the section attribute. The linker script must assign the section to an output section.

__attribute__((section ".custom_data"))
uint32_t data_buffer[DATA_BUFFER_COUNT];

__attribute__((section ".custom_code"))
void custom_code_function1(void);

How to modify the linker to include a specific file into a custom memory section

GNU ld or LLVM lld

.custom_code :
{
main.o(.text* .rodata*)
} >CUSTOM_CODE
.custom_data :
{
main.o(.data*)
main.o(.bss*)
} >CUSTOM_DATA AT>CUSTOM_CODE
note

The toolchain does not automatically initialize data. Sections that require initialization must be added to the .zero.table and/or .copy .table manually.

armlink

LOAD_CUSTOM_CODE CYMEM_CM55_0_CUSTOM_CODE_START CYMEM_CM55_0_CUSTOM_CODE_SIZE
{
EXEC_CUSTOM_CODE +0
{
main.o(+RO)
}
EXEC_CUSTOM_DATA CYMEM_CM55_0_CUSTOM_DATA_START CYMEM_CM55_0_CUSTOM_DATA_SIZE
{
main.o(+RW,+ZI)
}
}

ilinkarm

place in CUSTOM_CODE { ro object main.o }
place in CUSTOM_DATA { rw object main.o }

How to modify the linker to include an entire middleware library into a custom memory section

The linker script example assigns all of the code and data from object files matching mtb_hal_*.o to the .custom_code and .custom_data sections respectively. If the middleware’s object files cannot be described in a single pattern, it may be necessary to use multiple patterns.

GNU ld or LLVM lld

.custom_code :
{
mtb_hal_*.o(.text* .rodata*)
} >CUSTOM_CODE
.custom_data :
{
mtb_hal_*.o(.data*)
mtb_hal_*.o(.bss*)
} >CUSTOM_DATA AT>CUSTOM_CODE
note

The toolchain does not automatically initialize data. Sections that require initialization must be added to the .zero.table and/or .copy .table manually.

armlink

LOAD_CUSTOM_CODE CYMEM_CM55_0_CUSTOM_CODE_START CYMEM_CM55_0_CUSTOM_CODE_SIZE
{
EXEC_CUSTOM_CODE +0
{
mtb_hal_*.o(+RO)
}
EXEC_CUSTOM_DATA CYMEM_CM55_0_CUSTOM_DATA_START CYMEM_CM55_0_CUSTOM_DATA_SIZE
{
mtb_hal_*.o(+RW,+ZI)
}
}

ilinkarm

place in CUSTOM_CODE { ro object mtb_hal_*.o }
place in CUSTOM_DATA { rw object mtb_hal_*.o }

How to re-balance the memory between the cores based on the build output

This is highly dependent on the needs of the customer’s application. Solutions may include:

How to switch between internal and external memory

In the** Memory Regions** tab, use the context menu to move the desired memory region ID to another memory category.

  • If you want to let the tool just place it at the end of the other regions in the destination, select After existing regions .

  • If you want to specify exactly what offset to put it at, then select Specify Offset . Then enter the value in the dialog.

note

The regions required for initial application start up must be in a non-volatile memory.

note

Some toolchains including GNU and LLVM do not initialize data automatically. If a region is moved to a volatile memory, entries must be added to .zero.table and/or .copy.table manually.

Memory Address View subtab

The Memory Address View subtab displays the security status and access permissions enforced by the IDAU, SAU, and MPC at a given address or memory region. The Core pull-down allows you to switch to other cores, and the Search shows all occurrences of an entered term with Forward and Back buttons to jump to the next or previous term. This subtab also contains zoom commands.

  • The Address column shows the start address of every segment shown in the other columns.

  • The Memory Views column depicts all the physical memories and external memory reservations for the device, along with the size and capabilities for each. Possible capabilities include Executable, Writable, Readable, Programmable, Nonvolatile, Secure, and Instruction Cache.

  • The IDAU column shows the security across all address ranges determined by the device's IDAU. Each range lists a security status code and corresponding background color (S/green for Secure, NS/orange for Non-Secure, NSC/yellow for Non-Secure Callable, and X/gray for Exempted) and the address range size.

  • The SAU column depicts the security across all address ranges as configured in the designs SAU entries. Each range lists a security status code and corresponding background color (S/green for Secure, NS/orange for Non-Secure, NSC/yellow for Non-Secure Callable) and the address range size.

  • The IDAU / SAU column depicts the effective security across all address ranges combining the (fixed) device's IDAU and configured SAU entries. Each range lists a start address, end address, security status code and corresponding background color (S/green for Secure, NS/orange for Non-Secure, NSC/yellow for Non-Secure Callable, and X/gray for Exempted) and the address range size.

  • The MPC column shows the address ranges that will be under MPC control according to the configured Protection Domains and access details for each. Each range lists the name of the governing Protection Domain and a background color corresponding the range's security (S/green for Secure in the context of a secure core or S/gray in the context of a non-secure core, NS/orange for Non-Secure, NSC/yellow for Non-Secure Callable) and the access permissions (R for Read, W for Write) for each Protection Context granted by the Protection Domain. E.g., the access permission string "PC2: RW PC5: RW" denotes read and write access is granted to Protection Contexts PC2 and PC5.

  • The Regions column shows the memory regions that are configured in the Memory Regions subtab . For each region, the region id and size is shown, and has the same user-configured color coding from the Memory Regions tab.

In each of the columns, if the described content is not applicable – either because there is no such configuration or the device doesn't support it – the column will be omitted.

Peripheral Address View subtab

The Peripheral Address View subtab displays all peripheral regions and locations and (where used) the access permissions enforced by the PPC. The Core pull-down allows you to switch to other cores, and the Search shows all occurrences of an entered term with Forward and Back buttons to jump to the next or previous term. This subtab also contains zoom commands.

  • The Address column shows the start address of every segment shown in the proceeding columns.

  • The Regions column depicts all of the peripheral regions defined for the device. There is no meaning in the background colors of these regions; the colors simply alternate between two shades of blue for visual contrast.

  • If a PPC is configured, the PPC column shows the address ranges that will be under PPC control according to the configured Protection Domains and access details for each. Each range lists the name of the governing Protection Domain and a background color corresponding the range's security (S/green for Secure in the context of a secure core or S/gray in the context of a non-secure core, NS/orange for Non-Secure, NSC/yellow for Non-Secure Callable) and the Protection Contexts having access to the peripherals in the region per the Protection Domain.

  • The Locations column show all of the peripheral locations in the corresponding region. If there is no configured access to the locations in this region, they will be depicted with a gray background; if at least one Protection Context is granted access to the region and its locations, it will have the same blue or light blue coloring in the corresponding region.

note

For applications using the MCUboot library, memory ranges used to define the primary slot will be shown on the right side of the view.

In the Memory Regions subtab, there is a corresponding table with links to the Solution parameters where the range is defined.

Read Me subtab

This subtab displays an HTML generated document with information from the device-db’s memories.cydata file, combined with memory data exported from the QSPI configurator.

This file provides links to "how to" HTML topics to guide you how to configure memories.

MMIO-Clocks tab

For supported devices, the MMIO-Clocks tab lists all the clocks in a design used to drive the various Memory Mapped IOs. All available clocks are shown in an expandable tree. The filter box and the hide disabled button above the list of resources allows you to limit the items shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

Peripheral-Clocks tab

For supported devices, the Peripheral-Clocks tab lists all the clocks in a design used to drive the various peripherals. All available clocks are shown in an expandable tree. The filter box and the hide disabled button above the list of resources allows you to limit the items shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.

DMA tab

The DMA tab lists all the DMA resources in the design. All available DMA channels are shown in an expandable tree. The filter box and the hide disabled button above the list of resources allows you to limit the items shown in the tree. This tab allows you to enter one or more Name(s) for the resource. It also shows the selected Personality where applicable.