Skip to main content

Launch the USB Configurator

There are several ways to launch the USB Configurator, and those ways depend on how you use the various tools in ModusToolbox™.

make command

As described in the ModusToolbox ™ tools package user guide "Build System" chapter, you can run numerous make commands in the application directory, such as launching the USB Configurator. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:

make usbdev-configurator

This command opens the application USB Configurator GUI for an existing USB configuration (*.cyusbdev) file.

If there is no *. cyusbdev file, then this command launches the USB Configurator with default configuration. Open an existing *.cyusbdev file or create a new one for the application in which you want to configure the USB Configurator.

VS Code and Eclipse

VS Code and Eclipse have tools to launch the USB Configurator from within an open application. Refer to the applicable user guide for more details:

Executable (GUI)

Also, you can simply launch the USB Configurator GUI by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows Start menu). By default, it is installed here:

[install_dir]/ModusToolbox/tools_[version]/usbdev-configurator-[version]

On Windows, launch the tool from the Start menu. For other operating systems, navigate to the install location and run the executable. The USB Configurator opens with an untitled configuration file (*.cyusbdev). Save it as a new file and provide a file name, or open another existing *.cyusbdev file.

Executable (CLI)

You can run the usbdev-configurator executable from the command line. There is also a usbdev-configurator-cli executable, which re-generates the source code based on the latest configuration settings from a command-line prompt or from within batch files or shell scripts. The exit code for the usbdev-configurator-cli executable is zero if the operation is successful, or non-zero if the operation encounters an error. To use the usbdev-configurator-cli executable, you must provide at least the --config argument with a path to the configuration file.

For more information about the command-line options, run the usbdev-configurator or usbdev-configurator-cli executable using the -h option.