About this document​

Scope and purpose​

This application note describes the recommended process for mounting the HybridPACK™ DC6i power module. To ensure a robust design meeting the high quality demands of the automotive industry, it is important to use the right mounting order and appropriate printed circuit board (PCB) material, screw types, and processes.

Intended audience​

Engineers and operators involved in the assembly of the HybridPACK™ DC6i power module into power electronics systems.

General information​

This application note provides mounting instructions for the HybridPACK™ DC6i module with recommendations how to screw the module, assemble the PCB, and mount the module onto the heatsink.

Ensure that the ground straps should be worn while working with the components and that the ESD safety instructions must be followed at all times, since IGBT modules are electronic-static sensitive components. In addition, this application note does not cover all types of applications or conditions. As a result, the application note cannot replace a detailed assessment and examination of the suitability of the targeted applications carried out by you or your technical divisions. In any event, the application note will not become part of any supplier-agreed warranty, unless the supply agreement determines otherwise in writing.

All datasheet drawings specify the power module at the delivery point. When the power module is mounted to a cooling system, deformations can occur (that is, depending on the cooler flatness and screw torque). The following mounting order can be recommended:

  1. Align PCB to the power module (the X-pins will support this process)

  2. Press-in PCB (controlled way-force press-in process is recommended)

  3. Prepare cooling system using the sealing ring

  4. Attach the power module with PCB to the prepared cooling system

  5. Fix the module baseplate on the cooler by screws

  6. Fix the PCB on the power module by screws

  7. Connect the module power tabs to busbar, capacitor, etc.

Press-fit assembly​

Requirements for the PCB​

The press-fit technology used in the HybridPACK™ DC6i is designed based on IEC 60352-5 for standard FR4 printed circuit boards with immersion tin plating. The PCB material must be compliant with IEC 60249-2-4 or IEC 60249-2-5 for double-sided printed circuit boards and IEC 60249-2-11 or IEC 60249-2-12 for multilayer printed circuit boards.

The PCB requirements are given in Table 1. If these requirements are not met, there is a risk of a not gas tight signal pin connection, or that the pin and/or the PCB may be damaged. The PCB recommendations for the X-pin holes are given in Table 2.

It should be noted that the press-fit hole specifications are valid only for assembled PCB. For unassembled PCBs, such as for testing purposes, a standard reflow solder process is recommended before the power module assembly process begins.

Table 1. Requirements to the PCB

No.DescriptionUnitMinimumTypicalMaximumRemarks and known common mistakes
1Drill tool diametermm1.121.15Wrong drill tool used. Specify clearly the press-fit hole positions and required drill tool size to the PCB manufacturer
2Copper thickness in holeμm2550In case the via metallization is lower than the specification, the risk of a damaged/cracked via is high
3End hole diametermm1.021.10End-hole diameters lower than specification may lead to an increase in press-in forces (typically >115 N per pin,) which may damage the pins. Larger holes than specification may lead to low press-in forces (typically <40 N per pin) and can result in not gas tight connections
4Copper thickness of conductorsμm35

70

105

400No results are available for thinner or thicker copper layers
5Hole-to-hole pattern toleranceμm±100In a typical PCB manufacturing process, the hole-to-hole pattern is lower than ±80 μm
6Recommended PCB thicknessmm1.6Target value with tolerance of ±10% thickness
7Metallization of circuit boardImmersion tin (Sn chemically)Immersion tin has type 1–5 μm metallization in the hole. Other metallization types should be avoided because they can lead to strong deviations in press-in forces. For example, HAL leadless materials show high variations in press-in forces and could result in a non-gas-tight connection, which can fail over the application lifetime. PCBs with ENIG plating can lead to increased press forces due to their hard surfaces; however, this PCB type was not tested in the Infineon module qualification tests
8Metallization of pinNi/Sn (galvanic)Sn-plated pin with nickel underlayer avoids potential whisker growth out of the upper galvanic tin layer

Table 2. Recommendations for the printed circuit board X-pin holes

No.DescriptionUnitMinimumTypicalMaximumRemarks and known common mistakes
1End hole diameter X-pin mm5.9The hole should be drilled using a 6.0-mm drill tool and not milled to avoid unnecessary hole position tolerances
2End hole diameter Y-pin1mm5.4The hole should be drilled using a 5.5-mm drill tool and not milled to avoid unnecessary tolerances of the hole position
3Hole-to-hole pattern toleranceμm±100Plated holes are preferred to achieve a minimum tolerance between the “X-pin hole” and “press-fit hole” pattern

Figure 1 illustrates the structure of a PCB according to the specification in Table 1. The hole in the PCB is drilled using a 1.15-mm drill tool. It is normal for PCB material to shrink after drilling process. Therefore, a hole size of 1.15 mm should not be understood as a check gauge after drilling, but rather as an illustration for understanding the PCB stack.

Figure 1. Structure of a PCB according to the specification in Table 1



1 Experience has shown that the hole diameter of PCBs should be significantly larger than that of the module frame element in order to achieve a seamless assembly process. The given relatively large hole diameters in the PCB are the best compromise between module and PCB alignment and the necessary play during this assembly step. The specified relatively large hole size prevents unnecessary rotation of the PCB with respect to the signal pin coordinate system.

General hints for the PCB footprint​

The footprint of PCBs usually depends on PCB manufacturing processes and customer-specific design rules. The best practices and starting point for system design are summarized in Table 3.

Table 3. Hint for PCB footprint holesThe bottom layer of the PCB is defined on the side of the power module.

No.TypePCB implementation hint
1X-pin holes
  • End-hole diameter: 5.90 mm (see Table 2)

  • Top-layer copper diameter: ≥6.40 mm

  • Mid-layer copper diameter: ≥6.40 mm

  • Bottom-layer copper diameter: ≥8.00 mm

  • End-hole diameter: 5.4 mm (see Table 2)

  • Top-layer copper diameter: ≥5.90 mm

  • Mid-layer copper diameter: ≥5.90 mm

  • Bottom-layer copper diameter: ≥8.00 mm

2Signal press-fit pin holesSee Table 1
3Components keep out of the press-fit pins
  • ≥3 mm radius from the hole center

Others:

  • ≥4 mm radius from the hole center

4PCB fixing screw holes
  • End-hole diameter: 3.60 mm

  • Top-layer copper diameter: ≥7.00 mm

  • Mid-layer copper diameter: ≥6.50 mm

  • Bottom-layer copper diameter: ≥6.60 mm

Note: *The X-pin holes can be designed as plated or unplated holes. Plated holes with annular rings, as shown in the table, are the preferred solution. All plated holes are drilled at the PCB manufacturers in the same process, leading to the best hole-to-hole pattern tolerances.

Press-in tools​

This chapter describes a sample press-in tool, which can be adapted to project specific details such as PCB assembly locations, maximum height of other PCB parts, etc. to avoid mechanical collisions during the press-in process. The press-in tool is made of two parts (see Figure 2 and Figure 3).

Figure 2. Recommendation upper tool



Figure 3. Recommendation lower tool



The lower tool supports the baseplate of the power module and must avoid damage to the pin-fin cooling area. In order to prevent scratches and damage to the baseplate sealing area, the material and/or plating of the bottom part of the tool must be selected. The holes for the X-pins prevent the wrong orientation of the power module in the press-tool by using the poka yoke concept.

The upper tool supports the PCB with cylindrical shapes around the press-fit pins during the press-in process. This part of the tool must be made of material capable of withstanding press-in forces. In order to avoid a press-in process with an incorrectly oriented tool or power module, the top tool also has cylindrical holes around the X-pins.

The following points must be taken into account when using the press tool:

  • Press-tool distance keeper (Studs) should be placed at the positions of the 4× module baseplate holes

  • Press-tool distance keeper (Studs) should have a minimum diameter of 8 mm

  • Maximum press-in force specified in Table 4

  • Press-tool distance keeper height: typically, the gap between the PCB and module housing domes should be 150 µm after the press-in process

  • The total hight of the distance keeper is 14,6 mm (typical dome height is 12,85 mm + 150 μm gap between the PCB and module domes + 1,6 mm)



Press-in process​

For serial production, it is recommended to use a press-in process with a controlled force-distance.

Figure 4. Typical way-force press-in figure from a HybridPACK™ DC6i module with 21 signal pins



Figure 4 shows an example of a HybridPACK™ DC6i press-in process. When the force increases, the press-in process begins. The z-axis in this figure is set to 0 mm at this point. In case an initial high peak is detected, it may indicate a failure in the process, such as PCB hole plugged with solder, not properly inserted PCB before the process starts, machine collision with other external parts, etc.

The force curve increases smoothly when the PCB is pressed down (see Figure 4). Lower press-in speeds (see Table 4) are not allowed because the press-in forces may increase and damage the pin. High press-in speeds are not critical for the module.

A significant slope change can be detected at the end of the process considering the first derivative of the force-distance figure (see Figure 4). At this point, the PCB is fully pressed on the module housing and the effective part of the press-in process is completed.

At this point, the force should be at least 40 N per pin (that is, 840 N for HybridPACK™ DC6i with 21 pins).

It should be noted that the press-in equipment must be designed for the expected high forces. During the press-in process, the bottom and the top press tool must be parallel to each other and mechanically fixed without tilt.

Table 4. Overview press-in process

No.DescriptionUnitMinimumTypicalMaximumRemarks
1Press-in speedmm/s0.42–48During the press-in process, it is not allowed to exceed the minimum speed (no multistep press-in process). The maximum press-in speed is typically limited due to the non-ideal press machine
2Maximum allowed press forcekN4
1 Experience has shown that the hole diameter of PCBs should be significantly larger than that of the module frame element in order to achieve a seamless assembly process. The given relatively large hole diameters in the PCB are the best compromise between module and PCB alignment and the necessary play during this assembly step. The specified relatively large hole size prevents unnecessary rotation of the PCB with respect to the signal pin coordinate system.

PCB design hint for high thermal cycle system robustness​

In particular, in applications where high module ambient temperatures and/or high thermal cycle stress are expected, it is recommended that the system design be carefully designed to minimize pin-pull forces. The following parameters can be optimized in the system design:

  • PCB mounting positions (for example, see PCB design for module external mounting)

PCB design for module external mounting​

Press-in tools describes the press-tool and the distance (gap) between the PCB and the dome.

After press-in, a gap remains between the bottom side of the PCB and the housing domes of the power module (see area (2) in Figure 5). The inverter system designer can implement a PCB fixing point outside of the power module (see area (3) in Figure 5). The fixing point should be designed in such a way that a gap of 150 µm is achieved after pressing process (height of the fixing point is ~16 mm). After fixing the PCB with screws to the fixing point, no screws (that is, Ejot screws) are allowed at the module domes in the case of the external fixation method. There is a small gap between the module and PCB, which must remain after the final assembly.

Figure 5. Example module with externally mounted PCB. The distance keeper from the press tool ensures the distance between the PCB and the module dome (2). The PCB can be fixed externally of the module (3).



Power module cooling system​

The cooler design has a significant impact on the overall cooling performance, which means the combination of thermal resistance/impedance, pressure drop, and cooling flow rate. For all of these thermal-related product specifications, a reference cooling system is therefore needed where the given specifications are valid.

Note: Damage to the nickel plating or mechanical deformation of the cooling structure as well as contamination, scratches, or other damage in the sealing region (see Figure 7) must be strictly avoided during the mounting process.

Reference cooler design​

Figure 6. Reference cooler design for HybridPACK™ DC6i



Recommendation for the sealing ring​

The power module baseplate is designed with a flat 7-mm region surrounding the entire wave area (see Figure 7).

Figure 7. Sealing region with 7 mm surrounding the wave area



Figure 8. Drawing of sealing ring



The HybridPACK™ DC6i module with a sealing ring from Trelleborg is recommended. Trelleborg designed a sealing ring with the article number: C-01-0031956-00-1.

Note: Infineon does not recommend the use of a silicon gasket or other sealing methods. The use of sealing methods other than sealing rings can damage the HybridPACK™ DC6i modules.

Cooling fluid​

It is not possible to provide a general recommendation for a specific cooling fluid as the power module is only one part of the entire cooling system. To find appropriate coolant fluid, the following items must be considered at the system supplier:

  • Coolant fluid with its corrosion protection must be compatible with the aluminum of the cooler material and with the nickel overplated copper baseplate of the module

  • Other parts of the coolant system must also be compatible with the fluid type (for example, Zn screws and chrome parts are generally not allowed in the cooling system)

  • The fluid mixture must have sufficient anti-freeze for the application conditions. Freezing of the fluid must be strictly avoided. Freezing fluid leads to plastic deformation of the baseplate of the power module and may lead to fluid leakage and/or isolation failure

For power module tests at Infineon where cooling is required (for example, thermal characterization and power cycling tests), BASF Glysantin™ G30™ with an organic-acid-technology (OAT) silicate-free corrosion protection is typically applied. In combination with HybridPACK™ DC6i “Wave” FS650R08A4P2, a chemical reaction of the corrosion protection of Glysantin™ G30™ with the aluminum coolant structure is known (see Figure 9). This is a known effect of this type of coolant and has no effect on thermal performance or pressure drop in the tests.

Figure 9. Example of HybridPACK™ DC6i FS650R08A4P2 after long-term testing with G30™ fluid.

The aluminium cooling structure may appear black after the test. The organic corrosion protection reaction is a known effect and has no negative influence on the thermal performance or aging of modules.



Screw types and processes​

Baseplate mounting screws​

The clamping force of the module resulting from the assembly process to the heatsink depends on the torque applied and the heatsink material. The following torque values specified in the datasheet result from steel screws in aluminium heatsinks with a dry M5 thread.

The recommended screw order can be found in Screw orders (baseplate and PCB).

Table 5. Recommended baseplate fixing screw M5×10 DIN EN ISO 7380-1-TX

No.DescriptionMinimumTypicalMaximumRemarks
1Mounting torque3 Nm6 Nm
2Effective length of screw in cooler7 mm

Fixation/clamping of the module during the baseplate screw process​

To avoid tilting of the module with possible damage (that is, plastic deformation of the baseplate), it is necessary to properly fix the power module to the cooler during the screwing process.

The following methods are preferred for module fixation. Screw orders are listed in Screw orders (baseplate and PCB) as follows:

  1. Multi-step screw mounting: Place screws 1 and 2 and fix with the lowest torque. This prevents only module tilting and does not provide a high clamping force. Fix screws 3 and 4 with low torque (for example, 0.4–0.6 Nm). Fix screws with the final torque as specified

  2. Module clamping: After placing the power module (with PCB) onto the cooling system, the module should be clamped along the z axis with a total force of Fc = 600 N (300 N per AC/DC side). Clamping can be performed in the area where the power tabs are located (see Figure 10). During clamping, it is important that the PCB or the pins are not further pushed down

Note: The described fixing method with multi-step screw mounting is not suitable for self-tapping screws. In the case of self-tapping screws, it is mandatory to use proper clamping, which enables a single-step screw mounting.

Figure 10. Indicated area where the module can be normally clamped/hold down to the cooling system during the baseplate screw process



PCB mounting screws on the module housing​

It should be noted that after the module is attached to the cooling system, it is recommended to attach the PCB to the module with screws. The module dome is designed for the following screw type:

  • EJOT Delta PT WN5451 30 × 10 (for 1.6 mm PCB thickness)

The thread in the plastics will form when the EJOT screws are driven. It is important to have an appropriate minimum turn-in speed, which causes self-heating of the screw, in order to form a proper thread in the plastic housing without splitting and cracking. For this purpose, an electronically speed controlled screwdriver is preferred. Furthermore, a straight insertion of the screw into the stand-off must be observed during assembly.

Figure 11. Typical appearance of the EJOT Delta PT (a), the basic mounting torque diagram (b), and a cross-section drawing of the PCB screw in the module dome (c)



Table 6. PCB fixing screws EJOT Delta PT WN5151 30×10

No.DescriptionUnitMinimumTypicalMaximumRemarks
1

Mounting torque Meff

Meff + Mw (for 1.6 mm PCB)

Nm0.45

0.50

1.0

0.55Mw ≈ 0.45–0.5 Nm torque is required for the self-tapping of a 10-mm screw length and 1.6-mm PCB thickness. This torque is not effective for the mounting force Ft and may vary with screw length and PCB thickness
2Recommended mounting speedrpm400600Lower than 200 rpm is not recommended
3Screw length in the module dome (te)mm69Typical screw length of 10 mm for 1.6 mm thick PCBs

Screw orders (baseplate and PCB)​

The screw order shown in Figure 12 is crucial for avoiding damage to the part. Baseplate mounting screws and PCB mounting screws on the module housing specify the screw type and torque as well as the required processes, such as module fixation/clamping during the baseplate screw process.

Figure 12. Screw order for baseplate and PCB screws



Table 7. Screw order for baseplate and PCB screws

Baseplate fixing after module assembly into coolerPCB fixing after baseplate screwing
Baseplate screw orderPositionPCB screw orderPosition
1B11D1
2B32D3
3B23D2
4B44D4

Connecting to the power terminals​

For the connection of power terminals, DIN M5 screws which comply at least with class 6.8 are required in combination with a suitable washer and spring washer or a complete combination screw.

When selecting the bolt length, the layer thickness of the connecting parts must be subtracted from the total length of the screws. The actual length of engagement into the module thread should not exceed the maximum specified depth of 10 mm.

As shown in Figure 13, the connected parts must be mounted to the power terminals in such a way that the specified static forces are not exceeded during assembly or later in operation.

Note: The values of the specified forces refer only to static forces. The oscillation (vibration) forces are not allowed here.

Figure 13. Maximum permissible static pull-and-push forces at the power terminal



Table 8 show screws recommended for connecting the power terminals.

Table 8. Power tab recommended screw M5×10 DIN EN ISO 7380-2-TX

No.DescriptionMinimumTypicalMaximum
1Mounting torque3 Nm6 Nm

Storage and transport​

During transport and storage of modules, it is necessary to avoid extreme shocks or vibrations as well as extreme environmental influences.

It is possible to store modules at the temperature limits specified in the datasheet, but this is not recommended.

According to IEC60721-3-1, class 1K2, storage conditions should be ensured for a maximum storage time of 2 years.

  • Maximum air temperature: Tmaxair = +40°C

  • Minimum air temperature: Tminair = +5°C

  • Maximum relative humidity: 85%

  • Minimum relative humidity: 5%

  • Condensation: not permissible

  • Precipitation: not permitted

  • Icing: not permitted

The HybridPACK™ DC6i power modules do not require pre-drying of the power module prior to the press-in process (as is recommended for molded discrete components, such as microcontrollers, TO-cases, etc.

Traceability, data matrix, and part markings​

The traceability of materials, equipment, and processes is essential for key automotive components. Therefore, HybridPACK™ DC6i is produced at Infineon in a seamless traceability environment. However, traceability must not be interrupted once the modules have been shipped to the customer and assembled in the inverters. In order to make full use of the traceability chain, a unique module number (module ID) must be linked to an inverter ID at the customer's side.

Figure 14 shows the module labels and where to locate the DMX-code necessary for tracing the module ID.

Figure 14. Typical module label appearance. In order to ensure seamless traceability, the DMX code, which is the module ID (or, alternatively, the type designation + date code + serial number), should be recorded and linked to the inverter ID.



The DMX code can be read by all professional data matrix code scanners compatible with the IEC24720 and IEC16022 standard.

Engineers in the laboratory can also use free DMX code reader applications on smart phones:

  • Android: QR Extreme, QR Droid, and many other applications that support data matrix codes

  • iOS: i-nigma QR and many other applications that support data matrix codes

Pin position and pin gauge​

A pin gauge test is implemented in the production line at Infineon for power modules that have a note in product specification, as shown in Figure 15A. Figure 15B shows the specifications of this pin gauge for pinning as implemented in FS650R08A4P2. In the production of the power module, the parts are tested to see if the pin gauge can be applied to the module. A low force in the z-direction of the module on the gauge (typically up to 10–20 N, which is uncritical for the module and its pins) is allowed. If the pin gauge can be easily attached to the module, the test is rated as PASS, which can be seen as a test if the customer is able to smoothly assemble the PCBs on the power module.

A basic description of the test and pin gauge specifications is provided only for information on how these modules are tested at Infineon production. At the customer side, it is not necessary to test the power modules again at the incoming inspection.

Figure 15. Extract of the datasheet regarding the pin positions for example FS650R08A4P2 (A). Infineon pin gauge specifications for the power module production test (B)



Power module appearance​

This chapter explains frequently asked questions about typical power module appearance.

Pin rotation​

The position tolerance is an important value and ensures that the PCB designed according to the recommendations fits the power module. The positions of the pins are clearly indicated in the product datasheet.

The pin rotation is not fixed because the interface (PCB via) is totally symmetric. The asymmetric pin geometry (that is, three contact press-fit pins) clearly indicates the pin rotation. Figure 16 shows an example, where the rotation is indicated: Typically about 45° pin rotations can be seen. However, there may be different angles in the final product, which does not give rise to objections and has no influence on the quality of the final contact.

Figure 16. Pins are not symmetrical (three contact press-fit pins) and a rotation angle is visible. Different angles may occur in the final product, but does not affect the contact quality and there is no reason for objection.



Revision history​

Document versionDate of releaseDescription of changes
0.92019-09
  • Initial draft version

0.952020-04

Revised:

  • Traceability, data matrix, and part markings

  • Pin position and pin gauge

  • Cooling fluid

1.02020-09

Added new chapters:

  • PCB design for module external mounting

  • Fixation/clamping of the module during the baseplate screw process

  • Pin rotation

1.12023-12-07
  • Template update; no content update

1 Experience has shown that the hole diameter of PCBs should be significantly larger than that of the module frame element in order to achieve a seamless assembly process. The given relatively large hole diameters in the PCB are the best compromise between module and PCB alignment and the necessary play during this assembly step. The specified relatively large hole size prevents unnecessary rotation of the PCB with respect to the signal pin coordinate system.