Power Conversion
Example | Description |
|---|---|
PCCM buck converter multi-instance | This example implements a multi instance buck converter in peak current control mode for being used with the PSOC™ Control C3M5 Complete System Dual Buck Evaluation Kit. It demonstrates the capabilities and performance of the PSOC™ Control C3 MCU for implementating multi instance peak current control mode synchronous buck power converter. This code example is developed with PCC tool and Power-conversion middleware. For more details, see the README on GitHub. |
VCM buck converter multi-instance | This code example demonstrates a multi-instance buck converter in voltage control mode (VCM) with the PSOC™ Control C3M5 complete system dual buck evaluation kit. The power conversion configurator (PCC) tool and power conversion middleware are used for implementing this code example. For more details, see the README on GitHub. |