Tool change description
This section lists and describes the changes for each version of this tool.
| Version | Change descriptions |
|---|---|
| 1.0 | New tool. |
| 1.1 | Added Settings and Help menus. Moved link about version changes to the message console, when it is applicable. Added icon to indicate online/offline status. Removed Summary dialog; summary is shown in the console. |
| 1.2.0 | Added Retry button. Changed Apply button to Update. Added Close button. Tool can be launched from the Windows Start menu. Updated versioning to support patch releases. Updated for the MTB flow. Added toolbar commands to show/hide items, as well as collapse and expand the trees. |
| 1.30 | Added indications for newer versions of BSPs and libraries. For BSPs and libraries that are not selected, the displayed version was changed from Latest #.X release to the actual most recent X.Y.Z release. |
| 1.40 | Updated the handling on .mtbx files. |
| 2.0 | Entire GUI updated to support ModusToolbox™ version 3.0. |
| 2.10 | Added Rename BSP feature. Added Create from MPN feature. Changed Offline mode to Local Content mode. Removed online status icon. |
| 2.20 | Back-end changes and bug fixes. Updated the Properties tab to include descriptions. |
| 2.21 | Added Information Levels to Settings menu. |
| 2.30 | Added Manifest DB option to Settings menu. |
| 2.40 | Updated the Settings menu to add a link to the Settings tool and remove all of the items for general settings. |
| 2.50 | Back-end changes and bug fixes. |
| 2.60 | Back-end changes and bug fixes. Replaced X icon with garbage bin icon to more clearly indicate removal. Added SDK and SDK Version options in BSP/library controls. |
| 2.70 | Back-end changes and bug fixes. |