AIROC™ CYW20829 Wi-Fi & Bluetooth® combo chip global variables
DEBUG_CERTIFICATE
Allows to specify the location of the debug certificate binary file. This variable is used to configure a secure debug session. OpenOCD checks the status of the CM33 access port during the initialization phase and after each reset. It will attempt to reopen the CM33 AP by sending a debug certificate to a target and issuing WFA request #2.
This variable should contain the full path to the debug certificate binary file.
DEBUG_CERTIFICATE_ADDR
(Optional) Allows to specify the location in the RAM where the debug certificate will be loaded. The default address 0x2000FC00 will be used if this variable is not set by the user.