Launch the LIN Configurator
There are several ways to launch the LIN Configurator, and those ways depend on the application, and how you use the various tools.
make command
As described in the ModusToolbox ™ tools package user guide "ModusToolbox™ build system" chapter, you can run numerous make commands in the application directory, such as launching the LIN Configurator. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:
make lin-configurator
This command opens the LIN Configurator GUI for the specific application in which you are working.
VS Code and Eclipse IDE
VS Code and Eclipse have tools to launch the LIN Configurator from within an open application. Refer to the applicable user guide for more details:
Executable (GUI)
You can launch the LIN Configurator GUI by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows Start menu). By default, the configurator is installed here:
[install_dir]/ModusToolbox/tools_[version]/lin-configurator[version]
When launched this way, the LIN Configurator opens without any frames or signals configured (see Overview). You can either open a specific configuration file or create a new one. See Menus (under GUI description) for more information.
Launching the configurator this way is not recommended as part of application development.
Executable (CLI)
The LIN Configurator executable can be run from the command line and it has a "cli" version of the executable as well. Running the executable from the command line can be useful as part of batch files or shell scripts to re-generate the source code based on the latest configuration settings. The exit code for the executable is zero if the operation is successful, or non-zero if the operation encounters an error. For more information about the command-line options, run the executable using the -h option.