Skip to main content

Community Code Examples

Example

Supported kit

Description

KIT_XMC11_BOOT_001

KIT_XMC12_BOOT_001

KIT_XMC13_BOOT_001

KIT_XMC14_BOOT_001

KIT_XMC1300_DC_V1

KIT_XMC1400_DC_V1

XMC13-14 PMSM FOC SL

✓

✓

Disclaimer: This is a community code example (CCE) released for the benefit of the community users. These projects have only been tested for the listed BSPs, tools versions and toolchains documented in the Readme.This code example demonstrates the sensorless PMSM FOC motor control application using XMC1300/1400. In order to test this software, XMC1000 Motor Control Application Kit is needed. According to the user preference, XMC1300 or XMC1400 board can be used with this kit.For more details, see the README on GitHub.

XMC13-14 PMSM FOC SL DC

✓

✓

Disclaimer: This is a community code example (CCE) released for the benefit of the community users. These projects have only been tested for the listed BSPs, tools versions and toolchains documented in the Readme.This community code example (CCE) demonstrates the sensorless PMSM FOC motor control application using XMC1300/1400 Drive Card. In order to test this software; XMC1300 or XMC1400 Drive Card, 3-phase DC power board, and Nanotec DC motor (DB42S03) are needed.For more details, see the README on GitHub.

XMC1300 BLDC Scalar Hall

✓

Disclaimer: This is a community code example (CCE) released for the benefit of the community users. These projects have only been tested for the listed BSPs, tools versions and toolchains documented in the Readme.This community code example (CCE) demonstrates Hall sensor based three phase BLDC motor control application using XMC1300 Boot Kit. In order to test this software, XMC1000 Motor Control Application Kit is needed. For more details, see the README on GitHub.

XMC1300 BLDC Scalar Sensorless

✓

Disclaimer: This is a community code example (CCE) released for the benefit of the community users. These projects have only been tested for the listed BSPs, tools versions and toolchains documented in the Readme.This community code example (CCE) demonstrates sensorless three-phase BLDC motor control application using XMC1300 Boot Kit. In order to test this software, XMC1000 Motor Control Application Kit is needed. For more details, see the README on GitHub.