Skip to main content

Upgrading firmware

The ModusToolbox™ Programmer application allows you to upgrade KitProg2, KitProg3, and MiniProg4 device firmware.

Upgrade KitProg2 firmware

The following upgrade process is based on the CY8CKIT-062-WIFI-BT hardware.

  1. Run the ModusToolbox™ Programmer application.

  2. Go to Options > Programmer Options and select the Show Pop-Up value for the Upgrade Firmware option.

  3. Click OK to apply the changes.

  4. Connect the device with the KitProg2 firmware to the host PC. Ensure that the KitProg2 device is in Native KP2 mode.

  5. If LED2 is off, press the SW3 (Mode Select) button and hold it for about 1 second. When LED2 is on, the device is ready for upgrading the firmware.

    A warning dialog displays with the "Firmware is Out of Date" message.

  6. Select the KitProg2 device in the list and click the Upgrade Selected Devices button to start the upgrade process.

After the upgrade process completes, the message "Firmware of 'KitProg2-xx' upgraded successfully" displays in the Log view. The KitProg2-xx programmer disappears from the Programmer/Board ID drop-down. The Board Name drop-down is populated with the names of the supported KitProg3 Kits.

Upgrade KitProg3 on kit or MiniProg4 firmware

Follow this process to upgrade KitProg3 on a kit or MiniProg4 firmware:

  1. Run the ModusToolbox™ Programmer application.

  2. As needed, go to Options > Programmer Options and select the Show Pop-Up value for the Upgrade Firmware option.

  3. Connect the KitProg3/MiniProg4 device to the host PC. A warning dialog with the "There are ModusToolbox supported kits with out of date firmware" message displays.

  4. Select the KitProg3/MiniProg4 device(s) to be upgraded.

  5. Click the Upgrade Selected Devices button to start the upgrade process.

After the upgrade process completes, the message "Firmware of 'KitProg3-xx' upgraded successfully" or "Firmware of 'MiniProg4 xx' upgraded successfully" displays in the Log view.