Troubleshooting
Limitations
- ModusToolbox™ Programmer does not support RAM programming, you can program only the flash memory of a target device, except for devices that support only RAM such as CYW9M2BASE-43012BT and CYW955513EVK-01 kits.
- Programming devices in DAPLink mode is not supported. You have to switch your device into CMSIS-DAP BULK mode by pressing the mode selection button.
How to recover AIROC Bluetooth devices on failure
If the program operation for an AIROC™ Bluetooth® device fails, it is possible the memory on the board has been corrupted by a previously loaded application, or the application used a custom baud rate that the download process does not detect.
To recover from this, it may be necessary to reset the board to factory defaults, as follows:
- Press and hold the Recovery button (SW1).
- Press the Reset button (SW2).
- Release the Reset button (SW2).
- Release the Recovery button (SW1).
Incorrect PSOC 6 device names (MPN) in JTAG chain
Some PSOC™ 6 target devices may be displayed with incorrect part numbers in the JTAG chain. This issue shows only those PSOC™ 6 targets having incorrect value written to JTAG ID Code register.

You can ignore this inconsistency in device names if you see the warning "Selected device does not match the physical target device" after clicking Connect button.