Skip to main content

ModusToolbox™ for Wi-Fi and Ethernet

LibraryDetailsDocs
enterprise-securityThis library implements a collection of the most commonly used Extensible Authentication Protocols (EAP) used in enterprise Wi-Fi networks.API reference
ethernet-connection-managerEthernet Connection Manager (ECM) is a library which helps application developers to manage ethernet connectivity for XMC7200 devices.API Reference
ethernet-core-freertos-lwip-mbedtlsThis repo comprises core components needed for ethernet connectivity support for XMC7200 devicesAPI reference
ethernet-phy-driverProvides the Ethernet PHY-related interface APIs as required by Ethernet connection manager library to enable the completion of Ethernet-based applications on supported platforms.API reference
lwip-network-interface-integrationThis library is an integration layer that links the lwIP network stack with the underlying Wi-Fi host driver (WHD) and Ethernet driver. This library interacts with FreeRTOS, lwIP TCP/IP stack, Wi-Fi host driver (WHD), and Ethernet driver. It contains the associated code to bind these components together.API Reference
nonrtos-lwip-mbedtlsContains core components needed for non-rtos connectivity support. The library bundles lwIP TCP/IP stack, mbed TLS for security, connectivity utilities and configuration files.API reference
rtlabs-uphy-libPartner library for with support of RT-Labs Industrial Communication stack on XMC7000.RT-Labs u-phy website
smartcoexProvides an API to configure the coex parameters for WLAN and Bluetooth® Low Energy on platforms with Wi-Fi & Bluetooth® combo chip.API reference
whd-bsp-integrationThis library provides some convenience functions for connecting the Wi-Fi Host Driver (WHD) library to a BSP that includes a WLAN chip.API reference
wifi-connection-managerThe Wi-Fi Connection Manager (WCM) provides easy to use APIs to establish and monitor Wi-Fi connections on our devices that support Wi-Fi connectivity.API reference
wifi-core- freertos-lwip-mbedtlsThis repo comprises core components needed for Wi-Fi connectivity support. The library bundles FreeRTOS, lwIP TCP/IP stack, mbed TLS for security, Wi-Fi host driver (WHD), wifi connection manager (WCM), secure sockets, connectivity utilities and configuration files.API reference
wifi-host-driverThe Wi-Fi Host Driver (WHD) is an independent, embedded driver that provides a set of APIs to interact with our WLAN chips.API reference
wifi -mw-coreThe Wi-Fi Middleware Core library bundles the core libraries that any Wi-Fi application needs. This has been deprecated.API reference
wifi-resourcesThis repo contains clm and nvram files for the supported Wi-Fi boards from associated chip set.API reference
wpa3-external-supplicantThe WPA3 External Supplicant supports WPA3 SAE authentication using HnP (Hunting and Pecking Method) using RFC https://datatracker.ietf.org/doc/html/rfc7664 and H2E ( Hash to Element Method) using RFC https://datatracker.ietf.org/doc/html/draft-irtf-cfrg-hash-to-curve-10 and following 802.11 spec 2016.See links to the left.