Shift
Shift segment to a specific address.
Inputs
Name | Type | Optional/Required | Description |
|---|---|---|---|
file | string | required | Input hex file containing the segment to shift. |
address | string | optional | Address of the segment that has to be shifted. |
description | string | optional | Description for this field. |
Outputs
Name | Type | Optional/Required | Description |
|---|---|---|---|
file | string | required | Path to the output file. |
address | string | optional | The new address of the segment. |
description | string | optional | Description for this field. |
Example
{
"schema-version": 1.0,
"content": [
{
"name": "Shift command example",
"description": "Shifts a hex segment to a secondary address",
"enabled": true,
"commands": [
{
"command": "shift",
"inputs": [
{
"description": "CM33 Secure + CM33 Non-Secure application",
"file": "rram_3.hex",
"address" : "0x32030000"
}
],
"outputs": [
{
"description": "CM33 Secure + CM33 Non-Secure application shifted to secure region",
"address": "0x3202A000",
"file": "shifted_rram_3.hex"
}
]
}
]
}
]
}