Hex to bin
Converts hex file to binary.
Command name:
hex2bin
Inputs:
Name | Type | Optional/Required | Description |
|---|---|---|---|
file | string | required | The path to the input hex file. |
start | string, integer | optional | Start of address range. |
end | string, integer | optional | End of address range. |
description | string | optional | Description for this field. |
Outputs:
Name | Type | Optional/Required | Description |
|---|---|---|---|
file | string | required | The path to the output bin file. |
size | string, integer | optional | Size of the resulting file in bytes. |
fill-value | string, integer | optional | Value to fill the spaces between the segments. Available values: - . Default: . |
description | string | optional | Description for this field. |
Example:
{
"schema-version": 1.0,
"content": [
{
"name": "hex2bin command example",
"description": "Converts hex file to binary",
"enabled": true,
"commands": [
{
"command": "hex2bin",
"inputs": [
{
"description": "Input hex file",
"file": "input.hex",
"start": "0x32000000",
"end": "0x32000200"
}
],
"outputs": [
{
"description": "Output bin file",
"file": "output.bin",
"size": "0x400",
"fill-value": 0
}
]
}
]
}
]
}