Bin dump
Creates binary file from the hex string or random bytes.
Command name:
bin-dump
Inputs:
Name | Type | Optional/Required | Description |
|---|---|---|---|
data | string | optional | The hex string. Either or property must be specified. |
random | string, integer | optional | Generate random binary of the specified length. |
description | string | optional | Description for this field. |
Outputs:
Name | Type | Optional/Required | Description |
|---|---|---|---|
file | string | required | Path to the output bin file. |
description | string | optional | Description for this field. |
Example:
{
"schema-version": 1.0,
"content": [
{
"name": "bin-dump command example",
"description": "Creates binary file",
"enabled": true,
"commands": [
{
"command": "bin-dump",
"inputs": [
{
"description": "Hex string or random value",
"data": "0011223344556677889900AABBCCDDEEFF",
"random": null
}
],
"outputs": [
{
"description": "Output file",
"file": "output.bin"
}
]
}
]
}
]
}