Launch the Library Manager
There are numerous ways to launch the Library Manager, and that depends on how you use the various tools included with ModusToolbox™ software.
make command
As described in the
ModusToolbox™ tools package user guide
build system chapter, you can run numerous make commands in the application directory, such as launching the Library Manager. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:
make library-manager
This command opens the Library Manager GUI for the specific application in which you are working.
VS Code and Eclipse
VS Code and Eclipse have tools to launch the Library Manager from within an open application. Refer to the applicable user guide for more details:
Stand-alone GUI mode
You can launch the Library Manager in stand-alone mode by running its executable as applicable for your operating system (for example, double-click or select it using the Windows
Start
menu). By default, it is installed here:
<install_dir>/ModusToolbox/tools_<version>/library-manager
When run in stand-alone mode, the Library Manager opens with the target directory set as <user-home> or as the directory selected from a previous stand-alone session.
Note:
When launching from the executable, you can add the--verbose [0-3]option to specify more or less messaging in the console. The default level is 1.
If you haven’t opened the Library Manager tool previously, it starts at your home directory and looks for an application
Makefile
, and then it opens the first application it finds. If the tool does not find an application, it doesn't display any BSPs or libraries.

Click the
Browse…
button next to the
Application Directory
field and navigate to the appropriate directory that contains the desired application.
Note:
The next time you open the Library Manager in stand-alone mode, it will open with the most recently selected application.
Local Content mode
If the Library Manager cannot connect to the internet when launching, it displays messages/errors in the console that it cannot access the online manifest file. If you intend to work without Internet, enable
Local Content
mode from the
Settings
menu. Refer to the
Local Content Storage CLI user guide
for details about creating local content.
If you did not intend to work without Internet, check your Internet settings, adjust your proxy settings (from the
Settings
menu), and then click the
Retry
button to re-read library information.
Non-GUI command line interface (CLI)
You can run a non-graphical interface from the command line. However, there are only a few reasons to do this in practice. The primary use case would be part of an overall build script for the entire application. For information about command line options, run the
library-manager-cli
executable using the
-h
option.